Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
AESECB.h File Reference

Detailed Description

AESECB driver header.


Overview

The Electronic Code Book (ECB) mode of operation is a generic encryption block cipher mode. It can be used with any block cipher. AESECB encrypts or decrypts one or multiple blocks of plaintext or ciphertext using the Advanced Encryption Standard (AES) block cipher. Each input block is individually encrypted or decrypted. This means that blocks of ciphertext can be decrypted individually and out of order. Encrypting the same plaintext using the same key yields identical ciphertext. This raises several security issues. For this reason, ECB is not recommended unless interfacing with legacy systems which cannot be updated or where a standard specifies its use. Better alternatives would be an authenticated encryption with associated data (AEAD) mode such as CCM or GCM.

The AES key is a shared secret between the two parties and has a length of 128, 192, or 256 bits.

Usage

Before starting an ECB operation

Before starting an ECB operation, the application must do the following:

Starting an ECB operation

The AESECB_oneStepEncrypt and AESECB_oneStepDecrypt functions do an ECB operation in a single call. They will always be the most highly optimized routines with the least overhead and the fastest runtime. Since ECB plaintext blocks are simply encrypted with the block cipher block by block, there is no difference in the ciphertext between encrypting two blocks in one go or encrypting each block individually.

After the ECB operation completes

After the ECB operation completes, the application should either start another operation or close the driver by calling AESECB_close()

Synopsis

// Import AESECB Driver definitions
// Define name for AESECB channel index
#define AESECB_INSTANCE 0
handle = AESECB_open(AESECB_INSTANCE, NULL);
// Initialize symmetric key
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
// Set up AESECB_Operation
operation.key = &cryptoKey;
operation.input = plaintext;
operation.output = ciphertext;
// Input length must be a non-zero multiple of block-size (16 bytes)
// for one-step operations. The user or application should take care of
// necessary padding.
operation.inputLength = sizeof(plaintext);
encryptionResult = AESECB_oneStepEncrypt(handle, &operation);
AESECB_close(handle);

Examples

### Encryption of multiple plaintext blocks in blocking mode #

...
AESECB_Handle handle;
CryptoKey cryptoKey;
int_fast16_t encryptionResult;
uint8_t plaintext[] = {0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96,
0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a,
0xae, 0x2d, 0x8a, 0x57, 0x1e, 0x03, 0xac, 0x9c,
0x9e, 0xb7, 0x6f, 0xac, 0x45, 0xaf, 0x8e, 0x51};
uint8_t ciphertext[sizeof(plaintext)];
uint8_t keyingMaterial[16] = {0x2b, 0x7e, 0x15, 0x16, 0x28, 0xae, 0xd2, 0xa6,
0xab, 0xf7, 0x15, 0x88, 0x09, 0xcf, 0x4f, 0x3c}
handle = AESECB_open(0, NULL);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
AESECB_Operation operation;
AESECB_Operation_init(&operation);
operation.key = &cryptoKey;
operation.input = plaintext;
operation.output = ciphertext;
// Input length must be a non-zero multiple of block-size (16 bytes)
// for one-step operations. The user or application should take care of
// necessary padding.
operation.inputLength = sizeof(plaintext);
encryptionResult = AESECB_oneStepEncrypt(handle, &operation);
if (encryptionResult != AESECB_STATUS_SUCCESS) {
// handle error
}
// The resultant ciphertext should be:
// 0x3a, 0xd7, 0x7b, 0xb4, 0x0d, 0x7a, 0x36, 0x60,
// 0xa8, 0x9e, 0xca, 0xf3, 0x24, 0x66, 0xef, 0x97,
// 0xf5, 0xd3, 0xd5, 0x85, 0x03, 0xb9, 0x69, 0x9d,
// 0xe7, 0x85, 0x89, 0x5a, 0x96, 0xfd, 0xba, 0xaf
AESECB_close(handle);

### One step ECB decryption in callback mode #

...
uint8_t ciphertext[] = {0xf3, 0xee, 0xd1, 0xbd, 0xb5, 0xd2, 0xa0, 0x3c,
0x06, 0x4b, 0x5a, 0x7e, 0x3d, 0xb1, 0x81, 0xf8};
uint8_t keyingMaterial[32] = {0x60, 0x3d, 0xeb, 0x10, 0x15, 0xca, 0x71, 0xbe,
0x2b, 0x73, 0xae, 0xf0, 0x85, 0x7d, 0x77, 0x81,
0x1f, 0x35, 0x2c, 0x07, 0x3b, 0x61, 0x08, 0xd7,
0x2d, 0x98, 0x10, 0xa3, 0x09, 0x14, 0xdf, 0xf4};
uint8_t plaintext[sizeof(ciphertext)];
// The plaintext should be the following after the decryption operation:
// 0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96,
// 0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a,
void ecbCallback(AESECB_Handle handle,
int_fast16_t returnValue,
AESECB_Operation *operation,
AESECB_OperationType operationType) {
if (returnValue != AESECB_STATUS_SUCCESS) {
// handle error
}
}
AESECB_Operation operation;
void ecbStartFunction(void) {
AESECB_Handle handle;
CryptoKey cryptoKey;
int_fast16_t decryptionResult;
params.callbackFxn = ecbCallback;
handle = AESECB_open(0, &params);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
AESECB_Operation_init(&operation);
operation.key = &cryptoKey;
operation.input = plaintext;
operation.output = ciphertext;
// Input length must be a non-zero multiple of block-size (16 bytes)
// for one-step operations. The user or application should take care of
// necessary padding.
operation.inputLength = sizeof(plaintext);
decryptionResult = AESECB_oneStepDecrypt(handle, &operation);
if (decryptionResult != AESECB_STATUS_SUCCESS) {
// handle error
}
// do other things while ECB operation completes in the background
}

### Multi-step ECB encryption in blocking mode #

#define AES_BLOCK_SIZE 16 // bytes
...
AESECB_Handle handle;
CryptoKey cryptoKey;
int_fast16_t encryptionResult;
int_fast16_t setupEncryptionResult;
int_fast16_t finalizeEncryptionResult;
uint8_t plaintext[] = {0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96,
0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a,
0xae, 0x2d, 0x8a, 0x57, 0x1e, 0x03, 0xac, 0x9c,
0x9e, 0xb7, 0x6f, 0xac, 0x45, 0xaf, 0x8e, 0x51};
uint8_t ciphertext[sizeof(plaintext)];
uint8_t keyingMaterial[16] = {0x2b, 0x7e, 0x15, 0x16, 0x28, 0xae, 0xd2, 0xa6,
0xab, 0xf7, 0x15, 0x88, 0x09, 0xcf, 0x4f, 0x3c}
handle = AESECB_open(0, NULL);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
setupEncryptionResult = AESECB_setupEncrypt(handle, &cryptoKey);
if (setupEncryptionResult != AESECB_STATUS_SUCCESS) {
// handle error
}
AESECB_Operation operation;
// No need to set operation.key for multi-step operations.
operation.input = plaintext;
operation.output = ciphertext;
// Input length must be a non-zero multiple of block-size (16 bytes) for calling
// #AESECB_addData(). The user or application should take care of necessary padding
// if the final block of data is being added for the entire segmented operation.
operation.inputLength = AES_BLOCK_SIZE;
encryptionResult = AESECB_addData(handle, &operation);
if (encryptionResult != AESECB_STATUS_SUCCESS) {
// handle error
}
// No need to set operation.key for multi-step operations.
operation.input = plaintext + AES_BLOCK_SIZE;
operation.output = ciphertext + AES_BLOCK_SIZE;
// Input length must either be a non-zero multiple of block-size (16 bytes)
// for calling #AESECB_finalize(), or it could be zero in case of finalizing without
// any more data. The user or application should take care of necessary padding
// for the last block of data.
operation.inputLength = AES_BLOCK_SIZE;
finalizeEncryptionResult = AESECB_finalize(handle, &operation);
if (finalizeEncryptionResult != AESECB_STATUS_SUCCESS) {
// handle error
}
// The resultant ciphertext should be:
// 0x3a, 0xd7, 0x7b, 0xb4, 0x0d, 0x7a, 0x36, 0x60,
// 0xa8, 0x9e, 0xca, 0xf3, 0x24, 0x66, 0xef, 0x97,
// 0xf5, 0xd3, 0xd5, 0x85, 0x03, 0xb9, 0x69, 0x9d,
// 0xe7, 0x85, 0x89, 0x5a, 0x96, 0xfd, 0xba, 0xaf
AESECB_close(handle);
}

Multi-step ECB decryption in callback mode

#define AES_BLOCK_SIZE 16 // bytes
...
uint8_t ciphertext[] = {0xf3, 0xee, 0xd1, 0xbd, 0xb5, 0xd2, 0xa0, 0x3c,
0x06, 0x4b, 0x5a, 0x7e, 0x3d, 0xb1, 0x81, 0xf8};
uint8_t keyingMaterial[32] = {0x60, 0x3d, 0xeb, 0x10, 0x15, 0xca, 0x71, 0xbe,
0x2b, 0x73, 0xae, 0xf0, 0x85, 0x7d, 0x77, 0x81,
0x1f, 0x35, 0x2c, 0x07, 0x3b, 0x61, 0x08, 0xd7,
0x2d, 0x98, 0x10, 0xa3, 0x09, 0x14, 0xdf, 0xf4};
uint8_t plaintext[sizeof(ciphertext)];
// The plaintext should be the following after the decryption operation:
// 0x6b, 0xc1, 0xbe, 0xe2, 0x2e, 0x40, 0x9f, 0x96,
// 0xe9, 0x3d, 0x7e, 0x11, 0x73, 0x93, 0x17, 0x2a,
void ecbCallback(AESECB_Handle handle,
int_fast16_t returnValue,
AESECB_Operation *operation,
AESECB_OperationType operationType) {
if (returnValue != AESECB_STATUS_SUCCESS) {
// handle error
}
}
AESECB_Operation operation;
void ecbStartFunction(void) {
AESECB_Handle handle;
CryptoKey cryptoKey;
int_fast16_t decryptionResult;
int_fast16_t setupDecryptionResult;
int_fast16_t finalizeDecryptionResult;
params.callbackFxn = ecbCallback;
handle = AESECB_open(0, &params);
if (handle == NULL) {
// handle error
}
CryptoKeyPlaintext_initKey(&cryptoKey, keyingMaterial, sizeof(keyingMaterial));
setupDecryptionResult = AESECB_setupDecrypt(handle, &cryptoKey);
if (setupDecryptionResult != AESECB_STATUS_SUCCESS) {
// handle error
}
AESECB_Operation_init(&operation);
// No need to set operation.key for multi-step operations.
operation.input = plaintext;
operation.output = ciphertext;
// Input length must be a non-zero multiple of block-size (16 bytes) for calling
// #AESECB_addData(). The user or application should take care of necessary padding
// if the final block of data is being added for the entire segmented operation.
operation.inputLength = AES_BLOCK_SIZE;
decryptionResult = AESECB_addData(handle, &operation);
if (decryptionResult != AESECB_STATUS_SUCCESS) {
// handle error
}
// do other things while ECB operation completes in the background
// Input length must either be a non-zero multiple of block-size (16 bytes)
// for calling #AESECB_finalize(), or it could be zero in case of finalizing without
// any more data as shown in this example. There's no more data involved and padding
// is not applicable for this finalization operation.
operation.inputLength = 0;
finalizeDecryptionResult = AESECB_finalize(handle, &operation);
if (finalizeDecryptionResult != AESECB_STATUS_SUCCESS) {
// handle error
}
}
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/AESCommon.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Include dependency graph for AESECB.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  AESECB_Operation
 Struct containing the parameters required for encrypting/decrypting and a message. More...
 
struct  AESECB_Params
 ECB Parameters. More...
 

Macros

#define AESECB_STATUS_RESERVED   AES_STATUS_RESERVED
 
#define AESECB_STATUS_SUCCESS   AES_STATUS_SUCCESS
 Successful status code. More...
 
#define AESECB_STATUS_ERROR   AES_STATUS_ERROR
 Generic error status code. More...
 
#define AESECB_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE
 An error status code returned if the hardware or software resource is currently unavailable. More...
 
#define AESECB_STATUS_CANCELED   AES_STATUS_CANCELED
 The ongoing operation was canceled. More...
 
#define AESECB_STATUS_FEATURE_NOT_SUPPORTED   AES_STATUS_FEATURE_NOT_SUPPORTED
 The operation requested is not supported on the target hardware or by the current state of the SW implementation. More...
 
#define AESECB_STATUS_KEYSTORE_INVALID_ID   AES_STATUS_KEYSTORE_INVALID_ID
 The operation tried to load a key from the keystore using an invalid key ID. More...
 
#define AESECB_STATUS_KEYSTORE_GENERIC_ERROR   AES_STATUS_KEYSTORE_GENERIC_ERROR
 The key store module returned a generic error. See key store documentation for additional details. More...
 
#define AESECB_STATUS_UNALIGNED_IO_NOT_SUPPORTED   AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED
 The operation does not support non-word-aligned input and/or output. More...
 

Typedefs

typedef AESCommon_Config AESECB_Config
 AESECB Global configuration. More...
 
typedef AESECB_ConfigAESECB_Handle
 A handle that is returned from an AESECB_open() call. More...
 
typedef void(* AESECB_CallbackFxn) (AESECB_Handle handle, int_fast16_t returnValue, AESECB_Operation *operation, AESECB_OperationType operationType)
 The definition of a callback function used by the AESECB driver when used in AESECB_RETURN_BEHAVIOR_CALLBACK. More...
 

Enumerations

enum  AESECB_ReturnBehavior { AESECB_RETURN_BEHAVIOR_CALLBACK = AES_RETURN_BEHAVIOR_CALLBACK, AESECB_RETURN_BEHAVIOR_BLOCKING = AES_RETURN_BEHAVIOR_BLOCKING, AESECB_RETURN_BEHAVIOR_POLLING = AES_RETURN_BEHAVIOR_POLLING }
 The way in which ECB function calls return after performing an encryption + authentication or decryption + verification operation. More...
 
enum  AESECB_Mode { AESECB_MODE_ENCRYPT = 1, AESECB_MODE_DECRYPT = 2 }
 Enum for the direction of the ECB operation. More...
 
enum  AESECB_OperationType {
  AESECB_OPERATION_TYPE_ENCRYPT = 1, AESECB_OPERATION_TYPE_DECRYPT = 2, AESECB_OPERATION_TYPE_ENCRYPT_SEGMENTED = 3, AESECB_OPERATION_TYPE_DECRYPT_SEGMENTED = 4,
  AESECB_OPERATION_TYPE_FINALIZE_ENCRYPT_SEGMENTED = 5, AESECB_OPERATION_TYPE_FINALIZE_DECRYPT_SEGMENTED = 6
}
 Enum for the operation types supported by the driver. More...
 

Functions

void AESECB_init (void)
 This function initializes the ECB module. More...
 
void AESECB_Params_init (AESECB_Params *params)
 Function to initialize the AESECB_Params struct to its defaults. More...
 
AESECB_Handle AESECB_open (uint_least8_t index, const AESECB_Params *params)
 This function opens a given ECB peripheral. More...
 
void AESECB_close (AESECB_Handle handle)
 Function to close an ECB peripheral specified by the ECB handle. More...
 
void AESECB_Operation_init (AESECB_Operation *operationStruct)
 Function to initialize an AESECB_Operation struct to its defaults. More...
 
int_fast16_t AESECB_oneStepEncrypt (AESECB_Handle handle, AESECB_Operation *operation)
 Function to perform an AESECB encryption operation in one call. More...
 
int_fast16_t AESECB_oneStepDecrypt (AESECB_Handle handle, AESECB_Operation *operation)
 Function to perform an AESECB decryption in one call. More...
 
int_fast16_t AESECB_setupEncrypt (AESECB_Handle handle, const CryptoKey *key)
 Function to prepare a segmented AESECB encryption operation. More...
 
int_fast16_t AESECB_setupDecrypt (AESECB_Handle handle, const CryptoKey *key)
 Function to prepare a segmented AESECB decryption operation. More...
 
int_fast16_t AESECB_addData (AESECB_Handle handle, AESECB_Operation *operation)
 Encrypts or decrypts segment of data with a length. More...
 
int_fast16_t AESECB_finalize (AESECB_Handle handle, AESECB_Operation *operation)
 Finalize the AES transaction. If new data needs to be added, inputLength will be used to govern how many bytes will be written. More...
 
int_fast16_t AESECB_cancelOperation (AESECB_Handle handle)
 Cancels an ongoing AESECB operation. More...
 
AESECB_Handle AESECB_construct (AESECB_Config *config, const AESECB_Params *params)
 Constructs a new AESECB object. More...
 

Variables

const AESECB_Params AESECB_defaultParams
 Default AESECB_Params structure. More...
 

Macro Definition Documentation

§ AESECB_STATUS_RESERVED

#define AESECB_STATUS_RESERVED   AES_STATUS_RESERVED

Common AESECB status code reservation offset. AESECB driver implementations should offset status codes with AESECB_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define AESECBXYZ_STATUS_ERROR0 AESECB_STATUS_RESERVED - 0
#define AESECBXYZ_STATUS_ERROR1 AESECB_STATUS_RESERVED - 1
#define AESECBXYZ_STATUS_ERROR2 AESECB_STATUS_RESERVED - 2

§ AESECB_STATUS_SUCCESS

#define AESECB_STATUS_SUCCESS   AES_STATUS_SUCCESS

Successful status code.

Functions return AESECB_STATUS_SUCCESS if the function was executed successfully.

§ AESECB_STATUS_ERROR

#define AESECB_STATUS_ERROR   AES_STATUS_ERROR

Generic error status code.

Functions return AESECB_STATUS_ERROR if the function was not executed successfully and no more pertinent error code could be returned.

§ AESECB_STATUS_RESOURCE_UNAVAILABLE

#define AESECB_STATUS_RESOURCE_UNAVAILABLE   AES_STATUS_RESOURCE_UNAVAILABLE

An error status code returned if the hardware or software resource is currently unavailable.

AESECB driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

§ AESECB_STATUS_CANCELED

#define AESECB_STATUS_CANCELED   AES_STATUS_CANCELED

The ongoing operation was canceled.

§ AESECB_STATUS_FEATURE_NOT_SUPPORTED

#define AESECB_STATUS_FEATURE_NOT_SUPPORTED   AES_STATUS_FEATURE_NOT_SUPPORTED

The operation requested is not supported on the target hardware or by the current state of the SW implementation.

§ AESECB_STATUS_KEYSTORE_INVALID_ID

#define AESECB_STATUS_KEYSTORE_INVALID_ID   AES_STATUS_KEYSTORE_INVALID_ID

The operation tried to load a key from the keystore using an invalid key ID.

§ AESECB_STATUS_KEYSTORE_GENERIC_ERROR

#define AESECB_STATUS_KEYSTORE_GENERIC_ERROR   AES_STATUS_KEYSTORE_GENERIC_ERROR

The key store module returned a generic error. See key store documentation for additional details.

§ AESECB_STATUS_UNALIGNED_IO_NOT_SUPPORTED

#define AESECB_STATUS_UNALIGNED_IO_NOT_SUPPORTED   AES_STATUS_UNALIGNED_IO_NOT_SUPPORTED

The operation does not support non-word-aligned input and/or output.

AESECB driver implementations may have restrictions on the alignment of input/output data due to performance limitations of the hardware.

Typedef Documentation

§ AESECB_Config

AESECB Global configuration.

The AESECB_Config structure contains a set of pointers used to characterize the AESECB driver implementation.

This structure needs to be defined before calling AESECB_init() and it must not be changed thereafter.

See also
AESECB_init()

§ AESECB_Handle

A handle that is returned from an AESECB_open() call.

§ AESECB_CallbackFxn

typedef void(* AESECB_CallbackFxn) (AESECB_Handle handle, int_fast16_t returnValue, AESECB_Operation *operation, AESECB_OperationType operationType)

The definition of a callback function used by the AESECB driver when used in AESECB_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the ECB operation.
returnValueThe result of the ECB operation. May contain an error code. Informs the application of why the callback function was called.
operationA pointer to an operation struct.
operationTypeThis parameter determines which operation the callback refers to.

Enumeration Type Documentation

§ AESECB_ReturnBehavior

The way in which ECB function calls return after performing an encryption + authentication or decryption + verification operation.

Not all ECB operations exhibit the specified return behavior. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specified return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

AESECB functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
AESECB_RETURN_BEHAVIOR_CALLBACK X X X
AESECB_RETURN_BEHAVIOR_BLOCKING X
AESECB_RETURN_BEHAVIOR_POLLING X X X
Enumerator
AESECB_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the ECB operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

AESECB_RETURN_BEHAVIOR_BLOCKING 

The function call will block while ECB operation goes on in the background. ECB operation results are available after the function returns.

AESECB_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while ECB operation goes on in the background. ECB operation results are available after the function returns.

§ AESECB_Mode

Enum for the direction of the ECB operation.

Enumerator
AESECB_MODE_ENCRYPT 
AESECB_MODE_DECRYPT 

§ AESECB_OperationType

Enum for the operation types supported by the driver.

Enumerator
AESECB_OPERATION_TYPE_ENCRYPT 
AESECB_OPERATION_TYPE_DECRYPT 
AESECB_OPERATION_TYPE_ENCRYPT_SEGMENTED 
AESECB_OPERATION_TYPE_DECRYPT_SEGMENTED 
AESECB_OPERATION_TYPE_FINALIZE_ENCRYPT_SEGMENTED 
AESECB_OPERATION_TYPE_FINALIZE_DECRYPT_SEGMENTED 

Function Documentation

§ AESECB_init()

void AESECB_init ( void  )

This function initializes the ECB module.

Precondition
The AESECB_config structure must exist and be persistent before this function can be called. This function must also be called before any other ECB driver APIs. This function call does not modify any peripheral registers.

§ AESECB_Params_init()

void AESECB_Params_init ( AESECB_Params params)

Function to initialize the AESECB_Params struct to its defaults.

Parameters
paramsAn pointer to AESECB_Params structure for initialization

Defaults values are: returnBehavior = AESECB_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ AESECB_open()

AESECB_Handle AESECB_open ( uint_least8_t  index,
const AESECB_Params params 
)

This function opens a given ECB peripheral.

Precondition
ECB controller has been initialized using AESECB_init()
Parameters
[in]indexLogical peripheral number for the ECB indexed into the AESECB_config table
[in]paramsPointer to an parameter block, if NULL it will use default values.
Returns
An AESECB_Handle on success or a NULL on an error or if it has been opened already.
See also
AESECB_init()
AESECB_close()

§ AESECB_close()

void AESECB_close ( AESECB_Handle  handle)

Function to close an ECB peripheral specified by the ECB handle.

Precondition
AESECB_open() or AESECB_construct()
Parameters
[in]handleAn ECB handle returned from AESECB_open() or AESECB_construct()
See also
AESECB_open()

§ AESECB_Operation_init()

void AESECB_Operation_init ( AESECB_Operation operationStruct)

Function to initialize an AESECB_Operation struct to its defaults.

Parameters
[in]operationStructAn pointer to AESECB_Operation structure for initialization

Defaults values are all zeros.

§ AESECB_oneStepEncrypt()

int_fast16_t AESECB_oneStepEncrypt ( AESECB_Handle  handle,
AESECB_Operation operation 
)

Function to perform an AESECB encryption operation in one call.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted ciphertext or incorrect authentication.
Precondition
AESECB_open() or AESECB_construct(), and AESECB_Operation_init() have to be called first.
Parameters
[in]handleAn ECB handle returned from AESECB_open() or AESECB_construct()
[in]operationA pointer to a struct containing the parameters required to perform the operation.
Return values
AESECB_STATUS_SUCCESSThe operation succeeded.
AESECB_STATUS_ERRORThe operation failed.
AESECB_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESECB_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.
See also
AESECB_oneStepDecrypt()

§ AESECB_oneStepDecrypt()

int_fast16_t AESECB_oneStepDecrypt ( AESECB_Handle  handle,
AESECB_Operation operation 
)

Function to perform an AESECB decryption in one call.

Note
None of the buffers provided as arguments may be altered by the application during an ongoing operation. Doing so can yield corrupted plaintext or incorrectly failed verification.
Precondition
AESECB_open() or AESECB_construct(), and AESECB_Operation_init() have to be called first.
Parameters
[in]handleAn ECB handle returned from AESECB_open() or AESECB_construct()
[in]operationA pointer to a struct containing the parameters required to perform the operation.
Return values
AESECB_STATUS_SUCCESSThe operation succeeded.
AESECB_STATUS_ERRORThe operation failed.
AESECB_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESECB_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.
See also
AESECB_oneStepEncrypt()

§ AESECB_setupEncrypt()

int_fast16_t AESECB_setupEncrypt ( AESECB_Handle  handle,
const CryptoKey key 
)

Function to prepare a segmented AESECB encryption operation.

This functions sets up a segmented AESECB encryption operation.

Precondition
AESECB_open() or AESECB_construct()
Parameters
[in]handleAn ECB handle returned from AESECB_open() or AESECB_construct()
[in]keyA previously initialized CryptoKey.
Return values
AESECB_STATUS_SUCCESSThe operation succeeded.
AESECB_STATUS_ERRORThe operation failed.
Postcondition
AESECB_addData()

§ AESECB_setupDecrypt()

int_fast16_t AESECB_setupDecrypt ( AESECB_Handle  handle,
const CryptoKey key 
)

Function to prepare a segmented AESECB decryption operation.

This functions sets up a segmented AESECB decryption operation.

Precondition
AESECB_open() or AESECB_construct()
Parameters
[in]handleAn ECB handle returned from AESECB_open() or AESECB_construct()
[in]keyA previously initialized CryptoKey.
Return values
AESECB_STATUS_SUCCESSThe operation succeeded.
AESECB_STATUS_ERRORThe operation failed.
Postcondition
AESECB_addData()

§ AESECB_addData()

int_fast16_t AESECB_addData ( AESECB_Handle  handle,
AESECB_Operation operation 
)

Encrypts or decrypts segment of data with a length.

AESECB_addData() may be called an arbitrary number times before finishing the operation with AESECB_finalize(). Note that this function is called for use with segmented operations. For segmented operations, inputLength will govern the input/output lengths and must be a AES block size multiple (16-bytes).

Precondition
AESECB_setupEncrypt() or AESECB_setupDecrypt()
Parameters
[in]handleAn ECB handle returned from AESECB_open() or AESECB_construct()
[in]operationPointer to ECB operation structure()
Return values
AESECB_STATUS_SUCCESSThe operation succeeded.
AESECB_STATUS_ERRORThe operation failed.
AESECB_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESECB_STATUS_CANCELEDThe operation was canceled.
AESECB_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.
Postcondition
AESECB_addData() or AESECB_finalize()

§ AESECB_finalize()

int_fast16_t AESECB_finalize ( AESECB_Handle  handle,
AESECB_Operation operation 
)

Finalize the AES transaction. If new data needs to be added, inputLength will be used to govern how many bytes will be written.

Precondition
AESECB_addData()
Parameters
[in]handleAn ECB handle returned from AESECB_open() or AESECB_construct()
[in]operationPointer to ECB operation structure()
Return values
AESECB_STATUS_SUCCESSIn AESECB_RETURN_BEHAVIOR_BLOCKING and AESECB_RETURN_BEHAVIOR_POLLING, this means the ECB output was generated successfully. In AESECB_RETURN_BEHAVIOR_CALLBACK, this means the operation started successfully.
AESECB_STATUS_ERRORThe operation failed.
AESECB_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.
AESECB_STATUS_CANCELEDThe operation was canceled.
AESECB_STATUS_UNALIGNED_IO_NOT_SUPPORTEDThe input and/or output buffer were not word-aligned.

§ AESECB_cancelOperation()

int_fast16_t AESECB_cancelOperation ( AESECB_Handle  handle)

Cancels an ongoing AESECB operation.

Asynchronously cancels an AESECB operation. Only available when using AESECB_RETURN_BEHAVIOR_CALLBACK. The operation will terminate as though an error occurred. The return status code of the operation will be AESECB_STATUS_CANCELED.

Parameters
[in]handleHandle of the operation to cancel
Return values
AESECB_STATUS_SUCCESSThe operation was canceled, or the requested operation had already completed.

§ AESECB_construct()

AESECB_Handle AESECB_construct ( AESECB_Config config,
const AESECB_Params params 
)

Constructs a new AESECB object.

Unlike AESECB_open(), AESECB_construct() does not require the hwAttrs and object to be allocated in a AESECB_Config array that is indexed into. Instead, the AESECB_Config, hwAttrs, and object can be allocated at any location. This allows for relatively simple run-time allocation of temporary driver instances on the stack or the heap. The drawback is that this makes it more difficult to write device-agnostic code. If you use an ifdef with DeviceFamily, you can choose the correct object and hwAttrs to allocate. That compilation unit will be tied to the device it was compiled for at this point. To change devices, recompilation of the application with a different DeviceFamily setting is necessary.

Parameters
configAESECB_Config describing the location of the object and hwAttrs.
paramsAESECB_Params to configure the driver instance.
Returns
Returns a AESECB_Handle on success or NULL on failure.
Precondition
The object struct config points to must be zeroed out prior to calling this function. Otherwise, unexpected behavior may ensue.

Variable Documentation

§ AESECB_defaultParams

const AESECB_Params AESECB_defaultParams

Default AESECB_Params structure.

See also
AESECB_Params_init()
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale