![]() |
![]() |
============================================================================
This file contains the APIs to initialize and access plaintext CryptoKeys. Plaintext CryptoKeys point to keying material stored in flash or RAM and are not subject to enforced usage restrictions. That only means that calling a function that requires an asymmetric public key with a symmetric key will not return an error. It will likely not yield the desired results.
Plaintext keys are the simplest of the CryptoKeys. All they do is store the length of and a pointer to the keying material. Their use is hence simple as well. After calling the initialization function, the CryptoKey may be used in any of the crypto operation APIs that take a CryptoKey as an input.
#include <stddef.h>
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Go to the source code of this file.
Functions | |
int_fast16_t | CryptoKeyPlaintext_markAsBlank (CryptoKey *keyHandle) |
Marks a CryptoKey as 'blank'. More... | |
int_fast16_t | CryptoKeyPlaintext_initKey (CryptoKey *keyHandle, uint8_t *key, size_t keyLength) |
Initializes a CryptoKey type. More... | |
int_fast16_t | CryptoKeyPlaintext_initBlankKey (CryptoKey *keyHandle, uint8_t *keyLocation, size_t keyLength) |
Initializes an empty plaintext CryptoKey type. More... | |
int_fast16_t | CryptoKeyPlaintext_setKeyLocation (CryptoKey *keyHandle, uint8_t *location) |
Sets the CryptoKey keyMaterial pointer. More... | |
int_fast16_t | CryptoKeyPlaintext_getKeyLocation (CryptoKey *keyHandle, uint8_t **location) |
Gets the CryptoKey keyMaterial pointer. More... | |
int_fast16_t | CryptoKeyPlaintext_getKeyLength (CryptoKey *keyHandle, size_t *length) |
Gets the length of a plaintext key. More... | |
int_fast16_t | CryptoKeyPlaintext_setKeyLength (CryptoKey *keyHandle, size_t length) |
Sets the length of a plaintext key. More... | |
int_fast16_t | CryptoKeyPlaintextHSM_initKey (CryptoKey *keyHandle, uint8_t *key, size_t keyLength) |
Initializes a CryptoKey type. More... | |
int_fast16_t CryptoKeyPlaintext_markAsBlank | ( | CryptoKey * | keyHandle | ) |
int_fast16_t CryptoKeyPlaintext_initKey | ( | CryptoKey * | keyHandle, |
uint8_t * | key, | ||
size_t | keyLength | ||
) |
Initializes a CryptoKey type.
[in] | keyHandle | Pointer to a CryptoKey which will be initialized to type CryptoKey_PLAINTEXT and ready for use |
[in] | key | Pointer to keying material |
[in] | keyLength | Length of keying material in bytes |
int_fast16_t CryptoKeyPlaintext_initBlankKey | ( | CryptoKey * | keyHandle, |
uint8_t * | keyLocation, | ||
size_t | keyLength | ||
) |
Initializes an empty plaintext CryptoKey type.
[in] | keyHandle | Pointer to a CryptoKey which will be initialized to type CryptoKey_BLANK_PLAINTEXT |
[in] | keyLocation | Pointer to location where plaintext keying material can be stored |
[in] | keyLength | Length of keying material, in bytes |
int_fast16_t CryptoKeyPlaintext_setKeyLocation | ( | CryptoKey * | keyHandle, |
uint8_t * | location | ||
) |
Sets the CryptoKey keyMaterial pointer.
Updates the key location for a plaintext CryptoKey. Does not modify data at the pointer location.
[out] | keyHandle | Pointer to a plaintext CryptoKey who's key data pointer will be modified |
[in] | location | Pointer to key data location |
int_fast16_t CryptoKeyPlaintext_getKeyLocation | ( | CryptoKey * | keyHandle, |
uint8_t ** | location | ||
) |
Gets the CryptoKey keyMaterial pointer.
[in] | keyHandle | Pointer to an initialized plaintext CryptoKey |
[out] | location | Pointer to key data location |
int_fast16_t CryptoKeyPlaintext_getKeyLength | ( | CryptoKey * | keyHandle, |
size_t * | length | ||
) |
Gets the length of a plaintext key.
[in] | keyHandle | Pointer to a plaintext CryptoKey |
[out] | length | Length of the keying material, in bytes |
int_fast16_t CryptoKeyPlaintext_setKeyLength | ( | CryptoKey * | keyHandle, |
size_t | length | ||
) |
Sets the length of a plaintext key.
[out] | keyHandle | Pointer to a CryptoKey |
[in] | length | Length value in bytes to update keyHandle with |
int_fast16_t CryptoKeyPlaintextHSM_initKey | ( | CryptoKey * | keyHandle, |
uint8_t * | key, | ||
size_t | keyLength | ||
) |
Initializes a CryptoKey type.
[in] | keyHandle | Pointer to a CryptoKey which will be initialized to type CryptoKey_PLAINTEXT_HSM and ready for use |
[in] | key | Pointer to keying material |
[in] | keyLength | Length of keying material in bytes |