Data Fields
AESCommonLPF3_Object Struct Reference

AESCommonLPF3 Object. More...

#include <AESCommonLPF3.h>

Collaboration diagram for AESCommonLPF3_Object:
Collaboration graph
[legend]

Data Fields

uint32_t semaphoreTimeout
 
CryptoKey key
 
volatile int_fast16_t returnStatus
 
AES_ReturnBehavior returnBehavior
 
bool isOpen
 
volatile bool cryptoResourceLocked
 
volatile bool operationInProgress
 
volatile bool powerConstraintSet
 

Detailed Description

AESCommonLPF3 Object.

The application must not access any member variables of this structure!

Field Documentation

§ semaphoreTimeout

uint32_t AESCommonLPF3_Object::semaphoreTimeout

§ key

CryptoKey AESCommonLPF3_Object::key

§ returnStatus

volatile int_fast16_t AESCommonLPF3_Object::returnStatus

§ returnBehavior

AES_ReturnBehavior AESCommonLPF3_Object::returnBehavior

§ isOpen

bool AESCommonLPF3_Object::isOpen

§ cryptoResourceLocked

volatile bool AESCommonLPF3_Object::cryptoResourceLocked

§ operationInProgress

volatile bool AESCommonLPF3_Object::operationInProgress

§ powerConstraintSet

volatile bool AESCommonLPF3_Object::powerConstraintSet

The documentation for this struct was generated from the following file:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale