Graph Legend

This page explains how to interpret the graphs that are generated by doxygen.

Consider the following example:

/*! Invisible class because of truncation */
class Invisible { };
/*! Truncated class, inheritance relation is hidden */
class Truncated : public Invisible { };
/* Class not documented with doxygen comments */
class Undocumented { };
/*! Class that is inherited using public inheritance */
class PublicBase : public Truncated { };
/*! A template class */
template<class T> class Templ { };
/*! Class that is inherited using protected inheritance */
class ProtectedBase { };
/*! Class that is inherited using private inheritance */
class PrivateBase { };
/*! Class that is used by the Inherited class */
class Used { };
/*! Super class that inherits a number of other classes */
class Inherited : public PublicBase,
protected ProtectedBase,
private PrivateBase,
public Undocumented,
public Templ<int>
{
private:
Used *m_usedClass;
};

This will result in the following graph:

The boxes in the above graph have the following meaning:

The arrows have the following meaning:

© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale