![]() |
![]() |
AESCBCLPF3 Object. More...
#include <AESCBCLPF3.h>
Data Fields | |
AESCommonLPF3_Object | common |
volatile uint32_t | iv [AES_IV_LENGTH_BYTES/4] |
const uint8_t * | input |
uint8_t * | output |
AESCBC_CallbackFxn | callbackFxn |
AESCBC_OperationUnion * | operation |
AESCBC_OperationType | operationType |
bool | threadSafe |
size_t | inputLength |
int_fast16_t | hsmStatus |
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly. More... | |
bool | segmentedOperationInProgress |
AESCBCLPF3 Object.
The application must not access any member variables of this structure!
AESCommonLPF3_Object AESCBCLPF3_Object::common |
volatile uint32_t AESCBCLPF3_Object::iv[AES_IV_LENGTH_BYTES/4] |
const uint8_t* AESCBCLPF3_Object::input |
uint8_t* AESCBCLPF3_Object::output |
AESCBC_CallbackFxn AESCBCLPF3_Object::callbackFxn |
AESCBC_OperationUnion* AESCBCLPF3_Object::operation |
AESCBC_OperationType AESCBCLPF3_Object::operationType |
bool AESCBCLPF3_Object::threadSafe |
size_t AESCBCLPF3_Object::inputLength |
int_fast16_t AESCBCLPF3_Object::hsmStatus |
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
bool AESCBCLPF3_Object::segmentedOperationInProgress |