58 #ifndef ti_drivers_aescbc_AESCBCLPF3__include 59 #define ti_drivers_aescbc_AESCBCLPF3__include 68 #include <ti/devices/DeviceFamily.h> 69 #include DeviceFamily_constructPath(driverlib/aes.h) 92 volatile uint32_t iv[AES_IV_LENGTH_BYTES / 4];
99 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX) 127 __STATIC_INLINE
bool AESCBC_acquireLock(
AESCBC_Handle handle, uint32_t timeout)
141 __STATIC_INLINE
void AESCBC_releaseLock(
AESCBC_Handle handle)
155 __STATIC_INLINE
void AESCBC_enableThreadSafety(
AESCBC_Handle handle)
158 object->threadSafe =
true;
173 __STATIC_INLINE
void AESCBC_disableThreadSafety(
AESCBC_Handle handle)
176 object->threadSafe =
false;
AESCBC_OperationUnion * operation
Definition: AESCBCLPF3.h:96
AESCommonLPF3_HWAttrs AESCBCLPF3_HWAttrs
AESCBCLPF3 Hardware Attributes.
Definition: AESCBCLPF3.h:81
bool CryptoResourceLPF3_acquireLock(uint32_t timeout)
bool threadSafe
Definition: AESCBCLPF3.h:98
const uint8_t * input
Definition: AESCBCLPF3.h:93
AES Global configuration.
Definition: AESCommon.h:154
AESCBC_CallbackFxn callbackFxn
Definition: AESCBCLPF3.h:95
int_fast16_t hsmStatus
The staus of the HSM Boot up process if HSMLPF3_STATUS_SUCCESS, the HSM booted properly. if HSMLPF3_STATUS_ERROR, the HSM did not boot properly.
Definition: AESCBCLPF3.h:106
AESCBC_OperationType operationType
Definition: AESCBCLPF3.h:97
size_t inputLength
Definition: AESCBCLPF3.h:100
AESCommonLPF3 Hardware Attributes.
Definition: AESCommonLPF3.h:80
bool segmentedOperationInProgress
Definition: AESCBCLPF3.h:109
void CryptoResourceLPF3_releaseLock(void)
AESCommon driver implementation for the Low Power F3 family.
Shared resources to arbitrate access to the AES engine.
AESCBC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCBC.h:872
void * object
Definition: AESCommon.h:157
Union containing a reference to a one step or segmented operation.
Definition: AESCBC.h:863
AESCommonLPF3_Object common
Definition: AESCBCLPF3.h:91
AESCBCLPF3 Object.
Definition: AESCBCLPF3.h:88
uint8_t * output
Definition: AESCBCLPF3.h:94
void(* AESCBC_CallbackFxn)(AESCBC_Handle handle, int_fast16_t returnValue, AESCBC_OperationUnion *operation, AESCBC_OperationType operationType)
The definition of a callback function used by the AESCBC driver when used in AESCBC_RETURN_BEHAVIOR_C...
Definition: AESCBC.h:900
AESCommonLPF3 Object.
Definition: AESCommonLPF3.h:102