![Logo](ti_logo.svg) |
xWRL6432 MMWAVE-L-SDK
05.05.00.00
|
|
Go to the documentation of this file.
43 #ifndef CFAR_PROC_HWA_H
44 #define CFAR_PROC_HWA_H
62 #include <datapath/dpif/dpif_pointcloud.h>
78 #define DPU_CFARPROCHWA_DET_MATRIX_BYTE_ALIGNMENT (sizeof(uint16_t))
83 #define DPU_CFARPROCHWA_CFAR_DET_LIST_BYTE_ALIGNMENT DPIF_CFAR_DET_LIST_CPU_BYTE_ALIGNMENT
89 #define DPU_CFARPROCHWA_HWA_MEM_OUT_DOPPLER_BYTE_ALIGNMENT (sizeof(uint32_t))
95 #define DPU_CFARPROCHWA_HWA_MEM_OUT_RANGE_BYTE_ALIGNMENT (sizeof(uint32_t))
100 #define DPU_CFARPROCHWA_DOPPLER_DET_OUT_BIT_MASK_BYTE_ALIGNMENT (sizeof(uint32_t))
114 #define DPU_CFARPROCHWA_EINVAL (DP_ERRNO_CFAR_PROC_BASE-1)
119 #define DPU_CFARPROCHWA_EINVAL__DET_MATRIX_FORMAT (DP_ERRNO_CFAR_PROC_BASE-2)
124 #define DPU_CFARPROCHWA_EINVAL__NUM_PARAM_SETS (DP_ERRNO_CFAR_PROC_BASE-3)
129 #define DPU_CFARPROCHWA_ENOMEM (DP_ERRNO_CFAR_PROC_BASE-10)
134 #define DPU_CFARPROCHWA_ENOMEM__DET_MATRIX_EXCEEDS_HWA_INP_MEM (DP_ERRNO_CFAR_PROC_BASE-11)
139 #define DPU_CFARPROCHWA_ENOMEMALIGN_DET_MATRIX (DP_ERRNO_CFAR_PROC_BASE-12)
144 #define DPU_CFARPROCHWA_ENOMEMALIGN_HWA_MEM_OUT_RANGE (DP_ERRNO_CFAR_PROC_BASE-15)
149 #define DPU_CFARPROCHWA_NUM_RANGE_BINS_EXCEDED_LIMIT (DP_ERRNO_CFAR_PROC_BASE-18)
154 #define DPU_CFARPROCEDMA_ESEMA (DP_ERRNO_CFAR_PROC_BASE-19)
159 #define DPU_CFARPROCHWA_EINTERNAL (DP_ERRNO_CFAR_PROC_BASE-20)
164 #define DPU_CFARPROCHWA_EHWA_PARAM_SAVE_LOC_SIZE (DP_ERRNO_CFAR_PROC_BASE-21)
169 #define DPU_CFARPROCHWA_ENOTIMPL (DP_ERRNO_CFAR_PROC_BASE-30)
174 #define DPU_CFARPROCHWA_ESEMA (DP_ERRNO_CFAR_PROC_BASE-40)
183 #define DPU_CFARPROCHWA_SHIFT_Q8 8
184 #define DPU_CFARPROCHWA_ONE_Q8 (1<<DPU_CFARPROCHWA_SHIFT_Q8)
189 #define DPU_CFARPROCHWA_MAX_NUM_HWA_PARAMSET 2
200 typedef enum DPU_CFARProcHWA_Cmd_e
221 typedef struct DPU_CFARProcHWA_HwaParamSaveLoc_t
239 typedef struct DPU_CFARProcHWA_HwaCfarConfig_t
262 typedef volatile struct DPU_CFARProcHWA_CfarDetOutput_t
277 typedef volatile struct DPU_CFARProcHWA_HwaMaxOutput_t
293 typedef struct DPU_CFARProcHWA_InitParams_t
310 typedef struct DPU_CFARProcHWA_Resources_t
372 typedef struct DPU_CFARProcHWA_DynamicConfig_t
397 typedef struct DPU_CFARProcHWA_StaticConfig_t
462 typedef struct DPU_CFARProcHWA_Config_t
481 typedef struct DPU_CFARProcHWA_InputParams_t
501 typedef struct DPU_CFARProcHWA_OutParams_t
681 uint8_t *numUsedHwaParamSets
uint32_t detObjOutMaxSize
point-cloud output list size
Definition: cfarprochwa.h:516
uint16_t elevationFftSize
Elevation FFT size.
Definition: cfarprochwa.h:412
DPU_CFARProcHWA_CfarDetOutput * hwaMemOutDetList
HWA memory for intermediate cfar detection list
Definition: cfarprochwa.h:342
Detection matrix buffer interface.
Definition: dpif_detmatrix.h:81
CFAR Hardware resources.
Definition: cfarprochwa.h:311
uint8_t log2NumDopplerBins
Log2 of number of doppler bins.
Definition: cfarprochwa.h:400
DPIF_PointCloudRngAzimElevDopInd * detObjIndOut
point-cloud output list with range/azimuth/elevation/doppler indices (for testing)
Definition: cfarprochwa.h:513
float lambdaOverDistX
Lambda over antenna spacing in x-direction.
Definition: cfarprochwa.h:421
Defines the detection matrix buffer interface.
float rangeStep
Range conversion factor for FFT range index to meters.
Definition: cfarprochwa.h:415
Maximum peaks filled by HWA statistics block.
Definition: cfarprochwa.h:278
Implements Common definition across cfarcaProc DPU.
Field of view - AoA Configuration.
Definition: cfarproccommon.h:226
EDMA interrupt configuration object. The object is passed to the EDMA_registerIntr() function....
Definition: edma/v0/edma.h:451
HWA CFAR configuration.
Definition: cfarprochwa.h:463
uint32_t cellIdx
Sample index (i.e. cell under test index)
Definition: cfarprochwa.h:265
DPEDMA_ChanCfg edmaHwaIn
EDMA configuration for CFAR data In.
Definition: cfarprochwa.h:316
uint16_t * hwaMemInp
HWA scratch memory to page-in detection matrix. Note two contiguous M memory banks (of the 4 banks) c...
Definition: cfarprochwa.h:335
void * data
Pointer to save location for HWA PARAM sets.
Definition: cfarprochwa.h:224
uint16_t numDopplerBins
Number of doppler bins.
Definition: cfarprochwa.h:406
HWA CFAR static configuration.
Definition: cfarprochwa.h:398
DPIF_PointCloudCartesianExt * detObjOut
point-cloud output list
Definition: cfarprochwa.h:510
int32_t DPU_CFARProcHWA_control(DPU_CFARProcHWA_Handle handle, DPU_CFARProcHWA_Cmd cmd, void *arg, uint32_t argSize)
float rangeBias
Range bias.
Definition: cfarprochwa.h:427
uint32_t numCfarDetectedPoints
Number of CFAR detected points.
Definition: cfarprochwa.h:507
CFAR Configuration.
Definition: cfarproccommon.h:158
DPU_CFARProc_CfarCfg * cfarCfg
Definition: cfarprochwa.h:374
Base error codes for the data path Modules.
HWA CFAR dynamic configuration.
Definition: cfarprochwa.h:373
HWA_Handle hwaHandle
HWA Handle.
Definition: cfarprochwa.h:296
@ DPU_CFARProcHWA_Cmd_FovAoaCfg
Command to update field of view in angle domain, minimum and maximum angle limits (for azimuth and el...
Definition: cfarprochwa.h:210
uint8_t angleDimension
1 - 1D: 6x1 azimuth antenna array 2 - 2D: one lower row: 4 antennas, upper row 2 antennas
Definition: cfarprochwa.h:435
Data processing Unit statistics.
Definition: cfarproccommon.h:204
bool isDetMatrixLogScale
Detection matrix format 0 - Linear 32-bit integer, 1 - 16-bit log2 magnitude in Q11 format.
Definition: cfarprochwa.h:444
void * DPU_CFARProcHWA_Handle
CFARHwa DPU Handle.
Definition: cfarprochwa.h:536
uint32_t noise
Noise energy in CFAR cell.
Definition: cfarprochwa.h:264
Field of view - Range Configuration.
Definition: cfarproccommon.h:251
DPU_CFARProcHWA_HwaParamSaveLoc hwaParamsSaveLoc
HWA Params save location.
Definition: cfarprochwa.h:249
uint8_t detectionHeatmapType
0-Range-Azimuth heatmap, 1-Range-Doppler heatmap
Definition: cfarprochwa.h:438
Detected object parameters filled by HWA CFAR.
Definition: cfarprochwa.h:263
DPU_CFARProcHWA_HwaCfarConfig hwaCfg
HWA Configuration.
Definition: cfarprochwa.h:328
DPU_CFARProcHWA_HwaMaxOutput * hwaMemOutRangeProfile
HWA memory to store range profile.
Definition: cfarprochwa.h:349
DPEDMA_ChanCfg edmaHwaOut
EDMA configuration for CFAR data Out.
Definition: cfarprochwa.h:319
CFARCAProcHWA DPU initial configuration parameters.
Definition: cfarprochwa.h:294
float dopplerStep
Doppler conversion factor for Doppler FFT index to m/s.
Definition: cfarprochwa.h:418
CFAR Configuration.
Definition: cfarproccommon.h:90
DPU_CFARProcHWA_Cmd
cfarProc control command
Definition: cfarprochwa.h:201
uint16_t azimuthFftSize
Azimuth FFT size.
Definition: cfarprochwa.h:409
DPU_CFARProcHWA_Handle DPU_CFARProcHWA_init(DPU_CFARProcHWA_InitParams *initCfg, int32_t *errCode)
uint32_t peak
Maximum peak value.
Definition: cfarprochwa.h:280
DPU_CFARProcHWA_StaticConfig staticCfg
Static configuration.
Definition: cfarprochwa.h:471
DPU_CFARProc_Stats stats
CFARCAProc statistics.
Definition: cfarprochwa.h:504
uint8_t numParamSet
number of HWA paramset
Definition: cfarprochwa.h:245
DPEDMA_ChanCfg edmaHwaInSignature
EDMA configuration for EDMA In to trigger HWA.
Definition: cfarprochwa.h:322
@ DPU_CFARProcHWA_Cmd_CfarCfg
Command to update CFAR configuration in range domain.
Definition: cfarprochwa.h:204
DPIF_CFARRngDopDetListElement * detRngDopList
CFAR final output detection list filled by CFAR DPU when running on Range/Doppler heatmap.
Definition: cfarprochwa.h:525
bool enableCfarPointCloudListWithIndices
enable CFAR point cloud list with range/azimuth indices
Definition: cfarprochwa.h:447
@ DPU_CFARProcHWA_Cmd_FovRangeCfg
Command to update field of view in range domain, minimum and maximum range limits.
Definition: cfarprochwa.h:207
uint32_t hwaMemOutDetListSize
Maximum number of elements of type DPU_CFARProcHWA_CfarDetOutput of HWA memory for cfar detection lis...
Definition: cfarprochwa.h:346
DPU_CFARProc_RangeFovCfg * fovRange
Field of view configuration in range domain.
Definition: cfarprochwa.h:382
uint16_t numRangeBins
Number of range bins.
Definition: cfarprochwa.h:403
uint32_t reserved
Reserved.
Definition: cfarprochwa.h:267
bool isStaticClutterRemovalEnabled
Static Clutter Removal Cfg.
Definition: cfarprochwa.h:441
uint32_t hwaMemInpSize
Number of elements of type uint16_t of HWA memory to hold detection matrix (associated with hwaMemInp...
Definition: cfarprochwa.h:339
Structure for the HWA Params save location.
Definition: cfarprochwa.h:222
DPU_CFARProcHWA_CfarDetOutput * cfarRangeDetOutList
CFAR output detection list filled by HWA.
Definition: cfarprochwa.h:522
DPU_CFARProcHWA_DynamicConfig dynCfg
Dynamic configuration.
Definition: cfarprochwa.h:468
Edma_IntrObject * intrObj
EDMA interrupt object.
Definition: cfarprochwa.h:325
uint32_t * rangeProfile
range profile
Definition: cfarprochwa.h:519
CFAR HWA configuration.
Definition: cfarprochwa.h:240
void * EDMA_Handle
A handle that is returned from a EDMA_open() call.
Definition: edma/v0/edma.h:471
DPU_CFARProc_AoaFovCfg * fovAoaCfg
CFAR configuration in range direction.
Definition: cfarprochwa.h:379
DPIF_DetMatrix detMatrix
Pointer to detection matrix.
Definition: cfarprochwa.h:331
uint32_t * rangeDopplerDetPointBitMap
Range Doppler detection bitmap.
Definition: cfarprochwa.h:358
int32_t DPU_CFARProcHWA_process(DPU_CFARProcHWA_Handle handle, DPIF_DetMatrix *detMatrix, DPU_CFARProcHWA_InputParams *inputParams, DPU_CFARProcHWA_OutParams *outParams)
float lambdaOverDistZ
Lambda over antenna spacing in z-direction.
Definition: cfarprochwa.h:424
DPIF_DetMatrix dopplerIndexMatrix
Doppler index matrix.
Definition: cfarprochwa.h:352
EDMA_Handle edmaHandle
EDMA Handle.
Definition: cfarprochwa.h:313
uint8_t selectCoherentPeakInDopplerDim
1 - select the coherent peak in Doppler, 0 - non-coherently combine accross Doppler,...
Definition: cfarprochwa.h:432
int32_t DPU_CFARProcHWA_deinit(DPU_CFARProcHWA_Handle handle)
DPIF_DetMatrix elevationIndexMatrix
Elevation index matrix.
Definition: cfarprochwa.h:355
Output parameters populated during Processing time.
Definition: cfarprochwa.h:502
EDMA Configuration Utility API definitions.
DPU_CFARProcHWA_HW_Resources res
Hardware resources.
Definition: cfarprochwa.h:465
uint32_t sizeBytes
Size of the save location for HWA PARAM sets in Bytes.
Definition: cfarprochwa.h:227
int32_t DPU_CFARProcHWA_config(DPU_CFARProcHWA_Handle handle, DPU_CFARProcHWA_Config *cfarHwaCfg)
void * HWA_Handle
A handle that is returned from a HWA_open() call.
Definition: hwa/v0/hwa.h:612
uint32_t maxInd
Maximum peak index position.
Definition: cfarprochwa.h:279
uint8_t paramSetStartIdx
HWA paramset Start index.
Definition: cfarprochwa.h:242
DPU_CFARProc_CfarScndPassCfg * cfarScndPassCfg
Definition: cfarprochwa.h:376
uint32_t iterNum
Iteration number (i.e. REG_BCNT counter value)
Definition: cfarprochwa.h:266
EDMA channel configuration.
Definition: dpedma.h:132
int32_t DPU_CFARProcHWA_GetNumUsedHwaParamSets(DPU_CFARProcHWA_Handle handle, uint8_t *numUsedHwaParamSets)
uint8_t dmaTrigSrcChan
HWA param set dma trigger source channel.
Definition: cfarprochwa.h:253