xWRL6432 MMWAVE-L-SDK  05.05.00.00
dpedma.h File Reference

Introduction

EDMA Configuration Utility API definitions.

NOTE: (C) Copyright 2018 - 2021 Texas Instruments, Inc.

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Go to the source code of this file.

Data Structures

struct  DPEDMA_ChanCfg
 EDMA channel configuration. More...
 
struct  DPEDMA_3LinkChanCfg
 EDMA channel configuration with 3 shadow channels. More...
 
struct  DPEDMA_2LinkChanCfg
 EDMA channel configuration with 2 shadow channels. More...
 
struct  DPEDMA_ChainingCfg
 EDMA chaining configuration. More...
 
struct  DPEDMA_syncACfg
 EDMA configuration for Sync A copy. More...
 
struct  DPEDMA_syncABCfg
 EDMA configuration for Sync AB copy. More...
 

Macros

#define DPEDMA_NO_ERROR   ((int32_t)0)
 
#define DPEDMA_EINVAL   (DP_ERRNO_DPEDMA_BASE-1)
 Error Code: Invalid argument. More...
 
#define DPEDMA_EINVAL_EDMAADDR   (DP_ERRNO_DPEDMA_BASE-2)
 Error Code: Invalid EDMA baseaddress. More...
 
#define DPEDMA_EDMA_TRIGGER_FAIL   (DP_ERRNO_DPEDMA_BASE-3)
 Error Code: EDMA transfer trigger failure. More...
 

Functions

int32_t DPEDMA_configDummyChannel (EDMA_Handle handle, uint32_t chType, uint32_t *dmaCh, uint32_t *tcc, uint32_t *param)
 
int32_t DPEDMA_setSourceAddress (EDMA_Handle handle, uint32_t chanId, uint32_t addressVal)
 
int32_t DPEDMA_setDestinationAddress (EDMA_Handle handle, uint32_t chanId, uint32_t addressVal)
 
int32_t DPEDMA_setBcntAcnt (EDMA_Handle handle, uint32_t chanId, uint32_t BcntAcnt)
 
int32_t DPEDMA_startTransfer (EDMA_Handle handle, uint32_t chanId)
 
uint32_t DPEDMA_local2Global (uint32_t addr)
 
int32_t DPEDMA_configSyncTransfer (EDMA_Handle handle, DPEDMA_ChanCfg *chanCfg, DPEDMA_ChainingCfg *chainingCfg, DPEDMA_syncABCfg *syncABCfg, bool isEventTriggered, bool isIntermediateTransferCompletionEnabled, bool isTransferCompletionEnabled, Edma_EventCallback transferCompletionCallbackFxn, void *transferCompletionCallbackFxnArg, Edma_IntrObject *intrObj, uint8_t transferType)
 
int32_t DPEDMA_linkParamSets (EDMA_Handle handle, uint16_t fromParamId, uint16_t toParamId)
 
int32_t DPEDMA_configSyncAB (EDMA_Handle handle, DPEDMA_ChanCfg *chanCfg, DPEDMA_ChainingCfg *chainingCfg, DPEDMA_syncABCfg *syncABCfg, bool isEventTriggered, bool isIntermediateTransferCompletionEnabled, bool isTransferCompletionEnabled, Edma_EventCallback transferCompletionCallbackFxn, void *transferCompletionCallbackFxnArg, Edma_IntrObject *intrObj)
 
int32_t DPEDMA_configSyncA_singleFrame (EDMA_Handle handle, DPEDMA_ChanCfg *chanCfg, DPEDMA_ChainingCfg *chainingCfg, DPEDMA_syncACfg *syncACfg, bool isEventTriggered, bool isIntermediateTransferInterruptEnabled, bool isTransferCompletionEnabled, Edma_EventCallback transferCompletionCallbackFxn, void *transferCompletionCallbackFxnArg, Edma_IntrObject *intrObj)
 
int32_t DPEDMA_configSyncA (EDMA_Handle handle, DPEDMA_ChanCfg *chanCfg, DPEDMA_ChainingCfg *chainingCfg, DPEDMA_syncACfg *syncACfg, bool isEventTriggered, bool isIntermediateTransferInterruptEnabled, bool isTransferCompletionEnabled, Edma_EventCallback transferCompletionCallbackFxn, void *transferCompletionCallbackFxnArg, Edma_IntrObject *intrObj)
 
int32_t DPEDMA_updateAddressAndTrigger (EDMA_Handle handle, uint32_t srcAddress, uint32_t destAddress, uint8_t channel, uint8_t triggerEnabled)
 
void DPEDMA_allocateEDMAChannel (EDMA_Handle handle, uint32_t *dmaCh, uint32_t *tcc, uint32_t *param)
 
void DPEDMA_freeEDMAChannel (EDMA_Handle handle, uint32_t *dmaCh, uint32_t *tcc, uint32_t *param, uint32_t *shadowParam)
 
int32_t DPEDMA_edmaStartTransferManualTrigger (EDMA_Handle handle, uint32_t channel)
 

Macro Definition Documentation

◆ DPEDMA_NO_ERROR

#define DPEDMA_NO_ERROR   ((int32_t)0)

Function Documentation

◆ DPEDMA_configDummyChannel()

int32_t DPEDMA_configDummyChannel ( EDMA_Handle  handle,
uint32_t  chType,
uint32_t *  dmaCh,
uint32_t *  tcc,
uint32_t *  param 
)

◆ DPEDMA_setSourceAddress()

int32_t DPEDMA_setSourceAddress ( EDMA_Handle  handle,
uint32_t  chanId,
uint32_t  addressVal 
)

◆ DPEDMA_setDestinationAddress()

int32_t DPEDMA_setDestinationAddress ( EDMA_Handle  handle,
uint32_t  chanId,
uint32_t  addressVal 
)

◆ DPEDMA_setBcntAcnt()

int32_t DPEDMA_setBcntAcnt ( EDMA_Handle  handle,
uint32_t  chanId,
uint32_t  BcntAcnt 
)

◆ DPEDMA_startTransfer()

int32_t DPEDMA_startTransfer ( EDMA_Handle  handle,
uint32_t  chanId 
)

◆ DPEDMA_local2Global()

uint32_t DPEDMA_local2Global ( uint32_t  addr)

◆ DPEDMA_configSyncTransfer()

int32_t DPEDMA_configSyncTransfer ( EDMA_Handle  handle,
DPEDMA_ChanCfg chanCfg,
DPEDMA_ChainingCfg chainingCfg,
DPEDMA_syncABCfg syncABCfg,
bool  isEventTriggered,
bool  isIntermediateTransferCompletionEnabled,
bool  isTransferCompletionEnabled,
Edma_EventCallback  transferCompletionCallbackFxn,
void *  transferCompletionCallbackFxnArg,
Edma_IntrObject intrObj,
uint8_t  transferType 
)

◆ DPEDMA_linkParamSets()

int32_t DPEDMA_linkParamSets ( EDMA_Handle  handle,
uint16_t  fromParamId,
uint16_t  toParamId 
)

◆ DPEDMA_configSyncAB()

int32_t DPEDMA_configSyncAB ( EDMA_Handle  handle,
DPEDMA_ChanCfg chanCfg,
DPEDMA_ChainingCfg chainingCfg,
DPEDMA_syncABCfg syncABCfg,
bool  isEventTriggered,
bool  isIntermediateTransferCompletionEnabled,
bool  isTransferCompletionEnabled,
Edma_EventCallback  transferCompletionCallbackFxn,
void *  transferCompletionCallbackFxnArg,
Edma_IntrObject intrObj 
)

◆ DPEDMA_configSyncA_singleFrame()

int32_t DPEDMA_configSyncA_singleFrame ( EDMA_Handle  handle,
DPEDMA_ChanCfg chanCfg,
DPEDMA_ChainingCfg chainingCfg,
DPEDMA_syncACfg syncACfg,
bool  isEventTriggered,
bool  isIntermediateTransferInterruptEnabled,
bool  isTransferCompletionEnabled,
Edma_EventCallback  transferCompletionCallbackFxn,
void *  transferCompletionCallbackFxnArg,
Edma_IntrObject intrObj 
)

◆ DPEDMA_configSyncA()

int32_t DPEDMA_configSyncA ( EDMA_Handle  handle,
DPEDMA_ChanCfg chanCfg,
DPEDMA_ChainingCfg chainingCfg,
DPEDMA_syncACfg syncACfg,
bool  isEventTriggered,
bool  isIntermediateTransferInterruptEnabled,
bool  isTransferCompletionEnabled,
Edma_EventCallback  transferCompletionCallbackFxn,
void *  transferCompletionCallbackFxnArg,
Edma_IntrObject intrObj 
)

◆ DPEDMA_updateAddressAndTrigger()

int32_t DPEDMA_updateAddressAndTrigger ( EDMA_Handle  handle,
uint32_t  srcAddress,
uint32_t  destAddress,
uint8_t  channel,
uint8_t  triggerEnabled 
)

◆ DPEDMA_allocateEDMAChannel()

void DPEDMA_allocateEDMAChannel ( EDMA_Handle  handle,
uint32_t *  dmaCh,
uint32_t *  tcc,
uint32_t *  param 
)

◆ DPEDMA_freeEDMAChannel()

void DPEDMA_freeEDMAChannel ( EDMA_Handle  handle,
uint32_t *  dmaCh,
uint32_t *  tcc,
uint32_t *  param,
uint32_t *  shadowParam 
)

◆ DPEDMA_edmaStartTransferManualTrigger()

int32_t DPEDMA_edmaStartTransferManualTrigger ( EDMA_Handle  handle,
uint32_t  channel 
)