xWRL6432 MMWAVE-L-SDK  05.05.00.00
DataPath EDMA Error Codes

Introduction

The section has a list of all the error codes which are generated by the module.

Base error code for the dpedma is defined in the

Macros

#define DPEDMA_EINVAL   (DP_ERRNO_DPEDMA_BASE-1)
 Error Code: Invalid argument. More...
 
#define DPEDMA_EINVAL_EDMAADDR   (DP_ERRNO_DPEDMA_BASE-2)
 Error Code: Invalid EDMA baseaddress. More...
 
#define DPEDMA_EDMA_TRIGGER_FAIL   (DP_ERRNO_DPEDMA_BASE-3)
 Error Code: EDMA transfer trigger failure. More...
 

Macro Definition Documentation

◆ DPEDMA_EINVAL

#define DPEDMA_EINVAL   (DP_ERRNO_DPEDMA_BASE-1)

Error Code: Invalid argument.

◆ DPEDMA_EINVAL_EDMAADDR

#define DPEDMA_EINVAL_EDMAADDR   (DP_ERRNO_DPEDMA_BASE-2)

Error Code: Invalid EDMA baseaddress.

◆ DPEDMA_EDMA_TRIGGER_FAIL

#define DPEDMA_EDMA_TRIGGER_FAIL   (DP_ERRNO_DPEDMA_BASE-3)

Error Code: EDMA transfer trigger failure.