The section has a list of all the data structures which are exposed to the application.
Data Structures | |
struct | DPU_RangeProcHWA_FFTtuning |
rangeProc FFT tuning parameters for HWA based Range FFT More... | |
struct | DPU_RangeProcHWA_HwaConfig |
RangeProc HWA configuration. More... | |
struct | DPU_RangeProcHWA_EDMAInputConfig |
RangeProc EDMA configuration. More... | |
struct | DPU_RangeProcHWA_EDMAOutputConfigPath |
RangeProc EDMA configuration. More... | |
struct | DPU_RangeProcHWA_EDMAOutputConfig |
RangeProc output EDMA configuration. More... | |
struct | DPU_RangeProcHWA_HW_Resources |
RangeProcHWA hardware resources. More... | |
struct | DPU_RangeProcHWA_compressCfg |
Compression parameters. More... | |
struct | DPU_RangeProcHWA_StaticConfig |
RangeProcHWA static configuration. More... | |
struct | DPU_RangeProcHWA_DynamicConfig |
RangeProcHWA dynamic configuration. More... | |
struct | DPU_RangeProcHWA_Config |
Range FFT configuration. More... | |
struct | DPU_RangeProcHWA_InitParams |
rangeProcHWA output parameters populated during rangeProc Processing time More... | |
struct | DPU_RangeProcHWA_OutParams |
rangeProcHWA output parameters populated during rangeProc Processing time More... | |
Typedefs | |
typedef uint32_t | DPU_RangeProcHWA_InputMode |
RangeProc data input mode. More... | |
typedef uint32_t | DPU_RangeProcHWA_Cmd |
rangeProc control command More... | |
typedef void * | DPU_RangeProcHWA_Handle |
rangeProc DPU Handle More... | |
typedef uint32_t DPU_RangeProcHWA_InputMode |
RangeProc data input mode.
This enum defines if the rangeProc input data is from RF front end or it is in M0 but standalone from RF.
typedef uint32_t DPU_RangeProcHWA_Cmd |
rangeProc control command
The enum defines the rangeProc supported run time command
typedef void* DPU_RangeProcHWA_Handle |
rangeProc DPU Handle