RangeProc output EDMA configuration.
The structure is used to hold the EDMA configuration needed for Range FFT
Fmt1: Generic EDMA ping/pong output mode
Fmt2: Specific EDMA ping/pong output mode used ONLY for 3 TX anntenna for radar cube layout format: DPIF_RADARCUBE_FORMAT_1, ADCbuf interleave mode DPIF_RXCHAN_NON_INTERLEAVE_MODE
Data Fields | |
DPU_RangeProcHWA_EDMAOutputConfigPath | path [2] |
uint32_t | dummySrc |
Dummy location. More... | |
uint32_t | dummyDst |
Dummy location More... | |
DPU_RangeProcHWA_EDMAOutputConfigPath DPU_RangeProcHWA_EDMAOutputConfig::path[2] |
uint32_t DPU_RangeProcHWA_EDMAOutputConfig::dummySrc |
Dummy location.
uint32_t DPU_RangeProcHWA_EDMAOutputConfig::dummyDst |
Dummy location