Defines RF ADCBuf interface.
Go to the source code of this file.
Data Structures | |
struct | DPIF_ADCBufProperty |
ADC Data buffer property. More... | |
struct | DPIF_ADCBufData |
ADC Data buffer definition. More... | |
Macros | |
#define | DPIF_RXCHAN_NON_INTERLEAVE_MODE (uint32_t) 0U |
#define | DPIF_RXCHAN_INTERLEAVE_MODE (uint32_t) 1U |
Typedefs | |
typedef uint32_t | DPIF_RXCHAN_INTERLEAVE |
RX channel ADC data interleave mode. More... | |
#define DPIF_RXCHAN_NON_INTERLEAVE_MODE (uint32_t) 0U |
#define DPIF_RXCHAN_INTERLEAVE_MODE (uint32_t) 1U |
typedef uint32_t DPIF_RXCHAN_INTERLEAVE |
RX channel ADC data interleave mode.
The enumeration describes the data interleave mode across RF RX channels