3.2.2.6. HSR PRP¶
Introduction
High-availability Seamless Redundancy (HSR) and Parellel Redundancy Protocol (PRP) are protocols supporting redundant network connections defined by IEC 62439-3. Both operate by using two ethernet ports together, and duplicating every frame to be sent over both ports, so if one connection fails, the transmission succeeds. Frames are tagged with a sequence number, so the receiving node can identify and discard duplicates. HSR/PRP provides an advantage over other protocols that handle link failure (e.g. STP/RSTP) because there is no downtime or packet loss on link failure. This is required in some industrial networking situations.
The major difference between HSR and PRP is that HSR networks are configured as a ring, then frames are sent both directions around the ring by all nodes. PRP networks can take any configuration, and all connections are simply physically duplicated. Additionally, PRP nodes can interoperate with standard ethernet networks, while HSR cannot. (See more details below and full details in IEC 62439-3)
Linux HSR PRP Support
Linux supports HSR/PRP protocol to be run over two EMAC ports where Linux takes care of duplicating the packets sent over the two ethernet ports and discarding the received duplicate packet. This is the non-offload HSR/PRP mechanism.
Getting Started
To try out HSR/PRP (assuming two supported platforms are set up already, and the ethernet ports are eth1/eth2):
1) Connect the Ethernet ports between devices, eth1 to eth1 and eth2 to eth2. (This acts as a 2 node ring for HSR, or a 2 node point-to-point for PRP)
2) The below script automates the steps to create a HSR/PRP interface using ethernet interfaces and IP address for HSR/PRP provided as arguments
#!/bin/sh
if [ "$#" != "4" ]
then
echo "$0 <hsr|prp> <intf1> <intf2> <ip addr>"
exit
fi
if [ "$1" != "hsr" ] && [ "$1" != "prp" ]
then
echo "$0 <hsr|prp>"
exit
fi
if [ "$1" == "hsr" ]
then
if=hsr0
else
if=prp0
fi
ifa=$2
ifb=$3
ip=$4
mac=`ifconfig $ifa | grep ether | cut -d " " -f 10`
echo "ip=$ip"
echo "if=$if"
echo "mac=$mac"
echo "slave-a=$ifa"
echo "slave-b=$ifb"
if [ "$1" == "hsr" ]
then
ip link delete prp0 2> /dev/null
else
ip link delete hsr0 2> /dev/null
fi
ip link set $ifa down
ip link set $ifb down
sleep 1
ip link set dev $ifa address $mac
ip link set dev $ifb address $mac
ip link set $ifa up
sleep 1
ip link set $ifb up
sleep 1
if [ "$1" == "hsr" ]
then
ip link add name $if type hsr slave1 $ifa slave2 $ifb supervision 45 version 1
else
ip link add name $if type hsr slave1 $ifa slave2 $ifb supervision 45 proto 1
fi
sleep 3
ip addr add $ip/24 dev $if
ip link set $if up
To create HSR interface with IP address 192.168.2.20 using eth1 and eth2, run the script by passing the arguments as below
sh ./<script_filename.sh> hsr eth1 eth2 192.168.2.20
To create a PRP interface with IP address 192.168.2.20 using eth1 and eth2, run the script by passing the arguments as below
sh ./<script_filename.sh> prp eth1 eth2 192.168.2.20
Please make sure that the IP address on both the platforms are unique
With the above configuration, if a ping is run between the two platforms on the HSR/PRP interface, the ping will continue even if one of the connections is removed.
Linux HSR Offload Support
HSR framework in linux allows offloading certain functionalities to the device and port-to-port forwarding in one such offloadable functionality. The ICSSG HSR firmware supports port-to-port forwarding and this allows to offload the forwarding capability from HSR driver in software to the PRU-ICSSG.
The below script automates setting up HSR interface with the port-to-port forwarding offloaded.
#!/bin/sh
#For non offload - sh hsr_setup.sh hsr_sw <INTF_A> <INTF_B> <HSR_INTF_IP_ADDR>
#For offload - sh hsr_setup.sh hsr_hw <INTF_A> <INTF_B> <HSR_INTF_IP_ADDR>
if [ "$#" != "4" ]
then
echo "$0 <hsr_sw/hsr_hw> <intf1> <intf2> <ip addr>"
exit
fi
if [ "$1" != "hsr_sw" ] && [ "$1" != "hsr_hw" ]
then
echo "$0 <hsr_sw|hsr_hw>"
exit
fi
if=hsr0
ifa=$2
ifb=$3
ip=$4
mac=`ifconfig $ifa | grep ether | cut -d " " -f 10`
device="platform/"
device+=`dmesg | grep $ifa | grep icssg-prueth | grep -m 1 "Link is Up" | awk '{print $4}'`
echo "ip=$ip"
echo "if=$if"
echo "mac=$mac"
echo "slave-a=$ifa"
echo "slave-b=$ifb"
echo "device=$device"
ip link delete hsr0 2> /dev/null
ip link set $ifa down
ip link set $ifb down
sleep 1
if [ "$1" == "hsr_hw" ]
then
ethtool -k $ifa | grep hsr
ethtool -K $ifa hsr-fwd-offload on
ethtool -k $ifa | grep hsr
ethtool -k $ifb | grep hsr
ethtool -K $ifb hsr-fwd-offload on
ethtool -k $ifb | grep hsr
devlink dev param set $device name hsr_offload_mode value true cmode runtime
fi
ip link set dev $ifa address $mac
ip link set dev $ifb address $mac
ip link set $ifa up
sleep 1
ip link set $ifb up
sleep 1
ip link add name $if type hsr slave1 $ifa slave2 $ifb supervision 45 version 1
sleep 3
ip addr add $ip/24 dev $if
ip link set $if up
To create HSR interface with IP address 192.168.2.20 using eth1 and eth2 and port-to-port forwarding offloaded, run the script by passing the arguments as below
sh ./<script_filename.sh> hsr_hw eth1 eth2 192.168.2.20
VLAN
ifconfig hsr0 0.0.0.0
ip link add link hsr0 name hsr0.2 type vlan id 2
ip link add link hsr0 name hsr0.3 type vlan id 3
ip addr add 192.168.2.3 dev hsr0.2
ip addr add 192.168.3.3 dev hsr0.3
With the above configuration, tracing using tcpdump -i <hsr0> -xxx on the remote side will show VLAN header with id information.
VLAN Filtering
ip link add link hsr0 name hsr0.4 type vlan id 4
Suppose on the remote side a new VLAN ID ‘4’ is created and attempt to ping a system with only VLAN ID ‘2’ and ‘3’, the packet will be filtered and dropped.
Multicast Filtering
All multi-cast addresses not registered will be filtered out.
Multicast Add/Delete
Multicast MAC address can be added/deleted using ip maddr commands or Linux socket ioctl SIOCADDMULTI/SIOCDELMULTI.
Show muliticast address
# ip maddr show dev <dev>
2: eth0
link 01:00:5e:00:00:01
link 01:80:c2:00:00:00
link 01:80:c2:00:00:03
link 01:80:c2:00:00:0e
link 01:00:5e:00:00:fc
inet 224.0.0.252
inet 224.0.0.1
Add muliticast address
# ip maddr add 01:00:5e:00:00:05 dev eth0
# ip maddr show dev eth0
2: eth0
link 01:00:5e:00:00:01
link 01:80:c2:00:00:00
link 01:80:c2:00:00:03
link 01:80:c2:00:00:0e
link 01:00:5e:00:00:fc
link 01:00:5e:00:00:05 static
inet 224.0.0.252
inet 224.0.0.1
Delete muliticast address
# ip maddr del 01:00:5e:00:00:05 dev eth0
PTP Ordinary Clock
PTP Master Clock
The PTP Ordinary Clock (OC) implementation is provided by the linuxptp application. The following command should be executed for master mode clock.
ptp4l -f gm_hsr0.cfg -m
The gm_hsr0.cfg is given below
root@am65xx-evm:~# cat gm_hsr0.cfg
[global]
sanity_freq_limit 0
step_threshold 0.00002
tx_timestamp_timeout 20
domainNumber 0
priority1 127
priority2 128
slaveOnly 0
twoStepFlag 1
summary_interval 0
doubly_attached_clock 1
[hsr0]
redundancy 1
delay_mechanism P2P
network_transport L2
[eth1]
redundancy 1
redundancy_master_interface hsr0
redundancy_slave_number 1
logAnnounceInterval 0
logSyncInterval 0
logMinPdelayReqInterval 0
announceReceiptTimeout 3
syncReceiptTimeout 2
delay_mechanism P2P
network_transport L2
egressLatency 726
ingressLatency 186
fault_reset_interval 0
[eth2]
redundancy 1
redundancy_master_interface hsr0
redundancy_slave_number 2
logAnnounceInterval 0
logSyncInterval 0
logMinPdelayReqInterval 0
announceReceiptTimeout 3
syncReceiptTimeout 2
delay_mechanism P2P
network_transport L2
egressLatency 726
ingressLatency 186
fault_reset_interval 0
PTP Slave Clock
The following command should be executed for slave mode clock.
ptp4l -f oc_hsr0.cfg -m -s
The oc_hsr0.cfg is given below
[global]
sanity_freq_limit 0
step_threshold 0.00002
tx_timestamp_timeout 20
domainNumber 0
priority1 128
priority2 128
slaveOnly 0
twoStepFlag 1
summary_interval 0
doubly_attached_clock 1
[hsr0]
redundancy 1
delay_mechanism P2P
network_transport L2
[eth1]
redundancy 1
redundancy_master_interface hsr0
redundancy_slave_number 1
logAnnounceInterval 0
logSyncInterval 1
logMinPdelayReqInterval 0
announceReceiptTimeout 3
syncReceiptTimeout 2
delay_mechanism P2P
network_transport L2
egressLatency 726
ingressLatency 186
fault_reset_interval 0
[eth2]
redundancy 1
redundancy_master_interface hsr0
redundancy_slave_number 2
logAnnounceInterval 0
logSyncInterval 1
logMinPdelayReqInterval 0
announceReceiptTimeout 3
syncReceiptTimeout 2
delay_mechanism P2P
network_transport L2
egressLatency 726
ingressLatency 186
fault_reset_interval 0
PPS
PPS can be tested using testptp.c tool.
To find out the PTP device number i.e. PTP Hardware Clock, use
ethtool -T DEVNAME
To turn on PPS,
# ip link set dev eth1 up
# ./testptp -d /dev/ptp2 -P 1
pps for system time request okay
To turn off PPS,
# ./testptp -d /dev/ptp2 -P 0
pps for system time request okay
PTP Over VLAN
For PTP Over VLAN, the PTP oc_hsr0.cfg and gm_hsr0.cfg should use VLAN interface instead of hsr0.