3.9. ARM Trusted Firmware-AΒΆ
Overview
Trusted Firmware-A (TF-A) provides a reference implementation of secure world software for Armv7-A and Armv8-A, including a Secure Monitor executing at Exception Level 3 (EL3).
ATF is used as the initial start code on ARMv8-A cores for all K3 platforms. After setting up the initial core state and applying any needed errata fixes it sets up itself as the EL3 monitor handler. After this is installs the secure world software (OP-TEE) and passes execution on to either the Linux kernel or U-Boot in the non-secure world.
Getting the ATF Source Code
$ git clone https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git
$ git checkout 1309c6c805190bd376c0561597653f3f8ecd0f58
Building ATF
$ export TFA_DIR=<path-to-arm-trusted-firmware>
$ cd $TFA_DIR
$ make ARCH=aarch64 CROSS_COMPILE=aarch64-none-linux-gnu- PLAT=k3 TARGET_BOARD=lite SPD=opteed
Default load locations
ATF image | 0x701c0000 |
OP-TEE image | 0x9e800000 |
U-Boot/Linux kernel image | 0x80080000 |
DTB | 0x82000000 |
To change the default load address of these binaries, an adress has to be changed in several source trees. The following is an example for AM64x family devices. Other family devices might not at the moment have binman dtsi files associated with them but they could in the future.
Source | ATF | OPTEE | A53 SPL | A53 U-Boot | DTB | kernel | Comments |
---|---|---|---|---|---|---|---|
<atf>/plat/ti/k3/board/lite/board.mk | BL32_BASE | PRELOADED_BL33_BASE | K3_HW_CONFIG_BASE | Change K3_HW_CONFIG_BASE for u-boot a53 skip case | |||
<optee>/core/arch/arm/plat-k3/conf.mk | CFG_TZDRAM_START | ||||||
<uboot>/configs/am64x_evm_r5_defconfig | K3_ATF_LOAD_ADDR | ||||||
<uboot>/configs/am64x_evm_a53_defconfig | SPL_TEXT_BASE | SYS_TEXT_BASE | SYS_TEXT_BASE can be set in defconfig, has default value in Kconfig | ||||
<uboot/linux>/arch/arm/dts/k3-am642*.dts files | reserved-memory nodes | ||||||
<uboot>/arch/arm/dts/k3-am642-evm-binman.dtsi file | tee nodes | uboot nodes | uboot nodes | ||||
<uboot>/include/configs/ti_armv7_common.h | fdtaddr | loadaddr | If not defined here, u-boot will pick any adress | ||||
uEnv.txt | fdtaddr | loadaddr | Overwrite the u-boot environment variables |