3.3.5. Low Power Modes

3.3.5.1. Overview

The following sections describe a high-level description of the different low power modes (LPM) of the device. If your application requires inactive power management, you must determine which low power mode described below satisfies your requirements. Each mode must be evaluated based on power consumption and latency (the time it takes to wakeup to Active mode) requirements. Specific values are detailed in the device-specific data sheet. As part of this SDK offering, Texas Instruments has added support for the following low power modes (ordered from lowest power consumption to highest power consumption):

  1. Partial I/O

  2. I/O Only Plus DDR

  3. DeepSleep

  4. MCU Only

More details about the low power mode architecture can be found in LPM constraints framework section.

3.3.5.2. Partial I/O

In Partial I/O, only the I/O pins and a small digital logic in the CANUART I/O Bank are active, while the rest of the SoC is turned off. The user can use the I/O pins to aggregate multiple I/O wakeup events and toggle PMIC_LPM_EN pin to enable PMIC or discrete power solution when an I/O wakeup event is triggered.

Note

The system looses nearly all its state as DDR is also turned-off. Partial I/O is comparable with a Linux poweroff state.

Important

Only AM62 LP-SK EVM supports Partial I/O mode.

Partial I/O is a poweroff state. Upon poweroff, the Linux ti_sci driver chooses Partial I/O entry if any CAN I/O wakeup sources are present.

Partial I/O supports wakeup sources mcu_mcan0 and mcu_mcan1. For more information about enabling CAN wakeup, see CAN I/O Daisy Chain.

Enter Partial I/O mode with the following command:

root@<machine>:~# poweroff

At this point, Linux kernel will go through its poweroff process and the console output will stop at the following lines:

[   74.310565] systemd-shutdown[1]: Powering off.
[   74.396204] reboot: Power down
[   74.399358] ti-sci 44043000.system-controller: Entering Partial-IO because a powered wakeup-enabled device was found.

The above output indicates that the system has entered Partial I/O. The system will resume to through a normal Linux boot process by triggering activity on the wakeup I/O pin programmed.

3.3.5.3. I/O Only Plus DDR

This mode is not applicable for AM62X.

3.3.5.4. DeepSleep

DeepSleep, also known as Suspend-to-RAM, is a low-power mode that allows an embedded device to retain its state in RAM while the processor is turned off. This can save a significant amount of power, especially in devices that are battery-powered.

The benefits of using deep sleep in embedded devices:

  1. Faster wake-up: devices can wake up from this low-power state much faster than a complete power cycle.

  2. Better efficiency: deep sleep can help to improve the efficiency of embedded devices by reducing the amount of time that the processor is idle. This is because the processor can be kept in a low-power state when it is not needed.

In order to enter DeepSleep, use the following command:

root@am62xx-evm:~# echo mem > /sys/power/state
[  444.719520] PM: suspend entry (deep)
[  444.723374] Filesystems sync: 0.000 seconds
[  444.751309] Freezing user space processes
[  444.756923] Freezing user space processes completed (elapsed 0.001 seconds)
[  444.763924] OOM killer disabled.
[  444.767141] Freezing remaining freezable tasks
[  444.772908] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[  444.780328] printk: Suspending console(s) (use no_console_suspend to debug)
[  444.796853] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 179: state: 1: ret 0
[  444.797037] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 178: state: 1: ret 0
[  444.805604] omap8250 2800000.serial: PM domain pd:146 will not be powered off
[  444.806188] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 117: state: 1: ret 0
[  444.816592] remoteproc remoteproc0: stopped remote processor 5000000.m4fss
[  444.820627] Disabling non-boot CPUs ...
[  444.822859] psci: CPU1 killed (polled 0 ms)
[  444.826567] psci: CPU2 killed (polled 0 ms)
[  444.830170] psci: CPU3 killed (polled 0 ms)

This partially indicates that Linux has finished it’s DeepSleep suspend sequence.

For further confirmation, program the PMCTRL_SYS register (0x43018080) to 0x15. The PMIC_LPM_EN pin on the EVM is 3.3V when active and 0V when in DeepSleep.

Note

The system will enter deep sleep mode only if DM selects it based on existing constraints.

Refer to the Wakeup Sources section for information on how to wakeup the device from DeepSleep mode using one of the supported wakeup sources.

3.3.5.5. MCU Only

Similar to DeepSleep, with the major distinction being that the MCU core is kept alive to run applications. The benefits of using MCU Only mode:

  1. Low power consumption: MCU Only mode can save a significant amount of power, especially in battery-powered devices. This is because the rest of the SoC status is the same as DeepSleep and DDR is in self-refresh.

  2. Run background tasks: This mode can be used to run background tasks that do not require the full power of the system. For example, you could use the firmware on the MCU core to run a watchdog timer, a sensor polling loop, or a network communication task.

  3. Respond to interrupts: This allows the system to still respond to external events, while it is in a low-power state.

To enter MCU Only mode, set 100 msec resume latency for CPU0 in Linux:

root@<machine>:~# echo 100000 > /sys/devices/system/cpu/cpu0/power/pm_qos_resume_latency_us

Now, the SoC can be suspended using the following command:

root@<machine>:~# rtcwake -s 5 -m mem
rtcwake: wakeup from "mem" using /dev/rtc0 at Thu Jan  1 00:01:02 1970
[   45.548480] PM: suspend entry (deep)
[   45.552187] Filesystems sync: 0.000 seconds
[   45.566606] Freezing user space processes
[   45.572093] Freezing user space processes completed (elapsed 0.001 seconds)
[   45.579083] OOM killer disabled.
[   45.582309] Freezing remaining freezable tasks
[   45.587984] Freezing remaining freezable tasks completed (elapsed 0.001 seconds)
[   45.595432] printk: Suspending console(s) (use no_console_suspend to debug)
[   45.627136] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 179: state: 1: ret 0
[   45.640758] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 178: state: 1: ret 0
[   45.648341] omap8250 2800000.serial: PM domain pd:146 will not be powered off
[   45.648892] ti-sci 44043000.system-controller: ti_sci_cmd_set_device_constraint: device: 117: state: 1: ret 0
[   45.648993] cpu cpu3: ti_sci_suspend: sending max CPU latency=100
[   45.649033] ti-sci 44043000.system-controller: ti_sci_cmd_set_latency_constraint: latency: 100: state: 1: ret 0
[   45.669270] Disabling non-boot CPUs ...
[   45.671353] psci: CPU1 killed (polled 0 ms)
[   45.674819] psci: CPU2 killed (polled 0 ms)
[   45.676640] psci: CPU3 killed (polled 4 ms)
[   45.677311] Enabling non-boot CPUs ...
[   45.677632] Detected VIPT I-cache on CPU1
[   45.677672] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[   45.677724] CPU1: Booted secondary processor 0x0000000001[0x410fd034]
[   45.678694] CPU1 is up
[   45.678934] Detected VIPT I-cache on CPU2
[   45.678962] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
[   45.679002] CPU2: Booted secondary processor 0x0000000002[0x410fd034]
[   45.679778] CPU2 is up
[   45.680016] Detected VIPT I-cache on CPU3
[   45.680045] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
[   45.680088] CPU3: Booted secondary processor 0x0000000003[0x410fd034]
[   45.680939] CPU3 is up
[   45.681332] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50
[   45.703650] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[   45.719704] am65-cpsw-nuss 8000000.ethernet eth0: PHY[8000f00.mdio:00] driver[TI DP83867] (irq=POLL)
[   45.719730] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[   46.004264] OOM killer enabled.
[   46.007406] Restarting tasks ... done.
[   46.012454] random: crng reseeded on system resumption
[   46.026923] platform 79000000.r5f: Core is on in resume
[   46.032206] platform 79000000.r5f: received echo reply from 79000000.r5f
[   46.032262] PM: suspend exit

Once the SoC enters MCU Only mode, the following log should be printed on the MCU UART (in most cases it will be /dev/ttyUSB3)

[IPC RPMSG ECHO] Next MCU mode is 1
[IPC RPMSG ECHO] Suspend request to MCU-only mode received
[IPC RPMSG ECHO] Press a single key on this terminal to resume the kernel from MCU only mode

Note

The system will enter MCU Only mode only if DM selects it based on existing constraints.

Refer to the Wakeup Sources section for information on how to wakeup the device from MCU Only mode using one of the supported wakeup sources.

3.3.5.6. Limitations

Important

SK-AM62-SIP EVM does NOT support low power modes.

Important

When using low power modes on SK-AM62-LP EVM, USB1 cannot be connected to anything. When USB1 is connected and a low power mode is entered, the EVM fails to resume to an active Linux state.

Hardware Workaround: Remove resistor R131 from the SK-AM62-LP EVM to resolve this limitation and enable proper resume from low power modes.

RT (Real-Time) Linux does not support any low power modes.

HWRNG support on GP devices is incompatible with DeepSleep and MCU Only modes. To test LPM on GP devices, HWRNG has to be unloaded one-time before running the Suspend-to-RAM command:

root@<machine>:@~# modprobe -r optee_rng

3.3.5.6.1. Compatibility

The compatibility between Kernel version and firmware version to enter low power mode is listed in the below table:

LPM

Firmware v10.0

Firmware < v10.0

TI Kernel 6.6

All low power modes supported

Only DeepSleep supported

TI Kernel < 6.6

All low power modes supported

All low power modes supported

Important

In case of Kernel 6.6 and Firmware < v10.0, the firmware is unaware of the constraints framework. Hence, the system will always enter deep sleep low power mode irrespective of the constraints set.

Note

All low power mode supported implies all low power mode supported by the firmware as per firmware capabilities. TISCI_MSG_QUERY_FW_CAPS can be sent to firmware to get the low power modes supported by firmware.