3.2.2.10. GPIO
GPIO Driver Overview
The GPIO Driver enables the GPIO controllers available on the device. The driver configures the GPIO hardware and interfaces and makes them available to user space as character device or other device drivers that need to access pins. For example, a MMC/SD driver may need to read a GPIO as in input to determine if a card is present. The H/W GPIO controllers available will vary by SoC and system configuration.
Overview
The GPIO controllers allow interaction with GPIO pins for input/output and interrupt generation.
User Layer
The GPIO driver can be used in user space via Linux CLI. This section provides examples, command-line-tools, and guidance for using GPIOs in user space.
Note
Since Linux 4.8, the GPIO sysfs interface is deprecated. User space should use the character device instead.
Example: Using GPIOs with the libgpiod library in user space to toggle a GPIO pin, which is connected to an LED on the SK-AM62B-P1 board:
Locate Table 2-23 under 2.6.16.3 User Test LEDs in the AM62x Starter Kit User’s Guide (Rev. C): https://www.ti.com/lit/pdf/spruj40.
This example uses LED “LD11”, AKA the IO_EXP_TEST_LED. It is connected to GPIO U70.24(P27), AKA pin 27 of the GPIO Port Expander on the SK-AM62B-P1 board:
Detect every available gpiochip:
$ gpiodetect gpiochip0 [600000.gpio] (92 lines) gpiochip1 [601000.gpio] (52 lines) gpiochip2 [1-0022] (24 lines)
This shows 92+52+24=168 total GPIO lines available across 3 GPIO chips: 0, 1, and 2.
Read info for every available gpiochip:
$ gpioinfo gpiochip0 - 92 lines: line 0: unnamed input line 1: unnamed input {...} line 91: unnamed input gpiochip1 - 52 lines: line 0: unnamed input line 1: unnamed input {...} line 51: unnamed input gpiochip2 - 24 lines: line 0: "GPIO_CPSW2_RST" input line 1: "GPIO_CPSW1_RST" input {...} line 23: "IO_EXP_TEST_LED" input
This should result in a large output, 168+ lines in this case. It outputs all GPIO lines available on every GPIO chip, as well as their names and input/output directions. The above output is truncated.
For more info on gpioinfo, see its man page: https://libgpiod.readthedocs.io/en/latest/gpioinfo.html.
To see info for a specific GPIO chip, use the ‘-c’ flag and the GPIO chip number.
Read info for gpiochip2 (for this example):
$ gpioinfo -c 2 gpiochip2 - 24 lines: line 0: "GPIO_CPSW2_RST" input line 1: "GPIO_CPSW1_RST" input line 2: "PRU_DETECT" input line 3: "MMC1_SD_EN" output consumer="regulator-3" line 4: "VPP_LDO_EN" input line 5: "EXP_PS_3V3_En" input line 6: "EXP_PS_5V0_En" input line 7: "EXP_HAT_DETECT" input line 8: "GPIO_AUD_RSTn" input line 9: "GPIO_eMMC_RSTn" input line 10: "UART1_FET_BUF_EN" input line 11: "WL_LT_EN" input line 12: "GPIO_HDMI_RSTn" input line 13: "CSI_GPIO1" input line 14: "CSI_GPIO2" input line 15: "PRU_3V3_EN" input line 16: "HDMI_INTn" input consumer="interrupt" line 17: "PD_I2C_IRQ" input line 18: "MCASP1_FET_EN" input line 19: "MCASP1_BUF_BT_EN" input line 20: "MCASP1_FET_SEL" input line 21: "UART1_FET_SEL" input line 22: "TSINT#" input line 23: "IO_EXP_TEST_LED" output
We see that IO_EXP_TEST_LED is connected to GPIO2_23 on the SK-AM62B-P1 board.
Read the value of the GPIO pin:
$ gpioget --numeric -c 2 23 0
Use variations of gpioget to read the value of the GPIO pin:
$ gpioget -c 2 23 "23"=inactive $ gpioget IO_EXP_TEST_LED "IO_EXP_TEST_LED"=inactive $ gpioget --numeric IO_EXP_TEST_LED 0
For more info on gpioget, see its man page: https://libgpiod.readthedocs.io/en/latest/gpioget.html.
Set the GPIO pin to turn on the LED
$ gpioset -c 2 23=1 ^C $ gpioset -c 2 23=0 ^C
Note:
In Bash, ‘^C’ (Ctrl + C) exits the command with SIGINT, else the gpioset command would not exit on its own. For more info, refer to the 3.7.6 Signals section in the GNU Bash manual: https://www.gnu.org/software/bash/manual/bash.html.
The new GPIO value will remain until an exit signal, like SIGKILL, SIGTERM, or SIGINT; after that, its value is not guaranteed. For more info, reference the Description section of the gpioset man page: https://libgpiod.readthedocs.io/en/latest/gpioset.html.
This should have turned the active-high LED “LD11” on the SK-AM62B-P1 on and off.
Use variations of gpioset to set the value of the GPIO pin:
$ gpioset IO_EXP_TEST_LED=1 ^C $ gpioset IO_EXP_TEST_LED=0 ^C
This should have also turned the active-high LED “LD11” on the SK-AM62B-P1 on and off.
Example: Toggle GPIO2_23 (blink “LD11”) at 10Hz, then turn it off:
$ gpioset --toggle 50ms IO_EXP_TEST_LED=1 ^C $ gpioset IO_EXP_TEST_LED=0 ^C
For more info on gpioset, see its man page: https://libgpiod.readthedocs.io/en/latest/gpioset.html.
For more command-line tools, refer to the libgpiod documentation: https://libgpiod.readthedocs.io/en/latest/gpio_tools.html.
Example: Using GPIOs on the Raspberry Pi Compatible 40-pin Header on the SK-AM62B-P1 board:
Locate Table 2-25 under 2.6.17.2 User Expansion Connector in the AM62x Starter Kit User’s Guide (Rev. C): https://www.ti.com/lit/pdf/spruj40.
Identify the desired GPIO pin number and pin multiplexed signal. For example, GPIO1_25 corresponds to physical pin 8 on the 40-pin header.
Use libgpiod mentioned in the previous example to control the GPIO pin, ensuring that the GPIO pin is not being used already.
Additional Resources
For more information about GPIO usage in Linux and U-Boot, refer to these resources:
SDK:
Kernel: ti-processor-sdk-linux-am62xx-evm-<sdk version>/board-support/ti-linux-kernel-<kernel version>+git-ti/Documentation/devicetree/bindings/gpio/gpio.txt
U-Boot: ti-processor-sdk-linux-am62xx-evm-<sdk version>/board-support/ti-u-boot-<u-boot version>+git/doc/device-tree-bindings/gpio/gpio.txt
Online:
GPIO on Sitara: https://www.ti.com/lit/ab/spradk0/spradk0.pdf
(Note: AM62P-specific, but similar to AM62x): https://software-dl.ti.com/processor-sdk-linux/esd/AM62PX/latest/exports/docs/linux/Foundational_Components/Tools/GPIO_Tools.html
Consuming Drivers
The GPIO Driver can also be easily leveraged by other drivers to “consume” a GPIO.
For an example of a driver using a GPIO pin, examine this entry in a dts file for how the MMC/SD interface could use a GPIO as a card detect pin:
ti-processor-sdk-linux-am62xx-evm-<sdk version>/board-support/ti-linux-kernel-<kernel version>+git-ti/arch/arm/boot/dts/ti/omap/am335x-bone-common.dtsi.
Features
Access GPIO from user space as input or output
Leverage GPIO from another “consumer” driver