3.9.2. Rogue debug info

Rogue graphics drivers include the following tools bundled with their user mode libraries:

Table 3.18 Included rogue debug tools

pvrdebug

Control debug verbosity and other device info

pvrlogdump

Dump diagnostic information for an application

pvrsrvctl

Start, Stop, Restart and configure the GPU using a powervr.ini file

rgx_blit_test

Try several blit operations and display them to the screen

rgx_compute_test

Try several different compute tasks on the core

rgx_triangle_test

Render a triangle to the attached display

rgx_twiddling_test

Twiddle several textures in several different pixel formats

Future releases of ti-img-rogue-umlibs can include more tools. This is the core set expected to be available in most ti-img-rogue-umlibs releases and are the most useful for verifying GPU functionality.

The order of operation to verify fundamental GPU functionality is as follows:

  1. Use rgx_compute_test to verify that the GPU is able to handle a proper compute load.

  2. Use rgx_triangle_test to verify that the GPU is able to render to an output buffer.

If you are still experiencing issues after verifying fundamental functionality, try checking the output of the following:

# pvrdebug -dd

Note

When raising a ticket on e2e forums it is useful to include the output of this command if available.

This will dump all device information as reported by the kernel module. Please ensure that the debug info reports:

Comparison of UM/KM components: MATCHING

User mode and kernel mode components must move in lockstep. If they do not match this could lead to the kernel module failing to initialize or undefined behavior.