2.5.1. RT-linux 12.00.00 Performance Guide
2.5.1.1. Read This First
All performance numbers provided in this document are gathered using following Evaluation Modules unless otherwise specified.
Name |
Description |
|---|---|
AM64x EVM |
AM64x Evaluation Module rev E1 with ARM running at 1GHz, DDR data rate 1600 MT/S |
Table: Evaluation Modules
2.5.1.2. About This Manual
This document provides performance data for each of the device drivers which are part of the Processor SDK Linux package. This document should be used in conjunction with release notes and user guides provided with the Processor SDK Linux package for information on specific issues present with drivers included in a particular release.
For further information or to report any problems, contact https://e2e.ti.com/ or https://support.ti.com/
2.5.1.3. System Benchmarks
2.5.1.3.1. Stress-ng and Cyclic Test
stress-ng (next-generation) will stress test a embedded platform in various selectable ways. It was designed to exercise various physical subsystems as well as the various operating system kernel interfaces. stress-ng can also measure test throughput rates; this can be useful to observe performance changes across different operating system or types of hardware.
Cyclictest is most commonly used for benchmarking RT systems. It is one of the most frequently used tools for evaluating the relative performance of real-time systems. Some performance tests which use Cyclictest are System benchmarking, Latency debugging with tracing and -approximating application performance.
Test commands used for running stress-ng and cyclictest together
stress-ng --cpu-method=all -c 4 &
cyclictest -m -Sp80 -D6h -h400 -i200 -M -q
The following summarizes the latencies observed using the yocto based default SDK image:
Note
A known issue in this SDK release is affecting this benchmark. Using OP-TEE’s PRNG drivers rather than the hardware accelerated TRNG drivers restores the context switch latencies to the values you see here.
More information on switching to the PRNG drivers can be found in the Foundational Components section, here Building OP-TEE with Pseudo RNG drivers
Latencies |
CPU 0 |
CPU 1 |
|---|---|---|
Minimum (usec) |
5 |
5 |
Average (usec) |
7 |
8 |
Maximum (usec) |
69 |
77 |
2.5.1.3.2. LMBench
LMBench is a collection of microbenchmarks of which the memory bandwidth and latency related ones are typically used to estimate processor memory system performance. More information about lmbench at https://lmbench.sourceforge.net/whatis_lmbench.html and https://lmbench.sourceforge.net/man/lmbench.8.html
Latency: lat_mem_rd-stride128-szN, where N is equal to or smaller than the cache size at given level measures the cache miss penalty. N that is at least double the size of last level cache is the latency to external memory.
Bandwidth: bw_mem_bcopy-N, where N is equal to or smaller than the cache size at a given level measures the achievable memory bandwidth from software doing a memcpy() type operation. Typical use is for external memory bandwidth calculation. The bandwidth is calculated as byte read and written counts as 1 which should be roughly half of STREAM copy result.
Execute the LMBench with the following:
cd /opt/ltp
./runltp -P j721e-idk-gw -f ddt/lmbench -s LMBENCH_L_PERF_0001
Benchmarks |
am64xx-hsevm: perf |
|---|---|
af_unix_sock_stream_latency (microsec) |
29.27 (min 24.87, max 39.15) |
af_unix_socket_stream_bandwidth (mbs) |
558.67 (min 544.62, max 577.21) |
bw_file_rd-io-1mb (mb/s) |
842.86 (min 820.61, max 860.44) |
bw_file_rd-o2c-1mb (mb/s) |
494.65 (min 478.77, max 505.56) |
bw_mem-bcopy-16mb (mb/s) |
949.99 (min 921.34, max 973.47) |
bw_mem-bcopy-1mb (mb/s) |
943.11 (min 906.76, max 975.93) |
bw_mem-bcopy-2mb (mb/s) |
933.38 (min 918.70, max 958.47) |
bw_mem-bcopy-4mb (mb/s) |
960.36 (min 924.21, max 978.47) |
bw_mem-bcopy-8mb (mb/s) |
954.73 (min 901.51, max 986.19) |
bw_mem-bzero-16mb (mb/s) |
2117.57 (min 2115.56, max 2118.36) |
bw_mem-bzero-1mb (mb/s) |
1530.94 (min 906.76, max 2120.52) |
bw_mem-bzero-2mb (mb/s) |
1525.61 (min 918.70, max 2118.64) |
bw_mem-bzero-4mb (mb/s) |
1538.69 (min 924.21, max 2117.90) |
bw_mem-bzero-8mb (mb/s) |
1536.19 (min 901.51, max 2118.92) |
bw_mem-cp-16mb (mb/s) |
561.34 (min 542.93, max 581.71) |
bw_mem-cp-1mb (mb/s) |
1606.01 (min 557.72, max 2718.38) |
bw_mem-cp-2mb (mb/s) |
1439.68 (min 534.62, max 2352.94) |
bw_mem-cp-4mb (mb/s) |
1383.16 (min 524.25, max 2227.17) |
bw_mem-cp-8mb (mb/s) |
1359.16 (min 537.42, max 2167.43) |
bw_mem-fcp-16mb (mb/s) |
1043.67 (min 1008.64, max 1082.84) |
bw_mem-fcp-1mb (mb/s) |
1605.66 (min 1081.08, max 2120.52) |
bw_mem-fcp-2mb (mb/s) |
1568.44 (min 966.81, max 2118.64) |
bw_mem-fcp-4mb (mb/s) |
1582.47 (min 951.70, max 2117.90) |
bw_mem-fcp-8mb (mb/s) |
1571.60 (min 959.23, max 2118.92) |
bw_mem-frd-16mb (mb/s) |
1311.63 (min 1279.49, max 1329.57) |
bw_mem-frd-1mb (mb/s) |
1200.07 (min 1081.08, max 1331.78) |
bw_mem-frd-2mb (mb/s) |
1168.93 (min 966.81, max 1370.33) |
bw_mem-frd-4mb (mb/s) |
1181.54 (min 951.70, max 1369.63) |
bw_mem-frd-8mb (mb/s) |
1170.23 (min 959.23, max 1367.05) |
bw_mem-fwr-16mb (mb/s) |
2128.04 (min 2125.96, max 2129.93) |
bw_mem-fwr-1mb (mb/s) |
1965.95 (min 1273.19, max 2718.38) |
bw_mem-fwr-2mb (mb/s) |
1819.17 (min 1265.22, max 2352.94) |
bw_mem-fwr-4mb (mb/s) |
1760.80 (min 1275.31, max 2227.17) |
bw_mem-fwr-8mb (mb/s) |
1737.99 (min 1241.85, max 2167.43) |
bw_mem-rd-16mb (mb/s) |
1332.85 (min 1270.14, max 1382.89) |
bw_mem-rd-1mb (mb/s) |
1102.66 (min 850.77, max 1419.88) |
bw_mem-rd-2mb (mb/s) |
1086.05 (min 821.81, max 1365.89) |
bw_mem-rd-4mb (mb/s) |
1104.47 (min 856.62, max 1380.74) |
bw_mem-rd-8mb (mb/s) |
1116.97 (min 863.84, max 1397.38) |
bw_mem-rdwr-16mb (mb/s) |
878.96 (min 870.37, max 884.08) |
bw_mem-rdwr-1mb (mb/s) |
698.17 (min 557.72, max 847.46) |
bw_mem-rdwr-2mb (mb/s) |
684.70 (min 534.62, max 828.16) |
bw_mem-rdwr-4mb (mb/s) |
697.23 (min 524.25, max 855.25) |
bw_mem-rdwr-8mb (mb/s) |
713.67 (min 537.42, max 878.54) |
bw_mem-wr-16mb (mb/s) |
898.11 (min 890.57, max 901.46) |
bw_mem-wr-1mb (mb/s) |
835.61 (min 768.34, max 890.31) |
bw_mem-wr-2mb (mb/s) |
823.57 (min 790.62, max 852.64) |
bw_mem-wr-4mb (mb/s) |
850.08 (min 805.07, max 878.64) |
bw_mem-wr-8mb (mb/s) |
875.81 (min 858.74, max 897.87) |
bw_mmap_rd-mo-1mb (mb/s) |
1288.67 (min 1251.79, max 1327.27) |
bw_mmap_rd-o2c-1mb (mb/s) |
503.15 (min 477.40, max 532.86) |
bw_pipe (mb/s) |
559.24 (min 519.56, max 584.19) |
bw_unix (mb/s) |
558.67 (min 544.62, max 577.21) |
lat_connect (us) |
69.65 (min 68.59, max 71.76) |
lat_ctx-2-128k (us) |
17.41 (min 8.52, max 35.96) |
lat_ctx-2-256k (us) |
59.43 (min 18.26, max 137.82) |
lat_ctx-4-128k (us) |
33.39 (min 10.30, max 79.35) |
lat_ctx-4-256k (us) |
57.09 (min 5.26, max 145.73) |
lat_fs-0k (num_files) |
222.33 (min 204.00, max 253.00) |
lat_fs-10k (num_files) |
97.33 (min 88.00, max 117.00) |
lat_fs-1k (num_files) |
138.83 (min 128.00, max 152.00) |
lat_fs-4k (num_files) |
129.17 (min 126.00, max 135.00) |
lat_mem_rd-stride128-sz1000k (ns) |
46.99 (min 46.70, max 48.08) |
lat_mem_rd-stride128-sz125k (ns) |
7.81 (min 7.80, max 7.85) |
lat_mem_rd-stride128-sz250k (ns) |
13.11 (min 10.29, max 17.26) |
lat_mem_rd-stride128-sz31k (ns) |
4.69 (min 3.06, max 5.89) |
lat_mem_rd-stride128-sz50 (ns) |
3.02 |
lat_mem_rd-stride128-sz500k (ns) |
42.92 (min 42.10, max 44.04) |
lat_mem_rd-stride128-sz62k (ns) |
7.37 (min 7.35, max 7.39) |
lat_mmap-1m (us) |
61.50 (min 58.00, max 71.00) |
lat_ops-double-add (ns) |
4.02 |
lat_ops-double-div (ns) |
22.13 (min 22.12, max 22.14) |
lat_ops-double-mul (ns) |
4.02 |
lat_ops-float-add (ns) |
4.02 |
lat_ops-float-div (ns) |
13.08 (min 13.06, max 13.11) |
lat_ops-float-mul (ns) |
4.02 |
lat_ops-int-add (ns) |
1.01 |
lat_ops-int-bit (ns) |
0.67 |
lat_ops-int-div (ns) |
6.04 (min 6.03, max 6.05) |
lat_ops-int-mod (ns) |
6.38 (min 6.37, max 6.40) |
lat_ops-int-mul (ns) |
4.34 (min 4.27, max 4.38) |
lat_ops-int64-add (ns) |
1.01 |
lat_ops-int64-bit (ns) |
0.67 |
lat_ops-int64-div (ns) |
9.55 |
lat_ops-int64-mod (ns) |
7.38 (min 7.37, max 7.38) |
lat_ops-int64-mul (ns) |
5.05 (min 4.98, max 5.11) |
lat_pagefault (us) |
1.66 (min 1.57, max 1.75) |
lat_pipe (us) |
21.07 (min 20.07, max 21.69) |
lat_proc-exec (us) |
1192.27 (min 1137.20, max 1275.60) |
lat_proc-fork (us) |
1074.68 (min 1031.00, max 1137.60) |
lat_proc-proccall (us) |
0.01 |
lat_select (us) |
42.85 (min 42.28, max 43.92) |
lat_sem (us) |
2.57 (min 1.71, max 3.19) |
lat_sig-catch (us) |
6.09 (min 5.83, max 6.30) |
lat_sig-install (us) |
0.94 (min 0.87, max 1.10) |
lat_sig-prot (us) |
0.81 (min 0.66, max 0.94) |
lat_syscall-fstat (us) |
2.31 (min 2.13, max 2.49) |
lat_syscall-null (us) |
0.52 (min 0.44, max 0.65) |
lat_syscall-open (us) |
345.64 (min 311.94, max 360.53) |
lat_syscall-read (us) |
0.80 (min 0.69, max 0.89) |
lat_syscall-stat (us) |
5.88 (min 5.61, max 6.20) |
lat_syscall-write (us) |
0.76 (min 0.66, max 0.87) |
lat_tcp (us) |
0.97 (min 0.75, max 1.22) |
lat_unix (us) |
29.27 (min 24.87, max 39.15) |
latency_for_0.50_mb_block_size (nanosec) |
42.92 (min 42.10, max 44.04) |
latency_for_1.00_mb_block_size (nanosec) |
23.50 (min 0.00, max 48.08) |
pipe_bandwidth (mbs) |
559.24 (min 519.56, max 584.19) |
pipe_latency (microsec) |
21.07 (min 20.07, max 21.69) |
procedure_call (microsec) |
0.01 |
select_on_200_tcp_fds (microsec) |
42.85 (min 42.28, max 43.92) |
semaphore_latency (microsec) |
2.57 (min 1.71, max 3.19) |
signal_handler_latency (microsec) |
0.94 (min 0.87, max 1.10) |
signal_handler_overhead (microsec) |
6.09 (min 5.83, max 6.30) |
tcp_ip_connection_cost_to_localhost (microsec) |
69.65 (min 68.59, max 71.76) |
tcp_latency_using_localhost (microsec) |
0.97 (min 0.75, max 1.22) |
2.5.1.3.3. Dhrystone
Dhrystone is a core only benchmark that runs from warm L1 caches in all modern processors. It scales linearly with clock speed. For standard ARM cores the DMIPS/MHz score will be identical with the same compiler and flags.
Benchmarks |
am64xx-hsevm: perf |
|---|---|
cpu_clock (mhz) |
1000.00 |
dhrystone_per_mhz (dmips/mhz) |
2.76 (min 2.70, max 2.80) |
dhrystone_per_second (dhrystonep) |
4855981.60 (min 4761905.00, max 5000000.00) |
2.5.1.3.4. Whetstone
Benchmarks |
am64xx-hsevm: perf |
|---|---|
whetstone (mips) |
3611.08 (min 3333.30, max 5000.00) |
2.5.1.3.5. Linpack
Linpack measures peak double precision (64 bit) floating point performance in solving a dense linear system.
Benchmarks |
am64xx-hsevm: perf |
|---|---|
linpack (kflops) |
411621.33 (min 411424.00, max 411819.00) |
2.5.1.3.6. CoreMarkPro
CoreMark®-Pro is a comprehensive, advanced processor benchmark that works with and enhances the market-proven industry-standard EEMBC CoreMark® benchmark. While CoreMark stresses the CPU pipeline, CoreMark-Pro tests the entire processor, adding comprehensive support for multicore technology, a combination of integer and floating-point workloads, and data sets for utilizing larger memory subsystems.
Benchmarks |
am64xx-hsevm: perf |
|---|---|
cjpeg-rose7-preset (workloads/) |
29.60 (min 29.41, max 29.85) |
core (workloads/) |
0.21 |
coremark-pro () |
592.17 (min 585.01, max 602.59) |
linear_alg-mid-100x100-sp (workloads/) |
10.41 (min 10.38, max 10.43) |
loops-all-mid-10k-sp (workloads/) |
0.48 (min 0.48, max 0.49) |
nnet_test (workloads/) |
0.76 (min 0.76, max 0.77) |
parser-125k (workloads/) |
5.61 (min 5.29, max 6.17) |
radix2-big-64k (workloads/) |
20.77 (min 20.27, max 21.14) |
sha-test (workloads/) |
57.80 |
zip-test (workloads/) |
15.75 (min 15.63, max 16.13) |
Benchmarks |
am64xx-hsevm: perf |
|---|---|
cjpeg-rose7-preset (workloads/) |
58.09 (min 57.47, max 58.82) |
core (workloads/) |
0.43 |
coremark-pro () |
1037.34 (min 981.69, max 1065.66) |
linear_alg-mid-100x100-sp (workloads/) |
20.81 (min 20.78, max 20.83) |
loops-all-mid-10k-sp (workloads/) |
0.88 |
nnet_test (workloads/) |
1.53 |
parser-125k (workloads/) |
5.99 (min 4.91, max 6.99) |
radix2-big-64k (workloads/) |
32.45 (min 31.58, max 33.23) |
sha-test (workloads/) |
114.94 |
zip-test (workloads/) |
26.01 (min 14.39, max 28.57) |
2.5.1.3.7. Boot-time Measurement
2.5.1.3.7.1. Boot media: MMCSD
Boot Configuration |
am64xx-hsevm: Boot time in seconds: avg(min,max) |
|---|---|
Linux boot time from SD with default rootfs (20 boot cycles) |
28.67 (min 22.45, max 36.73) |
Boot time numbers [avg, min, max] are measured from “Starting kernel” to Linux prompt across 20 boot cycles.
2.5.1.3.8. Ethernet
Ethernet performance benchmarks were measured using netperf 2.7.1 https://hewlettpackard.github.io/netperf/doc/netperf.html Test procedures were modeled after those defined in RFC-2544: https://tools.ietf.org/html/rfc2544, where the DUT is the TI device and the “tester” used was a Linux PC. To produce consistent results, it is recommended to carry out performance tests in a private network and to avoid running NFS on the same interface used in the test. In these results, CPU utilization was captured as the total percentage used across all cores on the device, while running the performance test over one external interface.
UDP Throughput (0% loss) was measured by the procedure defined in RFC-2544 section 26.1: Throughput. In this scenario, netperf options burst_size (-b) and wait_time (-w) are used to limit bandwidth during different trials of the test, with the goal of finding the highest rate at which no loss is seen. For example, to limit bandwidth to 500Mbits/sec with 1472B datagram:
burst_size = <bandwidth (bits/sec)> / 8 (bits -> bytes) / <UDP datagram size> / 100 (seconds -> 10 ms)
burst_size = 500000000 / 8 / 1472 / 100 = 425
wait_time = 10 milliseconds (minimum supported by Linux PC used for testing)
UDP Throughput (possible loss) was measured by capturing throughput and packet loss statistics when running the netperf test with no bandwidth limit (remove -b/-w options).
In order to start a netperf client on one device, the other device must have netserver running. To start netserver:
netserver [-p <port_number>] [-4 (IPv4 addressing)] [-6 (IPv6 addressing)]
Running the following shell script from the DUT will trigger netperf clients to measure bidirectional TCP performance for 60 seconds and report CPU utilization. Parameter -k is used in client commands to summarize selected statistics on their own line and -j is used to gain additional timing measurements during the test.
#!/bin/bash
for i in 1
do
netperf -H <tester ip> -j -c -l 60 -t TCP_STREAM --
-k DIRECTION,THROUGHPUT,MEAN_LATENCY,LOCAL_CPU_UTIL,REMOTE_CPU_UTIL,LOCAL_BYTES_SENT,REMOTE_BYTES_RECVD,LOCAL_SEND_SIZE &
netperf -H <tester ip> -j -c -l 60 -t TCP_MAERTS --
-k DIRECTION,THROUGHPUT,MEAN_LATENCY,LOCAL_CPU_UTIL,REMOTE_CPU_UTIL,LOCAL_BYTES_SENT,REMOTE_BYTES_RECVD,LOCAL_SEND_SIZE &
done
Running the following commands will trigger netperf clients to measure UDP burst performance for 60 seconds at various burst/datagram sizes and report CPU utilization.
For UDP egress tests, run netperf client from DUT and start netserver on tester.
netperf -H <tester ip> -j -c -l 60 -t UDP_STREAM -b <burst_size> -w <wait_time> -- -m <UDP datagram size>
-k DIRECTION,THROUGHPUT,MEAN_LATENCY,LOCAL_CPU_UTIL,REMOTE_CPU_UTIL,LOCAL_BYTES_SENT,REMOTE_BYTES_RECVD,LOCAL_SEND_SIZE
For UDP ingress tests, run netperf client from tester and start netserver on DUT.
netperf -H <DUT ip> -j -C -l 60 -t UDP_STREAM -b <burst_size> -w <wait_time> -- -m <UDP datagram size>
-k DIRECTION,THROUGHPUT,MEAN_LATENCY,LOCAL_CPU_UTIL,REMOTE_CPU_UTIL,LOCAL_BYTES_SENT,REMOTE_BYTES_RECVD,LOCAL_SEND_SIZE
2.5.1.3.8.1. CPSW/CPSW2g/CPSW3g Ethernet
CPSW3g: AM64x
2.5.1.3.8.1.1. TCP Bidirectional Throughput
Command Used |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: CPU Load % (LOCAL_CPU_UTIL) |
|---|---|---|
netperf -H 192.168.0.1 -j -c -C -l 60 -t TCP_STREAM; netperf -H 192.168.0.1 -j -c -C -l 60 -t TCP_MAERTS |
1051.83 |
98.0 |
2.5.1.3.8.1.2. TCP Bidirectional Throughput Interrupt Pacing
Command Used |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: CPU Load % (LOCAL_CPU_UTIL) |
|---|---|---|
netperf -H 192.168.0.1 -j -c -C -l 60 -t TCP_STREAM; netperf -H 192.168.0.1 -j -c -C -l 60 -t TCP_MAERTS |
1141.56 |
98.7 |
2.5.1.3.8.1.3. UDP Throughput
Frame Size(bytes) |
am64xx-hsevm: UDP Datagram Size(bytes) (LOCAL_SEND_SIZE) |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: Packets Per Second (kPPS) |
am64xx-hsevm: CPU Load % (LOCAL_CPU_UTIL) |
|---|---|---|---|---|
64 |
44.26 |
86 |
87.2 |
|
128 |
84.74 |
83 |
87.4 |
|
256 |
168.40 |
82 |
90.2 |
|
1024 |
612.56 |
75 |
89.4 |
|
1518 |
864.47 |
73 |
89.6 |
Frame Size(bytes) |
am64xx-hsevm: UDP Datagram Size(bytes) (LOCAL_SEND_SIZE) |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: Packets Per Second (kPPS) |
am64xx-hsevm: CPU Load % (LOCAL_CPU_UTIL) |
|---|---|---|---|---|
64 |
30.77 |
60 |
35.0 |
|
128 |
74.65 |
73 |
43.7 |
|
256 |
150.12 |
73 |
44.4 |
|
1024 |
566.07 |
69 |
48.6 |
|
1518 |
876.13 |
74 |
66.7 |
Frame Size(bytes) |
am64xx-hsevm: UDP Datagram Size(bytes) (LOCAL_SEND_SIZE) |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: Packets Per Second (kPPS) |
am64xx-hsevm: CPU Load % (LOCAL_CPU_UTIL) |
am64xx-hsevm: Packet Loss % |
|---|---|---|---|---|---|
128 |
92.68 (min 84.84, max 97.29) |
90.50 (min 83.00, max 95.00) |
66.28 (min 64.69, max 67.86) |
72.37 (min 68.17, max 79.35) |
|
256 |
190.43 (min 175.08, max 202.24) |
93.00 (min 85.00, max 99.00) |
67.43 (min 65.94, max 68.79) |
69.29 (min 67.47, max 71.90) |
|
1024 |
586.35 (min 540.95, max 621.28) |
71.67 (min 66.00, max 76.00) |
66.59 (min 65.50, max 68.59) |
30.88 (min 27.41, max 35.21) |
|
1518 |
634.14 (min 592.61, max 686.45) |
53.75 (min 50.00, max 58.00) |
65.50 (min 64.50, max 66.73) |
32.49 (min 28.27, max 35.88) |
2.5.1.3.8.2. ICSSG Ethernet
2.5.1.3.8.2.1. ICSSG TCP Bidirectional Throughput
Command Used |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: CPU Load % (LOCAL_CPU_UTIL) |
|---|---|---|
netperf -H 192.168.2.1 -j -c -C -l 60 -t TCP_STREAM; netperf -H 192.168.2.1 -j -c -C -l 60 -t TCP_MAERTS |
1073.37 |
95.6 |
2.5.1.3.8.2.2. ICSSG TCP Bidirectional Throughput Interrupt Pacing
Command Used |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: CPU Load % (LOCAL_CPU_UTIL) |
|---|---|---|
netperf -H 192.168.2.1 -j -c -C -l 60 -t TCP_STREAM; netperf -H 192.168.2.1 -j -c -C -l 60 -t TCP_MAERTS |
1039.79 |
83.8 |
2.5.1.3.8.2.3. UDP Egress Throughput
Frame Size(bytes) |
am64xx-hsevm: UDP Datagram Size(bytes) (LOCAL_SEND_SIZE) |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: Packets Per Second (kPPS) |
am64xx-hsevm: CPU Load % (LOCAL_CPU_UTIL) |
|---|---|---|---|---|
64 |
45.31 |
88 |
87.5 |
|
128 |
87.49 |
85 |
88.4 |
|
256 |
166.04 |
81 |
89.2 |
|
1024 |
610.00 |
74 |
89.3 |
|
1472 |
855.64 |
73 |
90.1 |
2.5.1.3.8.2.4. UDP Ingress Throughput
Frame Size(bytes) |
am64xx-hsevm: UDP Datagram Size(bytes) (LOCAL_SEND_SIZE) |
am64xx-hsevm: THROUGHPUT (Mbits/sec) |
am64xx-hsevm: Packets Per Second (kPPS) |
am64xx-hsevm: CPU Load % |
|---|---|---|---|---|
64 |
36.35 |
71 |
44.2 |
|
128 |
70.25 |
69 |
47.0 |
|
256 |
138.03 |
67 |
45.5 |
|
1024 |
530.84 |
65 |
52.5 |
|
1472 |
626.48 |
53 |
48.6 |
2.5.1.3.9. PCIe
2.5.1.3.9.1. PCIe-NVMe-SSD
To run the performance test, connect an NVMe SSD to the PCIe slot of the EVM, and execute the following commands:
cd /opt/ltp
./runltp -P am64xx-hsevm -f ddt/pci_gen3ssd_perf -s "PCI_L_PERF_NVMESSD_EXT4_FIO_10G "
Buffer size (bytes) |
Write EXT4 Throughput (Mbytes/sec) |
Write EXT4 CPU Load (%) |
Read EXT4 Throughput (Mbytes/sec) |
Read EXT4 CPU Load (%) |
|---|---|---|---|---|
1m |
397 (min 393.4, max 400.6) |
24.39 |
422 (min 419.0, max 425.9) |
15.49 |
4m |
398 (min 385.9, max 411.0) |
19.26 |
424 (min 410.2, max 436.1) |
15.11 |
4k |
74.2 (min 71.1, max 76.3) |
50.47 |
103 (min 100.8, max 105.5) |
50.78 |
256k |
397 (min 390.3, max 399.3) |
25.54 |
420 (min 416.3, max 422.7) |
15.16 |
File size used: 10G
FIO command options: –ioengine=’libaio’ –iodepth=4 –numjobs=1 –direct=1 –group_reporting –runtime=60 –time_based –eta=never
Platform: Speed 5GT/s, Width x1
SSD used: Intel SSDPED1D280GA
2.5.1.3.10. OSPI
2.5.1.3.10.1. OSPI RAW
File size (Mbytes) |
am64xx-hsevm: Raw Read Throughput (Mbytes/sec) |
|---|---|
50 |
120.03 (min 34.72, max 142.86) |
2.5.1.3.11. EMMC
Warning
IMPORTANT: The performance numbers can be severely affected if the media is mounted in sync mode. Hot plug scripts in the filesystem mount removable media in sync mode to ensure data integrity. For performance sensitive applications, umount the auto-mounted filesystem and re-mount in async mode.
2.5.1.3.11.1. EMMC EXT4 FIO 1G
Buffer size (bytes) |
am64xx-hsevm: Write EXT4 Throughput (Mbytes/sec) |
am64xx-hsevm: Write EXT4 CPU Load (%) |
am64xx-hsevm: Read EXT4 Throughput (Mbytes/sec) |
am64xx-hsevm: Read EXT4 CPU Load (%) |
|---|---|---|---|---|
1m |
60.85 (min 59.80, max 61.40) |
4.01 (min 3.82, max 4.19) |
175.00 |
7.54 (min 6.84, max 8.58) |
4m |
60.92 (min 60.10, max 61.70) |
3.00 (min 2.94, max 3.09) |
175.00 |
6.21 (min 6.08, max 6.67) |
4k |
51.03 (min 50.40, max 51.40) |
47.71 (min 47.11, max 48.21) |
56.20 (min 55.90, max 56.50) |
43.39 (min 42.04, max 44.59) |
256k |
60.88 (min 59.70, max 61.40) |
5.90 (min 5.76, max 6.02) |
174.00 |
8.94 (min 8.35, max 9.48) |
2.5.1.3.11.2. EMMC EXT4
Buffer size (bytes) |
am64xx-hsevm: Write EXT4 Throughput (Mbytes/sec) |
am64xx-hsevm: Write EXT4 CPU Load (%) |
am64xx-hsevm: Read EXT4 Throughput (Mbytes/sec) |
am64xx-hsevm: Read EXT4 CPU Load (%) |
|---|---|---|---|---|
102400 |
53.52 (min 50.76, max 55.23) |
10.85 (min 9.02, max 15.05) |
177.10 (min 170.77, max 178.65) |
29.75 (min 26.36, max 31.19) |
262144 |
53.44 (min 49.12, max 55.01) |
11.09 (min 9.71, max 14.70) |
180.91 (min 177.95, max 182.21) |
30.50 (min 27.93, max 33.04) |
524288 |
53.65 (min 49.96, max 55.45) |
10.94 (min 9.33, max 14.80) |
182.81 (min 182.59, max 182.93) |
27.26 (min 24.55, max 28.83) |
1048576 |
53.88 (min 49.84, max 55.29) |
10.68 (min 9.47, max 14.43) |
182.82 (min 182.64, max 182.99) |
28.13 (min 25.89, max 29.46) |
5242880 |
54.16 (min 49.90, max 55.64) |
10.63 (min 9.14, max 14.63) |
182.84 (min 182.76, max 182.90) |
27.89 (min 27.03, max 28.57) |
2.5.1.3.11.3. EMMC VFAT
Buffer size (bytes) |
am64xx-hsevm: Write VFAT Throughput (Mbytes/sec) |
am64xx-hsevm: Write VFAT CPU Load (%) |
am64xx-hsevm: Read VFAT Throughput (Mbytes/sec) |
am64xx-hsevm: Read VFAT CPU Load (%) |
|---|---|---|---|---|
102400 |
48.54 (min 40.00, max 51.49) |
12.98 (min 10.62, max 19.53) |
168.22 (min 167.35, max 168.71) |
31.87 (min 28.81, max 34.48) |
262144 |
50.03 (min 40.70, max 53.63) |
13.61 (min 11.41, max 19.72) |
169.22 (min 167.80, max 170.47) |
30.98 (min 27.27, max 37.82) |
524288 |
49.42 (min 39.94, max 52.77) |
13.40 (min 11.16, max 19.84) |
168.08 (min 166.94, max 169.46) |
27.37 (min 25.20, max 28.69) |
1048576 |
48.91 (min 40.22, max 51.96) |
13.10 (min 10.95, max 19.49) |
166.64 (min 165.06, max 168.68) |
27.83 (min 25.62, max 28.80) |
5242880 |
49.84 (min 40.55, max 54.04) |
13.15 (min 11.19, max 19.67) |
166.79 (min 165.93, max 167.42) |
28.51 (min 27.87, max 29.03) |
2.5.1.3.11.4. UBoot EMMC
File size (bytes in hex) |
am64xx-hsevm: Write Throughput (Kbytes/sec) |
am64xx-hsevm: Read Throughput (Kbytes/sec) |
|---|---|---|
2000000 |
59848.32 (min 58724.01, max 61134.33) |
169053.08 (min 168907.22, max 169782.38) |
4000000 |
60759.37 (min 59308.60, max 61651.93) |
172614.84 (min 172463.16, max 172918.21) |
2.5.1.3.12. MMCSD
Warning
IMPORTANT: The performance numbers can be severely affected if the media is mounted in sync mode. Hot plug scripts in the filesystem mount removable media in sync mode to ensure data integrity. For performance sensitive applications, umount the auto-mounted filesystem and re-mount in async mode.
2.5.1.3.12.1. MMC EXT4 FIO 1G
Buffer size (bytes) |
am64xx-hsevm: Write EXT4 Throughput (Mbytes/sec) |
am64xx-hsevm: Write EXT4 CPU Load (%) |
am64xx-hsevm: Read EXT4 Throughput (Mbytes/sec) |
am64xx-hsevm: Read EXT4 CPU Load (%) |
|---|---|---|---|---|
1m |
42.42 (min 41.30, max 44.00) |
3.46 (min 3.11, max 3.71) |
86.77 (min 84.80, max 87.90) |
5.25 (min 5.00, max 5.40) |
4m |
41.77 (min 40.30, max 42.70) |
2.57 (min 2.51, max 2.68) |
85.97 (min 82.60, max 87.30) |
3.78 (min 3.35, max 4.18) |
4k |
2.77 (min 2.72, max 2.81) |
6.96 (min 6.71, max 7.31) |
12.82 (min 12.70, max 12.90) |
12.76 (min 12.13, max 13.58) |
256k |
38.15 (min 37.80, max 38.70) |
4.64 (min 4.50, max 4.76) |
83.47 (min 83.10, max 83.90) |
6.51 (min 6.19, max 7.09) |
2.5.1.3.12.2. MMC EXT4
Buffer size (bytes) |
am64xx-hsevm: Write Raw Throughput (Mbytes/sec) |
am64xx-hsevm: Write Raw CPU Load (%) |
am64xx-hsevm: Read Raw Throughput (Mbytes/sec) |
am64xx-hsevm: Read Raw CPU Load (%) |
|---|---|---|---|---|
102400 |
28.91 (min 27.03, max 32.81) |
5.91 (min 4.58, max 8.99) |
39.25 (min 37.68, max 40.92) |
7.04 (min 6.25, max 7.95) |
262144 |
28.72 (min 27.22, max 32.30) |
6.29 (min 4.81, max 8.97) |
41.56 (min 39.87, max 42.87) |
6.69 (min 6.28, max 7.44) |
524288 |
29.68 (min 28.38, max 32.45) |
6.11 (min 4.99, max 9.66) |
45.38 (min 45.00, max 45.57) |
6.76 (min 6.05, max 7.38) |
1048576 |
30.06 (min 28.89, max 32.57) |
6.01 (min 4.93, max 8.69) |
45.34 (min 45.16, max 45.45) |
6.75 (min 6.33, max 7.17) |
5242880 |
31.13 (min 28.88, max 33.47) |
6.14 (min 4.65, max 9.08) |
45.36 (min 45.00, max 45.55) |
6.87 (min 6.37, max 7.21) |
The performance numbers were captured using the following:
SanDisk Max Endurance SD card (SDSQQVR-032G-GN6IA)
Partition was mounted with async option
2.5.1.3.13. CRYPTO
2.5.1.3.13.1. OpenSSL Performance
Algorithm |
Buffer Size (in bytes) |
am64xx-hsevm: throughput (KBytes/Sec) |
|---|---|---|
aes-128-cbc |
1024 |
23012.35 |
aes-128-cbc |
16 |
345.75 |
aes-128-cbc |
16384 |
138062.51 |
aes-128-cbc |
256 |
5988.95 |
aes-128-cbc |
64 |
1506.60 |
aes-128-cbc |
8192 |
100433.92 |
aes-128-ecb |
1024 |
22891.52 |
aes-128-ecb |
16 |
345.72 |
aes-128-ecb |
16384 |
144796.33 |
aes-128-ecb |
256 |
5978.97 |
aes-128-ecb |
64 |
1483.33 |
aes-128-ecb |
8192 |
105411.93 |
aes-192-cbc |
1024 |
22946.13 |
aes-192-cbc |
16 |
322.59 |
aes-192-cbc |
16384 |
130547.71 |
aes-192-cbc |
256 |
5987.33 |
aes-192-cbc |
64 |
1483.73 |
aes-192-cbc |
8192 |
96985.09 |
aes-192-ecb |
1024 |
23038.29 |
aes-192-ecb |
16 |
323.43 |
aes-192-ecb |
16384 |
132852.39 |
aes-192-ecb |
256 |
5995.86 |
aes-192-ecb |
64 |
1401.62 |
aes-192-ecb |
8192 |
100335.62 |
aes-256-cbc |
1024 |
20581.72 |
aes-256-cbc |
16 |
320.95 |
aes-256-cbc |
16384 |
122339.33 |
aes-256-cbc |
256 |
5605.12 |
aes-256-cbc |
64 |
1392.06 |
aes-256-cbc |
8192 |
92940.97 |
aes-256-ecb |
1024 |
21534.04 |
aes-256-ecb |
16 |
326.69 |
aes-256-ecb |
16384 |
127320.06 |
aes-256-ecb |
256 |
5676.46 |
aes-256-ecb |
64 |
1498.28 |
aes-256-ecb |
8192 |
97176.23 |
sha256 |
1024 |
24602.62 |
sha256 |
16 |
407.77 |
sha256 |
16384 |
206176.26 |
sha256 |
256 |
6433.96 |
sha256 |
64 |
1622.78 |
sha256 |
8192 |
137366.19 |
sha512 |
1024 |
20061.53 |
sha512 |
16 |
393.69 |
sha512 |
16384 |
79216.64 |
sha512 |
256 |
5904.04 |
sha512 |
64 |
1574.76 |
sha512 |
8192 |
65959.25 |
Algorithm |
am64xx-hsevm: CPU Load |
|---|---|
aes-128-cbc |
44.00 |
aes-128-ecb |
45.00 |
aes-192-cbc |
43.00 |
aes-192-ecb |
44.00 |
aes-256-cbc |
42.00 |
aes-256-ecb |
43.00 |
sha256 |
94.00 |
sha512 |
94.00 |
Listed for each algorithm are the code snippets used to run each benchmark test.
time -v openssl speed -elapsed -evp aes-128-cbc
2.5.1.3.13.2. RP Message Inter-Processor Communication (IPC) Latency
2.5.1.3.13.2.1. RP Message latency Performance
RP Message latency is the delay measured from sending a round trip echo message from a Linux application to a remote processor and back. The following measurements use a RP message length of 1 byte and 490 bytes for comparison.
The Linux user space application rpmsg_char_benchmark captures these latency values.
Test commands used for running IPC latency tests:
rpmsg_char_benchmark -r 2 -n 100000 -m 1 & chrt -f -p 80 $!
Latencies reported:
Remote Processor |
Message Size (in bytes) |
Average round trip (usecs) |
Max round trip (usecs) |
|---|---|---|---|
R5F0_0 |
1 |
35 |
194 |
R5F0_0 |
490 |
154 |
255 |
M4F |
1 |
43 |
162 |
M4F |
490 |
282 |
439 |