2.5.2. Linux 12.00.00 Performance Guide
2.5.2.1. Read This First
All performance numbers provided in this document are gathered using following Evaluation Modules unless otherwise specified.
Name |
Description |
|---|---|
AM64x EVM |
AM64x Evaluation Module rev E1 with ARM running at 1GHz, DDR data rate 1600 MT/S |
Table: Evaluation Modules
2.5.2.2. About This Manual
This document provides performance data for each of the device drivers which are part of the Processor SDK Linux package. This document should be used in conjunction with release notes and user guides provided with the Processor SDK Linux package for information on specific issues present with drivers included in a particular release.
For further information or to report any problems, contact https://e2e.ti.com/ or https://support.ti.com/
2.5.2.3. System Benchmarks
2.5.2.3.1. CRYPTO
2.5.2.3.1.1. Crypto Performance Comparison
The following table shows different AES/SHA algorithms throughput measured using openssl speed across the SA2UL accelerator, ARM Cryptographic Extension (CE), and baseline ARM CPU.
Algorithm |
Size (bytes) |
Accelerator (MB/s) |
ARM CE (MB/s) |
ARM (MB/s) |
|---|---|---|---|---|
aes-128-cbc |
16 |
0.36 |
67.74 |
22.19 |
aes-128-cbc |
64 |
1.61 |
212.79 |
28.35 |
aes-128-cbc |
256 |
6.34 |
449.47 |
30.64 |
aes-128-cbc |
1024 |
19.02 |
637.13 |
31.25 |
aes-128-cbc |
8192 |
101.91 |
727.25 |
31.44 |
aes-128-cbc |
16384 |
136.80 |
734.06 |
31.44 |
aes-128-ecb |
16 bytes |
0.36 |
72.76 |
23.15 |
aes-128-ecb |
64 bytes |
1.62 |
199.11 |
28.66 |
aes-128-ecb |
256 bytes |
6.39 |
456.68 |
30.60 |
aes-128-ecb |
1024 bytes |
18.95 |
685.38 |
31.12 |
aes-128-ecb |
8192 bytes |
101.67 |
806.09 |
31.28 |
aes-128-ecb |
16384 bytes |
139.55 |
814.81 |
31.27 |
aes-192-cbc |
16 bytes |
0.36 |
66.82 |
19.97 |
aes-192-cbc |
64 bytes |
1.59 |
196.38 |
24.62 |
aes-192-cbc |
256 bytes |
6.36 |
376.01 |
26.25 |
aes-192-cbc |
1024 bytes |
18.88 |
496.14 |
26.68 |
aes-192-cbc |
8192 bytes |
97.58 |
547.43 |
26.84 |
aes-192-cbc |
16384 bytes |
130.47 |
551.05 |
26.71 |
aes-192-ecb |
16 bytes |
0.37 |
70.86 |
21.01 |
aes-192-ecb |
64 bytes |
1.68 |
191.99 |
25.32 |
aes-192-ecb |
256 bytes |
6.67 |
426.36 |
26.77 |
aes-192-ecb |
1024 bytes |
19.54 |
621.73 |
27.15 |
aes-192-ecb |
8192 bytes |
101.79 |
717.97 |
27.27 |
aes-192-ecb |
16384 bytes |
134.23 |
725.00 |
27.24 |
aes-256-cbc |
16 bytes |
0.34 |
71.41 |
22.53 |
aes-256-cbc |
64 bytes |
1.52 |
211.82 |
27.12 |
aes-256-cbc |
256 bytes |
5.98 |
405.04 |
28.65 |
aes-256-cbc |
1024 bytes |
18.14 |
532.25 |
29.18 |
aes-256-cbc |
8192 bytes |
74.33 |
566.03 |
29.24 |
aes-256-cbc |
16384 bytes |
103.42 |
578.21 |
29.25 |
aes-256-ecb |
16 bytes |
0.36 |
65.54 |
18.39 |
aes-256-ecb |
64 bytes |
1.62 |
175.31 |
21.71 |
aes-256-ecb |
256 bytes |
6.44 |
370.39 |
22.80 |
aes-256-ecb |
1024 bytes |
18.90 |
535.87 |
23.08 |
aes-256-ecb |
8192 bytes |
94.67 |
609.52 |
23.17 |
aes-256-ecb |
16384 bytes |
124.78 |
615.11 |
23.15 |
sha2-256 |
16 bytes |
0.36 |
8.34 |
5.37 |
sha2-256 |
64 bytes |
1.41 |
30.63 |
15.83 |
sha2-256 |
256 bytes |
5.61 |
100.69 |
35.91 |
sha2-256 |
1024 bytes |
21.55 |
233.92 |
52.80 |
sha2-256 |
8192 bytes |
124.61 |
383.28 |
61.20 |
sha2-256 |
16384 bytes |
190.61 |
400.21 |
61.86 |
sha2-512 |
16 bytes |
0.34 |
5.15 |
5.15 |
sha2-512 |
64 bytes |
1.38 |
20.53 |
20.52 |
sha2-512 |
256 bytes |
5.19 |
44.68 |
44.68 |
sha2-512 |
1024 bytes |
17.93 |
75.68 |
75.66 |
sha2-512 |
8192 bytes |
61.53 |
94.91 |
94.83 |
sha2-512 |
16384 bytes |
74.50 |
96.57 |
96.52 |
Algorithm |
Accelerator (%) |
ARM CE (%) |
ARM (%) |
|---|---|---|---|
aes-128-cbc |
38% |
99% |
99% |
aes-128-ecb |
38% |
99% |
99% |
aes-192-cbc |
38% |
99% |
99% |
aes-192-ecb |
38% |
99% |
99% |
aes-256-cbc |
38% |
99% |
99% |
aes-256-ecb |
38% |
99% |
99% |
sha2-256 |
90% |
99% |
99% |
sha2-512 |
91% |
99% |
99% |