AM243x Motor Control SDK  2025.00.00
Introduction

Welcome to Motor Control SDK for AM243X. This SDK contains examples, libraries, and tools to develop RTOS and no-RTOS based applications for real-time motor control on the Arm® Cortex®-R5F CPU and related peripherals. It includes position sense examples, current sense examples, PRU-ICSS PWM examples, real-time control library examples, time synchronization examples, and a universal single-chip servo drive reference design (TIDEP-01032).

Real-time communication with encoders and current sensing is typically handled by the Programmable Real-Time Unit Industrial Communication Subsystem (PRU-ICSS). The PRU-ICSS is a co-processor subsystem containing Programmable Real-Time (PRU) cores that implement the low-level firmware. The PRU-ICSS frees up the main Arm-based cores in the device for other functions, such as control and data processing.

Applications and PRU-ICSS firmwares for position sense and current sense are provided in the SDK.

Attention
Motor Control SDK 9.x/11.x included the Industrial Communications SDK and MCU+ SDK in bundled ind_comms_sdk and mcu_plus_sdk folders. Starting with Motor Control SDK 2025.00.00, these folders are no longer included and must be downloaded separately. Motor Control SDK installer provides an option to install the required Industrial Communications SDK and MCU+ SDK.

Getting Started

To get started, see GETTING STARTED page.

Block Diagram

Given below is a block diagram of the software modules in this SDK

Software Block Diagram

The main software components in the block diagram specific to motor control are described below

Software Components Documentation Page Description
Position Sense Encoders
BISS-C BISS-C Driver and PRU-ICSS firmware for BISS-C encoder interface
EnDat EnDat Driver and PRU-ICSS firmware for EnDat encoder interface
HDSL HDSL Driver and PRU-ICSS firmware for Hiperface DSL encoder interface
Nikon A-format Nikon A-format Driver and PRU-ICSS firmware for Nikon A-format encoder interface
Tamagawa Tamagawa Driver and PRU-ICSS firmware for Tamagawa encoder interface
Current Sense
SDFM SDFM Driver and firmware for current sense using Sigma-Delta Filtering Module
Real Time Libraries
Control algorithms Control algorithms Library for control algorithms and techniques used in motors such as PMSM and BLDC
Datalog Datalog Library for storing the real time values of user selectable variables
Digital Control Library (DCL) Digital Control Library (DCL) Header-only library for digital control applications
Observer algorithms Observer algorithms Header-only library for encoder/observer algorithms used in both sensored/sensorless field oriented control (FOC)
Software Frequency Response Analyzer Software Frequency Response Analyzer Library that enables developers to quickly measure the frequency response of their digital power converter.
Transforms Transformation Algorithm Transformation including Clarke, Park, Space Vector Generation used in motor control applications.
PRU-ICSS PWM
PRU-ICSS PWM PRU-ICSS PWM Driver for using PRU-ICSS PWM Peripheral
TIDEP-01032 EtherCAT-Connected Single-Chip Dual-Servo Motor Drive Reference Design
Reference design TIDEP-01032 EtherCAT-Connected Single-Chip Dual-Servo Motor Drive Reference Design Reference design showcasing the ability of the AM243x device to support a fully integrated real-time servo motor drive control and industrial communication.
PRU-ICSS TIME SYNC
Timesync PRU-ICSS TIME SYNC Example showing clock synchronization between multiple devices using PRU-ICSS.
Examples and Demos
Examples and Demos Examples and Demos Examples and demos showing usage of different SW libraries and APIs for position sense, current sense, PRU-ICSS PWM and real-time libraries.

For details on software components of Industrial Communications SDK and MCU+ SDK, please refer to AM243X Industrial Communications SDK and AM243X MCU+ SDK respectively.

Directory Structure

Given below is an overview of the directory structure to help you navigate the SDK and related tools.

Folder/Files Description
${SDK_INSTALL_PATH}/
README_FIRST_AM243X.html Open this file in a web browser to reach this user guide
makefile Top level makefile to build the whole SDK using "make"
imports.mak Top level makefile to list paths to dependent tools
docs/ Offline browseable HTML documentation
examples/ Example applications for AM243X, across multiple boards
source/ Device drivers, middleware libraries and APIs

Given below are the paths where the different tools needed outside the SDK, like CCS, SysConfig are installed by default in Windows. In Linux, the tools are installed by default in ${HOME}/ti.

Folder/Files Description
C:/ti/ccs20.2.0 Code composer studio
C:/ti/sysconfig_1.23.0 SysConfig. NOTE, SysConfig is also installed as part of CCS at ${CCS_INSTALL_PATH}/ccs/utils/sysconfig_x.x.x
C:/ti/ti-cgt-armllvm_4.0.1.LTS TI ARM CLANG compiler tool chain

Licenses

The licensing information of this SDK, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest.

A complete manifest along with export control information is detailed in "${SDK_INSTALL_PATH}/docs/manifest.html" file.

Help and Support

For additional help and support, see https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum

Documentation Credits

This user guide is generated using Doxygen, v1.8.20. See https://www.doxygen.nl/index.html

Note
Arm is a registered trademark of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere.