1 #ifndef __DSPLIB_UTILITY_H__
2 #define __DSPLIB_UTILITY_H__
304 #endif //__DSPLIB_UTILITY_H__
uint16_t numChannels
Number of channels being separated.
Definition: DSPLib_utility.h:140
Parameters for IQ31 real vector fill.
Definition: DSPLib_utility.h:72
uint16_t length
Length of each channel, must be a multiple of two.
Definition: DSPLib_utility.h:136
Parameters for Q15 real vector fill.
Definition: DSPLib_utility.h:58
uint16_t numChannels
Number of channels being separated.
Definition: DSPLib_utility.h:124
int32_t _iq31
Signed fixed point data type with 1 integer bit and 31 fractional bits.
Definition: DSPLib_types.h:59
uint16_t length
Length of the source data, must be a multiple of two.
Definition: DSPLib_utility.h:60
Parameters for Q15 vector deinterleave.
Definition: DSPLib_utility.h:118
msp_status msp_copy_iq31(const msp_copy_iq31_params *params, const _iq31 *src, _iq31 *dst)
Real IQ31 vector copy.
msp_status
Enumerated type to return the status of an operation.
Definition: DSPLib_types.h:78
_q15 imagValue
Imaginary constant value to fill imaginary indices with.
Definition: DSPLib_utility.h:92
_iq31 realValue
Real constant value to fill real indices with.
Definition: DSPLib_utility.h:106
msp_status msp_copy_q15(const msp_copy_q15_params *params, const _q15 *src, _q15 *dst)
Real Q15 vector copy.
uint16_t length
Length of the source data, must be a multiple of two.
Definition: DSPLib_utility.h:48
uint16_t length
Length of the source data, must be a multiple of two.
Definition: DSPLib_utility.h:74
msp_status msp_deinterleave_q15(const msp_deinterleave_q15_params *params, _q15 *src, _q15 *dst)
Extract a single channel from multiple-channel source.
msp_status msp_fill_iq31(const msp_fill_iq31_params *params, _iq31 *dst)
Real IQ31 vector fill with constant.
_q15 value
Scalar constant to fill the destination vector with.
Definition: DSPLib_utility.h:62
msp_status msp_cmplx_fill_iq31(const msp_cmplx_fill_iq31_params *params, _iq31 *dst)
Complex IQ31 vector fill with constant.
_iq31 imagValue
Imaginary constant value to fill imaginary indices with.
Definition: DSPLib_utility.h:108
uint16_t channel
Specific zero-indexed channel to pull from source.
Definition: DSPLib_utility.h:122
int16_t _q15
Signed fixed point data type with 1 integer bit and 15 fractional bits.
Definition: DSPLib_types.h:38
Parameters for IQ31 vector copy function.
Definition: DSPLib_utility.h:46
uint16_t length
Length of the source data, must be a multiple of two.
Definition: DSPLib_utility.h:88
Parameters for Q15 complex vector fill.
Definition: DSPLib_utility.h:86
_iq31 value
Scalar constant to fill the destination vector with.
Definition: DSPLib_utility.h:76
Parameters for IQ31 complex vector fill.
Definition: DSPLib_utility.h:102
uint16_t length
Length of each channel, must be a multiple of two.
Definition: DSPLib_utility.h:120
msp_status msp_cmplx_fill_q15(const msp_cmplx_fill_q15_params *params, _q15 *dst)
Complex Q15 vector fill with constant.
_q15 realValue
Real constant value to fill real indices with.
Definition: DSPLib_utility.h:90
uint16_t length
Length of the source data, must be a multiple of two.
Definition: DSPLib_utility.h:104
Parameters for Q15 vector copy function.
Definition: DSPLib_utility.h:34
uint16_t length
Length of the source data, must be a multiple of two.
Definition: DSPLib_utility.h:36
msp_status msp_fill_q15(const msp_fill_q15_params *params, _q15 *dst)
Real Q15 vector fill with constant.
Parameters for IQ31 vector deinterleave.
Definition: DSPLib_utility.h:134
msp_status msp_deinterleave_iq31(const msp_deinterleave_iq31_params *params, _iq31 *src, _iq31 *dst)
Extract a single channel from multiple-channel source.
uint16_t channel
Specific zero-indexed channel to pull from source.
Definition: DSPLib_utility.h:138