4.20. WDG¶
4.20.1. About This Document¶
Document Title |
User Guide of MCAL WDG Driver |
Document Version |
Version 1.6 |
Company |
Texas Instruments |
Document Name |
WDG User Guide |
4.20.2. Revision History¶
Version |
Date |
Revision History |
Status |
|---|---|---|---|
Versiont 1.0 |
26 April 2022 |
Initial Release |
Approved |
Versiont 1.1 |
05 Aug 2022 |
Updated AM263 to AM263x |
Approved |
Versiont 1.2 |
23 Dec 2022 |
WDG Example application testing procedure is added |
Approved |
Versiont 1.3 |
8 May 2023 |
WDG Example application testing procedure updated |
Approved |
Versiont 1.4 |
12 Jun 2023 |
Updated as per HTML format. |
Approved |
Versiont 1.5 |
25 Aug 2023 |
Document release version column removed |
Approved |
Versiont 1.6 |
16 Jan 2024 |
Updated Assumptions and Dependencies |
Approved |
4.20.3. Table of contents¶
4.20.4. Acronyms and Definitions¶
Acronyms and Definitions Used are presented in below table.
Acronyms |
Descriptions |
|---|---|
BSW |
Basic Software |
DET |
Default Error Tracer |
WDG |
Watchdog Timer |
MCU |
Micro Controller Unit |
OS |
Operating System |
4.20.5. Functional Overview¶
4.20.5.1. Brief Overview¶
This document describes the functionality, API and configuration of the AUTOSAR BSW module Wdg.
Supported AUTOSAR Release |
4.3.1 |
Supported Configuration Variants |
Pre-Compile, Post-build & Link-Time |
Vendor ID |
WDG_VENDOR_ID (44) |
Module ID |
WDG_MODULE_ID (102) |
Supported Platform |
AM263x |
The WDG driver depends on some other modules, like DET for error handling, OSEK/AUTOSAR OS for interrupt handling and the Mcu module for system clock settings.
4.20.5.1.1. Wdg Driver Architecture¶
The Wdg driver has architecture as shown in below figure from the AUTOSAR spec
Fig. 4.9 Figure : Wdg in AUTOSAR architecture¶
The WDG driver provides services for handling the watch dog timer on the microcontroller.
The WDG driver performs two main tasks, which are as follows:
Initialization of WDG
Reset WDG expiration time (trigger)
4.20.5.1.2. Initialization¶
The initialization covers the following steps
Set selected watchdog timer expiration time
Set selected trigger timeout
Set selected window size (Digital Windowed Watchdog)
Set selected mode (Fast or slow can be selected but cannot be switched runtime)
4.20.5.1.3. States¶
WDG_IDLE: This is indicating the module is initialized and not busy.
WDG_BUSY: This is indicating the module is busy.
4.20.5.2. Features Supported and Not Supported¶
Features Supported |
Features Not Supported |
|---|---|
Setting default mode and timeout during initialization. |
Off mode not supported |
Setting window size (Digital Windowed Watchdog). |
Due to hardware limitations, Mode and Timeout can’t be modified if watchdog is running. |
Enable watchdog timer |
|
Service watchdog timer. |
4.20.5.3. Assumptions¶
The clock and PLL configuration is outside driver and should be configured for proper WDG operation.
The Pin Muxing should be initialized before initializing the Wdg module.
4.20.5.4. Limitations¶
None
4.20.5.5. Design overview¶
Please refer SITARA MCU MCAL Architecture Document and MCAL: WDG Detailed Design Document provided as part of CSP.
4.20.5.6. File Structure¶
Static source C File Structure is defined below in the table.
File Name |
Description |
|---|---|
Wdg.c |
Main part of the module functionality, implements the AUTOSAR APIs for WDG driver |
Wdg_Priv.c and Wdg_Priv.h |
platform specific internal file |
Wdg.h |
WDG module header file. Needs to be included by higher layers |
Wdg_Irq.c and Wdg_Irq.h |
WDG Interrupt service routine |
Plugin structure is defined below in the table.
Plugin Structure |
Descriptions |
|---|---|
Wdg_Cfg.h |
Contains the base addresses, Precompile switches, Macros for channels, counters etc. |
Wdg_PBcfg.c |
Contains all channels Post-Build Configuration parameters |
Wdg_Cfg.c |
Contains all channels Pre-Compile Configuration parameters |
The below diagram shows the files structure for the Wdg driver.
fig4 :WDG header file include structure
4.20.6. Deviations to requirements (Requirement Traceability)¶
4.20.6.1. Module Requirements¶
Please refer Software Product Specification document provided as part of CSP.
4.20.6.2. Deviation of requirements against AUTOSAR specification requirements¶
Will be updated in future release
4.20.7. Integration Details¶
4.20.7.1. Dependency on Other Software Modules¶
4.20.7.1.1. MCU¶
The module MCU powers up the microcontroller’s peripherals at startup time and initializes the PLL.
4.20.7.1.2. OS¶
An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table. The WDG module may use AUTOSAR OS to suspend and restore global interrupts.
4.20.7.1.3. SchM¶
There are no exclusive areas.
4.20.7.1.4. Critical Sections¶
There are no critical sections.
4.20.7.1.5. DEM¶
By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus(). The DEM is enabled if the DemEventParameterRefs container is defined.
4.20.7.2. Error Handling module¶
4.20.7.2.1. DET¶
By default, production code related errors are reported to the DET using the service Det_ReportError(). If development error reporting is enabled (i.e. pre-compile parameter WDG_DEV_ERROR_DETECT== STD_ON). The reported service IDs identify the services which are described in 3.4. The following table presents the service IDs and the related services:
The errors reported to DET and DEM are described in the following table
Type of Error |
Relevance |
Related Error Code |
Value |
|---|---|---|---|
API service used in wrong context (e.g. module not initialized). |
Development |
WDG_E_DRIVER_STATE |
0x10 |
API service called with wrong / inconsistent parameter(s) |
Development |
WDG_E_PARAM_MODE |
0x11 |
API service called with wrong / inconsistent parameter(s) |
Development |
WDG_E_PARAM_CONFIG |
0x12 |
The passed timeout value is higher than the max timeout value. |
Development |
WDG_E_PARAM_TIMEOUT |
0x13 |
API is called with wrong pointer value (e.g. NULL pointer) |
Development |
WDG_E_PARAM_POINTER |
0x14 |
4.20.7.2.2. Parameter Checking¶
AUTOSAR requires that API functions check the validity of their parameters. The checks are described in spec and are done as internal parameter checks of the API functions. These checks are for development error reporting and can be en/dis-abled separately. Refer to the configuration chapter where the en/dis-abling of the checks is described. En/dis-abling of single checks is an addition to the AUTOSAR standard which requires to en/dis-able the complete parameter checking via the parameter WDG_DEV_ERROR_DETECT. The following table shows which parameter checks are performed on which services:
Services |
Wdg_Init |
Wdg_SetMode |
Wdg_SetTriggerCondition |
Wdg_GetVersionInfo |
Wdg_Trigger |
|---|---|---|---|---|---|
WDG_E_DRIVER_STATE |
X |
X |
|||
WDG_E_PARAM_MODE |
X |
||||
WDG_E_PARAM_CONFIG |
|||||
WDG_E_PARAM_TIMEOUT |
X |
||||
WDG_E_PARAM_POINTER |
X |
X |
|||
WDG_E_MODE_FAILED |
X |
||||
WDG_E_DISABLE_REJECTED |
X |
4.20.7.2.3. Production Code Error Reporting¶
By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus(). The errors reported to DEM are described in the following table:
ErrorCode |
Description |
|
|---|---|---|
Assigned by DEM |
WDG_E_MODE_FAILED |
This error is raised when setting the watchdog mode fails. |
Assigned by DEM |
WDG_E_DISABLE_REJECTED |
Initialization or watchdog mode switch failed because it would disable the watchdog though this is not allowed in this configuration. |
Assigned by DEM |
WDG_E_HARDWARE_ERROR |
This error is raised when register write failure occurs. (Hardware Failure) |
4.20.7.2.4. Callback Function¶
The WDG driver does not provide any call back functions.
4.20.7.3. Hardware - Software - ISR API name mapping¶
None
4.20.7.4. Scheduling Strategy¶
None
4.20.8. API Description¶
4.20.8.1. Description of the API’s¶
Please refer MCAL_AM263_ApiGuide.CHM document provided as part of CSP.
4.20.8.2. API’s with Service ID¶
The following table presents the service IDs and the related services:
Service ID |
Service |
|---|---|
0x00 |
Wdg_Init |
0x01 |
Wdg_SetMode |
0x03 |
Wdg_SetTriggerCondition |
0x04 |
Wdg_GetVersionInfo |
0x05 |
Wdg_Trigger |
4.20.8.3. Description on Non Standard API’s¶
Wdg_RegisterReadback API–This function is non-autosar based and is used to read the data in the registers of Wdg if we keep Wdg_REGISTER_READBACK_API Macro as ON.
4.20.9. Configuration Description¶
4.20.9.1. Configuration Variants¶
The Wdg is configured through GUI in Post-Build ,Pre-Compile Variants and Link Time Variants.
Variants |
Generated Files |
|---|---|
PostBuild |
Wdg_PBcfg.c , Wdg_Cfg.h |
Pre-Compile |
Wdg_Cfg.c , Wdg_Cfg.h |
Link-Time |
Wdg_Lcfg.c , Wdg_Cfg.h |
4.20.9.2. Parameter Description¶
4.20.9.2.1. Standard Configuration¶
Standard Parameters |
Description |
Default Value |
Range |
Unit |
|---|---|---|---|---|
WDG_E_DISABLE_REJECTED |
Reference to the DemEventParameter which shall be issued when the error “Initialization or mode switch failed because it would disable the watchdog” has occurred. |
FALSE |
0..1 |
Boolean |
WDG_E_MODE_FAILED |
Setting a watchdog mode failed (during initialization or mode switch) |
FALSE |
0..1 |
Boolean |
WdgDevErrorDetect |
Switches the development error detection and notification on or off. |
FALSE |
0..1 |
Boolean |
WdgDisableAllowed |
Compile switch to allow / forbid disabling the watchdog driver during runtime. |
FALSE |
0..1 |
Boolean |
WdgIndex |
Specifies the InstanceId of this module instance. If only one instance is present it shall have the Id 0. |
0 |
0 .. 255 |
Integer |
WdgInitialTimeout |
The initial timeout (sec) for the trigger condition to be initialized during Init function. |
0 |
0 .. 65.535] |
Integer |
WdgMaxTimeout |
The maximum timeout (sec) to which the watchdog trigger condition can be initialized. |
0 |
0 .. 65.535] |
Integer |
WdgVersionInfoApi |
Compile switch to enable / disable the version information API |
TRUE |
0..1 |
Boolean |
WdgDefaultMode |
Default mode for watchdog driver initialization. |
WDGIF_FAST_MODE |
Wdg_ModeInfoType |
Enumeration |
WdgInstanceId |
Watchdog HW instance id. 0 - R5F0_0, 1 - R5F0_1, 2 - R5F1_0, 3 - R5F1_1 |
0 |
0..3 |
Integer |
WdgTriggerMode |
Watchdog trigger mode (toggle/window/both) |
WDG_WINDOW |
WdgTriggerMode |
Enumeration |
4.20.9.2.2. IP Specific Configuration¶
Standard Parameters |
Description |
Default Value |
Range |
Unit/Datatype |
|---|---|---|---|---|
WdgWindowSize |
The Digital Windowed Watchdog window size. Selecting 100% enables standard watchdod |
WINDOW_SIZE_100_PERCENT |
Wdg_WindowSize |
Enumeration |
WdgRegisterReadbackApi |
Compile switch to enable / disable the Register Readback API |
FALSE |
0..1 |
Boolean |
WdgRtiFrequency |
RTI Clock Frequency (MHz) |
200 |
0..200 |
MHz |
WdgPreloadValue |
Watchdog preload value to be set in RTIDWDPRLD register. Expiration time is calculated using this function: texp = (WdgPreloadValue + 1) x 2^13 / RTICLK1 |
4095 |
0..4095 |
ms |
WdgDeviceVariant |
Select SOC AM263x variant |
AM263x |
AM263x |
|
WdgReaction |
Watchdog reaction for timer expiration or incorrect service. |
WDG_GENERATE_RESET |
Wdg_Reaction |
Enumeration |
WDG_E_HARDWARE_ERROR |
This error is raised when Hardware failed detected |
NULL |
NA |
NA |
4.20.10. Memory mapping¶
Memory Mapping Sections |
WDG_CODE |
WDG_CODE_ISR |
WDG_VAR_NO_INIT |
WDG_VAR_ZERO_INIT |
WDG_PBCFG |
WDG_PBCFG_ROOT |
|---|---|---|---|---|---|---|
WDG_START_SEC_VAR_INIT_UNSPECIFIED(.bss) WDG _STOP_SEC_VAR_INIT_UNSPECIFIED |
x |
|||||
WDG _START_SEC_CODE_APPL(.text) WDG _STOP_SEC_CODE_APPL |
x |
|||||
WDG _START_SEC_VAR_UNSPECIFIED(.data) WDG _STOP_SEC_VAR_UNSPECIFIED |
x |
|||||
WDG _START_SEC_CODE(.text) WDG _STOP_SEC_CODE |
x |
|||||
WDG_START_SEC_PBCFG(.data) WDG_STOP_SEC_PBCFG |
x |
|||||
WDG_START_SEC_PBCFG_ROOT(.const) WDG_STOP_SEC_PBCFG_ROOT |
x |
4.20.11. Memory footprint¶
Please refer Memory Footprint for more details.
4.20.12. Performance¶
None
4.20.13. Example Usage¶
4.20.13.1. Steps to build and run example¶
WDG example application demonstrates the MCAL WDG driver features, which is referred from folder <MCAL_ROOT>/examples/WDG.
This application can be built from the build folder by giving “gmake –s wdg_app PLATFORM=am263” command in command prompt.
Once the build is completed we get an appimage file, which is flashed in am263x controller and executed.
To Flash the appimage at the respective memory location as the SBL expects, path of the appimage file is provided in “default_sbl_qspi” file in “..<MCU_PLUS_SDK_INSTALLATION>toolsbootsbl_prebuiltam263x-cc”
Set the boot mode of board to UART mode.(UART boot mode: 1000)
Open command prompt at the path “..<MCU_PLUS_SDK_INSTALLATION>toolsboot" and provide command as follows: “python uart_uniflash.py -p COM<x> –cfg=sbl_prebuilt/am263x-cc/default_sbl_qspi.cfg” Here <x> depicts the COM PORT number where hardware is connected to system, which can be detected from device manager
Once the appimage is flashed after the command is executed, change the boot mode of board to QSPI mode.(QSPI boot mode: 0010)
Open the terminal to get the expected application log after doing hard reset on board.
Verify that the application produces the correct results as expected shown below.
4.20.13.2. Document external set up Information¶
None
4.20.13.3. Flow of the example application¶
Default Example program is configured in Non-Maskable Interrupt method (WDT will trigger interrupt when counter becomes zero).
WDT window reaction can be changed to “reset” through configuration (EB Tresos).
In example, service interval is 25ms and service count is 100. So, every 25ms core will service the WDT for 100 times (25*100 = 2500 ms).
WDG is integrated with WDG in order to service WDG.
WDG_SetTriggerCondition API is servicing WDG by passing non zero timeout value
Then after it will raise an interrupt and interrupt will run (WDT_Isr() function). In ISR function core reset will occurs and start running program again automatically.
It checks for reset reason, if reset happened due to WDT then “Test Passed”
In Reset window reaction mode, after counter reaches to zero POR(Power ON Reset) happens.
4.20.13.4. Example Logs¶
WDG_APP: Sample Application - STARTS !!!
WDG MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 102
SW Major Version : 9
SW Minor Version : 1
SW Patch Version : 0
----------------------------------------------------------------------------------
Starting WDG test !!!
----------------------------------------------------------------------------------
Service Count 100
Service Interval 25 milliseconds
------------------------------------------
Trigger Value = 2500 milliseconds
------------------------------------------
Maximum Service Interval 74 milliseconds
Initializing channels
Post-Build variant is being used .
Reset Reason 2
Test Passed!!
WDG Stack Usage: 800 bytes
------------------------------------------
4.20.14. FAQ’s¶
Will be updated in future release
4.20.15. Test Report¶
Please refer AM26x WDG Driver Test Case Report provided as part of CSP.
4.20.16. References¶
4.20.17. TI Disclaimer¶
Texas Instruments and its subsidiaries (TI) reserve the right to make changes to their products or to discontinue any product or service without notice, and advise customers to obtain the latest version of relevant information to verify, before placing orders, that information being relied on is current and complete. All products are sold subject to the terms and conditions of sale supplied at the time of order acknowledgment, including those pertaining to warranty, patent infringement, and limitation of liability.
TI warrants performance of its products to the specifications applicable at the time of sale in accordance with TI’s standard warranty. Testing and other quality control techniques are utilized to the extent TI deems necessary to support this warranty. Specific testing of all parameters of each device is not necessarily performed, except those mandated by government requirements.
Customers are responsible for their applications using TI components. In order to minimize risks associated with the customer’s applications, adequate design and operating safeguards must be provided by the customer to minimize inherent or procedural hazards.
TI assumes no liability for applications assistance or customer product design. TI does not warrant or represent that any license, either express or implied, is granted under any patent right, copyright, mask work right, or other intellectual property right of TI covering or relating to any combination, machine, or process in which such products or services might be or are used. TI’s publication of information regarding any third party’s products or services does not constitute TI’s approval, license, warranty or endorsement thereof.
Reproduction of information in TI data books or data sheets is permissible only if reproduction is without alteration and is accompanied by all associated warranties, conditions, limitations and notices. Representation or reproduction o f this information with alteration voids all warranties provided for an associated TI product or service, is an unfair and deceptive business practice, and TI is not responsible nor liable for any such use.
Resale of TI’s products or services with statements different from or beyond the parameters stated by TI for that product or service voids all express and any implied warranties for the associated TI product or service, is an unfair and deceptive business practice, and TI is not responsible nor liable for any such use.
Also see: Standard Terms and Conditions of Sale for Semiconductor Products https://www.ti.com/sc/docs/stdterms.htm
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265