4.21. WDG Module
4.21.1. Acronyms and Definitions
Abbreviation/Term |
Explanation |
|---|---|
AUTOSAR |
Automotive Open System Architecture |
BSW |
Basic Software |
DET |
Default Error Tracer |
HW |
Hardware |
SW |
Software |
WDG |
Watchdog Timer |
MCU |
Micro Controller Unit |
OS |
Operating System |
4.21.2. Introduction
This document describes the functionality and configuration of the AUTOSAR BSW module Wdg.
Supported AUTOSAR Release |
4.3.1 |
|---|---|
Supported Configuration Variants |
Pre-Compile, Post-build |
Vendor ID |
WDG_VENDOR_ID (44) |
Module ID |
WDG_MODULE_ID (102) |
Supported Platform |
AM263Px |
The WDG driver depends on some other modules, like DET for error handling, OSEK/AUTOSAR OS for interrupt handling and the Mcu module for system clock settings.
4.21.3. Functional Overview
4.21.3.1. WDG Driver Architecture
The Wdg driver has architecture as shown in below figure from the AUTOSAR spec
Fig. 4.96 Wdg in AUTOSAR architecture
The WDG driver provides services for handling the watch dog timer on the microcontroller.
The WDG driver performs two main tasks, which are as follows:
Initialization of WDG
Reset WDG expiration time (trigger)
4.21.3.2. Initialization
The initialization covers the following steps
Set selected watchdog timer expiration time
Set selected trigger timeout
Set selected window size (Digital Windowed Watchdog)
Set selected mode (Fast or slow can be selected but cannot be switched runtime)
4.21.3.3. States
WDG_IDLE: This is indicating the module is initialized and not busy.
WDG_BUSY: This is indicating the module is busy.
4.21.3.4. Assumptions
None
4.21.3.5. Limitations
None
4.21.3.6. Design overview
Will be updated in future release
4.21.4. Hardware Features
4.21.4.1. Hardware Features supported
Setting default mode and timeout during initialization.
Setting window size (Digital Windowed Watchdog).
Enable watchdog timer.
Service watchdog timer.
4.21.4.2. Not supported Features
Off mode not supported
Due to hardware limitations, Mode and Timeout can’t be modified if watchdog is running.
4.21.4.3. Non compliance
4.21.4.3.1. Deviations to requirements (Requirement Traceability)
4.21.4.3.1.1. Deviation of requirements against AUTOSAR specification requirements
Will be updated in next release
4.21.5. Source files
Static source C Files are defined below
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Wdg
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Wdg.h : WDG module header file. Needs to be included by higher layers.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Wdg.c : Main part of the module functionality, implements the AUTOSAR APIs for WDG driver.
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┗ 📜Wdg_Priv.c : Platform specific internal file.
┃ ┃ ┃ ┣ 📜Wdg_Priv.h : Platform specific internal file.
┃ ┃ ┗ 📜Makefile
┃ 📂mcal_config
┃ 📂mcal_docs
┃ 📜README.txt
Plugin files are defined below in the table.
Plugin Files |
Description |
|---|---|
Wdg_Cfg.h |
Contains the base addresses, Precompile switches, Macros for channels, counters etc. |
Wdg_PBcfg.c |
Contains all channels Post-Build Configuration parameters |
Wdg_Cfg.c |
Contains all channels Pre-Compile Configuration parameters |
Fig. 4.97 WDG header file include structure
4.21.6. Module requirements
4.21.6.1. Memory Mapping
Memory Mapping Sections |
WDG_CODE |
WDG_CODE_ISR |
WDG_VAR_NO_INIT |
WDG_VAR_ZERO_INIT |
WDG_PBCFG |
WDG_PBCFG_ROOT |
|---|---|---|---|---|---|---|
WDG_START_SEC_VAR_INIT_UNSPECIFIED(.bss) |
x |
|||||
WDG _STOP_SEC_VAR_INIT_UNSPECIFIED |
x |
|||||
WDG _START_SEC_CODE_APPL(.text) |
x |
|||||
WDG _STOP_SEC_CODE_APPL |
x |
|||||
WDG _START_SEC_VAR_UNSPECIFIED(.data) |
x |
|||||
WDG _STOP_SEC_VAR_UNSPECIFIED |
x |
|||||
WDG _START_SEC_CODE(.text) |
x |
|||||
WDG _STOP_SEC_CODE |
x |
|||||
WDG_START_SEC_PBCFG(.data) |
x |
|||||
WDG_STOP_SEC_PBCFG |
x |
|||||
WDG_START_SEC_PBCFG_ROOT(.const) |
x |
|||||
WDG_STOP_SEC_PBCFG_ROOT |
x |
4.21.6.2. Scheduling
None
4.21.6.3. Error handling
4.21.6.3.1. Development Error Reporting (DET)
The errors reported to DET and DEM are described in the following table
Type of Error |
Related Error code |
Value (Hex) |
|---|---|---|
API service used in wrong context (e.g. module not initialized). |
WDG_E_DRIVER_STATE |
0x10 |
API service called with wrong / inconsistent parameter(s) |
WDG_E_PARAM_MODE |
0x11 |
API service called with wrong / inconsistent parameter(s) |
WDG_E_PARAM_CONFIG |
0x12 |
The passed timeout value is higher than the max timeout value. |
WDG_E_PARAM_TIMEOUT |
0x13 |
API is called with wrong pointer value (e.g. NULL pointer) |
WDG_E_PARAM_POINTER |
0x14 |
4.21.6.3.2. Parameter Checking
AUTOSAR requires that API functions check the validity of their parameters. The checks are described in spec and are done as internal parameter checks of the API functions. These checks are for development error reporting and can be en/dis-abled separately. Refer to the configuration chapter where the en/dis-abling of the checks is described. En/dis-abling of single checks is an addition to the AUTOSAR standard which requires to en/dis-able the complete parameter checking via the parameter WDG_DEV_ERROR_DETECT. The following table shows which parameter checks are performed on which services:
Services |
Wdg_Init |
Wdg_SetMode |
Wdg_SetTriggerCondition |
Wdg_GetVersionInfo |
Wdg_Trigger |
|---|---|---|---|---|---|
WDG_E_DRIVER_STATE |
X |
X |
|||
WDG_E_PARAM_MODE |
X |
||||
WDG_E_PARAM_CONFIG |
|||||
WDG_E_PARAM_TIMEOUT |
X |
||||
WDG_E_PARAM_POINTER |
X |
X |
|||
WDG_E_MODE_FAILED |
X |
||||
WDG_E_DISABLE_REJECTED |
X |
4.21.6.3.3. Production Code Error Reporting
By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus(). The errors reported to DEM are described in the following table:
Type of Error |
Related Error code |
Description |
|---|---|---|
Assigned by DEM |
WDG_E_MODE_FAILED |
This error is raised when setting the watchdog mode fails. |
Assigned by DEM |
WDG_E_DISABLE_REJECTED |
Initialization or watchdog mode switch failed because it would disable the watchdog though this is not allowed in this configuration |
4.21.7. Used resources
4.21.7.1. Interrupt Handling
Will be updated in the future release
4.21.8. Integration description
4.21.8.1. Dependent modules
4.21.8.1.1. MCU
The module MCU powers up the microcontroller’s peripherals at startup time and initializes the PLL.
4.21.8.1.2. OS
An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table. The WDG module may use AUTOSAR OS to suspend and restore global interrupts.
4.21.8.1.3. SchM
There are no exclusive areas.
4.21.8.1.4. Critical Sections
There are no critical sections.
4.21.8.1.5. DEM
By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus().
Note: Dem Event is enable only if $(Module_Name)DemEventParameterRefs is enabled.
4.21.8.1.6. DET
By default, production code related errors are reported to the DET using the service Det_ReportError(). If development error reporting is enabled (i.e. pre-compile parameter WDG_DEV_ERROR_DETECT== STD_ON). The reported service IDs identify the services which are described in 3.4.
4.21.8.1.7. Callback Notification
The WDG driver does not provide any call back functions.
4.21.8.2. Multi-core and Resource allocator
Will be updated in the future release
4.21.9. Configuration
The Wdg is configured through GUI in Post-Build and Pre-Compile Variants.
Variants |
Configured Files |
|---|---|
PostBuild |
Wdg_PBcfg.c , Wdg_Cfg.h |
Pre-Compile |
Wdg_Cfg.c , Wdg_Cfg.h |
4.21.9.1. Parameter Description
4.21.9.1.1. Standard Configuration
Standard Parameters |
Description |
Default Value |
Range |
Unit |
|---|---|---|---|---|
WDG_E_DISABLE_REJECTED |
Reference to the DemEventParameter which shall be issued when the error “Initialization or mode switch failed because it would disable the watchdog” has occurred. |
FALSE |
0..1 |
Boolean |
WDG_E_MODE_FAILED |
Reference to the DemEventParameter which shall be issued when the error “Setting a watchdog mode failed (during initialization or mode switch)” has occurred. |
FALSE |
0..1 |
Boolean |
WdgDevErrorDetect |
Switches the development error detection and notification on or off. |
FALSE |
TRUE FALSE |
Boolean |
WdgDisableAllowed |
Compile switch to allow / forbid disabling the watchdog driver during runtime. |
FALSE |
TRUE FALSE |
Boolean |
WdgIndex |
Specifies the InstanceId of this module instance. If only one instance is present it shall have the Id 0. |
0 |
0 .. 255 |
Integer |
WdgInitialTimeout |
The initial timeout (sec) for the trigger condition to be initialized during Init function. |
0 |
0 .. 65.535 |
Integer |
WdgMaxTimeout |
The maximum timeout (sec) to which the watchdog trigger condition can be initialized. |
0 |
0 .. 65.535 |
Integer |
WdgVersionInfoApi |
Compile switch to enable / disable the version information API |
TRUE |
TRUE FALSE |
Boolean |
WdgDefaultMode |
Default mode for watchdog driver initialization. |
WDGIF_FAST_MODE |
WDGIF_FAST_MODE WDGIF_OFF_MODE WDGIF_SLOW_MODE |
Enumeration |
WdgInstanceId |
Watchdog HW instance id. 0 - R5F0_0, 1 - R5F0_1, 2 - R5F1_0, 3 - R5F1_1 |
0 |
0..3 |
Integer |
WdgTriggerMode |
Watchdog trigger mode (toggle/window/both) |
WDG_WINDOW |
WDG_BOTH WDG_TOGGLE WDG_WINDOW |
Enumeration |
WdgRunArea |
Represents the watchdog driver execution area is either from ROM(Flash) or RAM as required with the particular microcontroller |
RAM |
RAM ROM |
Enumeration |
4.21.9.1.2. IP Specific Configuration
Standard Parameters |
Description |
Default Value |
Range |
Unit/Datatype |
|---|---|---|---|---|
WdgWindowSize |
The Digital Windowed Watchdog window size. Selecting 100% enables standard watchdog |
WINDOW_SIZE_100_PERCENT |
WINDOW_SIZE_3_125_PERCENT WINDOW_SIZE_6_25_PERCENT WINDOW_SIZE_12_5_PERCENT WINDOW_SIZE_25_PERCENT WINDOW_SIZE_50_PERCENT WINDOW_SIZE_100_PERCENT |
Enumeration |
WdgRegisterReadbackApi |
Compile switch to enable / disable the Register Readback API |
FALSE |
TRUE FALSE |
Boolean |
WdgRtiFrequency |
RTI Clock Frequency (MHz) |
200 |
0..200 |
Integer |
WdgPreloadValue |
Watchdog preload value to be set in RTIDWDPRLD register. Expiration time is calculated using this function: texp = (WdgPreloadValue + 1) x 2^13 / RTICLK1 |
4095 |
0..4095 |
Integer |
WdgDeviceVariant |
Select SOC AM263Px variant |
AM263Px |
AM263Px |
String |
WdgReaction |
Watchdog reaction for timer expiration or incorrect service. |
WDG_GENERATE_NMI |
WDG_GENERATE_RESET WDG_GENERATE_NMI |
Enumeration |
WDG_E_HARDWARE_ERROR |
This error is raised when Hardware failed detected |
NULL |
NA |
NA |
WDG_INITIAL_TIMEOUT: This is the initial wdg timeout period.
WDG_MAX_TIMEOUT: Maximum timeout for the wdg is 65 * 1000.
WDG_MAX_PRELOAD_VALUE: To define wdg maximum preload value.
WDG_RTI_FREQUENCY: This is defined to get the desired frequency.
WdgDeviceVariant: To Select SOC AM263Px variant
4.21.9.2. Symbolic Names deviations
None
4.21.9.3. Configuration rules and constraints to enable plausibility checks
Will be updated in future release
4.21.10. Examples
4.21.10.1. Overview
Will be updated in the future release
4.21.10.2. Hardware Software Setup and Tools
None
4.21.10.3. Steps to build and run example
WDG example application demonstrates the MCAL WDG driver features, which is referred from folder <MCAL_ROOT>/examples/WDG.
This application can be built from the build folder by giving “gmake –s wdg_app PLATFORM=am263px” command in command prompt.
Once the build is completed we get a binary file, which is loaded in our controller and executed.
4.21.10.4. Flow of the example application
Default Example program is configured in Non-Maskable Interrupt method (WDT will trigger interrupt when counter becomes zero).
WDT window reaction can be changed to “reset” through configuration (EB Tresos).
In example, service interval is 25ms and service count is 100. So, every 25ms core will service the WDT for 100 times (25*100 = 2500 ms).
WDG is integrated with WDG in order to service WDG.
WDG_SetTriggerCondition API is servicing WDG by passing non zero timeout value
Then after it will raise an interrupt and interrupt will run (WDT_Isr() function). In ISR function core reset will occurs and start running program again automatically.
It checks for reset reason, if reset happened due to WDT then “Test Passed”
In Reset window reaction mode, after counter reaches to zero POR(Power ON Reset) happens.
4.21.10.5. Example Logs
WDG_APP: Sample Application - STARTS !!!
WDG MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 102
SW Major Version : 9
SW Minor Version : 1
SW Patch Version : 0
----------------------------------------------------------------------------------
Starting WDG test !!!
----------------------------------------------------------------------------------
Service Count 100
Service Interval 25 milliseconds
------------------------------------------
Trigger Value = 2500 milliseconds
------------------------------------------
Maximum Service Interval 74 milliseconds
Initializing channels
Post-Build variant is being used .
Reset Reason 2
Test Passed!!
WDG Stack Usage: 800 bytes
------------------------------------------
4.21.10.6. File Structure
📦AM263Px
┣ 📂build
┃ ┣ 📂examples
┃ ┃ ┣ 📂Wdg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜WdgApp.c : Contains WDG test example.
┃ ┃ ┃ ┣ 📜WdgApp.h : Contains WDG test example headers.
┃ ┃ ┃ ┣ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Wdg_Demo_Cfg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263px
┃ ┃ ┃ ┃ ┃ ┣ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Wdg_Cfg.h : Contains the Precompile switches, Macros etc.
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Wdg_Cfg.c : Contains Pre-Compile Configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Wdg_Lcfg.c : Contains linker Configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Wdg_PBcfg.c : Contains Post-Build Configuration parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┣ 📜README.txt
4.21.11. FAQ’s
Will be updated in next release
4.21.12. Test Report
Please refer AM26x WDG Driver Test Case Report as part of CSP provided in the release package.