4.7. CDD_IPC Module
4.7.1. Acronyms and Definitions
Abbreviation/Term |
Explanation |
|---|---|
AUTOSAR |
Automotive Open System Architecture |
BSW |
Basic Software |
MCAL |
Micro Controller Abstraction Layer |
API |
Application Programming Interface |
DET |
Default Error Tracer |
IPC |
Inter Process Communication |
SW |
Software |
MCU |
Micro Controller Unit |
OS |
Operating System |
CDD |
Complex Device Driver |
4.7.2. Introduction
This document describes the functionality, API and configuration of the AUTOSAR BSW module Complex Device driver for IPC on AM263Px device.
Supported AUTOSAR Release |
4.3.1 |
Supported Configuration Variants |
Post Build |
Vendor ID |
CDD_IPC_VENDOR_ID (44) |
Module ID |
CDD_IPC_MODULE_ID (255) |
Supported Platform |
AM263Px |
4.7.3. Functional Overview
The main tasks of Complex Device Driver for IPC are the following:
Initialization of the mailbox driver
Simplifies reading and writing to the mailbox peripheral.
4.7.3.1. Complex Device Driver Architecture
The following figure shows where the Complex device driver is located in the AUTOSAR architecture.
Fig. 4.39 CDD in AUTOSAR architecture
4.7.3.2. Initialization
The initialization covers the following steps:
Initialize the mailbox peripheral.
Cdd_Ipc_Init should be called only once during initialization.
No other CDD API can be invoked until this API is called.
4.7.4. Hardware Features
4.7.4.1. Supported Features
Open/Close mailbox instance
Send/Receive both Notify and RpMsg messages
RpMsg Callback functionality supported
4.7.4.2. Not supported Features
Multiple mailbox channels between the cores
Applications are validated only for the R50_0 core
4.7.5. Source files
Description of static files is provided below:
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Ipc
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Cdd_Ipc.h : Contains interface header for Complex device driver for IPC
┃ ┃ ┃ ┣ 📜Cdd_Ipc_Irq.h : contains ISR function declaration for Complex Device Driver
┃ ┃ ┃ ┣ 📜ipc_notify_lld_utils.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_notify_v1_lld.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_notify_v1_mailbox.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_rpmsg_linux_resource_table.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_rpmsg_lld.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_rpmsg_lld_priv.h : Contains Internal functions declaration
┃ ┃ ┃ ┗ 📜ipc_rpmsg_lld_queue.h : Contains Internal functions declaration
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Cdd_Ipc.c : Contains function definitions for the Complex device driver for IPC and helper functions
┃ ┃ ┃ ┣ 📜Cdd_Ipc_Irq.c : Contains ISR function definitions for Complex Device Driver
┃ ┃ ┃ ┣ 📜ipc_notify_lld_utils.c : Contains Internal functions definition
┃ ┃ ┃ ┣ 📜ipc_notify_v1_lld.c : Contains Internal functions definition
┃ ┃ ┃ ┣ 📜ipc_rpmsg_lld.c : Contains Internal functions definition
┃ ┃ ┃ ┗ 📜ipc_rpmsg_lld_vring.c : Contains Internal functions definition
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┣ 📜hw_mailbox.h : Contains Internal functions definition
┃ ┃ ┃ ┣ 📜ipc_notify_v1_cfg_lld.c : Contains Internal functions definition
┃ ┃ ┃ ┗ 📜ipc_notify_v1_cfg_lld.h : Contains Internal functions definition
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt
The below diagram shows the files structure for the CDD driver.
Fig. 4.40 CDD header file include structure
4.7.6. Module requirements
4.7.6.1. Memory Mapping
Memory Mapping Sections |
CDD_CODE |
CDD_CODE_ISR |
CDD_VAR_NO_INIT |
CDD_VAR_ZERO_INIT |
|---|---|---|---|---|
CDD_IPC_START_SEC_VAR_INIT_UNSPECIFIED (.bss) |
x |
|||
CDD_IPC_STOP_SEC_VAR_INIT_UNSPECIFIED |
x |
|||
CDD_IPC_START_SEC_CODE_APPL (.text) |
x |
|||
CDD_IPC_STOP_SEC_CODE_APPL |
x |
|||
CDD_IPC_START_SEC_VAR_UNSPECIFIED (.data) |
x |
|||
CDD_IPC_STOP_SEC_VAR_UNSPECIFIED |
x |
|||
CDD_IPC_START_SEC_CODE(.rodata) |
x |
|||
CDD_IPC_START_SEC_CODE |
x |
4.7.6.2. Scheduling
4.7.6.2.1. SchM
Will be added in future releases:
4.7.6.2.2. Critical Sections
Will be added in future releases:
4.7.6.3. Error handling
4.7.6.3.1. Development Error Reporting
Development errors are reported to the DET using the service Det_ReportError().
4.7.6.4. Error codes
4.7.6.4.1. Development Errors
The errors reported to DET and DEM are described in the following table
Type of Error |
Related Error code |
Value (Hex) |
|---|---|---|
Error code indicating the IPC is uninitialized |
CDD_IPC_E_UNINIT |
0x01 |
Error code indicating register client failed event |
CDD_IPC_E_REGISTER_CLIENT_FAILED |
0x02 |
Error code indicating IPC Initialization Failed |
CDD_IPC_E_INIT_FAILED |
0x03 |
Error code indicating IPC Deinitialization Failed |
CDD_IPC_E_DEINIT_FAILED |
0x04 |
Error code indicating invalid parameter |
CDD_IPC_E_PARAM_POINTER |
0x05 |
Error code indicating IPC already initialized |
CDD_IPC_E_ALREADY_INITIALIZED |
0x06 |
Error code indicating Service called with wrong param |
CDD_IPC_E_PARAM_VALUE |
0x07 |
Error code indicating Service called with invalid length |
CDD_IPC_E_PARAM_LENGTH |
0x08 |
Error code indicating invalid IPC Channel |
CDD_IPC_E_INVALID_CHANNEL |
0x09 |
Error code indicating invalid IPC configuration |
CDD_IPC_E_INVALID_CONFIG |
0x0A |
Error code indicating IPC Write Failed configuration |
CDD_IPC_E_WRITE_FAILED |
0x0B |
Error code indicating unregister client failed event |
CDD_IPC_E_UNREGISTER_CLIENT_FAILED |
0x0C |
Error code indicating construct failed event |
CDD_IPC_E_CONSTRUCT_FAILED |
0x0D |
Error code indicating RpMsg Write failed event |
CDD_IPC_E_RPMSG_WRITE_FAILED |
0x0E |
Error code indicating Rpmsg read failed event |
CDD_IPC_E_RPMSG_READ_FAILED |
0x0F |
Error code indicating destruct failed event |
CDD_IPC_E_DESTRUCT_FAILED |
0x10 |
4.7.6.4.2. Parameter Checking
AUTOSAR requires that API functions check the validity of their parameters. These checks are for development error reporting and can be en-/disabled via the parameter CDD_IPC_DEV_ERROR_DETECT. The following table shows which parameter checks are performed on which services:
Services |
CDD_IPC_E_UNINIT |
CDD_IPC_E_REGISTER_CLIENT_FAILED |
CDD_IPC_E_UNREGISTER_CLIENT_FAILED |
CDD_IPC_E_PARAM_POINTER |
CDD_IPC_E_ALREADY_INITIALIZED |
CDD_IPC_E_PARAM_VALUE |
CDD_IPC_E_WRITE_FAILED |
CDD_IPC_E_CONSTRUCT_FAILED |
CDD_IPC_E_RPMSG_WRITE_FAILED |
CDD_IPC_E_RPMSG_READ_FAILED |
|---|---|---|---|---|---|---|---|---|---|---|
Cdd_Ipc_Init |
x |
x |
||||||||
Cdd_Ipc_DeInit |
x |
x |
||||||||
Cdd_Ipc_Notify_RegisterClient |
x |
x |
x |
|||||||
Cdd_Ipc_Notify_UnregisterClient |
x |
x |
x |
|||||||
Cdd_Ipc_Notify_Write |
x |
x |
x |
x |
||||||
Cdd_Ipc_Construct |
x |
x |
||||||||
Cdd_Ipc_Destruct |
x |
x |
||||||||
Cdd_Ipc_RpMsg_SendMsg |
x |
x |
x |
|||||||
Cdd_Ipc_RpMsg_SendMsg |
x |
x |
x |
4.7.7. Used resources
4.7.7.1. Interrupt Handling
Will be updated in future release:
4.7.8. Integration description
4.7.8.1. Dependent modules
4.7.8.1.1. OSEK/AUTOSAR OS (Optional)
An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table. The CDD module may use OSEK/AUTOSAR OS to suspend and restore global interrupts.
4.7.8.1.2. DET (Optional)
The module CDD depends on the DET (by default) in order to report development errors. The mailbox operations like write, read are protected by a critical section.
Service ID |
Service |
|---|---|
0x01 |
Cdd_Ipc_Init |
0x02 |
Cdd_IpcGetVersionInfo |
0x03 |
Cdd_Ipc_RpMsg_RecvMsg |
0x04 |
Cdd_Ipc_RpMsg_SendMsg |
0x05 |
Cdd_Ipc_Notify_RegisterClient |
0x06 |
Cdd_Ipc_Construct |
0x07 |
Cdd_Ipc_DeInit |
0x09 |
Cdd_Ipc_Notify_UnregisterClient |
0x0A |
Cdd_Ipc_Destruct |
4.7.8.1.3. Services used by Complex device Driver
The CDD does not provide any call back functions.
4.7.8.1.4. Notifications
At its configurable interfaces the CDD defines notifications that can be mapped to callback functions provided by other modules. The mapping is not statically defined by the CDD but can be performed at configuration time. The function prototypes that can be used for the configuration have to match the appropriate function prototype signatures, which are described in the following.
Cdd_Ipc_notify_msgHandler: This is defined in the Cdd_Ipc_notify_app.c for reference.
4.7.8.2. Multi-core and Resource allocator
Will be updated in future release:
4.7.9. Configuration
4.7.9.1. Configuration Parameter
Texas Instruments Parameters |
Description |
Default Value |
|---|---|---|
CddIpcLocalCoreId |
This param contains the local coreId on which the IPC instance is running |
CDD_IPC_R5FSS0_0_ID |
CddIpcRemoteCoreIdIndex |
The cores that are participating the IPC message exchange (Exclude the local core from these) |
CDD_IPC_R5FSS0_0_ID |
CddIpcSafeIpcCoresEnable |
Switch to enable Safe Ipc between local and remote core |
False |
CddIpcLocalEndPt |
This parameter is used to register a local call back especially for receiving or sending a RPMsg message |
12 |
CddIpcRecvCallBack |
Function pointer to RPMSG callback function |
NULL |
CddIpcrecvCallbackArguments |
Function Pointer to receive callback function’s arguments |
NULL |
CddIpcrecvNotifyCallback |
Function pointer to IPC notify message Callback function. User can pass a pointer to a custom defined arguments structure and the callback passes this pointer when a notify interrupt is received |
NULL |
CddIpcrecvNotifyCallbackArguments |
Pointer to IPC notify message callback function’s arguments |
NULL |
CddVersionInfoApi |
Switches the Cdd_IpcGetVersionInfo function ON or OFF |
True |
CddDeinitApi |
Switches the Cdd_IpcDeinit function ON or OFF |
True |
CddIpcWriteApi |
Switches the Cdd_IpcWrite function ON or OFF |
True |
CddIpcReadApi |
Switches the Cdd_IpcRead function ON or OFF |
True |
CddIpcRpMsgEnable |
Switch to enable RpMsg API’s to be enabled or not |
True |
CddIpcRecvCallBackEnable |
Switch to enable RPMsg Recv Callback (This is different from Notify Callback) |
True |
CddIpcRecvNotifyCallbackEnable |
Switch to enable RPMsg Notify message Recv Callback |
False |
CddRegisterReadBackApi |
Switches the Cdd_IpcRegisterReadBack function ON or OFF |
True |
CddDevErrorDetect |
Switches the Development Error Detection and Notification ON or OFF |
True |
CddIpcSafeIpcEnable |
Switch to enable Safe Ipc to be enabled or not |
False |
CddIpcCrcEnable |
Switch to enable Crc to be enabled or not |
False |
CddIpcCrcHookFunc |
Hook function in application for Crc Calculation |
NULL |
CddIrqType |
Type of Isr function: void functionname(void) CAT1 : interrupt void func(void) CAT2 : ISR(func) |
CDD_IPC_ISR_VOID |
CddIpcTimeout |
Timeout value for send/receive/wait API’s. Unit is in clock ticks |
2000000 |
CddIpcNumOfBuffers |
This parameter indicates the number of buffers for sending RPMsg |
8 |
CddIpcMaxBufferSize |
This parameter indicates the Max size of each buffer. Note that the actual size available is 16 bytes less than the above chosen value (16 bytes are used for the header in RPMsg) |
128 |
CddDefaultOSCounterId |
Default Os Counter Id if node reference to OsCounter ref CddOsCounterRef is not set |
0 |
CddOsCounterRef |
This parameter contains a reference to the OsCounter, which is used by the GPT driver |
ASPathDataOfSchema:/AUTOSAR /EcucDefs/Os/OsCounter |
CddDeviceVariant |
Device variant AM263Px |
AM263Px |
Note: In case of CddIpcRecvCallBack , when RPMsg arrive then that is invoked along with the data in the VRING buffer.So now if the msg size is less then what we are transferring between cores then we will send the echo msg back to the core from which we are receiving and will do UNLOCK of core only if complete msg transfer happens.So by this way we are acknowledging the remote core.
For details of configuration supported refer the MCAL_Configurator_UserGuide.pdf present in mcal_config/docs folder
4.7.10. Examples
CDD example application demonstrating the Complex device driver features 2 different examples namely ipc_notify_app and ipc_rpmsg_app.
4.7.10.1. Ipc_notify_app_working
This application is low payload, low latency message type where user will be able to send a maximum of 28bits of data as the payload. The first 4 bits are used internally by the driver for the client ID. Notify app sends 1000000, to all the other 3 cores and waits for all of them to echo back. To make the example work with lesser cores, edit the following parameters in the example.
#define MAX 4To the number of cores user needs to reduce.uint32 gRemoteCoreId[];Enable only the cores that are required.uint32 gIpcTransferMutex[MAX]Remove the extra Lock variables (These can be replced with any kind of mutex or semaphore implementation at the user End).In addition to these please also ensure the Cdd_Ipc_PBCfg.c has the proper cores configured from the XDM file.
The same changes stand valid for the rpmsg_echo_app as well.
4.7.10.2. Ipc_rpmsg_app working
RpMsg application uses Vrings as the medium to send larger data whose size and buffer depth can be configured using the parameters CDD_IPC_NUM_OF_BUFFERS and CDD_IPC_MAX_BUFFER_SIZE.
The application exchanges 100000 messages, the payload data is integer value where it gets incremented on every echo back from each core. In order to change the data from the integer to other data i.e., String or characters for command use-cases please change the following line.
snprintf(msgBuf, MAX_MSG_SIZE-1, "%d", msg);
to
snprintf(msgBuf, MAX_MSG_SIZE-1, "%s", Your String Data);
The notify application is present under the path <MCAL_ROOT>/examples/Ipc/Ipc_app_notify. This application can be built from the build folder by giving "gmake -s ipc_notify_app".
The rpmsg application is present under the path <MCAL_ROOT>/examples/Ipc/Ipc_app_rpmsg. This
application can be built from the build folder by giving "gmake -s ipc_rpmsg_app".
4.7.10.2.1. Sample Log
Will be updated in future release:
4.7.10.3. Changing and Compiling SDK examples
Examples to import from SDK to validate the CDD_IPC example,
Use all the other cores except R50-0 (this is where CDD_IPC app will be run), the path to the examples inside MCU+SDK directory
$(MCU_PLUS_SDK_PATH)\examples\drivers\ipc\ipc_notify_echo\am263px-cc
$(MCU_PLUS_SDK_PATH) \examples\drivers\ipc\ipc_rpmsg_echo\am263px-cc
4.7.10.3.1. Notify App Sample Output
4.7.10.3.2. RPMsg App Sample Output
4.7.10.4. Sample log
Ipc Notify:
CDD_IPC_NOTIFY_APP: Sample IPC Application started!
CDD_IPC_NOTIFY_APP: Sync All Completed
CDD_IPC_NOTIFY_APP: Message exchange started by main core
CDD_IPC_NOTIFY_APP: All echoed messages received by main core from 3 remote cores !!!
CDD_IPC_NOTIFY_APP: Messages sent to each core = 1000000
CDD_IPC_NOTIFY_APP: Number of remote cores = 3
All tests have passed
Ipc Rpmsg:
CDD_IPC_RPMSG_APP: Sample IPC Application started!
CDD_IPC_RPMSG_APP: Sync All Completed
CDD_IPC_RPMSG_APP: RpMsg Message exchange started by main core
CDD_IPC_RPMSG_APP: All echoed messages received by main core from 3 remote cores !!!
CDD_IPC_RPMSG_APP: Messages sent to each core = 100000
CDD_IPC_RPMSG_APP: Number of remote cores = 3
All tests have passed
Ipc Rpmsg Callback:
CDD_IPC_RPMSG_CALLBACK_APP: Sample IPC Application started!
CDD_IPC_RPMSG_CALLBACK_APP: Sync All Completed
CDD_IPC_RPMSG_CALLBACK_APP: RpMsg Message exchange started by main core
CDD_IPC_RPMSG_CALLBACK_APP: All echoed messages received by main core from 3 remote cores !!!
CDD_IPC_RPMSG_CALLBACK_APP: Messages sent to each core = 100000
CDD_IPC_RPMSG_CALLBACK_APP: Number of remote cores = 3
All tests have passed
4.7.10.5. File Structure
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Ipc
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📂Ipc_app_notify
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_app.h : Contains Cdd Ipc example header file
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_notify_app.c : contains the IPC R50 test app for IPC Notify
┃ ┃ ┃ ┃ ┗ 📜Makefile
┃ ┃ ┃ ┣ 📂Ipc_app_rpmsg
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_app.h : Contains Cdd Ipc example header file
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_rpmsg_app.c : Contains IPC R50 test app for RpMsg
┃ ┃ ┃ ┃ ┗ 📜Makefile
┃ ┃ ┃ ┣ 📂Ipc_app_rpmsg_callback_mode
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_app.h : Contains Cdd Ipc example header file
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_rpmsg_callback_app.c : Contains IPC R50 test app for RpMsg
┃ ┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Ipc_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263px
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Cdd_Ipc_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Cdd_Ipc_Callback_app_PBCfg.c : Contains all Pre-Compile Configured parameters with Recv CallBack Function
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Cdd_Ipc_PBCfg.c : Contains all Pre-Compile Configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt
4.7.10.6. Test Report
Please refer AM26x CDD IPC Driver Test Case Report as part of CSP provided in the release package.