4.13. FLS Module
4.13.1. Acronyms and Definitions
Abbreviation/Term |
Explanation |
|---|---|
AUTOSAR |
Automotive Open System Architecture |
BSW |
Basic Software |
MCAL |
Micro Controller Abstraction Layer |
API |
Application Programming Interface |
DET |
Default Error Tracer |
HW |
Hardware |
SW |
Software |
FLS |
Flash Driver |
DMA |
Direct Memory Access |
MCU |
Micro Controller Unit |
OS |
Operating System |
OSPI |
Octal Serial Peripheral Interference |
DAC |
Direct Access Mode |
INDAC |
Indirect Access Mode |
4.13.2. Introduction
This document describes MCAL FLS Driver functionality and configuration details as per AUTOSAR version 4.3.1 .
Supported AUTOSAR Release |
4.3.1 |
|---|---|
Supported Configuration Variants |
Pre-Compile, Post-build |
Vendor ID |
FLS_VENDOR_ID (44) |
Module ID |
FLS_MODULE_ID (92) |
Supported Platform |
AM263Px |
The Flash Driver provides services for reading, writing, erasing flash memory for external Flash device.
4.13.3. Functional Overview
4.13.3.1. FLS Driver Architecture
The FLS driver has architecture as shown in below figure from the AUTOSAR specification.
Fig. 4.62 FLS in AUTOSAR architecture
The below figure shows typical connection of the OSPI module to the
Fig. 4.63 OSPI connected to an external flash memory
4.13.3.2. Initialization
The driver FLS is initialized by calling Fls_Init() function and takes FlsConfigSet as input and Initializes Flash and OSPI. This will also make driver status to IDLE.
4.13.3.3. States
The Fls driver maintains states for:
MEMIF_UNINIT -> This is the state when hardware is not initialized.
MEMIF_IDLE -> when FLS driver initialized, it will go to IDLE state.
MEMIF_BUSY-> In case of any on-going operation i.e., Erase OR read OR write, the state will be maintained as busy until the operation is completed.
MEMIF_BUSY_INTERNAL ->This is not supported.
4.13.3.4. Assumptions
None
4.13.3.5. Constraints
For read and write operation offset should be page alligned
For read and write operation length of operation should be byte alligned.
For interrupt mode to be enabled, indac mode should be enabled.
For interrupt mode to be enabled, maxReadNormalMode and maxWriteNormalMode should be set to pagesize.
For interrupt mode to be enabled, FLS_ERASE_VERIFICATION_ENABLED, FLS_WRITE_VERIFICATION_ENABLED, FLS_TIMEOUT_SUPERVISION_ENABLED macros should be STD_OFF.
4.13.3.6. Design overview
Will be available in future release.
4.13.4. Hardware Features
4.13.4.1. AUTOSAR Features supported
Only one OSPI instance will support
Perform storage mode applications
1. Read from flash.
2. Write to flash.
3. Erase Flash.
4. Cancel job is supported.
5. Compare and Blank Check flash memory location.Configure error detection (DET)
Only polling mode is supported.
DAC and INDAC mode of operation are supported.
Interrupt mode is supported (only in INDAC Mode)
4.13.4.2. Not supported Features
XIP Mode is not supported.
PHY Tune Module is not supported.
DMA mode is not supported.
4.13.4.3. IP specific Features supported
4.13.4.3.1. DAC Mode
Direct Access Controller (or DAC) refers to the operation where data interface accesses directly trigger a read or write to Flash memory. It is memory mapped and can be used to both access and directly execute code from external Flash memory. Access that use DAC do not use the embedded SRAM within the OSPI module. DAC mode does not support interrupt handling as it does not involve SRAM for data transfer.
4.13.4.3.2. INDAC Mode
Indirect Access Controller (INDAC) uses the internal SRAM of the OSPI module. Data transfers then happen between the SRAM and Flash memory or SRAM and system memory, so no memory mapping is needed. The aim of the indirect mode of operation is to transfer significant numbers of bytes to/from Flash memory. Indirect operations are controlled and triggered by software via specific read/write transfer registers. Bulk transfers take place between system and flash memory in the most efficient manner. Fewest possible write cycles carried out inside flash device to maximize life of device. INDAC supports poll and interrupt based implementation. The embedded SRAM used by INDAC provides interrupt mechanism. Interrupts are triggered when SRAM levels fall below a watermark, and also when a write/read operation finishes from within the SRAM. Design implementation is non-blocking and allows the control to return to the application (CPU) while the data is still transferring in hardware.
4.13.4.3.3. STIG
Software Triggered Instruction Generator - While DAC and INDAC are used for data transfer, STIG is used to access the volatile and non-volatile configuration registers, status registers, and for erase functions. This Flash Driver Module Write, Read, Erase, BlankCheck and Compare APIs are asynchronous such that control will return to the application after the job from one of the APIs has been accepted. A “job” describes the action that will perform actual transactions to the hardware. The driver’s Fls_MainFunction () API will do the job processing internally, after the APIs have been called and the job has been accepted. During job processing, the module will perform the programming of the flash device, and will make data transfers between system and flash device.
The below figure shows typical connection of the OSPI module to the flash memory
Fig. 4.64 OSPI connected to an external flash memory
4.13.4.4. Non compliance
4.13.4.4.1. Deviations to requirements (Requirement Traceability)
4.13.4.4.1.1. Deviation of requirements against AUTOSAR specification requirements
Will be updated in next release
4.13.5. Source files
Static source C Files are defined below
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Fls
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Fls.h : Contains the APIs of the FLS driver to be used by upper layers.
┃ ┃ ┃ ┣ 📜Fls_Cbk.h : Contains the callback functions.
┃ ┃ ┃ ┗ 📜Fls_Irq.h : Contains ISR function declarations.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Fls.c : Contains the pre-complier switches.
┃ ┃ ┃ ┗ 📜Fls_Irq.c : Contains ISR function definitions..
┃ ┃ ┣ 📂V2
┃ ┃ ┃ ┣ 📜Fls_Brd_Nor.h : Contains internal functions and data structures.
┃ ┃ ┃ ┗ 📜Fls_Brd_Nor_Ospi.c : Contains internal functions and data structures.
┃ ┃ ┃ ┣ 📜Fls_Nor_config.c : Contains flash specific commands
┃ ┃ ┃ ┣ 📜Fls_Nor_config.h : Contains device specific configuration parameters.
┃ ┃ ┃ ┣ 📜Fls_Ospi.c : Contains internal functions definitions.
┃ ┃ ┃ ┗ 📜Fls_Ospi.h : Contains internal functions definitions and data structures.
structures.*
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt
Plugin files are defined below in the table.
Plugin Files |
Description |
|---|---|
Fls_Cfg.h |
Contains the Precompile switches |
Fls_PBcfg.c |
Contains all Post-Build Configured parameters |
Fls_Cfg.c |
Contains all Pre-Compile Configured parameters |
Fig. 4.65 FLS header file include structure
4.13.6. Module requirements
Will be updated in future release
4.13.6.1. Memory Mapping
Memory Mapping Sections |
Compiler Abstraction Definitions |
|||
|---|---|---|---|---|
FLS_CODE |
FLS_CODE_ISR |
FLS_VAR_NO_INIT |
FLS_CFG |
|
FLS_START_SEC_ISR_CODE (.text) |
x |
|||
FLS_STOP_SEC_ISR_CODE |
||||
FLS_START_SEC_VAR_NO_INIT_UNSPECIFIED (.data) |
x |
|||
FLS_STOP_SEC_VAR_NO_INIT_UNSPECIFIED |
||||
FLS_START_SEC_CODE (.text) |
x |
|||
FLS_START_SEC_CODE |
||||
FLS_START_SEC_CONFIG_DATA (.data) |
x |
|||
FLS_STOP_SEC_CONFIG_DATA |
4.13.6.2. Scheduling
4.13.6.2.1. SchM
This implementation requires one level of exclusive access to guard critical sections. Invokes SchM_Enter_Fls_FLS_EXCLUSIVE_AREA_0 (), SchM_Exit_Fls_FLS_EXCLUSIVE_AREA_0 () to enter critical section and exit.
4.13.6.2.2. Critical Sections
There is only one critical section in this driver. Within these sections all read /modify / write accesses to internal FLS status variables must be protected. Therefore, switching to tasks that also access FLS must be avoided and all FLS interrupts must be suspended. This is managed internally by Fls Driver
4.13.6.3. Error handling
4.13.6.3.1. DET Errors
The errors reported to DET module are described in the following table:
Type of Error |
Related Error code |
Value (Hex) |
|---|---|---|
API service called with wrong parameter |
FLS_E_PARAM_CONFIG |
0x01 |
API service called with wrong parameter |
FLS_E_PARAM_ADDRESS |
0x02 |
API service called with wrong parameter |
FLS_E_PARAM_LENGTH |
0x03 |
API service called with wrong parameter |
FLS_E_PARAM_DATA |
0x04 |
API service used without module initialization |
FLS_E_UNINIT |
0x05 |
API called when module is busy |
FLS_E_BUSY |
0x06 |
API called with a Null Pointer |
FLS_E_PARAM_POINTER |
0x0A |
The run time errors reported to DET module are described in the following table:
Type of Error |
Related Error code |
Value (Hex) |
|---|---|---|
Erase verification (blank check) failed |
FLS_E_VERIFY_ERASE_FAILED |
0x07 |
Write verification (compare) failed |
FLS_E_VERIFY_WRITE_FAILED |
0x08 |
AUTOSAR requires that API functions check the validity of their parameters. The check in below table shows the various Development Error Reporting: Assignment of checks to services are internal parameter checks of the API functions. These checks are for development error reporting and can be enabled or disabled. The following table shows which parameter checks are performed on which services:
Check Services |
FLS_E_PARAM_CONFIG |
FLS_E_PARAM_ADDRESS |
FLS_E_PARAM_LENGTH |
FLS_E_PARAM_DATA |
FLS_E_UNINIT |
FLS_E_BUSY |
FLS_E_PARAM_POINTER |
|---|---|---|---|---|---|---|---|
Fls_Init |
x |
x |
|||||
Fls_Erase |
x |
x |
x |
x |
|||
Fls_Read |
x |
x |
x |
x |
x |
||
Fls_Write |
x |
x |
x |
x |
x |
||
Fls_Compare |
x |
x |
x |
x |
x |
||
Fls_BlankCheck |
x |
x |
x |
x |
|||
Fls_GetJobResult |
x |
||||||
Fls_GetVersionInfo |
x |
||||||
Fls_MainFunction |
x |
||||||
Fls_Cancel |
x |
4.13.7. Used resources
4.13.7.1. Interrupt Handling
Will be updated in the next release
4.13.8. Integration description
4.13.8.1. Dependent modules
4.13.8.1.1. MCU
The Fls Modules expects the MCU modules to enable the OSPI clock through the configuration. Required parameter for clock enabling:
Module ID: MCU_CLKSRC_MODULE_ID_OSPI
Source ID: MCU_CLKSRC_4
Divider value: 2
4.13.8.1.2. PORT
The Fls Modules expects that pinmux is set correctly to configure the Data line, Chip select and Clock pins for OSPI module. This is done by the PORT driver.
4.13.8.1.3. MemIf
This implementation depends on MemIf module and uses its imported types such as MemIf_JobResultType, MemIf_ModeType and MemIf_StatusType.
4.13.8.1.4. Fee
This implementation depends on Fee module for callback notification to notify the module environment about job end and job error.
4.13.8.1.5. DET
The module FLS depends on the DET (by default) in order to report development errors.
The following table represents the service IDs:
Service ID |
Code |
Service |
|---|---|---|
FLS_SID_INIT |
0x00 |
Fls_Init |
FLS_SID_ERASE |
0x01 |
Fls_Erase |
FLS_SID_WRITE |
0x02 |
FLS_Write() |
FLS_SID_CANCEL |
0x03 |
FLS_Cancel() |
FLS_SID_GET_STATUS |
0x04 |
FLS_GetStatus() |
FLS_SID_GET_JOB_RESULT |
0x05 |
Fls_GetJobResult() |
FLS_SID_READ |
0x07 |
FLS_Read() |
FLS_SID_COMPARE |
0x08 |
FLS_Compare() |
FLS_SID_GET_VERSION_INFO |
0x10 |
Fls_GetVersionInfo() |
FLS_SID_BLANK_CHECK |
0x0A |
FLS_BlankCheck() |
FLS_SID_MAIN_FUNCTION |
0x06 |
FLS_MainFunction() |
4.13.8.1.6. DEM
FLS modules does not report DEM errors.
4.13.8.1.7. Callback Functions
The FLS driver does not provide any callback functions.
4.13.8.1.8. Main Functions
The function Fls_MainFunction perform the processing of the flash read, write, erase and compare jobs. When a job has been initiated, the FLS module’s environment shall call the function Fls_MainFunction cyclically until the job is finished.
4.13.8.1.9. Fls Set Erase Function
This function is called from example app based on the macros enabled in application itself. Implementation of this function is done to allow user to select one or more erase types based on the requirement. The function Fls_SetEraseType sets the parameters like data size, data_value, erase type(sector/block/chip), “typeoferase” for Fls_DrvObj, based on the erase type parameter passed to this function while calling from example app. These parameters are required in example app.
4.13.8.1.10. Callback Notification
This implementation depends on Fee module for callback notification to notify the module environment about job end and job error
4.13.8.2. Multi-core and Resource allocator
Will be updated in the next release
4.13.9. Configuration
The Fls can be configured as Post-Build or Pre-Compile variant, using EB tresos tool.
Variants |
Configured Files |
|---|---|
PostBuild |
Fls_PBcfg.c , Fls_Cfg.h |
Pre-Compile |
Fls_Cfg.c , Fls_Cfg.h |
4.13.9.1. Parameter Description
4.13.9.1.1. Standard Configuration
Standard Parameters |
Description |
Default Value |
Range |
Unit |
|---|---|---|---|---|
FlsJobEndNotification |
Mapped to the job end notification routine provided by some upper layer module, typically the Fee module. |
NA |
NA |
FUNCTION-NAME |
FlsJobErrorNotification |
Mapped to the job error notification routine provided by some upper layer module, typically the Fee module. |
NA |
NA |
FUNCTION-NAME |
FlsMaxReadNormalMode |
The maximum number of bytes to read or compare in one cycle of the flash driver’s job processing function in normal mode. |
768 |
0 .. 4294967295 |
INTEGER |
FlsMaxWriteNormalMode |
The maximum number of bytes to write in one cycle of the flash driver’s job processing function in normal mode. |
768 |
0 .. 4294967295 |
INTEGER |
FlsNumberOfSectors |
Number of continuous sectors with identical configuration |
32 |
0..65535 |
INTEGER |
FlsPageSize |
Size of one page of this sector. |
256 |
0 .. 4294967295 |
INTEGER |
FlsSectorSize |
Size of this sector. |
4096 |
0 .. 4294967295 |
INTEGER |
FlsSectorStartaddress |
Start address of this sector. |
0 |
0 .. 4294967295 |
INTEGER |
FlsBlankCheckApi |
Compile switch to enable/disable the Fls_BlankCheck function. |
FALSE |
TRUE FALSE |
BOOLEAN |
FlsCancelApi |
Compile switch to enable and disable the Fls_Cancel function. Cancel API currently not supported. |
TRUE |
TRUE FALSE |
BOOLEAN |
FlsCompareApi |
Compile switch to enable and disable the Fls_Compare function. |
TRUE |
TRUE FALSE |
BOOLEAN |
FlsDevErrorDetect |
Switches the development error detection and notification on or off. |
FALSE |
TRUE FALSE |
BOOLEAN |
FlsDriverIndex |
Index of the driver, used by FEE. |
0 |
0..254 |
INTEGER |
FlsEraseVerificationEnabled |
Compile switch to enable erase verification. Currently not supported. |
FALSE |
TRUE FALSE |
BOOLEAN |
FlsGetJobResultApi |
Compile switch to enable and disable the Fls_GetJobResult function. |
TRUE |
TRUE FALSE |
BOOLEAN |
FlsGetStatusApi |
Compile switch to enable and disable the Fls_GetStatus function. |
TRUE |
TRUE FALSE |
BOOLEAN |
FlsSetModeApi |
Compile switch to enable and disable the Fls_SetMode function. Not relevant as only one mode supported. |
FALSE |
TRUE FALSE |
BOOLEAN |
FlsTimeoutSupervisionEnabled |
Compile switch to enable timeout supervision. Currently, not supported. |
FALSE |
TRUE FALSE |
BOOLEAN |
FlsUseInterrupts |
Job processing triggered by hardware interrupt. |
FALSE |
TRUE FALSE |
BOOLEAN |
FlsVersionInfoApi |
Pre-processor switch to enable / disable the API to read out the modules version information. |
FALSE |
TRUE FALSE |
BOOLEAN |
4.13.9.1.2. IP Specific Configuration
Standard Parameters |
Description |
Default Value |
Range |
Unit |
|---|---|---|---|---|
OspiInstanceId |
Instance Id of OSPI. In this variant only one is supported |
0 |
0 |
INTEGER |
FlsBaudRateDiv |
To Select the baud rate divider values |
0 |
0..4294967295 |
INTEGER |
FlsOspiCtrlBaseAddr |
This parameter used to select the OSPI base Address |
1400930304 |
0..4294967295 |
INTEGER |
FlsOsCounterRef |
This parameter contains a reference to the OsCounter, which is used by the FLS driver. |
NA |
ASPathDataOfSchema:/AUTOSAR/EcucDefs/Os/OsCounter |
REFERENCE |
FlsIrqType |
Type of Isr function: void functionname(void) CAT1 see description in oil tool : interrupt void func(void) CAT2 see description in oil tool : ISR(func) |
FLS_ISR_CAT1 |
FLS_ISR_VOID FLS_ISR_CAT1 FLS_ISR_CAT2 |
ENUMERATION |
FlsDefaultOSCounterId |
Default Os Counter Id if node reference to OsCounter ref FlsOsCounterRef is not set |
0 |
0..16 |
INTEGER |
FlsDeviceVariant |
Select required Device Variant |
AM263Px |
AM263Px |
ENUMERATION |
FlsBaseAddress |
The flash memory start address (see also SWS_Fls_00208 and SWS_Fls_00209). |
3321888768 |
0..4294967295 |
INTEGER |
FlsTotalSize |
The total amount of flash memory in bytes (see also SWS_Fls_00208 and SWS_Fls_00209). |
1073741824 |
0 .. 4294967295 |
INTEGER |
FlsWriteVerificationEnabled |
Compile switch to enable write verification. Currenly, not supported. |
FALSE |
TRUE / FALSE |
BOOLEAN |
FlsErasedValue |
The contents of an erased flash memory cell. |
255 |
0 .. 4294967295 |
INTEGER |
FlsEraseTime |
Maximum time to erase one complete flash sector. |
1000 |
0..INFINITY |
FLOAT |
FlsExpectedHwId |
Unique identifier of the hardware device that is expected by this driver (the device for which this driver has been implemented). |
23322 |
– |
STRING |
FlsSpecifiedEraseCycles |
Number of erase cycles specified for the flash device (usually given in the device data sheet). |
0 |
0..4294967295 |
INTEGER |
FlsWriteTime |
Maximum time to program one complete flash page. |
1000 |
0..INFINITY |
FLOAT |
FlsDacEnable |
The driver shall enable Direct Access Mode for OSPI |
TRUE |
TRUE / FALSE |
BOOLEAN |
FlsOspiClkSpeed |
The driver shall specify the OSPI Clk speed to be used |
133333333 |
NA |
INTEGER |
FlsPhyEnable |
The driver shall enable Phy Speed mode for DAC |
FALSE |
TRUE / FALSE |
BOOLEAN |
4.13.9.2. Configuration rules and constraints to enable plausibility checks
Will be updated in next release
4.13.9.3. Configuration changes with DMA mode
Flash configuration should include Cdd_Dma in module configurations to use DMA.
Fig. 4.66 FLS Module Configurations
Flash DMA handler is required for Flash DMA support in DMA configurations and CDD_TRANSFER_MODE_CHAINING should be used in Flash DMA Handler.
Fig. 4.67 FLS Handler in Cdd_Dma configuration
Flash Dma Handler should have two channels because it uses CDD_TRANSFER_MODE_CHAINING mode.
Fig. 4.68 FLS Handler Channels in Cdd_Dma configuration
Flash configuration should enable Memmap mode and Interrupt mode to use DMA.
Fig. 4.69 Dma, Memmap in FLS configuration (FlsConfigSet)
Fig. 4.70 Interrupt in FLS configuration (FlsGeneral)
4.13.9.3.1. Program changes with DMA mode
For DMA mode support, DMA TPCC0 Interrupt aggregation (INTR) line number 72 gets used to register ISR (CDD_EDMA_lld_transferCompletionMasterIsrFxn) with EDMA and Cache invalidation on destination buffers should happen using Mcal_CacheP_inv APIs before using Flash DMA support for read.
4.13.10. Examples
4.13.10.1. Overview
Will be updated in the next release
4.13.10.2. Hardware Software Setup and Tools
None
4.13.10.3. Steps to build and run example
FLS example application demonstrating the MCAL Fls driver features is in folder <MCAL_ROOT>/examples/Fls.
This application can be built from the root folder by giving gmake –s fls_app PLATFORM=am263px.
after the build is completed we get a binary file,which is loaded in our controller and executed.
4.13.10.4. Example Logs
FlsApp: Sample Application - STARTS !!!
FLS_APP: Variant - Pre Compile being used !!!
FLS MCAL version info:9.1.0
FLS MCAL Module/Driver:92.44
FLS_APP:Executing Sector configuration number : 1
FLS_APP:Number of sector/blocks to erase/read/write: 1
FLS_APP:Total data size: 0x1000
FLS_APP:Offset is 0x0
FLS_APP: Erasing
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Blank Checking
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Writing
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Reading
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Write Compare
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP: Read Compare
FLS_APP: Job Processing in Progress.
FLS_APP: Job Ends: SUCCESS
FLS_APP:
FLS_APP: Job Cancel
FLS_APP: 1. Writing
FLS_APP: 2. Canceling
FLS_APP: Job Canceled (SUCCESS) !
FLS_APP:
FLS_APP:
FLS_APP: ---------- FLS Sample application Done !! ----------
FLS_APP:
4.13.10.5. File Structure
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Fls
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜Flsapp.c : Contains Fls test example
┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Fls_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263px
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Fls_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Fls_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗ 📜Fls_PBcfg.c : contains all Post build configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt
4.13.11. FAQ’s
Q1. What if some flashes also support write enable for non-volatile registers?
Before writing to any register in flash, write enable command is issued to the flash. The Write enable can be issued to both volatile and non volatile registers depending on what the flash supports. Currently the existing flash in the device supports write enable to volatile registers. In case any external flash (e.g. S25FL064LABMFB01X) supports write enable to both volatile and non volatile registers, the user can issue write enable command for non volatile registers using Nor_OspiCmdWrite API. User can also update the fls_config_sfdp_1.cmdWren parameter in Flash_sfdpParams_init API in V2/Fls_Nor_config.c file by following the flash datasheet.
Q2. How to enable interrupt mode in Flash?
To enable interrupt mode, FLS_USE_INTERRUPTS should be set to STD_ON. INDAC mode should be enabled in interrupt mode as ospi controller uses SRAM level to trigger interrupt and INDAC mode of operation uses SRAM for data transfer. Also maxReadNormalMode and maxWriteNormalMode should be set to page size of the flash. Further, FLS_ERASE_VERIFICATION_ENABLED,FLS_WRITE_VERIFICATION_ENABLED and FLS_TIMEOUT_SUPERVISION_ENABLED should be disabled in interrupt mode.
4.13.12. Test Report
Please refer AM26x FLS Driver Test Case Report as part of CSP provided in the release package.