4.20. SPI Module
4.20.1. Acronyms and Definitions
Abbreviation/Term |
Explanation |
|---|---|
AUTOSAR |
Automotive Open System Architecture |
BSW |
Basic Software |
MCAL |
Micro Controller Abstraction Layer |
API |
Application Programming Interface |
DET |
Default Error Tracer |
SPI |
Serial Peripheral Interface |
MCU |
Micro Controller Unit |
OS |
Operating System |
SW |
Software |
HW |
Hardware |
4.20.2. Introduction
This document describes MCAL SPI Driver functionality, its application interfaces and configuration details as per AUTOSAR version 4.3.1.
Supported AUTOSAR Release |
4.3.1 |
Supported Configuration Variants |
Post-build, Pre-Compile, Link-Time |
Vendor ID |
SPI_VENDOR_ID (44) |
Module ID |
SPI_MODULE_ID (83) |
Supported Platform |
AM263Px |
4.20.3. Functional Overview
The SPI driver provides services for basic communication with external components. These components can be used by an application.
The main tasks of the SPI are:
Handle data transmission to the components connected via SPI
Take care of the settings required by external components (baud rate etc.)
4.20.3.1. SPI Driver Architecture
The following figure shows where the SPI is located in the AUTOSAR architecture
Fig. 4.90 SPI in AUTOSAR architecture
The next figure shows the interfaces to adjacent modules of the SPI. These interfaces are described in further chapters.
Fig. 4.91 SPI Interfaces
4.20.3.2. Initialization
The SPI driver is initialized by calling Spi_Init(), with parameter ConfigPtr referencing a runtime configuration set. Spi_DeInit() will deinitialize the driver.
4.20.3.3. States
There are 3 states in which the SPI driver can be in.
SPI_UNINIT: The SPI Handler/Driver is not initialized or not usable.
SPI_IDLE : The SPI Handler/Driver is not currently transmitting any Job.
SPI_BUSY : The SPI Handler/Driver is performing a SPI Job (transmit).
So the user knows the ongoing action of the driver during a transmission.
4.20.3.4. Baudrate calculation
SPI Baud Rate Calculation is as follows:
Baud rate = fSPI / CLKD
Where fSPI – SPI Functional clock frequency. fSPI can be set from MCU clocksetting configuration, where user can configure clock source(as per TRM) and clock division value for required fSPI (fSPI=clk/clkdiv+1).
Refer the figure below:
Fig. 4.92 MCU Clock setting in Ebtresos
CLKD – Prescalar clock divider (SpiExtDeviceClockDivider value as per EBtresos Configuration). SpiExtDeviceClockDivider can be set from EBtresos as in below figure:
Fig. 4.93 SpiExtDeviceClockDivider value as per EBtresos Configuration
CLKD value should be set such a way to get the expected baudrate as per calculation below:
For example, if fSPI of MCSPI is 50 MHz:
1.For Baudrate = 50Mbps , CLKD should be given as 0 , calculation will be as following
Baudrate = 50/(0+1) = 50Mbps
2.For Baudrate =25Mbps ,CLKD should be given as 1 , calculation will be as following
Baudrate = 50/(1+1) = 25Mbps
4.20.3.5. Assumptions
For using DMA feature, driver assumes that cache initialization is done in application only and not done by the driver.
4.20.3.6. Limitations
A job queued in a sequence cannot be queued via another sequence. This is a design limitation to reduce driver complexity.
A channel in a job in a sequence cannot be part of another active job or sequence. This is a design limitation to reduce driver complexity.
If a sequence is started, another high priority job belonging to another sequence cannot
interrupt the job belonging to the same hardware unit. But the job can be scheduled ahead of another pending job of the started sequence if it belongs to another HW queue.
4.20.3.7. Design overview
Will be updated in future release:
4.20.4. Hardware Features
4.20.4.1. SPI IP Supported Features
Serial clock with programmable frequency, polarity and phase for each channel
Wide selection of SPI word lengths, ranging from 4 to 32 bits
Each SPI controller operates at up to 50 MHz
SPI0 and SPI4 support 2 chip selects while SPI1, SPI2, and SPI3 support 1 chip select
Interruptible Sequences
Controller multichannel mode
Transmit only/transmit and receive modes
Flexible input/output(I/O) port controls per channel
Programmable clock granularity
Per channel configuration for clock definition, polarity enabling and word width
Enable the addition of a programmable start-bit for MCSPI transfer per channel (start-bit mode)
4.20.4.2. AUTOSAR Supported Features
Spi initilaizes all features required for transmission and reception.
Spi Supports using of internal buffers for transfer and receiving of data
Spi supports asynchronous transmission and reception
Spi supports synchronous transmission and reception.
Spi supports setting of external buffers.
Spi Supports getting the status of
Hwunit
Job Result
Sequence result
Spi Supports setting mode of the communication
Spi Supports cancel of sequence
4.20.4.3. Not supported Features
Slave Mode not supported
4.20.5. Source files
Description of static files is provided below:
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Spi
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┗ 📜Spi.h : Contains the API’s of the SPI driver to be used by upper layers
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┗ 📜Spi.c : Contains the implementation of the API’s for SPI driver
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┣ 📜hw_mcspi.h : Contains Internal functions declaration of SPI driver
┃ ┃ ┃ ┣ 📜lldr_mcspi.h : Contains Register definition
┃ ┃ ┃ ┣ 📜Spi_Dbg.h : Contains Internal functions definition of SPI driver
┃ ┃ ┃ ┣ 📜Spi_Dma.c : Contains SPI MCAL driver functions for using EDMA
┃ ┃ ┃ ┣ 📜Spi_Irq.h : Contains ISR function declaration
┃ ┃ ┃ ┣ 📜Spi_Irq.c : Contains ISR function definitions
┃ ┃ ┃ ┣ 📜Spi_Mcspi.c : Contains Internal functions definition of SPI driver
┃ ┃ ┃ ┣ 📜Spi_Priv.c : Contains Internal functions definition of SPI driver
┃ ┃ ┃ ┣ 📜Spi_Priv.h : Contains Internal functions declaration of SPI driver
┃ ┃ ┃ ┣ 📜Spi_Utils.c : Contains Internal functions definition of SPI driver
┃ ┃ ┃ ┗ 📜Spi_Utils.h : Contains Internal functions declaration of SPI driver
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt
Description of generated files is provided below:
Plugin Files |
Description |
|---|---|
Spi_Cfg.h |
Contains the Precompile switches, Symbolic names of Group, channels and hardware units, Configured maximum number Groups and hardware units |
Spi_PBcfg.c |
Contains all channels Post-Build Configured parameters |
Spi_Lcfg.c |
Contains all channels Link time Configured parameters |
Spi_Cfg.c |
Contains all channels Pre-Compile Configured parameters |
The below diagram shows the files structure for the SPI driver.
Fig. 4.94 SPI header file include structure
4.20.6. Module requirements
Will be updated in future release:
4.20.6.1. Memory Mapping
Memory Mapping Sections |
SPI_CODE |
SPI_VAR |
SPI_VAR_NOINIT |
SPI_CONST |
SPI_APPL_DATA |
SPI_APPL_CODE |
|---|---|---|---|---|---|---|
SPI_START_SEC_VAR_INIT_UNSPECIFIED (.data) |
x |
|||||
SPI_STOP_SEC_VAR_INIT_UNSPECIFIED |
x |
|||||
SPI_START_SEC_CODE (.text) |
x |
|||||
SPI_STOP_SEC_CODE |
x |
|||||
SPI_START_SEC_VAR_NO_INIT_UNSPECIFIED (.bss) |
x |
|||||
SPI_STOP_SEC_VAR_NO_INIT_UNSPECIFIED |
x |
|||||
SPI_START_SEC_CONST_UNSPECIFIED(.rodata) |
x |
|||||
SPI_STOP_SEC_CONST_UNSPECIFIED |
x |
|||||
SPI_START_SEC_ISR_CODE (.text) |
x |
|||||
SPI_STOP_SEC_ISR_CODE |
x |
|||||
For application code used by SPI (like callback functions) |
x |
4.20.6.2. Scheduling
4.20.6.2.1. SchM (Optional)
Beside the OS the BSW Scheduler provides functions that SPI calls at begin and end of critical sections.
Example: SchM_Enter_Spi_SPI_EXCLUSIVE_AREA_0(), SchM_Exit_Spi_SPI_EXCLUSIVE_AREA_0().
4.20.6.2.2. Critical Sections
There is only one kind of critical sections in this driver. Within these sections all read /modify / write accesses to internal SPI driver data structures must be protected. Therefore switching to tasks that also access SPI has to be avoided and all SPI interrupts have to be suspended.
4.20.6.3. Error handling
4.20.6.3.1. Development Error Reporting
The module SPI depends on the DET (by default) in order to report development errors.
The DET can be replaced optionally by an equivalent component which is responsible to recognize development errors, if no DET component is available.
The DET error is reported with Module ID.
The reported service IDs identify the services which are described earlier.
The following table represents the service IDs:
Service ID |
Service |
|---|---|
SPI_SID_INIT = 0x00 |
Spi_Init |
SPI_SID_DEINIT = 0x01 |
Spi_DeInit |
SPI_SID_WRITEIB = 0x02 |
Spi_WriteIB |
SPI_SID_ASYNCTRANSMIT = 0x03 |
Spi_AsyncTransmit |
SPI_SID_READIB = 0x04 |
Spi_ReadIB |
SPI_SID_SETUPEB = 0x05 |
Spi_SetupEB |
SPI_SID_GETSTATUS = 0x06 |
Spi_GetStatus |
SPI_SID_GETJOBRESULT = 0x07 |
Spi_GetJobResult |
SPI_SID_GETSEQUENCERESULT = 0x08 |
Spi_GetSequenceResult |
SPI_SID_GETVERSIONINFO = 0x09 |
Spi_GetVersionInfo |
SPI_SID_SYNCTRANSMIT = 0x0A |
Spi_SyncTransmit |
SPI_SID_GETHWUNITSTATUS = 0x0B |
Spi_GetHwUnitStatus |
SPI_SID_CANCEL = 0x0C |
Spi_Cancel |
SPI_SID_SETASYNCMODE = 0x0D |
Spi_SetAsyncMode |
SPI_SID_MAINFUNCTION_HANDLING = 0x10 |
Spi_MainfunctionHandling |
4.20.6.4. Error codes
4.20.6.4.1. Development Errors
The errors reported to DET module are described in the following table:
Type of Error |
Related Error code |
Value (Hex) |
|---|---|---|
Channel out of bounds, exceeds the maximum number of configured channels |
SPI_E_PARAM_CHANNEL |
0x0A |
Job out of bounds, exceeds the maximum number of configured jobs |
SPI_E_PARAM_JOB |
0x0B |
Sequence out of bounds, exceeds the maximum number of configured sequences |
SPI_E_PARAM_SEQ |
0x0C |
Length out of bounds, exceeds the maximum number of configured EB- or IB- buffer length |
SPI_E_PARAM_LENGTH |
0x0D |
The requested hardware unit does not exist |
SPI_E_PARAM_UNIT |
0x0E |
An invalid configuration has been passed (i.e., a NULL_PTR).This is an extension to AUTOSAR. |
SPI_E_PARAM_POINTER |
0x10 |
A service was requested, but the driver has not been initialized |
SPI_E_UNINIT |
0x1A |
The requested sequence is still pending |
SPI_E_SEQ_PENDING |
0x2A |
Transmission of synchronous sequence in progress (not supported) |
SPI_E_SEQ_IN_PROCESS |
0x3A |
The driver is already initialized |
SPI_E_ALREADY_INITIALIZED |
0x4A |
AUTOSAR requires to check the validity of function parameters. These checks are for development error reporting and can be en/dis-abled separately. En/dis-abling of single checks is an addition to the AUTOSAR standard which requires to en/dis-able the complete parameter checking via the parameter SPI_DEV_ERROR_DETECT. The following table shows which parameter checks are performed on which services:
Check Services |
SPI_E_PARAM_CHANNEL |
SPI_E_PARAM_JOB |
SPI_E_PARAM_SEQ |
SPI_E_PARAM_LENGTH |
SPI_E_PARAM_UNIT |
SPI_E_PARAM__POINTER |
SPI_E_PARAM_UNINIT |
SPI_E_SEQ_PENDING |
SPI_E_SEQ_PROCESS |
SPI_E_ALREADY_INITILAIZE |
|---|---|---|---|---|---|---|---|---|---|---|
Spi_Init |
x |
x |
x |
x |
x |
|||||
Spi_DeInit |
x |
|||||||||
Spi_AsyncTransmit |
x |
x |
x |
|||||||
Spi_SetupEB |
x |
x |
x |
x |
||||||
Spi_GetStatus |
||||||||||
Spi_GetJobResult |
x |
x |
||||||||
Spi_GetSequenceResult |
x |
x |
||||||||
Spi_GetVersionInfo |
x |
|||||||||
Spi_GetHwUnitStatus |
x |
x |
||||||||
Spi_Cancel |
x |
x |
4.20.6.4.2. DEM Errors
The errors reported to DEM are described in the following table:
Error Code |
Error Macro |
Description |
|---|---|---|
Assigned by DEM |
SPI_E_HARDWARE_ERROR |
This error is raised when McSPI RX FIFO overflows |
Assigned by DEM |
SPI_E_BIT_ERROR |
A bit error was detected |
Assigned by DEM |
SPI_E_DESYNC_ERROR |
Slave desynchronized |
Assigned by DEM |
SPI_E_DLEN_ERROR |
Data length mismatch detected during transmission |
Assigned by DEM |
SPI_E_TXSTALL_ERROR |
This error occurs if the driver tries to write data which has not been transmitted yet |
Assigned by DEM |
SPI_E_RXSTALL_ERROR |
The driver tries to read data, but no data has been provided by the hardware |
Assigned by DEM |
SPI_E_DOVR_ERROR |
The hardware reported an internal receive buffer overrun |
Assigned by DEM |
SPI_E_TO_ERROR |
The hardware reported a Timeout error because of non-activation of ENA pin |
4.20.7. Used resources
4.20.7.1. Interrupt Handling
For interrupt notification, ISR’s are provided in SPI driver. There are two ISR for each SPI hardware unit. Depending on hardware unit configured, it will call group notify function. The interrupt service routines shall be mapped to the interrupt sources of the respective cross bar interrupt. The supported ISR’s are part of the Spi_Irq.h file.
Following are SPI module ISRs for each hardware unit:
1.SPI HW UNIT 0
Spi_IrqUnitMcspi0TxRx()
ISR(Spi_IrqUnitMcspi0TxRx)
2.SPI HW UNIT 1
Spi_IrqUnitMcspi1TxRx()
ISR(Spi_IrqUnitMcspi1TxRx)
3.SPI HW UNIT 2
Spi_IrqUnitMcspi2TxRx()
ISR(Spi_IrqUnitMcspi2TxRx)
4.SPI HW UNIT 3
Spi_IrqUnitMcspi3TxRx()
ISR(Spi_IrqUnitMcspi3TxRx)
5.SPI HW UNIT 4
Spi_IrqUnitMcspi4TxRx()
ISR(Spi_IrqUnitMcspi4TxRx)
6.SPI HW UNIT 5
Spi_IrqUnitMcspi5TxRx()
ISR(Spi_IrqUnitMcspi5TxRx)
7.SPI HW UNIT 6
Spi_IrqUnitMcspi6TxRx()
ISR(Spi_IrqUnitMcspi6TxRx)
8.SPI HW UNIT 7
Spi_IrqUnitMcspi7TxRx()
ISR(Spi_IrqUnitMcspi7TxRx)
For using SPI wth DMA mode, register CDD_EDMA_lld_transferCompletionMasterIsrFxn with appropriate INTAGG line.
4.20.8. Integration description
4.20.8.1. Dependent modules
4.20.8.1.1. MCU
The module MCU powers up the microcontroller’s peripherals at startup time and initializes the PLL and the internal clock domains which go to the SPI unit. The SPI module also supports an internal divider which can be changed at configuration time using the ‘clkDivider’ member of Spi_McSPIExternalDeviceConfigType structure to configure the actual SPI functional clock.
4.20.8.1.2. PORT
The module PORT enables the SPI lines at startup time. To operate the SPI properly, the PORT driver must be configured. The PORT driver sets the PINs to the required mux values for the SPI to operate.
4.20.8.1.3. OSEK / AUTOSAR OS (Optional)
An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table. The SPI module may use OSEK/AUTOSAR OS to suspend and restore global interrupts.
4.20.8.1.4. DET
This implementation depends on the DET in order to report development errors. The detection of development errors is configurable (ON / OFF).
4.20.8.1.5. DEM
By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus ().
Note
Dem Event is enable only if $(Module_Name)DemEventParameterRefs is enabled.
4.20.8.1.6. Callback Functions
The SPI driver does not provide any call back functions.
4.20.8.1.7. Callback Notification
At its configurable interfaces, the SPI defines notifications that can be mapped to callback functions provided by other modules. The mapping is not statically defined by the SPI but can be performed at configuration time. The function prototypes that can be used for the configuration have to match the appropriate function prototype signatures, which are described in the following.
Example:Spi_JobEndNotification:
4.20.8.2. Multi-core and Resource allocator
Not Supported
4.20.9. Configuration
4.20.9.1. Configuration Variants
The SPI can be configured as Post-Build or Pre-Compile or Link-time variant, using EB tresos tool.
Variants |
Generated Files |
|---|---|
PostBuild |
Spi_PBcfg.c , Spi_Cfg.h |
Link-time |
Spi_Lcfg.c , Spi_Cfg.h |
Pre-Compile |
Spi_Cfg.c , Spi_Cfg.h |
4.20.9.2. Parameter Description
4.20.9.2.1. Standard Configuration
Standard Parameters |
Description |
Default Value |
Range |
Unit |
|---|---|---|---|---|
SPI_E_HARDWARE_ERROR |
Reference to configured DEM event to report “Hardware failure”. If the reference is not configured the error shall not be reported. |
NA |
ASPathDataOfSchema:/AUTOSAR/EcucDefs/Dem/DemConfigSet/DemEventParameter |
Reference |
SpiMaxChannel |
This parameter contains the number of Channels configured. It will be gathered by tools during the configuration stage. |
24 |
1..255 |
Integer |
SpiMaxJob |
Total number of Jobs configured. |
10 |
1–65535 |
Integer |
SpiMaxSequence |
Total number of Sequences configured. |
10 |
1..255 |
Integer |
SpiChannelId |
SPI Channel ID, used as parameter in SPI API functions. |
0 |
0..255 |
Integer |
SpiChannelType |
Buffer usage with EB/IB channel. |
EB |
EB IB |
Enumeration |
SpiDataWidth |
This parameter is the width of a transmitted data unit. |
8 |
1..32 |
Integer |
SpiDefaultData |
The default data to be transmitted when (for internal buffer or external buffer) the pointer passed to Spi_WriteIB (for internal buffer) or to Spi_SetupEB (for external buffer) is NULL. |
0 |
0..4294967295 |
Integer |
SpiEbMaxLength |
This parameter contains the maximum size (number of data elements) of data buffers in case of EB Channels and only. |
255 |
0..65535 |
Integer |
SpiIbNBuffers |
This parameter contains the maximum number of data buffers in case of IB Channels and only. |
10 |
0..65535 |
Integer |
SpiTransferStart |
This parameter defines the first starting bit for transmission. |
MSB |
LSB MSB |
Enumeration |
SpiBaudrate |
This parameter is the communication baudrate - This parameter allows |
500 |
0..INF |
Float |
SpiCsIdentifier |
This parameter is the symbolic name to identify the Chip Select (CS) allocated to this Job (CS0 to CS3). |
SCS0 |
– |
String |
SpiCsPolarity |
This parameter defines the active polarity of Chip Select. |
HIGH |
LOW HIGH |
Enumeration |
SpiCsSelection |
When the Chip select handling is enabled (see SpiEnableCs), then this parameter specifies if the chip select is handled automatically by Peripheral HW engine or via general purpose IO by Spi driver. |
CS_VIA_PERIPHERAL_ENGINE |
CS_VIA_GPIO CS_VIA_PERIPHERAL_ENGINE |
Enumeration |
SpiDataShiftEdge |
This parameter defines the SPI data shift edge. |
LEADING |
LEADING TRAILING |
Enumeration |
SpiEnableCs |
This parameter enables or not the Chip Select handling functions. If this parameter is enabled then parameter SpiCsSelection further details the type of chip selection. |
TRUE |
TRUE/ FALSE |
Boolean |
SpiHwUnit |
This parameter is the symbolic name to identify the HW SPI Hardware |
CSIB0 |
CSIB0 CSIB1 CSIB2 CSIB3 CSIB4 |
Enumeration |
SpiShiftClockIdleLevel |
This parameter defines the SPI shift clock idle level. |
LOW |
LOW HIGH |
Boolean |
SpiTimeClk2Cs |
Timing between clock and chip select (in seconds) - This parameter allows to use a range of values from 0 up to 0.0001 seconds. |
0.0001 |
0.0 .. 1.0E-4 |
Float |
SpiHwUnitSynchronous |
If SpiHwUnitSynchronous is set to “SYNCHRONOUS”,the SpiJob uses its containing SpiDriver in a synchronous manner. If it is set to “ASYNCHRONOUS”, it uses the driver in an asynchronous way. If the parameter is not set, the SpiChannel uses the driver also in an asynchronous way. |
ASYNCHRONOUS |
ASYNCHRONOUS SYNCHRONOUS |
Enumeration |
SpiJobEndNotification |
This parameter is a reference to a notification function. |
NULL_PTR |
NA |
Function |
SpiJobId |
SPI Job ID, used as parameter in SPI API functions. |
NA |
0..65535 |
Integer |
SpiJobPriority |
Priority set accordingly to SPI093: 0, lowest, 3, highest priority |
3 |
0..3 |
Integer |
SpiDeviceAssignment |
Reference to the external device used by this job |
NA |
ASPathDataOfSchema:/AUTOSAR/EcucDefs/Spi/SpiDriver/SpiExternalDevice |
Reference |
SpiChannelIndex |
This parameter specifies the order of Channels within the Job. |
0 |
0..255 |
Integer |
SpiChannelAssignment |
A job reference to a SPI channel. |
NA |
ASPathDataOfSchema:/AUTOSAR/EcucDefs/Spi/SpiDriver/SpiChannel |
Reference |
SpiInterruptibleSequence |
This parameter allows or not this Sequence to be suspended by another one. |
TRUE |
TRUE/ FALSE |
Boolean |
SpiSeqEndNotification |
This parameter is a reference to a notification function. |
NULL_PTR |
NA |
Function |
SpiSequenceId |
SPI Sequence ID, used as parameter in SPI API functions. |
NA |
0..255 |
Integer |
SpiJobAssignment |
A sequence references several jobs, which are executed during a communication sequence |
NA |
ASPathDataOfSchema:/AUTOSAR/EcucDefs/Spi/SpiDriver/SpiJob |
Reference |
SpiCancelApi |
Switches the Spi_Cancel function ON or OFF. |
TRUE |
TRUE/ FALSE |
Boolean |
SpiChannelBuffersAllowed |
Selects the SPI Handler/Driver Channel Buffers usage allowed |
2 |
0..2 |
Integer |
SpiDevErrorDetect |
Switches the Development Error Detection and Notification ON or OFF. |
TRUE |
TRUE/ FALSE |
Boolean |
SpiHwStatusApi |
Switches the Spi_GetHWUnitStatus function ON or OFF. |
TRUE |
TRUE/ FALSE |
Boolean |
SpiInterruptibleSeqAllowed |
Switches the Interruptible Sequences handling functionality ON or OFF. |
TRUE |
TRUE/ FALSE |
Boolean |
SpiLevelDelivered |
Selects the SPI Handler/Driver level of scalable functionality: SYNC ONLY(0), ASYNC ONLY (1), SYNC/ASYNC(2) |
2 |
0..2 |
Integer |
SpiMainFunctionPeriod |
This parameter defines the cycle time of the function Spi_MainFunction_Handling in seconds. |
0.01 |
0..INF |
Float |
SpiSupportConcurrentSyncTransmit |
Specifies whether concurrent Spi_SyncTransmit() calls for different sequences shall be configurable. |
FALSE |
TRUE/ FALSE |
Boolean |
SpiUserCallbackHeaderFile |
Header file name which will be included by the Spi. The value of this parameter shall be used as h-char-sequence or q-char-sequence according to ISO C90 section 6.10.2 “source file inclusion”. |
FALSE |
TRUE/ FALSE |
Boolean |
SpiVersionInfoApi |
Switches the Spi_GetVersionInfo function ON or OFF. |
TRUE |
TRUE/ FALSE |
Boolean |
SpiMaxHwUnit |
Number of different SPI hardware microcontroller peripherals (units/busses) available and handled by this SPI Handler/Driver module. |
8 |
1..8 |
Integer |
Standard Parameters |
Description |
Default Value |
Range |
Unit |
|---|---|---|---|---|
SpiMaxHwUnit |
Maximum number of HW unit |
8 |
1..8 |
Integer |
SpiMaxExternalDeviceConfig |
Maximum Number of different SPI hardware microcontroller peripherals available and handled by this SPI Handler/Driver module.Max range is derived from SpiMaxExternalDevices. |
8 |
1..8 |
Integer |
SpiExternalDeviceId |
The index of the corresponding external device config associated with job. |
NA |
0..65535 |
Integer |
SpiCsMode |
This selects which CS mode the device should enter. SPI_SINGLE: the CS will return to default level after one transmission unit has been sent. SPI_CONTINUOUS: the CS will remain active during the whole transmission. |
SPI_CONTINUOUS |
SPI_SINGLE SPI_CONTINUOUS |
Enumeration |
SpiCsIdleTime |
CS idle time (Timing between clock and chip select) if single mode is chosen. |
SPI_DATADELAY_0 |
SPI_DATADELAY_0 SPI_DATADELAY_1 SPI_DATADELAY_2 SPI_DATADELAY_3 |
Enumeration |
SpiExtDeviceClockDivider |
Clock divider. This is used to derive the required baudrate from the QSPI functional clock. |
0 |
0..65535 |
Integer |
SpiExtDeviceMCSPITxRxMode |
TX and RX mode. Data is transmitted (shifted out serially on SPIDAT[0]) and received (shifted in serially on SPIDAT[1]) simultaneously on separate data lines.Tx only mode - Data is only transmiited (shifted out serially on SPIDAT). |
SPI_TX_RX_MODE_BOTH |
SPI_TX_RX_MODE_BOTH SPI_TX_RX_MODE_TX_ONLY |
Enumeration |
SpiExtDeviceMCSPIStartBitEnable |
Start bit D/CX added before SPI transfer. Polarity is defined by StartBitLevel |
TRUE |
TRUE/ FALSE |
Boolean |
SpiExtDeviceMCSPIStartBitLevel |
Start-bit polarity used when startBitEnable is TRUE. |
SPI_LOW |
SPI_LOW SPI_HIGH |
Enumeration |
SpiExtDeviceMCSPIDataLineSelectReception |
Data Line 0 or 1 selected for reception |
DATA_LINE_0_RECEPTION |
DATA_LINE_0_RECEPTION DATA_LINE_1_RECEPTION |
Enumeration |
SpiExtDeviceMCSPIDataLineSelectTransmission |
Data Line 0 or 1 or both selected for transmission.No transmission on data lines if DATA_LINE_NO_TRANSMISSION is selected |
DATA_LINE_1_TRANSMISSION |
DATA_LINE_NO_TRANSMISSION DATA_LINE_0_TRANSMISSION DATA_LINE_1_TRANSMISSION DATA_LINE_BOTH_TRANSMISSION |
Enumeration |
SpiHwUnitAssignment |
Reference to the HW unit used by this job |
NA |
ASPathDataOfSchema:/TI_AM263Px/Spi/SpiDriver/SpiHwUnitConfig |
Reference |
SpiHwUnitType |
SPI HW unit to use |
SPI_UNIT_MCSPI0 |
SPI_UNIT_MCSPI0 SPI_UNIT_MCSPI1 SPI_UNIT_MCSPI2 SPI_UNIT_MCSPI3 SPI_UNIT_MCSPI4 SPI_UNIT_MCSPI5 SPI_UNIT_MCSPI6 SPI_UNIT_MCSPI7 |
Enumeration |
SpiHwUnitDmaEnable |
Enables DMA support for MCSPI instance |
FALSE |
TRUE FALSE |
BOOLEAN |
SpiHwUnitCddDmaTxHandler |
References the CDD DMA handler used for MCSPI transmission |
NA |
ASPathDataOfSchema:/TI_AM263Px/Cdd_Dma/CddDmaDriverHandler |
Reference |
SpiHwUnitCddDmaRxHandler |
References the CDD DMA handler used for MCSPI reception |
NA |
ASPathDataOfSchema:/TI_AM263Px/Cdd_Dma/CddDmaDriverHandler |
Reference |
SpiEnableJobLog |
Enable/disable SPI job log |
TRUE |
TRUE FALSE |
Boolean |
SpiMaxExternalDevices |
Number of different SPI hardware microcontroller peripherals (units/busses) available and handled by this SPI Handler/Driver module. |
8 |
1..8 |
Integer |
SpiMaxJobLogLength |
Maximum job log entries when logging is ON |
100 |
1.65535 |
Integer |
SpiMaxTimeoutDuration |
Maximum time duration for SPI transmission.Unit is clock ticks. |
10000 |
1..4294967295 |
Integer |
SpiMaxChannelsPerJob |
Maximum channels allowed per job |
4 |
1..255 |
Integer |
SpiMaxJobsPerSequence |
Maximum jobs allowed per sequence |
4 |
1..255 |
Integer |
SpiMaxChannels |
Maximum channels across all jobs/sequence/hwunit |
24 |
1..255 |
Integer |
SpiMaxJobs |
Maximum jobs across all sequence/hwunit |
10 |
1..65535 |
Integer |
SpiMaxSequences |
Maximum sequence across all hwunit |
10 |
1..255 |
Integer |
SpiIrqType |
Type of Isr function: void functionname(void) 1.CAT1 : interrupt void func(void) 2.CAT2 : ISR(func) |
SPI_ISR_CAT2 |
SPI_ISR_VOID SPI_ISR_CAT1 SPI_ISR_CAT2 |
Enumeration |
SpiDefaultOSCounterId |
Default Os Counter Id if node reference to OsCounter ref SpiOsCounterRef is not set |
0 |
0..16 |
Integer |
SpiOsCounterRef |
This parameter contains a reference to the OsCounter, which is used by the SPI driver. |
NA |
/AUTOSAR/EcucDefs/Os/OsCounter |
Reference |
SpiTimeoutDuration |
SPI timeout - used in SPI busy wait |
32000 |
1..4294967295 |
Integer |
SpiRegisterReadbackApi |
Specifies whether RegisterReadback API is enabled |
TRUE |
TRUE FALSE |
Boolean |
SpiSafetyApi |
Enable API to do safety diagnostic |
TRUE |
TRUE FALSE |
Boolean |
SpiChannelInternalBufferMaxLength |
Internal Buffer length in bytes - applicable for SpiChannelBuffer type - SPI_IB. This is the maximum length that can be allocated by each channel and it is fixed.Can vary buffer length per channel by configuring SpiIbNBuffers and SpiDataWidth. |
64 |
1..4294967295 |
Integer |
SpiDeviceVariant |
Select SOC variant |
AM263Px |
AM263Px |
Enumeration |
SpiHwUnitEnabledFlag |
Group configurations |
SPI_HWUNIT_MCSPI0 |
SPI_HWUNIT_MCSPI0 SPI_HWUNIT_MCSPI1 SPI_HWUNIT_MCSPI2 SPI_HWUNIT_MCSPI3 SPI_HWUNIT_MCSPI4 SPI_HWUNIT_MCSPI5 SPI_HWUNIT_MCSPI6 SPI_HWUNIT_MCSPI7 |
Enumeration |
Note
SpiTimeoutDuration and SpiMaxTimeoutDuration parameter value should be passed as number of ticks according to clock frequency. The clock source have changed from RTI timers which used 200MHz clock frequency to R5f timers which uses 400MHz clock frequency, so the timeout values need to be configured accordingly.
4.20.9.3. Symbolic Names deviations
None
4.20.9.4. Configuration rules and constraints to enable plausibility checks
SPI DMA Tx and Rx Handler should be configured to match Channel IDs with the EDMA TRIG XBAR MODULE number selected with appropriate CDD DMA channel trigger source selected from the dropdown as per the instance. Channel crossbar and channel crossbar map can be left to default as SPI driver doesn’t make use of those parameters.
Fig. 4.95 CDD DMA Crossbar configuration matching Channel ID for SPI Handle
4.20.10. Examples
4.20.10.1. Overview
Will be updated in future release:
4.20.10.2. Setup required to run example
Will be updated in future release:
4.20.10.3. How to run examples
4.20.10.3.1. Steps to build and run example
Spi example application demonstrating the MCAL SPI driver features is in folder <MCAL_ROOT>/examples/Spi.
This application can be built from the root folder by giving gmake –s mcspi_app PLATFORM=am263px.
Then launch TI Code Composer Studio (CCS) and connect the Board with it using an appropriate target configuration, load the application binary in to R5_0 core and execute the binary.
4.20.10.3.2. Document external set up Information
None
4.20.10.3.3. Flow of the example application
In example application,the status of spi is checked,whether it is idle or busy.
After checking the status,it sets the external buffer as per requirement.
Then the mode of transmission is set and post that async transmission takes place with loopback enable.
After the transmission is completed,the recieve and transmit data is compared and the datas should be same.
4.20.10.3.4. Configuration used to test this example
The example application is configured with the following Parametrs:
Max Channels :10U
Max channels per Sequence :4U
Max Jobs per seq:4U
Max HwUnit :8U
Max External Devices:8U
Channel BufferType :SPI_EB
Maximum Buffer Length :1120U
Transfer Type :SPI_MSB
Mode of Transmission:Asynchronous
Method of Testing :Loopback
4.20.10.3.4.1. Program changes with DMA mode
For DMA mode support, DMA TPCC0 Interrupt aggregation (INTR) line number 72 gets used to register ISR with EDMA and Cache write back for source buffer before data transmission as well as Cache invalidation before validating destination buffers should happen using respective Mcal_CacheP_wb and Mcal_CacheP_inv APIs.
4.20.10.4. Sample Log
SPI_APP: Variant - Post Build being used !!!
SPI_APP
: Sample Application - STARTS !!!
SPI MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 83
SW Major Version : 9
SW Minor Version : 1
SW Patch Version : 0
SPI_APP: CH 10: JOBS 4: SEQ 3: HWUNIT 8: NUM OF WORDS 1120:!!!
SPI_APP: SPI Async transmit in progress!!
SPI_APP: SPI Loopback Test Passed!!!
SPI Stack Usage: 1000 bytes
4.20.10.5. File Structure
📦AM263Px
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Spi
┃ ┃ ┃ ┣ 📂mcspi_app
┃ ┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📜McspiApp.c : Contains the SPI test example for McSPI
┃ ┃ ┃ ┃ ┣ 📜McspiApp.h : Contains McSPI example header file
┃ ┃ ┃ ┃ ┗ 📜Makefile
┃ ┃ ┃ ┣ 📂mibspi_app
┃ ┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📜MibspiApp.c : Contains the SPI test example for MibSPI
┃ ┃ ┃ ┃ ┣ 📜MibspiApp.h : Contains MiBSPI example header file
┃ ┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Spi_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263px
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Spi_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Spi_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Spi_Lcfg.c : Contains all Link time configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗ 📜Spi_PBcfg.c : Contains all Post build configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt
4.20.10.6. Test Report
Please refer AM26x SPI Driver Test Case Report as part of CSP provided in the release package.