5. API Description
5.1. Table of Content
5.2. ADC
5.3. CAN
5.4 CDD DMA
5.5 CDD FSIRX
5.6 CDD FSITX
5.7. CDD I2C
5.8. CDD IPC
5.9 CDD PWM
5.10 CDD UART
5.11 DIO
5.12 ETH
5.13 ETHTRCV
5.14 FLS
5.15 GPT
5.16 ICU
5.17 LIN
5.18 MCU
5.19 PORT
5.20 PWM
5.21 SPI
5.22 WDG
5.2. ADC
5.2.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.2.2. API’s with Service ID
The following table presents the service IDs and the related services:
Service ID |
Autosar API’s Supported |
Autosar API’s not Supported |
|---|---|---|
0x00 |
Adc_Init |
|
0x01 |
Adc_DeInit |
|
0x02 |
Adc_StartGroupConversion |
|
0x03 |
Adc_StopGroupConversion |
|
0x04 |
Adc_ReadGroup |
|
0x05 |
Adc_EnableHardwareTrigger |
|
0x06 |
Adc_DisableHardwareTrigger |
|
0x07 |
Adc_EnableGroupNotification |
|
0x08 |
Adc_DisableGroupNotification |
|
0x09 |
Adc_GetGroupStatus |
|
0x0A |
Adc_GetVersionInfo |
|
0x0B |
Adc_GetStreamLastPointer |
|
0x0C |
Adc_SetupResultBuffer |
|
0x20 |
IoHwAb_AdcNotification |
|
0x10 |
Adc_SetPowerState |
|
0x11 |
Adc_GetCurrentPowerState |
|
0x12 |
Adc_GetTargetPowerState |
|
0x13 |
Adc_PreparePowerState |
|
0x14 |
Adc_Main_PowerTransitionManager |
|
0x15 |
Adc_PollingMainFunction |
|
0x70 |
IoHwAb_Adc_NotifyReadyForPowerState |
Refer Autosar SWS for API description mentioned in above table.
5.2.3. Description on Non Standard API’s
Adc_PollingMainFunction
This function will used when Group is in Polling mode.
Adc_RegisterReadback API
This function is Non- Autosar based and is used to read the data in the registers of ADC.
This functionality is enabled, if parameter AdcEnableRegisterReadbackApi is TRUE (The Parameter sets ADC_REGISTER_READBACK_API Macro as STD_ON ).
Service Id is 0x16.
Adc_InitTemperatureRead
This API not applicable for AM263.
Adc_ReadTemperature
This API not applicable for AM263.
Adc_ReadTemperatureResult
This API not applicable for AM263.
5.3. CAN
5.3.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.3.2. API’s with Service ID
The following table presents the service IDs and the related services:
Service ID |
Service |
|---|---|
0x00 |
Can_Init |
0x01 |
Can_MainFunction_Write |
0x03 |
Can_SetControllerMode |
0x04 |
Can_DisableControllerInterrupts |
0x05 |
Can_EnableControllerInterrupts |
0x06 |
Can_Write |
0x07 |
Can_GetVersionInfo |
0x08 |
Can_MainFunction_Read |
0x09 |
Can_MainFunction_BusOff |
0x0A |
Can_MainFunction_Wakeup |
0x0B |
Can_CheckWakeup |
0x0C |
Can_MainFunction_Mode |
0x0F |
Can_SetBaudrate |
0x10 |
Can_DeInit |
0x11 |
Can_GetControllerErrorState |
0x12 |
Can_GetControllerMode |
0x14 |
Can_TestLoopBackModeEnable |
0x15 |
Can_TestLoopBackModeDisable |
5.3.3. Description on Non Standard API’s
Can_TestLoopBackModeEnable API–This function is non-autosar based and is used to enable the CAN loopback.
Can_TestLoopBackModeDisable API–This function is non-autosar based and is used to disable the CAN loopback.
5.4. CDD DMA
5.4.1. Description of the API’s
API SERVICE |
DESCRIPTION |
|---|---|
Cdd_Dma_Init |
Service is used for initialization of the module. |
Cdd_Dma_DeInit |
Service to de-initialize the module. With this call all handlers registered are de-initialized. |
Cdd_Dma_GetInitStatus |
Service to provide the initialization status of the module. |
Cdd_Dma_CbkRegister |
Service to register callback function for a TCC. And this callback will be called once transfer completion happens for that particular TCC associated with the handle. |
Cdd_Dma_ParamSet |
Service to set the paramSet value with the param value associated with the channel of a particular handle.Here length of the transmission and how the data should be transferred is configured. |
Cdd_Dma_LinkChannel |
Service to link the params. Ofter used to link different params within the channel.With this functionality once the paramSet got empty after the transfer linked paramSet will be automatically loaded. |
Cdd_Dma_ChainChannel |
Service to chain multiple channels and used in transmission with one trigger.So when we chain multiple channels then with a single trigger it will transfer from both channels. |
Cdd_Dma_EnableTransferRegion |
Service to enable the trigger for transmission. Can be event based or manual. |
Cdd_Dma_GetStatus |
Service to Read the status of the transfer. Used in case of polling.In case of polling mode we need to continue poll this service in order to know the status of the transfer. |
Cdd_Dma_GetVersionInfo |
Service to get version information |
Cdd_Dma_GetParam |
Service to get the paramSet value with the param value associated with the channel of a particular handle.Here remaining data to be transferred is returned. |
Cdd_Dma_DisableTransferRegion |
Service to disable the trigger for transmission. Can be event based or manual. |
5.4.2. API’s with Service ID
Service ID |
Service |
|---|---|
0x01 |
Cdd_Dma_Init |
0x02 |
Cdd_Dma_DeInit |
0x0A |
Cdd_Dma_GetInitStatus |
0x03 |
Cdd_Dma_CbkRegister |
0x04 |
Cdd_Dma_ParamSet |
0x05 |
Cdd_Dma_LinkChannel |
0x06 |
Cdd_Dma_ChainChannel |
0x07 |
Cdd_Dma_EnableTransferRegion |
0x08 |
Cdd_Dma_GetStatus |
0x09 |
Cdd_Dma_GetVersionInfo |
0x0B |
Cdd_Dma_GetParam |
0x0C |
Cdd_Dma_DisableTransferRegion |
5.4.3. Description on Non Standard API’s
None
5.5. CDD FSIRX
5.5.1. Description of the CDD FSI RX API’s
All below mentioned API’s are user accessible and can be found in Cdd_FsiRx.c file
5.5.1.1. FUNC(void, CDD_FSIRX_CODE) Cdd_FsiRx_Init(P2CONST(Cdd_FsiRx_ConfigType, AUTOMATIC, CDD_FsiRx_CFG) ConfigurationPtr)
Argument passed to the function is ConfigurationPtr.
Function returns void
Function initializes configuration Parameters to default values.
5.5.1.2. FUNC(void, CDD_FSIRX_CODE) Cdd_FsiRx_DeInit(void)
Function used to de-initialize all initialized Fsi Rx Hardware Units
Function returns void
Function can not be called in case driver is uninitialized
5.5.1.3. Cdd_FsiRx_GetVersionInfo(P2VAR(Std_VersionInfoType, AUTOMATIC, CDD_FsiRx_APPL_DATA) VersionInfoPtr)
Argument passed to the function is a valid pointer of type Std_VersionInfoType
Function stores Version information in pointer
Function returns void
5.5.1.4. FUNC(void, CDD_FSIRX_CODE) Cdd_FsiRx_setUpBuffer(Cdd_FsiRx_HWUnitType hwUnitId, P2VAR( CddFsiRxDataBufferType, AUTOMATIC, CDD_FSI_RX_APPL_DATA) DataBufferPtr,CddFsiRx_DataLengthType RxDataLength)
Argument passed to the function are:
hwUnitId:Tx instance which Transmits.
DataBufferPtr: Pointer to the Data Buffer to which data has to be copied RxDataLength:Number of words in each Frame.
Function copies data from the source pointer to internal Transmit buffer of Fsi Tx instance.
Function returns E_OK/E_NOT_OK.
5.5.1.5. FUNC(void, CDD_FSIRX_CODE) Cdd_FsiRx_MainFunction(void)
The API is used in Polling Mode only.
The main function API Polls whether the reception status flags are set for each instance to ensure the data reception.
Function returns void.
5.5.1.6. FUNC(void, CDD_FSIRX_CODE) Cdd_FsiRx_Reset(Cdd_FsiRx_HWUnitType hwUnitId, VAR(Cdd_FsiRx_ResetSubModuleType, AUTOMATIC) ResetModule)
Argument passed to the function are:
hwUnitId:Tx instance which Transmits.
ResetModule: This argument specifies where the reset happens. Example:, Main Core Reset, Ping Watchdog Reset,Frame Watchdog Reset
Function initiates the reset of the particular module of Rx instance or the main core.
Function returns void.
5.5.1.7. FUNC(void, CDD_FSIRX_CODE) Cdd_FsiRx_DmaDataReceive(Cdd_FsiRx_HWUnitType hwUnitId)
Argument passed to the function are: hwUnitId:Tx instance which Transmits.\
Function transfers received data from Rx internal buffer to corresponding application buffer by using DMA.
Function returns void
5.5.1.8. FUNC(CddFsiRx_StatusType, CDD_FSIRX_CODE) CddFsiRx_GetStatus(void)
This service gets the status if FsiRx driver.
Function returns driver status:
CDD_FSI_RX_UNINIT: The Rx module has not initialized yet
CDD_FSI_RX_INIT: The Rx module has initialized
CDD_FSI_RX_IDLE: The reception through the Rx channel hasn’t started
CDD_FSI_RX_BUSY: The frame reception has been started and is still going on
CDD_FSI_RX_COMPLETED: The current reception has been completed
5.5.2. CDD FSI RX API’s with Service ID
The following table presents the service IDs and the related services: CDD FSI RX API’s Supported:
Service ID |
Service |
|---|---|
0x01 |
Cdd_FsiRx_Init |
0x02 |
Cdd_FsiRx_GetVersionInfo |
0x03 |
Cdd_FsiRx_MainFunction |
0x04 |
Cdd_FsiRx_DeInit |
0x05 |
CddFsiRx_GetStatus |
0x06 |
Cdd_FsiRx_Reset |
0x07 |
Cdd_FsiRx_SetUpBuffer |
0x08 |
Cdd_FsiRx_DmaDataReceive |
5.6. CDD FSITX
5.6.1. Description of the CDD FSI TX API’s
All below mentioned API’s are user accessible and can be found in Cdd_FsiTx.c file
5.6.1.1. FUNC(void, CDD_FSITX_CODE) Cdd_FsiTx_Init(P2CONST(Cdd_FsiTx_ConfigType, AUTOMATIC, CDD_FsiTx_CFG) ConfigurationPtr)
Argument passed to the function is ConfigurationPtr.
Function returns void
Function is used to initialize all configured hardware units at specified frequencies.
Function initializes configuration Parameters to default values.
5.6.1.2. FUNC(void, CDD_FSITX_CODE) Cdd_FsiTx_DeInit(void)
Function used to de-initialize all initialized Fsi Tx Hardware Units
Function returns void
Function can not be called in case driver is uninitialized
5.6.1.3. FUNC(void, CDD_FSITX_CODE) Cdd_FsiTx_GetVersionInfo(P2VAR(Std_VersionInfoType, AUTOMATIC, CDD_FSI_TX_APPL_DATA) VersionInfoPtr)
Argument passed to the function is a valid pointer of type Std_VersionInfoType
Function stores Version information in pointer
Function returns void
5.6.1.4. FUNC(Std_ReturnType, CDD_FSITX_CODE) Cdd_FsiTx_BufferLoad(Cdd_FsiTx_HWUnitType hwUnitId, P2VAR(Cdd_FsiTx_DataBufferType, AUTOMATIC, CDD_FSI_TX_APPL_DATA) SrcBufferPtr,Cdd_FsiTx_DataType Cdd_FsiTx_userData, Cdd_FsiTx_DataLengthType TxDataLength)
Argument passed to the function are:
hwUnitId:Tx instance which Transmits.
SrcBufferPtr: Pointer to the Data Buffer from which data has to be copied
Cdd_FsiTx_userData:User Specific 8 bit value passed from application for each frame.
TxDataLength:Number of words in each Frame.
Function copies data from the source pointer to internal Transmit buffer of Fsi Tx instance.
Function returns E_OK/E_NOT_OK.
5.6.1.5. FUNC(Std_ReturnType, CDD_FSITX_CODE) Cdd_FsiTx_Transmit(Cdd_FsiTx_HWUnitType hwUnitId, Cdd_FsiTx_UserDataType userData, Cdd_FsiTx_DataLengthType TxDataLength)
Argument passed to the function are:
hwUnitId:Tx instance which Transmits.
Cdd_FsiTx_userData:User Specific 8 bit value passed from application for each frame.
TxDataLength:Number of words in each Frame.
Function initiate the transmission of data from Tx Transmission buffer to Rx Internal reception Buffer.
Function returns E_OK/E_NOT_OK.
5.6.1.6. FUNC(Std_ReturnType, CDD_FSITX_CODE) Cdd_FsiTx_MainFunction(void)
The API is used in Polling Mode only.
The main function API Polls whether the transmission status flags are set for each instance to ensure the data transmission.
Function returns E_OK/E_NOT_OK.
5.6.1.7. FUNC(Std_ReturnType, CDD_FSITX_CODE) Cdd_FsiTx_Ping(Cdd_FsiTx_HWUnitType hwUnitId)
Argument passed to the function are:
hwUnitId:Tx instance which Transmits.
Function initiates the transmission of a Ping Frame(Frame without Data) to the Rx to verify the physical connection between Tx and Rx instances.
Function returns E_OK/E_NOT_OK.
5.6.1.8. FUNC(void, CDD_FSITX_CODE) Cdd_FsiTx_Reset(Cdd_FsiTx_HWUnitType hwUnitId, VAR(Cdd_FsiTx_ResetSubModuleType, AUTOMATIC) ResetModule)
Argument passed to the function are:
hwUnitId:Tx instance which Transmits.
ResetModule: This argument specifies where the reset happens. Example:, Main Core Reset, Ping Timer Reset,Clock Reset
Function resets either sub modules or main core in the Tx instance.
Function returns E_OK/E_NOT_OK.
5.6.1.9. FUNC(Cdd_FsiTx_StatusType, CDD_FSITX_CODE) CddFsiTx_GetStatus(void)
This service gets the status if FsiTx driver.
Function returns driver status:
CDD_FSI_TX_UNINIT: The Tx module has not initialized yet
CDD_FSI_TX_INIT: The Tx module has initialized
CDD_FSI_TX_IDLE: The transmission through the Tx channel hasn’t started
CDD_FSI_TX_BUSY: The frame transmission has been started and is still going on
5.6.2. CDD FSI TX API’s with Service ID
The following table presents the service IDs and the related services:
CDD FSI TX API’s Supported:
Service ID |
Service |
|---|---|
0x01 |
Cdd_FsiTx_Init |
0x02 |
Cdd_FsiTx_GetVersionInfo |
0x03 |
Cdd_FsiTx_Ping |
0x04 |
Cdd_FsiTx_BufferLoad |
0x05 |
Cdd_FsiTx_Transmit |
0x06 |
Cdd_FsiTx_MainFunction |
0x07 |
Cdd_FsiTx_DeInit |
0x08 |
Cdd_FsiTx_Reset |
5.7. CDD I2C
5.7.1. Description of the API’s
All below mentioned API’s are user accessible and can be found in Cdd_I2c.c file
5.7.1.1. void Cdd_I2c_Init( Cdd_I2c_ConfigPtrType* configPtr)
Argument passed to the function in NULL_PTR
Function returns void
Function is used to initialize all configured hardware units at specified frequencies
Function initializes queue to default values
5.7.1.2. Std_ReturnType Cdd_I2c_DeInit(void)
Function used to de-initialize all initialized I2c Hardware Units
Returns success upon successful initialization
Function can not be called in case driver is uninitialized
5.7.1.3. void Cdd_I2c_GetVersionInfo(Cdd_I2c_VersionInfoPtrType * versionInfoPtr)
Argument passed to the function is a valid pointer of type Cdd_I2c_VersionInfoPtrType
Function stores Version information in pointer
Function returns void
5.7.1.4. Std_ReturnType Cdd_I2c_SetupEB(I2c_ChannelType channelId, Cdd_I2c_DataPtrType txDataBufferPtr, Cdd_I2c_DataPtrType rxDataBufferPtr, Cdd_I2c_DataLengthType length)
Function sets up buffer for reception or transmission based on pre-configured channel ID’s passed as argument
Buffer pointer to store data for transmission/reception passed as argument
Length of message to read or write to slave device passed as argument
Both buffers can not be passed as NULL_PTR
Both buffers can not be passed as valid pointers
Pre-configured direction of the channel set up in the GUI should be maintained here as well to avoid development errors
Function returns success or failure
5.7.1.5. Std_ReturnType Cdd_I2c_SetupEBDynamic(I2c_ChannelType channelId, Cdd_I2c_AddressType address, Cdd_I2c_DataPtrType txDataBufferPtr, Cdd_I2c_DataPtrType rxDataBufferPtr, Cdd_I2c_DataLengthType length)
Function to set up buffer for reception or transmission of channel based on pre- configured channel ID’s passed as argument with a re-configurable slave address at run time
Buffer pointer to store data for transmission/reception passed as argument
Both Buffers can not be passed as NULL_PTR
Both buffers can not be passed as valid pointers
Valid slave address to be passed as an argument
Pre-configured direction of the channel set up in the GUI should be maintained here as well to avoid development errors
Function returns success or failure
5.7.1.6. Std_ReturnType Cdd_I2c_AsyncTransmit(I2c_SequenceType sequenceId)
Function use to transmit a sequence to receive/transmit data on the I2c bus
Sequence ID passed as parameter to the function
Transmission through this function can take place in both polling mode as well as interrupt mode
Reception through this function can only take place in interrupt mode
In case a sequence is not completed due to some reason, it is queued
Function returns success or failure
5.7.1.7. Std_ReturnType Cdd_I2c_Cancel(I2c_SequenceType sequenceId)
Function used to dequeue a sequence in queue
Sequence ID passed as argument
An ongoing sequence in transmission from queue can not be cancelled
Function returns success or failure
5.7.1.8. Cdd_I2c_ChannelResultType Cdd_I2c_GetResult(I2c_ChannelType channelId)
Function returns the channel result upon call, results depends on completion, failure or processing of a channel
Channel ID passed as a parameter
Function returns CDD_I2C_CH_RESULT_OK/CDD_I2C_CH_RESULT_NOT_OK/CDD_I2C_CH_RESULT_IN_PROGRESS/CDD_I2C_CH_RESULT_BUSFAIL/CDD_I2C_CH_RESULT_ARBFAIL/CDD_I2C_CH_RESULT_NACKFAIL
5.7.1.9. Cdd_I2c_SeqResultType Cdd_I2c_GetSequenceResult(I2c_SequenceType sequenceId)
Function returns the sequence result, result depends upon completion, failure or processing of a sequence
Sequence ID passed as a parameter
Function returns CDD_I2C_SEQ_OK/CDD_I2C_SEQ_NOT_OK/CDD_I2C_SEQ_PENDING/CDD_I2C_SEQ_QUEUED/CDD_I2C_SEQ_NACK/CDD_I2C_SEQ_FAILED/CDD_I2C_SEQ_CANCELLED
5.7.1.10. void Cdd_I2c_MainFunction(void)
Function used to process all the sequences in Queue and update sequence status accordingly
Function returns void
Function should be called periodically at the end
5.7.1.11. void Cdd_I2c_PollingModeProcessing(void)
Function used to receive data from the I2c bus in polling mode
Function returns void
Function process all sequences and receives data for all channels configured for read in one call
Only to be used in polling mode
5.7.1.12. void Cdd_I2c_SetHandling(Cdd_I2c_HandlingType handling)
Function used to handle arbitration loss condition
Handling parameter configured through GUI passed as argument
Function can either attempt to recover the bus control or detach from the bus after de-initializing the driver depending on the argument passed
Input parameter for function are CDD_I2C_BURST_MODE/CDD_I2C_RECURRENT_MODE
5.7.1.13. Cdd_I2c_ComponentStatusType Cdd_I2c_GetStatus(void)
Function used to return driver status
Requires no argument to be passed
Function returns CDD_I2C_UNINIT/CDD_I2C_IDLE/CDD_I2C_BUSY
5.7.2. Type definitions
The external visible and usable types defined by the I2C are described in this chapter.
TypeName |
C-Type |
Description |
Value Range |
|---|---|---|---|
Cdd_I2c_ComponentStatusType |
enum |
States of the I2C driver |
I2C_UNINIT- driver is not initialized |
Cdd_I2c_ChannelResultType |
enum |
The result of a channel |
I2C_CH_RESULT_OK- channel has finished successfully |
Cdd_I2c_HW_cfg |
enum |
Structure for CDD_I2C which contains Hw unit initialization parameters |
System clock frequency being used by the I2C instance |
Cdd_I2c_SeqResultType |
enum |
States of the sequence |
I2C_SEQ_OK- sequence finished normal |
Cdd_I2c_HandlingType |
enum |
Variants of timeout handling |
I2C_BURST- no timeout observation |
Cdd_I2c_AddressType |
uint16 |
Address for bus clients |
16 bits |
Cdd_I2c_DataType |
uint8 |
Data format of the I2c used for transmission and reception |
8 bits |
Cdd_I2c_DataLengthType |
uint16 |
Type for any length Parameter |
16 bits |
Cdd_I2c_DataPtrType |
uint8 * |
Pointer type for general buffer handling |
32 bits |
Cdd_I2c_DataConstPtrType |
const uint8 * |
Pointer type for TX buffer handling |
32 bits |
Cdd_I2c_SequenceType |
uint8 |
Type for sequence identifier |
8 bits |
Cdd_I2c_ChannelType |
uint8 |
Type for channel identifier |
8 bits |
5.7.3. Services used by I2C driver
Service ID |
Service |
|---|---|
0x00 |
CDD_I2C_Init |
0x01 |
CDD_I2c_DeInit |
0x02 |
CDD_I2c_GetVersionInfo |
0x03 |
CDD_I2c_SetupEB |
0x04 |
CDD_I2c_SetupEBDynamic |
0x05 |
CDD_I2c_AsyncTransmit |
0x06 |
CDD_I2c_Cancel |
0x07 |
CDD_I2c_GetResult |
0x08 |
CDD_I2c_GetSequenceResult |
0x09 |
CDD_I2c_MainFunction |
0x0A |
CDD_2c_PollingModeProcessing |
0x0B |
Cdd_I2c_SetHandling |
5.8. CDD IPC
5.8.1. Description of the Api’s
Cdd_Ipc_Init : This API will act as Service for CDD IPC Initialization.
Cdd_Ipc_DeInit : This API will act as Service for deinitializing CDD IPC.
Cdd_Ipc_Notify_RegisterClient : This API will act as Service to register a client for IPC.
Cdd_Ipc_Notify_UnregisterClient : This API will act as Service to un-register a client for IPC.
Cdd_Ipc_Notify_Write : This API will act as Service to write ipc notify message.
Cdd_Ipc_Construct : Used to Create a RPMessage object to receive messages at a specified end-point
Cdd_Ipc_Destruct : This API will act as Service to delete a previously created RPMessage object
Cdd_Ipc_RpMsg_SendMsg : This API will act as Service to Send a message to a remote core at a specified remote end point
Cdd_Ipc_RpMsg_RecvMsg : Blocking API to wait till a message is received from any CPU at the specified local end point.
Cdd_Ipc_Notify_SyncAll : This API will act as Service to sync all the cores that are participating in the IPC.
5.8.2. API’s with Service ID
Service ID |
Service |
|---|---|
0x01 |
Cdd_Ipc_Init |
0x02 |
Cdd_IpcGetVersionInfo |
0x03 |
Cdd_Ipc_RpMsg_RecvMsg |
0x04 |
Cdd_Ipc_RpMsg_SendMsg |
0x05 |
Cdd_Ipc_Notify_RegisterClient |
0x06 |
Cdd_Ipc_Construct |
0x07 |
Cdd_Ipc_DeInit |
0x09 |
Cdd_Ipc_Notify_UnregisterClient |
0x0A |
Cdd_Ipc_Destruct |
5.9. CDD PWM
5.9.1. Description of the API’s
Will be updated in future release
5.9.2. API’s with Service ID
The following table presents the service IDs and the related services:
Service ID |
Service |
|---|---|
0x0U |
Cdd_Pwm_Init |
0x1U |
Cdd_Pwm_DeInit |
0x2U |
Cdd_Pwm_StartChannelCounter |
0x3U |
Cdd_Pwm_StopChannelCounter |
0x5U |
Cdd_Pwm_SetPinAction |
0x6U |
Cdd_Pwm_GetCounter |
0x7U |
Cdd_Pwm_SetAbsoluteThreshold |
0x8U |
Cdd_Pwm_SetRelativeThreshold |
0x4U |
Cdd_Pwm_GetCounterStatus |
0x15U |
Cdd_Pwm_ClearCounterStatus |
0x2CU |
Cdd_Pwm_CounterComparatorCfg |
0x09U |
Cdd_Pwm_DisableNotification |
0x0AU |
Cdd_Pwm_EnableNotification |
0x16U |
Cdd_Pwm_EtIntrStatus |
0x17U |
Cdd_Pwm_EtIntrClear |
0x18U |
Cdd_Pwm_EtGetEventCount |
0x19U |
Cdd_Pwm_SetAdcTrigger |
0x1BU |
Cdd_Pwm_TzTripEventEnable |
0x1CU |
Cdd_Pwm_TzTripEventDisable |
0x1DU |
Cdd_Pwm_TzIntrEnable |
0x1EU |
Cdd_Pwm_TzIntrDisable |
0x1FU |
Cdd_Pwm_TzGetEventStatus |
0x20U |
Cdd_Pwm_TzEventStatusClear |
0xEU |
Cdd_Pwm_SetPeriodDutyPhase |
0xFU |
Cdd_Pwm_SetOutputToIdle |
0x2AU |
Cdd_Pwm_SyncEnable |
0x2BU |
Cdd_Pwm_SyncDisable |
0x10U |
Cdd_Pwm_DeadbandCfg |
0x11U |
Cdd_Pwm_DeadbandBypass |
0x12U |
Cdd_Pwm_ChopperCfg |
0x13U |
Cdd_Pwm_ChopperEnable |
0xDU |
Cdd_Pwm_RegisterReadback |
0xBU |
Cdd_Pwm_GetVersionInfo |
0x21U |
Cdd_Pwm_HrSetPeriodDutyPhase |
0x22U |
Cdd_Pwm_HrSfoCalibration |
0x23U |
Cdd_Pwm_HrSfoStatus |
5.10. CDD UART
5.10.1. API Definition
Cdd_Uart_Init
Cdd_Uart_DeInit
Cdd_Uart_Write
Cdd_Uart_Read
Cdd_Uart_Cancel
Cdd_Uart_GetRemainingWords
Cdd_Uart_GetVersionInfo
Cdd_Uart_RegisterReadback
5.10.2. API’s with Service ID
Service ID |
Service |
|---|---|
0x01 |
Cdd_Uart_Init |
0x02 |
Cdd_Uart_GetVersionInfo |
0x03 |
Cdd_Uart_DeInit |
0x04 |
Cdd_Uart_Write |
0x05 |
Cdd_Uart_Read |
0x06 |
Cdd_Uart_Cancel |
0x07 |
Cdd_Uart_GetRemainingWords |
0x08 |
Cdd_Uart_RegisterReadback |
5.11. DIO
5.11.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.11.2. API’s with Service ID
The following table presents the service IDs and the related services:
Autosar API’s Supported:
Service ID |
Service |
|---|---|
0x00 |
Dio_ReadChannel |
0x01 |
Dio_WriteChannel |
0x02 |
Dio_ReadPort |
0x03 |
Dio_WritePort |
0x04 |
Dio_ReadChannelGroup |
0x05 |
Dio_WriteChannelGroup |
0x11 |
Dio_FlipChannel |
0x12 |
Dio_GetVersionInfo |
5.11.3. Description on Non Standard API’s
None
5.12. ETH
5.12.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.12.2. API’s with Service ID
The following table presents the list of API’s:
Service ID |
Autosar API’s Supported |
Comments |
|---|---|---|
0x01 |
Eth_Init |
|
0x03 |
Eth_SetControllerMode |
|
0x04 |
Eth_GetControllerMode |
|
0x05 |
Eth_WriteMii |
|
0x06 |
Eth_ReadMii |
|
0x08 |
Eth_GetPhysAddr |
|
0x09 |
Eth_ProvideTxBuffer |
Priority/QoS option not supported. |
0x0A |
Eth_Transmit |
|
0x0B |
Eth_Receive |
Priority/QoS option not supported. |
0x0C |
Eth_TxConfirmation |
|
0x0D |
Eth_GetVersionInfo |
|
0x12 |
Eth_UpdatePhysAddrFilter |
|
0x13 |
Eth_SetPhysAddr |
|
0x14 |
Eth_GetCounterValues |
|
0x15 |
Eth_GetRxStats |
|
0x16 |
Eth_GetCurrentTime |
|
0x17 |
Eth_EnableEgressTimeStamp |
|
0x18 |
Eth_GetEgressTimeStamp |
|
0x19 |
Eth_GetIngressTimeStamp |
|
0x1C |
Eth_GetTxStats |
|
0x1D |
Eth_GetTxErrorCounterValues |
|
0x20 |
Eth_MainFunction |
|
0x50 |
Eth_SetBandwidthLimit |
|
0x51 |
Eth_GetBandwidthLimit |
Refer Autosar SWS for API description mentioned in above table.
5.12.3. Description on Non Standard API’s
Eth_SetBandwidthLimit API
This function is Non- Autosar based and is used to set a bandwidth limit on a specific channel for traffic shaping.
Eth_GetBandwidthLimit API
This function is Non- Autosar based and is used to get a bandwidth limit on a specific channel for traffic shaping.
5.13. ETHTRCV
5.13.1. Description of the API’s
Please refer MCAL_AM263Px_ApiGuide.CHM document provided as part of CSP.
5.13.2. API’s with Service ID
The following table presents the service IDs and the related services:
Autosar API’s Supported:
Service ID |
Autosar API’s Supported |
Autosar API’s not Supported |
|---|---|---|
0x01 |
EthTrcv_Init |
|
0x03 |
EthTrcv_SetTransceiverMode |
|
0x04 |
EthTrcv_GetTransceiverMode |
|
0x05 |
EthTrcv_StartAutoNegotiation |
|
0x06 |
EthTrcv_GetLinkState |
|
0x07 |
EthTrcv_GetBaudRate |
|
0x08 |
EthTrcv_GetDuplexMode |
|
0x09 |
EthTrcv_ReadMiiIndication |
|
0x0A |
EthTrcv_WriteMiiIndication |
|
0x0B |
EthTrcv_GetVersionInfo |
|
0x0C |
EthTrcv_MainFunction |
|
0x10 |
EthTrcv_GetPhySignalQuality |
|
0x11 |
EthTrcv_SetPhyTestMode |
|
0x12 |
EthTrcv_SetPhyLoopbackMode |
|
0x13 |
EthTrcv_SetPhyTxMode |
|
0x14 |
EthTrcv_GetCableDiagnosticsResult |
|
0x15 |
EthTrcv_GetPhyIdentifier |
|
0x0D |
EthTrcv_SetTransceiverWakeupMode |
|
0x0E |
EthTrcv_GetTransceiverWakeupMode |
|
0x0F |
EthTrcv_CheckWakeup |
Refer Autosar SWS for API description mentioned in above table.
5.13.3. Description on Non Standard API’s
Not Applicable.
5.14. FLS
5.14.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.14.2. API’s with Service ID
The following table presents the service IDs and the related services:
Autosar API’s Supported:
Service ID |
Service |
|---|---|
0x00 |
Fls_Init |
0x01 |
Fls_Erase |
0x02 |
FLS_Write |
0x03 |
FLS_Cancel |
0x04 |
FLS_GetStatus |
0x05 |
Fls_GetJobResult |
0x07 |
FLS_Read |
0x08 |
FLS_Compare |
0x10 |
Fls_GetVersionInfo |
0x0A |
FLS_BlankCheck |
0x06 |
FLS_MainFunction |
Autosar API’s not Supported:
Service ID |
Service |
|---|---|
0x09 |
Fls_SetMode |
Refer Autosar SWS for API description mentioned in above table.
5.15. GPT
5.15.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.15.2. API’s with Service ID
The following table presents the service IDs and the related services:
Service ID |
Service |
|---|---|
0x00 |
Gpt_GetVersionInfo |
0x01 |
Gpt_Init |
0x02 |
Gpt_DeInit |
0x03 |
Gpt_GetTimeElapsed |
0x04 |
Gpt_GetTimeRemaining |
0x05 |
Gpt_StartTimer |
0x06 |
Gpt_StopTimer |
0x07 |
Gpt_EnableNotification |
0x08 |
Gpt_DisableNotification |
5.15.3. Description on Non Standard API’s
Gpt_RegisterReadback API–This function is non-autosar based and is used to read the data in the registers of GPT if we keep GPT_REGISTER_READBACK_API Macro as ON.
5.16. ICU
The AUTOSAR BSW ICU Driver specification details the APIs required for Icu Driver. Please refer to SWS of ICU for detailed API description. APIs related to wakeup capability are not implemented.
5.16.1. Non Standard Service APIs
As noted from the previous MCAL implementation, some of the critical configuration registers could potentially be corrupted by other entities (s/w or h/w). One of the recommended detection methods would be to periodically read-back the configuration and confirm configuration is consistent. The service API defined below shall be implemented to enable this detection.
Description |
Comments |
|
|---|---|---|
Service Name |
Icu_RegisterReadback |
|
Syntax |
Icu_RegisterReadback(Icu_ChannelType Channel,P2VAR(Icu_RegisterReadbackType, AUTOMATIC, ICU_APPL_DATA) RegRbPtr) |
E_OK: Register read back has been done, |
Parameter in |
Channel |
Numeric identifier of the ICU channel |
Asyn/Syn |
Sync |
NA |
Re-entrancy |
Non Reentrant |
NA |
Parameter out |
RegRbPtr |
A pointer of type Icu_RegisterReadbackType, which holds the read back values |
Parameter out |
Std_ReturnType |
E_OK or E_NOT_OK in case of Icu not initialized or NULL buffer pointer |
5.17. LIN
5.17.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.17.2. API’s with Service ID
The following table presents the service IDs and the related services:
Service ID |
Service |
|---|---|
0x00 |
Lin_Init |
0x01 |
Lin_GetVersionInfo |
0x04 |
Lin_SendFrame |
0x06 |
Lin_GoToSleep |
0x07 |
Lin_Wakeup |
0x08 |
Lin_GetStatus |
0x09 |
Lin_GoToSleepInternal |
0x0a |
Lin_CheckWakeup |
0x0b |
Lin_WakeupInternal |
5.17.3. Description on Non Standard API’s
None
5.18. MCU
5.18.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.18.2. API’s with Service ID
The following table presents the service IDs and the related services:
Autosar API’s Supported:
Service ID |
Autosar API’s Supported Service |
Autosar API’s not Supported Service |
|---|---|---|
0x00 |
Mcu_Init |
|
0x01 |
Mcu_InitRamSection |
|
0x02 |
Mcu_InitClock |
|
0x03 |
Mcu_DistributePllClock |
|
0x04 |
Mcu_GetPllStatus |
|
0x05 |
Mcu_GetResetReason |
|
0x06 |
Mcu_GetResetRawValue |
|
0x07 |
Mcu_PerformReset |
|
0x09 |
Mcu_GetVersionInfo |
|
0x0A |
Mcu_GetRamState |
|
0x08 |
Mcu_SetMode |
Refer Autosar SWS for API description mentioned in above table.
5.18.3. Description on Non Standard API’s
Mcu_DeInit API
This function is Non- Autosar based and is used to de-initialize MCU module.
Mcu_RegisterReadback API
This function is non-autosar based and is used to read the data in the registers of MCU.
This functionality is enabled, if parameter McuEnableRegisterReadbackApi is TRUE (The Parameter sets MCU_REGISTER_READBACK_API Macro as STD_ON ).
5.19. PORT
5.19.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.19.2. List of API’s
The following table presents the list of API’s:
Service ID |
Autosar API’s Supported Service |
Autosar API’s not Supported Service |
|---|---|---|
0x00 |
Port_Init |
|
0x01 |
Port_SetPinDirection |
|
0x02 |
Port_RefreshPortDirection |
|
0x03 |
Port_GetVersionInfo |
|
0x04 |
Port_SetPinMode |
Refer Autosar SWS for API description mentioned in above table.
5.19.3. Description on Non Standard API’s
Port_DeInit API
This function is Non- Autosar based and is used to de-initialize port module.
Port_PinEnableIntrNotification API
This function is Non- Autosar based and is used to enable bank/channel GPIO Interrupts for particular channel.
Port_PinDisableIntrNotification API
This function is Non- Autosar based and is used to disable bank/channel GPIO Interrupts for particular channel.
Port_GetInterruptStatus API
This function is Non- Autosar based and is used to collect interrupt register value for each GPIO bank.
Port_ClearInterruptStatus API
This function is Non- Autosar based and is used to clear interrupt register for each GPIO bank.
5.20. PWM
5.20.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.20.2. API’s with Service ID
The following table presents the service IDs and the related services:
Service ID |
Service |
|---|---|
0x00 |
Pwm_Init |
0x01 |
Pwm_DeInit |
0x02 |
Pwm_SetDutyCycle |
0x03 |
Pwm_SetPeriodAndDuty |
0x04 |
Pwm_SetOutputToIdle |
0x06 |
Pwm_DisableNotification |
0x07 |
Pwm_EnableNotification |
0x08 |
Pwm_GetVersionInfo |
Autosar API’s not Supported:
Service ID |
Service |
|---|---|
0x09 |
Pwm_SetPowerState |
0x0a |
Pwm_GetCurrentPowerState |
0x0b |
Pwm_GetTargetPowerState |
0x0c |
Pwm_PreparePowerState |
0x05 |
Pwm_GetOuputState |
Refer Autosar SWS for API description mentioned in above table.
5.20.3. Description on Non Standard API’s
Pwm_RegisterReadback API–This function is non-autosar based and is used to read the data in the registers of Pwm if we keep PWM_REGISTER_READBACK_API Macro as ON. and Service Id is 0xD0.
5.21. SPI
5.21.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.21.2. API’s with Service ID
The following table presents the service IDs and the related services:
AUTOSAR API’s Supported:
Service ID |
Service |
|---|---|
SPI_SID_INIT = 0x00 |
Spi_Init |
SPI_SID_DEINIT = 0x01 |
Spi_DeInit |
SPI_SID_WRITEIB = 0x02 |
Spi_WriteIB |
SPI_SID_ASYNCTRANSMIT = 0x03 |
Spi_AsyncTransmit |
SPI_SID_READIB = 0x04 |
Spi_ReadIB |
SPI_SID_SETUPEB = 0x05 |
Spi_SetupEB |
SPI_SID_GETSTATUS = 0x06 |
Spi_GetStatus |
SPI_SID_GETJOBRESULT = 0x07 |
Spi_GetJobResult |
SPI_SID_GETSEQUENCERESULT = 0x08 |
Spi_GetSequenceResult |
SPI_SID_GETVERSIONINFO = 0x09 |
Spi_GetVersionInfo |
SPI_SID_SYNCTRANSMIT = 0x0A |
Spi_SyncTransmit |
SPI_SID_GETHWUNITSTATUS = 0x0B |
Spi_GetHwUnitStatus |
SPI_SID_CANCEL = 0x0C |
Spi_Cancel |
SPI_SID_SETASYNCMODE = 0x0D |
Spi_SetAsyncMode |
SPI_SID_MAINFUNCTION_HANDLING = 0x10 |
Spi_MainfunctionHandling |
AUTOSAR API’s not Supported:
None
Refer AUTOSAR SWS for API description per service mentioned in the above table.
5.21.3. Description on Non Standard API’s
None
5.22. WDG
5.22.1. Description of the API’s
Refer the AUTOSAR SWS for API documentation and Type definition.
5.22.2. API’s with Service ID
The following table presents the service IDs and the related services:
Service ID |
Service |
|---|---|
0x00 |
Wdg_Init |
0x01 |
Wdg_SetMode |
0x03 |
Wdg_SetTriggerCondition |
0x04 |
Wdg_GetVersionInfo |
0x05 |
Wdg_Trigger |
5.22.3. Description on Non Standard API’s
Wdg_RegisterReadback API–This function is non-autosar based and is used to read the data in the registers of Wdg if we keep Wdg_REGISTER_READBACK_API Macro as ON.