AM64x MCU+ SDK  12.01.00
soc.h File Reference

Go to the source code of this file.

Macros

#define SOC_BOOTMODE_MMCSD   (0X36C3)
 Switch value for SD card boot mode. More...
 
#define SOC_H_IO_DRVSTRNGTH0   (0x40C0U)
 IO Drive Strength Register offsets. More...
 
#define SOC_H_IO_DRVSTRNGTH2   (0x40C8U)
 
#define SOC_V_IO_DRVSTRNGTH0   (0x40D0U)
 
#define SOC_V_IO_DRVSTRNGTH2   (0x40D8U)
 
#define SOC_IO_DRVSTRNGTH_MASK   CSL_MCU_CTRL_MMR_CFG0_H_IO_DRVSTRNGTH0_DRV_STR_MASK
 IO Drive Strength field definitions. More...
 
#define SOC_IO_DRVSTRNGTH_MAX   CSL_MCU_CTRL_MMR_CFG0_H_IO_DRVSTRNGTH0_DRV_STR_MAX
 
#define SOC_FWL_OPEN_MAGIC_NUM   (0XFEDCBA98u)
 Software defined MAGIC number to indicate SRAM firewall open by SBL. More...
 
#define MCU_MCSPI0_CFG_BASE_AFTER_ADDR_TRANSLATE   (CSL_MCU_MCSPI0_CFG_BASE + 0x80000000)
 
#define MCU_MCSPI1_CFG_BASE_AFTER_ADDR_TRANSLATE   (CSL_MCU_MCSPI1_CFG_BASE + 0x80000000)
 
#define MCU_UART0_BASE_AFTER_ADDR_TRANSLATE   (CSL_MCU_UART0_BASE + 0x80000000)
 
#define MCU_UART1_BASE_AFTER_ADDR_TRANSLATE   (CSL_MCU_UART1_BASE + 0x80000000)
 
#define MCU_I2C0_CFG_BASE_AFTER_ADDR_TRANSLATE   (CSL_MCU_I2C0_CFG_BASE + 0x80000000)
 
#define MCU_I2C1_CFG_BASE_AFTER_ADDR_TRANSLATE   (CSL_MCU_I2C1_CFG_BASE + 0x80000000)
 
#define IS_OSPI_BASE_ADDR_VALID(baseAddr)   (baseAddr == CSL_FSS0_OSPI0_CTRL_BASE)
 Macro to check if the OSPI base address is valid. More...
 
#define IS_OSPI_DATA_BASE_ADDR_VALID(baseAddr)   (baseAddr == CSL_FSS0_DAT_REG1_BASE)
 Macro to check if the OSPI base address is valid. More...
 
SOC Domain ID

#define SOC_DOMAIN_ID_MAIN   (0U)
 
#define SOC_DOMAIN_ID_MCU   (1U)
 
#define SOC_PSC_DOMAIN_ID_MAIN   (0U)
 
#define SOC_PSC_DOMAIN_ID_MCU   (1U)
 
SOC PSC Module State

#define SOC_PSC_SYNCRESETDISABLE   (0x0U)
 
#define SOC_PSC_SYNCRESET   (0x1U)
 
#define SOC_PSC_DISABLE   (0x2U)
 
#define SOC_PSC_ENABLE   (0x3U)
 
SOC PSC Domain State

#define SOC_PSC_DOMAIN_OFF   (0x0U)
 
#define SOC_PSC_DOMAIN_ON   (0x1U)
 

Functions

static int32_t I2C_lld_isBaseAddrValid (uint32_t baseAddr)
 API to validate I2C base address. More...
 
static int32_t MCSPI_lld_isBaseAddrValid (uint32_t baseAddr)
 API to validate MCSPI base address. More...
 
static int32_t UART_IsBaseAddrValid (uint32_t baseAddr)
 API to validate UART base address. More...
 
static int32_t MMCSD_lld_isBaseAddrValid (uint32_t ctrlBaseAddr, uint32_t ssBaseAddr)
 API to validate MMCSD base addresses. More...
 
int32_t SOC_moduleClockEnable (uint32_t moduleId, uint32_t enable)
 Enable clock to specified module. More...
 
int32_t SOC_moduleSetClockFrequencyWithParent (uint32_t moduleId, uint32_t clkId, uint32_t clkParent, uint64_t clkRate)
 Set module clock to specified frequency and with a specific parent. More...
 
int32_t SOC_moduleSetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
 Set module clock to specified frequency. More...
 
int32_t SOC_moduleGetClockFrequency (uint32_t moduleId, uint32_t clkId, uint64_t *clkRate)
 Get module clock frequency. More...
 
const char * SOC_getCoreName (uint16_t coreId)
 Convert a core ID to a user readable name. More...
 
uint64_t SOC_getSelfCpuClk (void)
 Get the clock frequency in Hz of the CPU on which the driver is running. More...
 
void SOC_controlModuleLockMMR (uint32_t domainId, uint32_t partition)
 Lock control module partition to prevent writes into control MMRs. More...
 
void SOC_controlModuleUnlockMMR (uint32_t domainId, uint32_t partition)
 Unlock control module partition to allow writes into control MMRs. More...
 
void SOC_setEpwmTbClk (uint32_t epwmInstance, uint32_t enable)
 Enable or disable ePWM time base clock from Control MMR. More...
 
void SOC_allowEpwmTzReg (uint32_t epwmInstance, uint32_t enable)
 Enable or disable writes to the EPWM tripZone registers. More...
 
uint64_t SOC_virtToPhy (void *virtAddr)
 SOC Virtual (CPU) to Physical address translation function. More...
 
void * SOC_phyToVirt (uint64_t phyAddr)
 Physical to Virtual (CPU) address translation function. More...
 
void SOC_unlockAllMMR (void)
 Unlocks all the control MMRs. More...
 
void SOC_setDevStat (uint32_t bootMode)
 Change boot mode by setting devstat register. More...
 
uint32_t SOC_isR5FDualCoreMode (CSL_ArmR5CPUInfo *cpuInfo)
 Return R5SS supporting single or dual core mode. More...
 
void SOC_generateSwWarmResetMainDomain (void)
 Generate SW Warm Reset Main Domain. More...
 
void SOC_generateSwPORResetMainDomain (void)
 Generate SW POR Reset Main Domain. More...
 
uint32_t SOC_getWarmResetCauseMainDomain (void)
 Get the reset reason source for Main Domain. More...
 
void SOC_generateSwWarmResetMcuDomain (void)
 Generate SW WARM Reset Mcu Domain. More...
 
void SOC_generateSwWarmResetMainDomainFromMcuDomain (void)
 Generate SW WARM Reset Main Domain from Mcu Domain. More...
 
void SOC_generateSwPORResetMainDomainFromMcuDomain (void)
 Generate SW POR Reset Main Domain from Mcu Domain. More...
 
uint32_t SOC_getWarmResetCauseMcuDomain (void)
 Get the reset reason source for Mcu Domain. More...
 
void SOC_clearResetCauseMainMcuDomain (uint32_t resetCause)
 Clears reason for Warm and Main/Mcu Domain Power On Resets. CTRLMMR_RST_SRC is just a mirror of CTRLMMR_MCU_RST_SRC register. It is read only. So we need to write 1 to CTRLMMR_MCU_RST_SRC to clear the reset reason. More...
 
int32_t SOC_enableResetIsolation (uint32_t main2McuIsolation, uint32_t mcu2MainIsolation, uint32_t debugIsolationEnable)
 Enable reset isolation of MCU domain for safety applications. More...
 
void SOC_setMCUResetIsolationDone (uint32_t value)
 Set MCU reset isolation done flag. More...
 
void SOC_waitMainDomainReset (void)
 Wait for main domain reset to complete. More...
 
int32_t SOC_getPSCState (uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t *domainState, uint32_t *moduleState)
 Get PSC (Power Sleep Controller) state. More...
 
int32_t SOC_setPSCState (uint32_t instNum, uint32_t domainNum, uint32_t moduleNum, uint32_t pscState)
 Set PSC (Power Sleep Controller) state. More...
 
void SOC_waitForFwlUnlock (void)
 Wait for Firewall unlock from SBL. The function polls for a Software defined Magic number at the PSRAM location (Software defined) More...
 
int32_t SOC_isHsDevice (void)
 Check the device is HS or not. More...
 
uint32_t SOC_getFlashDataBaseAddr (void)
 This function gets the SOC mapped data base address of the flash. More...
 
void SOC_fixFastDriveStrength (void)
 Fix fast mode drive strength. More...