ICSS-EMAC (Industrial Communications Sub-system Ethernet Media Access Controller) APIs to transmit and receive packets with a firmware based Ethernet switch that has been implemented on PRUICSS.
Data Structures | |
struct | ICSS_EMAC_FwStaticMmap |
ICSS EMAC Static Firmware Memory Map offsets. These are offsets for PRU0 and PRU1 DRAM memory. More... | |
struct | ICSS_EMAC_FwDynamicMmap |
ICSS EMAC Dynamic Firmware Memory Map offsets. More... | |
struct | ICSS_EMAC_FwVlanFilterParams |
ICSS EMAC VLAN Filtering Parameters. More... | |
struct | ICSS_EMAC_FwMulticastFilterParams |
ICSS EMAC Multicast Filtering Parameters. More... | |
struct | ICSS_EMAC_Attrs |
struct | ICSS_EMAC_InternalObject |
Opaque ICSS EMAC driver object. More... | |
struct | ICSS_EMAC_Config |
Base EMAC handle containing pointers to all modules required for driver to work. More... | |
struct | ICSS_EMAC_CallBackConfig |
Generic callback configuration for protocol specific callbacks. ICSS_EMAC_CallBack is the function prototype used. While calling this, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (see ICSS_EMAC_CallBackObject), and third argument is userArg as specified in this structure. More... | |
struct | ICSS_EMAC_CallBackObject |
Different callbacks which can be registered. While calling the function set in ICSS_EMAC_CallBack, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (as mentioned in the member descriptions), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig. More... | |
struct | ICSS_EMAC_Params |
ICSS_EMAC Parameters. More... | |
struct | ICSS_EMAC_RxArgument |
Rx packet processing information block that needs to passed into call to ICSS_EMAC_RxPktGet. More... | |
struct | ICSS_EMAC_TxArgument |
Tx packet processing information block that needs to passed into call to ICSS_EMAC_TxPacket. More... | |
struct | ICSS_EMAC_IoctlCmd |
IOCTL command members for configuring switch/EMAC. More... | |
struct | ICSS_EMAC_PruStatistics |
Statistics structure for capturing statistics on PRU. More... | |
Functions | |
void | ICSS_EMAC_init (void) |
This function initializes the ICSS_EMAC module. More... | |
void | ICSS_EMAC_deinit (void) |
This function de-initializes the ICSS_EMAC module. More... | |
void | ICSS_EMAC_Params_init (ICSS_EMAC_Params *params) |
Initialize the parmeters data structure with defaults. More... | |
ICSS_EMAC_Handle | ICSS_EMAC_open (uint32_t idx, const ICSS_EMAC_Params *params) |
API to initialize and configure ICSS in MAC/Switch Mode. More... | |
void | ICSS_EMAC_close (ICSS_EMAC_Handle icssEmacHandle) |
API to stop MAC/Switch Mode. More... | |
int32_t | ICSS_EMAC_ioctl (ICSS_EMAC_Handle icssEmacHandle, uint32_t ioctlCommand, uint8_t portNo, void *ioctlParams) |
IOCTL Function for ICSS EMAC. More... | |
int32_t | ICSS_EMAC_rxPktGet (ICSS_EMAC_RxArgument *rxArg, void *userArg) |
Retrieves a frame from a host queue and copies it in the allocated stack buffer. More... | |
int32_t | ICSS_EMAC_rxPktInfo (ICSS_EMAC_Handle icssEmacHandle, int32_t *portNumber, int32_t *queueNumber) |
API to retrieve the information about the received frame which is then used to dequeue the frame from the host queues. More... | |
int32_t | ICSS_EMAC_txPacket (const ICSS_EMAC_TxArgument *txArg, void *userArg) |
API to queue a frame which has to be transmitted on the specified port queue. More... | |
Typedefs | |
typedef struct ICSS_EMAC_Config_s * | ICSS_EMAC_Handle |
Alias for ICSS EMAC Handle containing base addresses and modules. More... | |
typedef int32_t(* | ICSS_EMAC_CallBack) (void *arg0, void *arg1, void *arg2) |
Definition for a generic callback function used in ICSS-EMAC. While calling this, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (see ICSS_EMAC_CallBackObject), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig. More... | |
Macros | |
#define | ICSS_EMAC_MAX_PORTS_PER_INSTANCE (2) |
Maximum number of Ports in a single ICSS More... | |
#define | ICSS_EMAC_NUMQUEUES ((uint32_t)17U) |
Total Queues available. More... | |
#define | ICSS_EMAC_MAXMTU (1518U) |
Maximum Valid size (incl header + VLAN TAG..., no CRC) More... | |
#define | ICSS_EMAC_MINMTU (14U) |
Minimum Valid size ( DA + SA + Ethertype) More... | |
#define | ICSS_EMAC_PORT_0 (0) |
Used to specify host side port. More... | |
#define | ICSS_EMAC_PORT_1 (1U) |
Used to specify physical port 1 MII 0 (tx) More... | |
#define | ICSS_EMAC_PORT_2 (2U) |
Used to specify physical port 2 MII 1 (tx) More... | |
#define | ICSS_EMAC_IOCTL_PORT_CTRL_DISABLE (0u) |
ICSS_EMAC_IOCTL_PORT_CTRL options. More... | |
#define | ICSS_EMAC_IOCTL_PORT_CTRL_ENABLE (1u) |
Generic IOCTL Disable macro. More... | |
#define | ICSS_EMAC_LEARNING_PORT_STATE_LEARNING (0U) |
Macros for different port states in learning module. More... | |
#define | ICSS_EMAC_LEARNING_PORT_STATE_NOT_LEARNING (1U) |
#define | ICSS_EMAC_LEARNING_PORT_STATE_LOCKED (2U) |
#define | ICSS_EMAC_OBJECT_SIZE_IN_BYTES (42000) |
ICSS EMAC Modes | |
#define | ICSS_EMAC_MODE_MAC1 (1U) |
Single EMAC Mode. Port 1 Enabled. More... | |
#define | ICSS_EMAC_MODE_MAC2 (2U) |
Single EMAC Mode. Port 2 Enabled. More... | |
#define | ICSS_EMAC_MODE_SWITCH (3U) |
Switch Mode. More... | |
#define | ICSS_EMAC_MODE_DUALMAC (4U) |
Dual MAC Mode. Both Ports Enabled. More... | |
ICSS EMAC PHY to MAC Interface Modes | |
#define | ICSS_EMAC_MII_MODE (0U) |
Media-independent Interface. More... | |
#define | ICSS_EMAC_RGMII_MODE (1U) |
Reduced Gigabit Media-independent Interface More... | |
ICSS EMAC Learning Modes | |
#define | ICSS_EMAC_LEARNING_DISABLE (0U) |
Driver-based Learning Mode Disabled More... | |
#define | ICSS_EMAC_LEARNING_ENABLE (1U) |
Driver-based Learning Mode Enabled More... | |
ICSS EMAC Interrupt Pacing Configuration | |
#define | ICSS_EMAC_ENABLE_PACING (0) |
Interrupt pacing enabled. More... | |
#define | ICSS_EMAC_DISABLE_PACING (1) |
Interrupt pacing disabled. More... | |
ICSS EMAC Interrupt Pacing Modes | |
#define | ICSS_EMAC_INTR_PACING_MODE1 (0) |
Frame Count based Interrupt pacing. More... | |
ICSS EMAC Queues | |
#define | ICSS_EMAC_QUEUE1 ((uint32_t)0U) |
Priority Queue 1. More... | |
#define | ICSS_EMAC_QUEUE2 ((uint32_t)1U) |
Priority Queue 2. More... | |
#define | ICSS_EMAC_QUEUE3 ((uint32_t)2U) |
Priority Queue 3. More... | |
#define | ICSS_EMAC_QUEUE4 ((uint32_t)3U) |
Priority Queue 4. More... | |
#define | ICSS_EMAC_QUEUE5 ((uint32_t)4U) |
Priority Queue 5. More... | |
#define | ICSS_EMAC_QUEUE6 ((uint32_t)5U) |
Priority Queue 6. More... | |
#define | ICSS_EMAC_QUEUE7 ((uint32_t)6U) |
Priority Queue 7. More... | |
#define | ICSS_EMAC_QUEUE8 ((uint32_t)7U) |
Priority Queue 8. More... | |
#define | ICSS_EMAC_QUEUE9 ((uint32_t)8U) |
Priority Queue 9. More... | |
#define | ICSS_EMAC_QUEUE10 ((uint32_t)9U) |
Priority Queue 10. More... | |
#define | ICSS_EMAC_QUEUE11 ((uint32_t)10U) |
Priority Queue 11. More... | |
#define | ICSS_EMAC_QUEUE12 ((uint32_t)11U) |
Priority Queue 12. More... | |
#define | ICSS_EMAC_QUEUE13 ((uint32_t)12U) |
Priority Queue 13. More... | |
#define | ICSS_EMAC_QUEUE14 ((uint32_t)13U) |
Priority Queue 14. More... | |
#define | ICSS_EMAC_QUEUE15 ((uint32_t)14U) |
Priority Queue 15. More... | |
#define | ICSS_EMAC_QUEUE16 ((uint32_t)15U) |
Priority Queue 16. More... | |
#define | ICSS_EMAC_COLQUEUE ((uint32_t)16U) |
Collision Queue. More... | |
ICSS-EMAC Storm Prevention IOCTL Command Options | |
#define | ICSS_EMAC_STORM_PREV_CTRL_ENABLE (0u) |
IOCTL Storm Control Enable command. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_DISABLE (1u) |
IOCTL Storm Control Disable command. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS (2u) |
IOCTL Storm Control set credit command. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_INIT (3u) |
IOCTL Storm Control initialize command. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_RESET (4u) |
IOCTL Storm Control reset command. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_ENABLE_BC (5u) |
IOCTL Storm Control Enable command for BC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_DISABLE_BC (6u) |
IOCTL Storm Control Disable command for BC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_BC (7u) |
IOCTL Storm Control set credit command for BC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_INIT_BC (8u) |
IOCTL Storm Control initialize command for BC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_RESET_BC (9u) |
IOCTL Storm Control reset command for BC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_ENABLE_MC (10u) |
IOCTL Storm Control Enable command for MC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_DISABLE_MC (11u) |
IOCTL Storm Control Disable command for MC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_MC (12u) |
IOCTL Storm Control set credit command for MC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_INIT_MC (13u) |
IOCTL Storm Control initialize command for MC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_RESET_MC (14u) |
IOCTL Storm Control reset command for MC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_ENABLE_UC (15u) |
IOCTL Storm Control Enable command for UC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_DISABLE_UC (16u) |
IOCTL Storm Control Disable command for UC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_UC (17u) |
IOCTL Storm Control set credit command for UC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_INIT_UC (18u) |
IOCTL Storm Control initialize command for UC traffic. More... | |
#define | ICSS_EMAC_STORM_PREV_CTRL_RESET_UC (19u) |
IOCTL Storm Control reset command for UC traffic. More... | |
ICSS-EMAC Learning Control IOCTL Command Options | |
#define | ICSS_EMAC_LEARN_CTRL_UPDATE_TABLE (0u) |
IOCTL Learning Table update command. More... | |
#define | ICSS_EMAC_LEARN_CTRL_CLR_TABLE (1u) |
IOCTL Learning Table clear table command. More... | |
#define | ICSS_EMAC_LEARN_CTRL_AGEING (2u) |
IOCTL Learning Table age out entry command. More... | |
#define | ICSS_EMAC_LEARN_CTRL_FIND_MAC (3u) |
IOCTL Learning Table find port from MAC ID command. More... | |
#define | ICSS_EMAC_LEARN_CTRL_REMOVE_MAC (4u) |
IOCTL Learning Table remove a MAC ID from table command. More... | |
#define | ICSS_EMAC_LEARN_CTRL_INC_COUNTER (5u) |
IOCTL Learning Table increment counters (for ageing) command. More... | |
#define | ICSS_EMAC_LEARN_CTRL_INIT_TABLE (6u) |
IOCTL Learning Table initialize command. More... | |
#define | ICSS_EMAC_LEARN_CTRL_SET_PORTSTATE (7u) |
IOCTL Learning Table set port state command. More... | |
ICSS-EMAC Statistics IOCTL Command Options | |
#define | ICSS_EMAC_IOCTL_STAT_CTRL_GET (0u) |
IOCTL Statistics get from PRU command. More... | |
#define | ICSS_EMAC_IOCTL_STAT_CTRL_CLEAR (1u) |
IOCTL Statistics clear all counters command. More... | |
ICSS-EMAC IOCTL Command for selecting a module | |
#define | ICSS_EMAC_IOCTL_PORT_CTRL (0u) |
IOCTL select port control APIs command. More... | |
#define | ICSS_EMAC_IOCTL_LEARNING_CTRL (1u) |
IOCTL select learning Table APIs command. More... | |
#define | ICSS_EMAC_IOCTL_STORM_PREV_CTRL (2u) |
IOCTL select Storm Prevention APIs command. More... | |
#define | ICSS_EMAC_IOCTL_STATS_CTRL (3u) |
IOCTL select Statistics APIs command. More... | |
#define | ICSS_EMAC_IOCTL_PROMISCUOUS_CTRL (4u) |
IOCTL select Promiscuous Mode APIs command. More... | |
#define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL (5u) |
IOCTL select Multicast filtering APIs command. More... | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL (6u) |
IOCTL select Vlan filtering APIs command. More... | |
#define | ICSS_EMAC_IOCTL_PORT_FLUSH_CTRL (7u) |
IOCTL select Port flush APIs command. More... | |
ICSS-EMAC Multicast Filtering IOCTL Command Options | |
#define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_ENABLE (0u) |
IOCTL Multicast filter Control Enable command. More... | |
#define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_DISABLE (1u) |
IOCTL Multicast filter Control Disable command. More... | |
#define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_OVERRIDE_HASHMASK (2u) |
IOCTL Multicast filter Control override hashmask command. More... | |
#define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_ADD_MACID (3u) |
IOCTL Multicast filter Control allow MC MAC ID command. More... | |
#define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_REMOVE_MACID (4u) |
IOCTL Multicast filter Control do not allow MC MAC ID command. More... | |
#define | ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_GET_DROPPED (5u) |
IOCTL Multicast filter Control do not allow MC MAC ID command. More... | |
ICSS-EMAC VLAN Filtering IOCTL Command Options | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_ENABLE_CMD (0u) |
IOCTL Vlan filter Control Enable command. More... | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_DISABLE_CMD (1u) |
IOCTL Vlan filter Control Disable command. More... | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_UNTAG_HOST_RCV_ALL_CMD (2u) |
IOCTL Vlan filter allow Untagged frames Host Receive command. More... | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_UNTAG_HOST_RCV_NAL_CMD (3u) |
IOCTL Vlan filter do not allow Untagged frames Host Receive command. More... | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_PRIOTAG_HOST_RCV_ALL_CMD (4u) |
IOCTL Vlan filter allow Priority Tag frames Host Receive command. More... | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_PRIOTAG_HOST_RCV_NAL_CMD (5u) |
IOCTL Vlan filter do not allow Priority Tag frames Host Receive command. More... | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_ADD_VID_CMD (6u) |
IOCTL Vlan filter 4096 VIDs, 1 bit VIDs => 4096 bits = 512 bytes, ADD VLAN ID to allow packet to host More... | |
#define | ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_REMOVE_VID_CMD (7u) |
IOCTL Vlan filter 4096 VIDs, 1 bit VIDs => 4096 bits = 512 bytes, Remove VLAN ID to do not allow packet to host More... | |
#define ICSS_EMAC_MAX_PORTS_PER_INSTANCE (2) |
Maximum number of Ports in a single ICSS
#define ICSS_EMAC_MODE_MAC1 (1U) |
Single EMAC Mode. Port 1 Enabled.
#define ICSS_EMAC_MODE_MAC2 (2U) |
Single EMAC Mode. Port 2 Enabled.
#define ICSS_EMAC_MODE_SWITCH (3U) |
Switch Mode.
#define ICSS_EMAC_MODE_DUALMAC (4U) |
Dual MAC Mode. Both Ports Enabled.
#define ICSS_EMAC_MII_MODE (0U) |
Media-independent Interface.
#define ICSS_EMAC_RGMII_MODE (1U) |
Reduced Gigabit Media-independent Interface
#define ICSS_EMAC_LEARNING_DISABLE (0U) |
Driver-based Learning Mode Disabled
#define ICSS_EMAC_LEARNING_ENABLE (1U) |
Driver-based Learning Mode Enabled
#define ICSS_EMAC_ENABLE_PACING (0) |
Interrupt pacing enabled.
#define ICSS_EMAC_DISABLE_PACING (1) |
Interrupt pacing disabled.
#define ICSS_EMAC_INTR_PACING_MODE1 (0) |
Frame Count based Interrupt pacing.
#define ICSS_EMAC_QUEUE1 ((uint32_t)0U) |
Priority Queue 1.
#define ICSS_EMAC_QUEUE2 ((uint32_t)1U) |
Priority Queue 2.
#define ICSS_EMAC_QUEUE3 ((uint32_t)2U) |
Priority Queue 3.
#define ICSS_EMAC_QUEUE4 ((uint32_t)3U) |
Priority Queue 4.
#define ICSS_EMAC_QUEUE5 ((uint32_t)4U) |
Priority Queue 5.
#define ICSS_EMAC_QUEUE6 ((uint32_t)5U) |
Priority Queue 6.
#define ICSS_EMAC_QUEUE7 ((uint32_t)6U) |
Priority Queue 7.
#define ICSS_EMAC_QUEUE8 ((uint32_t)7U) |
Priority Queue 8.
#define ICSS_EMAC_QUEUE9 ((uint32_t)8U) |
Priority Queue 9.
#define ICSS_EMAC_QUEUE10 ((uint32_t)9U) |
Priority Queue 10.
#define ICSS_EMAC_QUEUE11 ((uint32_t)10U) |
Priority Queue 11.
#define ICSS_EMAC_QUEUE12 ((uint32_t)11U) |
Priority Queue 12.
#define ICSS_EMAC_QUEUE13 ((uint32_t)12U) |
Priority Queue 13.
#define ICSS_EMAC_QUEUE14 ((uint32_t)13U) |
Priority Queue 14.
#define ICSS_EMAC_QUEUE15 ((uint32_t)14U) |
Priority Queue 15.
#define ICSS_EMAC_QUEUE16 ((uint32_t)15U) |
Priority Queue 16.
#define ICSS_EMAC_COLQUEUE ((uint32_t)16U) |
Collision Queue.
#define ICSS_EMAC_NUMQUEUES ((uint32_t)17U) |
Total Queues available.
#define ICSS_EMAC_MAXMTU (1518U) |
Maximum Valid size (incl header + VLAN TAG..., no CRC)
#define ICSS_EMAC_MINMTU (14U) |
Minimum Valid size ( DA + SA + Ethertype)
#define ICSS_EMAC_PORT_0 (0) |
Used to specify host side port.
#define ICSS_EMAC_PORT_1 (1U) |
Used to specify physical port 1 MII 0 (tx)
#define ICSS_EMAC_PORT_2 (2U) |
Used to specify physical port 2 MII 1 (tx)
#define ICSS_EMAC_IOCTL_PORT_CTRL_DISABLE (0u) |
ICSS_EMAC_IOCTL_PORT_CTRL options.
Generic IOCTL Enable macro
#define ICSS_EMAC_IOCTL_PORT_CTRL_ENABLE (1u) |
Generic IOCTL Disable macro.
#define ICSS_EMAC_STORM_PREV_CTRL_ENABLE (0u) |
IOCTL Storm Control Enable command.
#define ICSS_EMAC_STORM_PREV_CTRL_DISABLE (1u) |
IOCTL Storm Control Disable command.
#define ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS (2u) |
IOCTL Storm Control set credit command.
#define ICSS_EMAC_STORM_PREV_CTRL_INIT (3u) |
IOCTL Storm Control initialize command.
#define ICSS_EMAC_STORM_PREV_CTRL_RESET (4u) |
IOCTL Storm Control reset command.
#define ICSS_EMAC_STORM_PREV_CTRL_ENABLE_BC (5u) |
IOCTL Storm Control Enable command for BC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_DISABLE_BC (6u) |
IOCTL Storm Control Disable command for BC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_BC (7u) |
IOCTL Storm Control set credit command for BC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_INIT_BC (8u) |
IOCTL Storm Control initialize command for BC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_RESET_BC (9u) |
IOCTL Storm Control reset command for BC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_ENABLE_MC (10u) |
IOCTL Storm Control Enable command for MC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_DISABLE_MC (11u) |
IOCTL Storm Control Disable command for MC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_MC (12u) |
IOCTL Storm Control set credit command for MC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_INIT_MC (13u) |
IOCTL Storm Control initialize command for MC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_RESET_MC (14u) |
IOCTL Storm Control reset command for MC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_ENABLE_UC (15u) |
IOCTL Storm Control Enable command for UC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_DISABLE_UC (16u) |
IOCTL Storm Control Disable command for UC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_SET_CREDITS_UC (17u) |
IOCTL Storm Control set credit command for UC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_INIT_UC (18u) |
IOCTL Storm Control initialize command for UC traffic.
#define ICSS_EMAC_STORM_PREV_CTRL_RESET_UC (19u) |
IOCTL Storm Control reset command for UC traffic.
#define ICSS_EMAC_LEARN_CTRL_UPDATE_TABLE (0u) |
IOCTL Learning Table update command.
#define ICSS_EMAC_LEARN_CTRL_CLR_TABLE (1u) |
IOCTL Learning Table clear table command.
#define ICSS_EMAC_LEARN_CTRL_AGEING (2u) |
IOCTL Learning Table age out entry command.
#define ICSS_EMAC_LEARN_CTRL_FIND_MAC (3u) |
IOCTL Learning Table find port from MAC ID command.
#define ICSS_EMAC_LEARN_CTRL_REMOVE_MAC (4u) |
IOCTL Learning Table remove a MAC ID from table command.
#define ICSS_EMAC_LEARN_CTRL_INC_COUNTER (5u) |
IOCTL Learning Table increment counters (for ageing) command.
#define ICSS_EMAC_LEARN_CTRL_INIT_TABLE (6u) |
IOCTL Learning Table initialize command.
#define ICSS_EMAC_LEARN_CTRL_SET_PORTSTATE (7u) |
IOCTL Learning Table set port state command.
#define ICSS_EMAC_IOCTL_STAT_CTRL_GET (0u) |
IOCTL Statistics get from PRU command.
#define ICSS_EMAC_IOCTL_STAT_CTRL_CLEAR (1u) |
IOCTL Statistics clear all counters command.
#define ICSS_EMAC_IOCTL_PORT_CTRL (0u) |
IOCTL select port control APIs command.
#define ICSS_EMAC_IOCTL_LEARNING_CTRL (1u) |
IOCTL select learning Table APIs command.
#define ICSS_EMAC_IOCTL_STORM_PREV_CTRL (2u) |
IOCTL select Storm Prevention APIs command.
#define ICSS_EMAC_IOCTL_STATS_CTRL (3u) |
IOCTL select Statistics APIs command.
#define ICSS_EMAC_IOCTL_PROMISCUOUS_CTRL (4u) |
IOCTL select Promiscuous Mode APIs command.
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL (5u) |
IOCTL select Multicast filtering APIs command.
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL (6u) |
IOCTL select Vlan filtering APIs command.
#define ICSS_EMAC_IOCTL_PORT_FLUSH_CTRL (7u) |
IOCTL select Port flush APIs command.
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_ENABLE (0u) |
IOCTL Multicast filter Control Enable command.
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_DISABLE (1u) |
IOCTL Multicast filter Control Disable command.
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_OVERRIDE_HASHMASK (2u) |
IOCTL Multicast filter Control override hashmask command.
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_ADD_MACID (3u) |
IOCTL Multicast filter Control allow MC MAC ID command.
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_REMOVE_MACID (4u) |
IOCTL Multicast filter Control do not allow MC MAC ID command.
#define ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_GET_DROPPED (5u) |
IOCTL Multicast filter Control do not allow MC MAC ID command.
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_ENABLE_CMD (0u) |
IOCTL Vlan filter Control Enable command.
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_DISABLE_CMD (1u) |
IOCTL Vlan filter Control Disable command.
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_UNTAG_HOST_RCV_ALL_CMD (2u) |
IOCTL Vlan filter allow Untagged frames Host Receive command.
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_UNTAG_HOST_RCV_NAL_CMD (3u) |
IOCTL Vlan filter do not allow Untagged frames Host Receive command.
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_PRIOTAG_HOST_RCV_ALL_CMD (4u) |
IOCTL Vlan filter allow Priority Tag frames Host Receive command.
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_PRIOTAG_HOST_RCV_NAL_CMD (5u) |
IOCTL Vlan filter do not allow Priority Tag frames Host Receive command.
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_ADD_VID_CMD (6u) |
IOCTL Vlan filter 4096 VIDs, 1 bit VIDs => 4096 bits = 512 bytes, ADD VLAN ID to allow packet to host
#define ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_REMOVE_VID_CMD (7u) |
IOCTL Vlan filter 4096 VIDs, 1 bit VIDs => 4096 bits = 512 bytes, Remove VLAN ID to do not allow packet to host
#define ICSS_EMAC_LEARNING_PORT_STATE_LEARNING (0U) |
Macros for different port states in learning module.
#define ICSS_EMAC_LEARNING_PORT_STATE_NOT_LEARNING (1U) |
#define ICSS_EMAC_LEARNING_PORT_STATE_LOCKED (2U) |
#define ICSS_EMAC_OBJECT_SIZE_IN_BYTES (42000) |
typedef struct ICSS_EMAC_Config_s* ICSS_EMAC_Handle |
Alias for ICSS EMAC Handle containing base addresses and modules.
typedef int32_t(* ICSS_EMAC_CallBack) (void *arg0, void *arg1, void *arg2) |
Definition for a generic callback function used in ICSS-EMAC.
While calling this, first argument is always of type ICSS_EMAC_Handle, second argument is specific to the callback (see ICSS_EMAC_CallBackObject), and third argument is userArg as specified in ICSS_EMAC_CallBackConfig.
void ICSS_EMAC_init | ( | void | ) |
This function initializes the ICSS_EMAC module.
void ICSS_EMAC_deinit | ( | void | ) |
This function de-initializes the ICSS_EMAC module.
void ICSS_EMAC_Params_init | ( | ICSS_EMAC_Params * | params | ) |
Initialize the parmeters data structure with defaults.
params | [out] Initialized parameters |
ICSS_EMAC_Handle ICSS_EMAC_open | ( | uint32_t | idx, |
const ICSS_EMAC_Params * | params | ||
) |
API to initialize and configure ICSS in MAC/Switch Mode.
[in] | idx | ICSS_EMAC instance number |
[in] | params | Structure of type ICSS_EMAC_Params |
void ICSS_EMAC_close | ( | ICSS_EMAC_Handle | icssEmacHandle | ) |
API to stop MAC/Switch Mode.
[in] | icssEmacHandle | Handle to ICSS_EMAC instance |
int32_t ICSS_EMAC_ioctl | ( | ICSS_EMAC_Handle | icssEmacHandle, |
uint32_t | ioctlCommand, | ||
uint8_t | portNo, | ||
void * | ioctlParams | ||
) |
IOCTL Function for ICSS EMAC.
This Function can be used to configure various ICSS EMAC Functionalities. The Supported features are: (1)Port Enable/Disable (2)StormControl (3)Learning configuration (4)Statistics module (5)Multicast filterring (6)VLAN filtering
[in] | icssEmacHandle | Handle to ICSS_EMAC instance |
[in] | ioctlCommand | Command from ICSS_EMAC_IOCTL_COMMANDS |
[in] | portNo | Port number for IOCTL |
[in,out] | ioctlParams | Pointer to structure of type ICSS_EMAC_IoctlCmd Please see following for setting ioctlParams.command ICSS_EMAC_IOCTL_STORM_PREV_CTRL_COMMANDS, ICSS_EMAC_IOCTL_LEARNING_CTRL_COMMANDS, ICSS_EMAC_IOCTL_STATISTICS_COMMANDS, ICSS_EMAC_IOCTL_MULTICAST_FILTER_CTRL_COMMANDS, ICSS_EMAC_IOCTL_VLAN_FILTER_CTRL_COMMANDS |
int32_t ICSS_EMAC_rxPktGet | ( | ICSS_EMAC_RxArgument * | rxArg, |
void * | userArg | ||
) |
Retrieves a frame from a host queue and copies it in the allocated stack buffer.
[in] | rxArg | Pointer to ICSS_EMAC_RxArgument structure |
[in] | userArg | Custom Rx packet callback packet options only required for custom RxPacket implementations, default to NULL when calling ICSS_EMAC_RxPktGet which is default Rx Packet API |
int32_t ICSS_EMAC_rxPktInfo | ( | ICSS_EMAC_Handle | icssEmacHandle, |
int32_t * | portNumber, | ||
int32_t * | queueNumber | ||
) |
API to retrieve the information about the received frame which is then used to dequeue the frame from the host queues.
[in] | icssEmacHandle | Handle to ICSS_EMAC instance |
[out] | portNumber | Return pointer of port number where frame was received |
[out] | queueNumber | Return pointer of host queue where the received frame is queued |
int32_t ICSS_EMAC_txPacket | ( | const ICSS_EMAC_TxArgument * | txArg, |
void * | userArg | ||
) |
API to queue a frame which has to be transmitted on the specified port queue.
[in] | txArg | Pointer to ICSS_EMAC_TxArgument |
[in] | userArg | Custom Tx packet callback packet options only required for custom TxPacket implementations, default to NULL when calling ICSS_EMAC_TxPacket which is default Tx Packet API |