AM275 FreeRTOS SDK  12.00.00

Introduction

AASRC channel related parameters and API.

Go to the source code of this file.

Data Structures

struct  AASRC_ChLockObj
 AASRC Channel lock semaphore structure. More...
 
struct  AASRC_FifoCfg
 Hardware FIFO setup structure. More...
 
struct  AASRC_FifoErrorStatus
 Hardware FIFO setup structure. More...
 
struct  AASRC_ChStatus
 AASRC channel status register. More...
 
struct  AASRC_ChCfg
 AASRC configuration parameters for the channel. More...
 
struct  AASRC_ClockZoneConfig
 Hardware setup clock zones. More...
 
struct  AASRC_ChClkCfg
 AASRC Channel Clock Config. More...
 
struct  AASRC_ChObj
 AASRC Channel object. More...
 

Macros

#define AASRC_DEFAULT_IN_FIFO_THRESHOLD   (16U)
 Default Input fifo threshold. More...
 
#define AASRC_DEFAULT_OUT_FIFO_THRESHOLD   (16U)
 Default Output fifo threshold. More...
 
#define AASRC_MAX_IN_FIFO_THRESHOLD   (32U)
 Max Input fifo threshold. More...
 
#define AASRC_MAX_OUT_FIFO_THRESHOLD   (32U)
 Max Output fifo threshold. More...
 
#define AASRC_MAX_ATTENUATION   (255U)
 AASRC maximum attenuation setting. More...
 
#define AASRC_MAX_DEEMPHASIS_MODES   (4U)
 AASRC maximum number of de-emphasis modes. More...
 
#define AASRC_SRC_FIFO_CONTROL_REG_OFFSET   (0x00000010U)
 SRC Fifo control register offset. More...
 
#define AASRC_SRC_FIFO_CONTROL(x)
 Find base address of SRC 'x' Fifo Control Register. More...
 
#define AASRC_SRC_CONTROL_REG_OFFSET   (0x00000010U)
 SRC control register offset. More...
 
#define AASRC_SRC_CONTROL(x)
 Find base address of SRC 'x' Control Register. More...
 
#define AASRC_SRC_STATUS_REG_OFFSET   (0x00000010U)
 SRC status register offset. More...
 
#define AASRC_SRC_STATUS(x)
 Find base address of SRC 'x' Status Register. More...
 
#define AASRC_GROUP_FIFO_CONTROL_REG_OFFSET   (0x00000008U)
 SRC Group fifo control register offset. More...
 
#define AASRC_GROUP_FIFO_CONTROL(x)
 Find base address of Group 'x' Fifo Control Register. More...
 
#define AASRC_GROUP_SRC_CONTROL_REG_OFFSET   (0x00000008U)
 SRC Group control register offset. More...
 
#define AASRC_GROUP_SRC_CONTROL(x)
 Find base address of Group 'x' Control Register. More...
 
#define AASRC_GROUP_SELECT_REG_OFFSET   (0x00000004U)
 SRC Group select register offset. More...
 
#define AASRC_INPUT_GROUP_SELECT(x)
 Find base address of Input Group 'x' Select Register. More...
 
#define AASRC_OUTPUT_GROUP_SELECT(x)
 Find base address of Output Group 'x' Select Register. More...
 
AASRC Channel Id

Values used to determine the channel number used for AASRC communication. This determines which ASRC channel to use.

#define AASRC_CHANNEL_0   (0U)
 
#define AASRC_CHANNEL_1   (1U)
 
#define AASRC_CHANNEL_2   (2U)
 
#define AASRC_CHANNEL_3   (3U)
 
#define AASRC_CHANNEL_4   (4U)
 
#define AASRC_CHANNEL_5   (5U)
 
#define AASRC_CHANNEL_6   (6U)
 
#define AASRC_CHANNEL_7   (7U)
 
AASRC Group Id

This represents the number of channel groups available in the AASRC IPs. Max number of groups in the chip is SOC dependent.

#define AASRC_GROUP0   (0U)
 
#define AASRC_GROUP1   (1U)
 
#define AASRC_GROUP2   (2U)
 
#define AASRC_GROUP3   (3U)
 
AASRC Data Length

AASRC allowed sample word length

#define AASRC_SAMPLE_WORD_LENGTH_24   (24U)
 
#define AASRC_SAMPLE_WORD_LENGTH_20   (20U)
 
#define AASRC_SAMPLE_WORD_LENGTH_18   (18U)
 
#define AASRC_SAMPLE_WORD_LENGTH_16   (16U)
 
AASRC Group Delay

Interpolation filter group delay supported by AASRC. This represents the number of samples which are prebuffered prior to the re-sampler function.

#define AASRC_GROUP_DELAY_64   (64U)
 
#define AASRC_GROUP_DELAY_32   (32U)
 
#define AASRC_GROUP_DELAY_16   (16U)
 
#define AASRC_GROUP_DELAY_8   (8U)
 

Functions

AASRC_ChHandle AASRC_chOpen (uint8_t chIdx, AASRC_Handle drvHandle)
 Function to allocate a required ASRC channel. More...
 
AASRC_ChHandle AASRC_getChHandle (uint8_t instIdx, uint8_t chIdx)
 This function returns the handle of an open AASRC Channel from the instance index & channel index. More...
 
int32_t AASRC_chConfigInit (AASRC_ChHandle chHandle)
 Function initialize AASRC_ChCfg. More...
 
int32_t AASRC_chConfig (AASRC_ChHandle chHandle)
 Function to configure ASRC channels. More...
 
int32_t AASRC_chEnable (AASRC_ChHandle chHandle)
 AASRC channel enable. More...
 
int32_t AASRC_chDisable (AASRC_ChHandle chHandle)
 AASRC channel disable. More...
 
int32_t AASRC_isChEnabled (AASRC_ChHandle chHandle, uint32_t *isEnabled)
 is ASRC channel enabled More...
 
int32_t AASRC_chClose (AASRC_ChHandle chHandle)
 AASRC channel close. More...
 
int32_t AASRC_setTxTxnCount (AASRC_ChHandle chHandle, uint32_t txnCount)
 Function to set the Tx transaction count. More...
 
int32_t AASRC_setRxTxnCount (AASRC_ChHandle chHandle, uint32_t txnCount)
 Function to set the Rx transaction count. More...
 

Variables

AASRC_ChObjgConfigAasrcChObj []
 Externally defined driver configuration array. More...
 
AASRC_ChLockObj gAasrcChLockObj
 AASRC Channel lock object. More...