AM275 FreeRTOS SDK  12.00.00

Introduction

This module contains APIs to program and use the AASRC module. The APIs can be used by other drivers to get access to AASRC hardware module and also by applications to convert sample rates of audio streams.

Sub Modules

 AASRC Channel Configuration APIs
 
 AASRC Channel Types
 
 AASRC Clock Zone Configuration
 
 AASRC DMA
 
 AASRC Soc Specific Parameters
 
 AASRC Transactions
 

Files

file  aasrc/v0/aasrc.h
 AASRC Driver API/interface file.
 

Data Structures

struct  AASRC_OpenParams
 AASRC Parameters. More...
 
struct  AASRC_Attrs
 AASRC hardware instance attributes - used during init time. More...
 
struct  AASRC_Object
 AASRC driver object. More...
 
struct  AASRC_Config
 AASRC global configuration array. More...
 

Functions

void AASRC_init (void)
 This function initializes the AASRC module. More...
 
void AASRC_deinit (void)
 This function de-initializes the AASRC module. More...
 
static void AASRC_OpenParamsInit (AASRC_Object *drvObj)
 Function to initialize the AASRC_OpenParams struct to its defaults. More...
 
AASRC_Handle AASRC_open (uint8_t instNum, const AASRC_OpenParams *openParams)
 This function opens a given AASRC IP Core. More...
 
void AASRC_close (AASRC_Handle drvHandle)
 Function to close a AASRC IP Core specified by the AASRC handle. More...
 
AASRC_Handle AASRC_getHandle (uint32_t index)
 This function returns the handle of an open AASRC Instance from the instance index. More...
 
void AASRC_softReset (AASRC_Handle drvHandle)
 Function to soft reset a AASRC IP Core specified by the AASRC handle. More...
 

Function Documentation

◆ AASRC_init()

void AASRC_init ( void  )

This function initializes the AASRC module.

◆ AASRC_deinit()

void AASRC_deinit ( void  )

This function de-initializes the AASRC module.

◆ AASRC_OpenParamsInit()

static void AASRC_OpenParamsInit ( AASRC_Object drvObj)
inlinestatic

Function to initialize the AASRC_OpenParams struct to its defaults.

Parameters
drvObjPointer to AASRC_Object structure for initialization of OpenParams with default

◆ AASRC_open()

AASRC_Handle AASRC_open ( uint8_t  instNum,
const AASRC_OpenParams openParams 
)

This function opens a given AASRC IP Core.

Precondition
AASRC driver parameters have to be initialized using AASRC_init()
Parameters
instNumIndex of config to use in the AASRC_Config array
openParamsPointer to parameters to open the driver with
Returns
A AASRC_Handle on success or a NULL on an error or if it has been opened already
See also
AASRC_init()
AASRC_close()

◆ AASRC_close()

void AASRC_close ( AASRC_Handle  drvHandle)

Function to close a AASRC IP Core specified by the AASRC handle.

Precondition
AASRC_open() has to be called first
Parameters
drvHandleAASRC_Handle returned from AASRC_open()
See also
AASRC_open()

◆ AASRC_getHandle()

AASRC_Handle AASRC_getHandle ( uint32_t  index)

This function returns the handle of an open AASRC Instance from the instance index.

Precondition
AASRC controller has been opened using AASRC_open()
Parameters
indexIndex of config to use in the AASRC_Config array
Returns
A AASRC_Handle if it has been opened already or NULL otherwise
See also
AASRC_init()
AASRC_open()

◆ AASRC_softReset()

void AASRC_softReset ( AASRC_Handle  drvHandle)

Function to soft reset a AASRC IP Core specified by the AASRC handle.

Precondition
AASRC_open() has to be called first
Parameters
drvHandleAASRC_Handle returned from AASRC_open()
See also
AASRC_open()

Variable Documentation

◆ gAasrcConfig

AASRC_Config gAasrcConfig[]
extern

Externally defined driver configuration array.

◆ gAasrcInstNum

uint8_t gAasrcInstNum
extern

Externally defined driver configuration array size.

◆ gAasrcConfigChNum

uint8_t gAasrcConfigChNum[]
extern

Externally defined channel configuration array size

◆ gAasrcRxClkZoneNum

uint8_t gAasrcRxClkZoneNum[]
extern

Externally defined Rx Clockzone configuration array size

◆ gAasrcTxClkZoneNum

uint8_t gAasrcTxClkZoneNum[]
extern

Externally defined Tx Clockzone configuration array size