AM275 FreeRTOS SDK  12.00.00

Detailed Description

Hardware FIFO setup structure.

Data Fields

uint32_t inFifoThreshold
 
uint32_t outFifoThreshold
 

Field Documentation

◆ inFifoThreshold

uint32_t AASRC_FifoCfg::inFifoThreshold

Number of spaces in the input fifo, that must be available for the interrupt/event to fire

◆ outFifoThreshold

uint32_t AASRC_FifoCfg::outFifoThreshold

Number of samples that must be available in the output fifo for the interrupt/event to fire