This file contains the type definitions and helper macros for the CPSW peripheral interface.
This CPSW peripheral implementation supports CPSW_2G, CPSW_5G and CPSW_9G found in SoCs of the Jacinto 7 family.
Go to the source code of this file.
Macros | |
| #define | CPSW_PER_PUBLIC_IOCTL(x) |
| Helper macro to create CPSW IOCTL commands. More... | |
| #define | CPSW_MAC_PORT_NUM (8U) |
| #define | CPSW_INTR_STATS_PEND0 (1U) |
| CPSW statistics interrupt id. More... | |
| #define | CPSW_INTR_MDIO_PEND (2U) |
| CPSW MDIO interrupt id. More... | |
| #define | CPSW_INTR_EVNT_PEND (3U) |
| CPSW event pending interrupt (CPTS) id. More... | |
CPSW InterVLAN ingress packet match types. | |
Ingress packet match criteria for interVLAN routing. Each packet match criteria is represented by a bit. To enable multiple match criteria create bitmask ORing required ingress packet match criteria defines | |
| #define | CPSW_INTERVLAN_INGRESSPKT_MATCH_PORT (CPSW_ALE_POLICER_MATCH_PORT) |
| Enable classifier match with PORT number. More... | |
| #define | CPSW_INTERVLAN_INGRESSPKT_MATCH_MACSRC (CPSW_ALE_POLICER_MATCH_MACSRC) |
| Enable classifier match with MAC source address entry. More... | |
| #define | CPSW_INTERVLAN_INGRESSPKT_MATCH_MACDST (CPSW_ALE_POLICER_MATCH_MACDST) |
| Enable classifier match with MAC destination address entry. More... | |
| #define | CPSW_INTERVLAN_INGRESSPKT_MATCH_ETHERTYPE (CPSW_ALE_POLICER_MATCH_ETHERTYPE) |
| Enable classifier match with MAC destination address entry. More... | |
| #define | CPSW_INTERVLAN_INGRESSPKT_MATCH_IPSRC (CPSW_ALE_POLICER_MATCH_IPSRC) |
| Enable classifier match with IPv4/IPv6 source address. More... | |
| #define | CPSW_INTERVLAN_INGRESSPKT_MATCH_IPDST (CPSW_ALE_POLICER_MATCH_IPDST) |
| Enable classifier match with IPv4/IPv6 destination address. More... | |
Typedefs | |
| typedef void(* | Cpsw_MdioLinkStateChangeCb) (Cpsw_MdioLinkStateChangeInfo *info, void *appArg) |
| CPSW PHY link state change callback function. More... | |
| typedef void(* | Cpsw_PortLinkStatusChangeCb) (Enet_MacPort macPort, bool isLinkUp, void *appArg) |
| CPSW port link status change callback function. More... | |
Enumerations | |
| enum | Cpsw_Ioctl { CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS = CPSW_PER_PUBLIC_IOCTL(0U), CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_UNI_EGRESS = CPSW_PER_PUBLIC_IOCTL(1U), CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS = CPSW_PER_PUBLIC_IOCTL(2U), CPSW_PER_IOCTL_CLEAR_INTERVLAN_ROUTE_MULTI_EGRESS = CPSW_PER_PUBLIC_IOCTL(3U), CPSW_PER_IOCTL_SET_SHORT_IPG_CFG = CPSW_PER_PUBLIC_IOCTL(4U), CPSW_PER_IOCTL_GET_SHORT_IPG_CFG = CPSW_PER_PUBLIC_IOCTL(5U) } |
| CPSW peripheral IOCTL commands. More... | |