Input args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_MULTI_EGRESS command.
Data Fields | |
| uint32_t | numEgressPorts |
| Cpsw_InterVlanEgressPortCfg | egressCfg [CPSW_ALE_NUM_MAC_PORTS] |
| Cpsw_InterVlanRouteIngressPktMatchCfg | inPktMatchCfg |
| uint32_t Cpsw_SetInterVlanRouteMultiEgressInArgs::numEgressPorts |
Number of egress ports the packet needs to be routed to
| Cpsw_InterVlanEgressPortCfg Cpsw_SetInterVlanRouteMultiEgressInArgs::egressCfg[CPSW_ALE_NUM_MAC_PORTS] |
Egress packet modification configuration for the interVLAN route for each port the packet will be routed to. numEgressPorts determine number of valid entries in this table
| Cpsw_InterVlanRouteIngressPktMatchCfg Cpsw_SetInterVlanRouteMultiEgressInArgs::inPktMatchCfg |
Ingress packet match criteria for the interVLAN route. If the packet matches the given criteria and the destination port of the packet is host port then the interVLAN route will take effect