Input args for CPSW_PER_IOCTL_SET_INTERVLAN_ROUTE_UNI_EGRESS command.
Data Fields | |
| Cpsw_InterVlanRouteIngressPktMatchCfg | inPktMatchCfg |
| Cpsw_InterVlanEgressPortCfg | egressCfg |
| Cpsw_InterVlanRouteIngressPktMatchCfg Cpsw_SetInterVlanRouteUniEgressInArgs::inPktMatchCfg |
Ingress packet match criteria for the interVLAN route. If the packet matches the given criteria and the destination port of the packet is host port then the interVLAN route will take effect
| Cpsw_InterVlanEgressPortCfg Cpsw_SetInterVlanRouteUniEgressInArgs::egressCfg |
Egress packet modification configuration for the interVLAN route