AM273x MCU+ SDK  08.03.00

Introduction

APIs related to CSIRX complex IO lanes

Data Structures

struct  CSIRX_ComplexioLaneConfig
 Lane configuration. More...
 
struct  CSIRX_ComplexioLaneIntr
 Complex IO per lane interrupt. More...
 
struct  CSIRX_ComplexioLanesIntr
 Complex IO all (logical) lanes interrupts. More...
 
struct  CSIRX_ComplexioLanesConfig
 All lanes configuration. More...
 
struct  CSIRX_ComplexioConfig
 Complex IO configuration. More...
 

Functions

void CSIRX_ComplexioConfig_init (CSIRX_ComplexioConfig *config)
 Sets default values for configuration. More...
 
int32_t CSIRX_complexioSetConfig (CSIRX_Handle handle, CSIRX_ComplexioConfig *config)
 Configure Complex IO. More...
 
int32_t CSIRX_complexioClearAllIntr (CSIRX_Handle handle)
 Celar all pending complex IO interrupts. More...
 
int32_t CSIRX_complexioGetPendingIntr (CSIRX_Handle handle, CSIRX_ComplexioLanesIntr *intrStatus)
 Get all pending complex IO interrupts. More...
 
int32_t CSIRX_complexioGetPowerStatus (CSIRX_Handle handle, uint8_t *powerStatus)
 Query about ComplexIO power status. More...
 
int32_t CSIRX_complexioSetPowerCommand (CSIRX_Handle handle, uint8_t powerCommand)
 Set Complex IO power command. More...
 
int32_t CSIRX_complexioDeassertReset (CSIRX_Handle handle)
 Deaasert complex IO reset. More...
 
int32_t CSIRX_complexioAssertForceRxModeOn (CSIRX_Handle handle)
 Assert Force Rx Mode on complex IO. More...
 
int32_t CSIRX_complexioDeassertForceRxModeOn (CSIRX_Handle handle)
 De-assert Force Rx Mode on complex IO. More...
 
int32_t CSIRX_complexioIsResetDone (CSIRX_Handle handle, bool *isDone)
 Check if complex IO reset is done. More...
 
int32_t CSIRX_complexioIsDeassertForceRxModeOn (CSIRX_Handle handle, bool *isDeasserted)
 Check if force RX mode on is deasserted. More...
 
static int32_t CSIRX_complexioPowerOn (CSIRX_Handle handle)
 Power ON complex IO. More...
 
static int32_t CSIRX_complexioPowerOff (CSIRX_Handle handle)
 Power OFF complex IO. More...
 
static int32_t CSIRX_complexioUltraLowPower (CSIRX_Handle handle)
 Put complex IO in ULP (Ultra Low Power) state. More...
 

Macros

#define CSIRX_DATA_LANES_MAX   (4U)
 Max possible data lanes. More...
 

Complex IO power commands

#define CSIRX_COMPLEXIO_POWER_COMMAND_OFF   (0U)
 Power off ComplexIO. More...
 
#define CSIRX_COMPLEXIO_POWER_COMMAND_ON   (1U)
 Power on ComplexIO. More...
 
#define CSIRX_COMPLEXIO_POWER_COMMAND_ULP   (2U)
 Put ComplexIO in ULP (Ultra Low Power) state. More...
 

Complex IO power status

#define CSIRX_COMPLEXIO_POWER_STATUS_OFF   (0U)
 Complex IO power status OFF. More...
 
#define CSIRX_COMPLEXIO_POWER_STATUS_ON   (1U)
 Complex IO power status ON. More...
 
#define CSIRX_COMPLEXIO_POWER_STATUS_ULP   (2U)
 Complex IO power status ULP (Ultra Low Power) More...
 

Lane polarity

#define CSIRX_LANE_POLARITY_PLUS_MINUS   (0U)
 Lane polarity +/-. More...
 
#define CSIRX_LANE_POLARITY_MINUS_PLUS   (1U)
 Lane polarity -/+. More...
 

Lane position

#define CSIRX_LANE_POSITION_LANE_NOT_USED   (0U)
 Lane not used. More...
 
#define CSIRX_LANE_POSITION_1   (1U)
 Physical lane position #1. More...
 
#define CSIRX_LANE_POSITION_2   (2U)
 Physical lane position #2. More...
 
#define CSIRX_LANE_POSITION_3   (3U)
 Physical lane position #3. More...
 
#define CSIRX_LANE_POSITION_4   (4U)
 Physical lane position #4. More...
 
#define CSIRX_LANE_POSITION_5   (5U)
 Physical lane position #5. More...
 

Macro Definition Documentation

◆ CSIRX_DATA_LANES_MAX

#define CSIRX_DATA_LANES_MAX   (4U)

Max possible data lanes.

◆ CSIRX_COMPLEXIO_POWER_COMMAND_OFF

#define CSIRX_COMPLEXIO_POWER_COMMAND_OFF   (0U)

Power off ComplexIO.

◆ CSIRX_COMPLEXIO_POWER_COMMAND_ON

#define CSIRX_COMPLEXIO_POWER_COMMAND_ON   (1U)

Power on ComplexIO.

◆ CSIRX_COMPLEXIO_POWER_COMMAND_ULP

#define CSIRX_COMPLEXIO_POWER_COMMAND_ULP   (2U)

Put ComplexIO in ULP (Ultra Low Power) state.

◆ CSIRX_COMPLEXIO_POWER_STATUS_OFF

#define CSIRX_COMPLEXIO_POWER_STATUS_OFF   (0U)

Complex IO power status OFF.

◆ CSIRX_COMPLEXIO_POWER_STATUS_ON

#define CSIRX_COMPLEXIO_POWER_STATUS_ON   (1U)

Complex IO power status ON.

◆ CSIRX_COMPLEXIO_POWER_STATUS_ULP

#define CSIRX_COMPLEXIO_POWER_STATUS_ULP   (2U)

Complex IO power status ULP (Ultra Low Power)

◆ CSIRX_LANE_POLARITY_PLUS_MINUS

#define CSIRX_LANE_POLARITY_PLUS_MINUS   (0U)

Lane polarity +/-.

◆ CSIRX_LANE_POLARITY_MINUS_PLUS

#define CSIRX_LANE_POLARITY_MINUS_PLUS   (1U)

Lane polarity -/+.

◆ CSIRX_LANE_POSITION_LANE_NOT_USED

#define CSIRX_LANE_POSITION_LANE_NOT_USED   (0U)

Lane not used.

◆ CSIRX_LANE_POSITION_1

#define CSIRX_LANE_POSITION_1   (1U)

Physical lane position #1.

◆ CSIRX_LANE_POSITION_2

#define CSIRX_LANE_POSITION_2   (2U)

Physical lane position #2.

◆ CSIRX_LANE_POSITION_3

#define CSIRX_LANE_POSITION_3   (3U)

Physical lane position #3.

◆ CSIRX_LANE_POSITION_4

#define CSIRX_LANE_POSITION_4   (4U)

Physical lane position #4.

◆ CSIRX_LANE_POSITION_5

#define CSIRX_LANE_POSITION_5   (5U)

Physical lane position #5.

Function Documentation

◆ CSIRX_ComplexioConfig_init()

void CSIRX_ComplexioConfig_init ( CSIRX_ComplexioConfig config)

Sets default values for configuration.

Parameters
config[in] configuration

◆ CSIRX_complexioSetConfig()

int32_t CSIRX_complexioSetConfig ( CSIRX_Handle  handle,
CSIRX_ComplexioConfig config 
)

Configure Complex IO.

Parameters
handle[in] CSIRX driver handle
config[in] Complex IO configuration
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioClearAllIntr()

int32_t CSIRX_complexioClearAllIntr ( CSIRX_Handle  handle)

Celar all pending complex IO interrupts.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioGetPendingIntr()

int32_t CSIRX_complexioGetPendingIntr ( CSIRX_Handle  handle,
CSIRX_ComplexioLanesIntr intrStatus 
)

Get all pending complex IO interrupts.

Parameters
handle[in] CSIRX driver handle
intrStatus[out] Interrupt status
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioGetPowerStatus()

int32_t CSIRX_complexioGetPowerStatus ( CSIRX_Handle  handle,
uint8_t *  powerStatus 
)

Query about ComplexIO power status.

See also
CSIRX_complexioPowerOn, CSIRX_complexioPowerOff, CSIRX_complexioUltraLowPower
Parameters
handle[in] CSIRX driver handle
powerStatus[out] One of CSIRX_COMPLEXIO_POWER_STATUS
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioSetPowerCommand()

int32_t CSIRX_complexioSetPowerCommand ( CSIRX_Handle  handle,
uint8_t  powerCommand 
)

Set Complex IO power command.

Parameters
handle[in] CSIRX driver handle
powerCommand[out] one of CSIRX_COMPLEXIO_POWER_COMMAND
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioDeassertReset()

int32_t CSIRX_complexioDeassertReset ( CSIRX_Handle  handle)

Deaasert complex IO reset.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioAssertForceRxModeOn()

int32_t CSIRX_complexioAssertForceRxModeOn ( CSIRX_Handle  handle)

Assert Force Rx Mode on complex IO.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioDeassertForceRxModeOn()

int32_t CSIRX_complexioDeassertForceRxModeOn ( CSIRX_Handle  handle)

De-assert Force Rx Mode on complex IO.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioIsResetDone()

int32_t CSIRX_complexioIsResetDone ( CSIRX_Handle  handle,
bool *  isDone 
)

Check if complex IO reset is done.

Parameters
handle[in] CSIRX driver handle
isDone[out] true: reset is done, false: reset is not done
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioIsDeassertForceRxModeOn()

int32_t CSIRX_complexioIsDeassertForceRxModeOn ( CSIRX_Handle  handle,
bool *  isDeasserted 
)

Check if force RX mode on is deasserted.

Parameters
handle[in] CSIRX driver handle
isDeasserted[out] true: deassert is done, false: deassert is not done
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioPowerOn()

static int32_t CSIRX_complexioPowerOn ( CSIRX_Handle  handle)
inlinestatic

Power ON complex IO.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioPowerOff()

static int32_t CSIRX_complexioPowerOff ( CSIRX_Handle  handle)
inlinestatic

Power OFF complex IO.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_complexioUltraLowPower()

static int32_t CSIRX_complexioUltraLowPower ( CSIRX_Handle  handle)
inlinestatic

Put complex IO in ULP (Ultra Low Power) state.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure