AM273x MCU+ SDK  08.03.00
CSIRX_ComplexioLanesIntr Struct Reference

Detailed Description

Complex IO all (logical) lanes interrupts.

This represents both status and configuration (enable/disable) structures. The description of the fields is in terms of status. For configuration they should be interpreted as "true if you want to enable the detection of this condition, false otherwise". For status, the interrupts can be cleared by issuing CSIRX_complexioClearAllIntr API

Data Fields

bool isAllLanesEnterULPM
 true if all lanes transitioned to ULPM (Ultra Low Power Mode) More...
 
bool isAllLanesExitULPM
 true if at least one of the active lanes has exit ULPM (Ultra Low Power Mode) More...
 
CSIRX_ComplexioLaneIntr dataLane [CSIRX_DATA_LANES_MAX]
 data lanes interrupt configuration More...
 
CSIRX_ComplexioLaneIntr clockLane
 clock lane interrupt configuration More...
 

Field Documentation

◆ isAllLanesEnterULPM

bool CSIRX_ComplexioLanesIntr::isAllLanesEnterULPM

true if all lanes transitioned to ULPM (Ultra Low Power Mode)

◆ isAllLanesExitULPM

bool CSIRX_ComplexioLanesIntr::isAllLanesExitULPM

true if at least one of the active lanes has exit ULPM (Ultra Low Power Mode)

◆ dataLane

CSIRX_ComplexioLaneIntr CSIRX_ComplexioLanesIntr::dataLane[CSIRX_DATA_LANES_MAX]

data lanes interrupt configuration

◆ clockLane

CSIRX_ComplexioLaneIntr CSIRX_ComplexioLanesIntr::clockLane

clock lane interrupt configuration