AM273x MCU+ SDK  08.03.00

Introduction

APIs to open/close top level CSIRX instance's

Data Structures

struct  CSIRX_Info
 CSIRX Instance information. More...
 
struct  CSIRX_ContextObject
 Context specific state information, not to be used by end users. More...
 
struct  CSIRX_Object
 CSIRX Instance Object. Used internally, not to be used by end users. More...
 
struct  CSIRX_HwAttrs
 CSIRX HW Attributes. Generated when using sysconfig. More...
 
struct  CSIRX_Config
 CSIRX Instance Config Object. More...
 

Functions

int32_t CSIRX_init ()
 Initialize CSIRX driver. More...
 
int32_t CSIRX_deinit ()
 De-Initialize CSIRX driver. More...
 
CSIRX_Handle CSIRX_open (uint32_t instanceId)
 Open CSIRX driver. More...
 
int32_t CSIRX_getInfo (CSIRX_Handle handle, CSIRX_Info *info)
 Get CSIRX instance info. More...
 
int32_t CSIRX_reset (CSIRX_Handle handle)
 Reset CSIRX instance. More...
 
int32_t CSIRX_close (CSIRX_Handle handle)
 Close CSIRX instance. More...
 

Typedefs

typedef struct CSIRX_Config_s * CSIRX_Handle
 CSIRX driver handle. More...
 

Macros

#define CSIRX_INTERRUPT_NOT_CONNECTED_ID   (0xFFFFU)
 Interrupt number ID to indicate, this interrupt line is not connected in this CPU. More...
 

FIFO depth

#define CSIRX_FIFODEPTH_8X68   (2U)
 FIFO depth is 8 times 68-bits. More...
 
#define CSIRX_FIFODEPTH_16X68   (3U)
 FIFO depth is 16 times 68-bits. More...
 
#define CSIRX_FIFODEPTH_32X68   (4U)
 FIFO depth is 32 times 68-bits. More...
 
#define CSIRX_FIFODEPTH_64X68   (5U)
 FIFO depth is 64 times 68-bits. More...
 
#define CSIRX_FIFODEPTH_128X68   (6U)
 FIFO depth is 128 times 68-bits. More...
 
#define CSIRX_FIFODEPTH_256X68   (7U)
 FIFO depth is 256 times 68-bits. More...
 

Macro Definition Documentation

◆ CSIRX_INTERRUPT_NOT_CONNECTED_ID

#define CSIRX_INTERRUPT_NOT_CONNECTED_ID   (0xFFFFU)

Interrupt number ID to indicate, this interrupt line is not connected in this CPU.

◆ CSIRX_FIFODEPTH_8X68

#define CSIRX_FIFODEPTH_8X68   (2U)

FIFO depth is 8 times 68-bits.

◆ CSIRX_FIFODEPTH_16X68

#define CSIRX_FIFODEPTH_16X68   (3U)

FIFO depth is 16 times 68-bits.

◆ CSIRX_FIFODEPTH_32X68

#define CSIRX_FIFODEPTH_32X68   (4U)

FIFO depth is 32 times 68-bits.

◆ CSIRX_FIFODEPTH_64X68

#define CSIRX_FIFODEPTH_64X68   (5U)

FIFO depth is 64 times 68-bits.

◆ CSIRX_FIFODEPTH_128X68

#define CSIRX_FIFODEPTH_128X68   (6U)

FIFO depth is 128 times 68-bits.

◆ CSIRX_FIFODEPTH_256X68

#define CSIRX_FIFODEPTH_256X68   (7U)

FIFO depth is 256 times 68-bits.

Typedef Documentation

◆ CSIRX_Handle

typedef struct CSIRX_Config_s* CSIRX_Handle

CSIRX driver handle.

Function Documentation

◆ CSIRX_init()

int32_t CSIRX_init ( )

Initialize CSIRX driver.

This does not touch the HW itself, it only initialized internal data structures. Called by SysConfig as part of System_init()

Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_deinit()

int32_t CSIRX_deinit ( )

De-Initialize CSIRX driver.

This does not touch the HW itself, it only de-initialized internal data structures. Called by SysConfig as part of System_deinit()

Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_open()

CSIRX_Handle CSIRX_open ( uint32_t  instanceId)

Open CSIRX driver.

Parameters
instanceId[in] CSIRX config to open. This acts as a index into gCsirxConfig[]
Returns
Handle to CSIRX driver for given instance. NULL in case of failure

◆ CSIRX_getInfo()

int32_t CSIRX_getInfo ( CSIRX_Handle  handle,
CSIRX_Info info 
)

Get CSIRX instance info.

Parameters
handle[in] CSIRX driver handle
info[out] Instance information
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_reset()

int32_t CSIRX_reset ( CSIRX_Handle  handle)

Reset CSIRX instance.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

◆ CSIRX_close()

int32_t CSIRX_close ( CSIRX_Handle  handle)

Close CSIRX instance.

Parameters
handle[in] CSIRX driver handle
Returns
SystemP_SUCCESS on success, else failure

Variable Documentation

◆ gCsirxConfig

CSIRX_Config gCsirxConfig[]
extern

Array of CSIRX instance enabled via SysConfig.

◆ gCsirxConfigNum

uint32_t gCsirxConfigNum
extern

Number of CSIRX instances enabled via SysConfig.