RadioTestLibrary  1.34.0
Public Member Functions
RTLDevice26_13xx Class Reference

#include <rtl_device_26_13xx.h>

Inheritance diagram for RTLDevice26_13xx:
Inheritance graph
[legend]
Collaboration diagram for RTLDevice26_13xx:
Collaboration graph
[legend]

Public Member Functions

 RTLDevice26_13xx (void)
 
virtual ~RTLDevice26_13xx (void)
 
int addDynamicOverride (const QString &devId, const QString &type, const QString &value, const QString &id)
 Add Dynamic Override. More...
 
int connect (const QString rfDevName, const QString &devId)
 Connect to target device. More...
 
int removeDynamicOverride (const QString &devId, const QString &id)
 Remove Dynamic Override. More...
 
int doLinkTest (const QString &txId, const QString &rxId, TestResult_t *pTestResult)
 Run link test. More...
 
int startPacketTx (const QString &txId)
 Start a packet transmission with pre configured packets, interval and number of packets. More...
 
int eraseFlash (const QString &devName, const QString &devId, EraseInfo_t *pEraseInfo=NULL, FPLFile *pFile=NULL)
 Erase Flash (FPL Feature) More...
 
int executeCmd (const QString &devId, quint8 *pCmd, const quint16 &cmdLength, quint32 *pCmdResult)
 Execute Command. More...
 
int programFlash (const QString &devName, const QString &devId, FPLFile *pFplFile, ProgramInfo_t *pProgInfo=NULL)
 Program Flash from file (FPL Feature) More...
 
int programFlash (const QString &devName, const QString &devId, const quint32 &address, const quint32 &length, quint8 *pBuffer)
 Program Flash from buffer (FPL Feature) More...
 
int readCmdSettingsFromFile (const QString &devId, TestConfig_t &testConfig)
 Read command settings from file. More...
 
int readFrequencyOffset (const QString &devId, TestResult_t *pTestResult)
 Read frequency offset value from given device. More...
 
int readFrequencyOffsetCW (const QString &devId, TestResult_t *pTestResult)
 Read frequency offset value from given device when receiving CW. More...
 
int readMcuReg (const QString &devId, const quint32 &address, quint32 *pValue)
 Read MCU Register. More...
 
int readMemory (const QString &devName, const QString &devId, const quint32 &address, quint32 *pLength, quint8 *pBuffer)
 Read memory (FPL Feature) More...
 
int readRfReg (const QString &devId, const quint32 &address, quint32 *pValue)
 Read RF core Register. More...
 
int verifyFlash (const QString &devName, const QString &devId, FPLFile *pFplFile, ProgramInfo_t *pProgInfo=NULL)
 Verify Flash (FPL Feature) More...
 
int writeMemory (const QString &devName, const QString &devId, const quint32 &address, const quint32 &length, quint8 *pBuffer)
 Write memory (FPL Feature) More...
 
int writeMcuReg (const QString &devId, const quint32 &address, const quint32 &value)
 Write MCU Register. More...
 
int writeRfReg (const QString &devId, const quint32 &address, const quint32 &value)
 Write RF core Register. More...
 
int runCpu (const QString &devName, const QString &devId, bool debugMode)
 Run CPU (FPL Feature) More...
 
int haltCpu (const QString &devName, const QString &devId)
 Halt CPU (FPL Feature) More...
 
int writeCpuReg (const QString &devName, const QString &devId, const CM3_CPU_REGISTERS &regNumber, const uint32_t &value)
 Write CPU register (FPL Feature) More...
 
int readCpuReg (const QString &devName, const QString &devId, const CM3_CPU_REGISTERS &regNumber, uint32_t *pValue)
 Read CPU register (FPL Feature) More...
 
int setCapArrayDelta (const QString &devId, const qint16 &value)
 Set Cap Array Delta. More...
 
- Public Member Functions inherited from RTLDevice
 RTLDevice (void)
 
virtual ~RTLDevice (void)
 
virtual void appendError (const QString &error)
 Append error. More...
 
virtual void clearAllErrors (void)
 Clear errors. More...
 
virtual int deleteFileObject (FPLFile *pFplFile)
 Delete file Object. More...
 
virtual int disconnect (const QString &devId)
 Disconnect target device. More...
 
virtual QStringList enumerateEbs (bool enableXdsDev=false)
 Enumerate EB devices. More...
 
virtual QString getRfDevNameFromDevId (const QString devId)
 Get RF Device name from Device ID. More...
 
virtual int executeCmd (const QString &devId, const QString &cmdName)
 Execute command. More...
 
virtual int getAverageRssi (void)
 
virtual QString getLastError (void)
 Get last error. More...
 
virtual QString getRfState (const QString &devId)
 Get RF State. More...
 
virtual int getRssi (const QString &devId, QString *pRssiInDbm, QString *pRssiRaw)
 Get RSSI. More...
 
virtual int initPacketTx (const QString rfDevName, const QString &devId)
 Initialize Packet TX. More...
 
virtual bool isConnected (const QString &devId)
 
virtual int isPacketReceived (const QString rfDevName, const QString &devId)
 Is Packet Received. More...
 
virtual FPLFile * readFile (const QString &devName, const QString &devId, const QString &fileName, const quint32 &startAddress=0)
 Read File. More...
 
virtual int readPacket (const QString rfDevName, const QString &devId, PacketData_t *pPacketData)
 Read Packet. More...
 
virtual int resetTarget (const QString rfDevName, const QString &devId, RESET_MODE mode)
 Reset Target device. More...
 
virtual int sendPacket (const QString rfDevName, const QString &devId)
 Send Packet. More...
 
virtual int setParameter (const QString &devId, const QString &parName, const QString &parValue)
 Set Parameter. More...
 
virtual void setPacketData (char *pPayload, int len)
 Set packet Data. More...
 
virtual int setPacketInterval (const QString &devId, const int &interval)
 Set Packet interval. More...
 
virtual void setNbrOfPackets (int n)
 
virtual int setIdle (const QString rfDevName, const QString &devId)
 Set device in Idle. More...
 
virtual int startContTx (const QString rfDevName, const QString &devId, TestResult_t *pTestResult)
 Start continuous TX. More...
 
virtual int startContRx (const QString rfDevName, const QString &devId, TestResult_t *pTestResult)
 Start continuous RX. More...
 
virtual int startPacketRx (const QString rfDevName, const QString &devId)
 Start Packet RX. More...
 

Additional Inherited Members

- Public Types inherited from RTLDevice
enum  TEST_MODE { TM_CONT_TX, TM_CONT_RX, TM_PACKET_TX, TM_PACKET_RX }
 
enum  TEST_RESULT {
  TST_OK, TST_FAILED, TST_PKT_RECEIVED, TST_PKT_RX_BUF_OVERFLOW,
  TST_UNKNOWN
}
 
enum  TEST_STATE { STATE_DAL, STATE_FPL }
 
- Static Public Member Functions inherited from RTLDevice
static void initEraseInfo (EraseInfo_t *pEraseInfo)
 
static void initProgramInfo (ProgramInfo_t *pProgInfo)
 
static void setCallBackProgressFunction (_PROGRESS_FUNC_PTR pPf)
 
- Protected Member Functions inherited from RTLDevice
QString normDeviceName (const QString &rfDevName)
 Function to normalize the device name for use in DAL. More...
 
RTLFlashHandler * getFlashHandler (const QString &devName, const QString &devId)
 Get Flash Handler. More...
 
bool fwUpdateRequired (const QString &devId)
 The function will return true if FW updated is required. More...
 
- Protected Attributes inherited from RTLDevice
int m_averageRssi
 Used to keep the average RSSI value calculated during a link test. More...
 
QByteArray m_packetData
 Buffer used for packet data during link test. More...
 
int m_nbrOfPackets
 Number of packets that will be sent during the link test. More...
 
QList< DeviceInfo_t > m_ebList
 List of connected EB devices (XDS serial number) returned from DALEbDevice::enumEB() More...
 
QMap< QString, DALEbDevice * > m_mapConDevices
 Map of connected devices. More...
 
QMultiMap< char, int > m_mapFreqOffset
 List used to average the frequency offset value. The offset value is used as key and the packet number as value. More...
 
QMap< QString, RTLFlashHandler * > m_mapFlashHandlers
 Mapped list of Flash handler objects. More...
 
- Static Protected Attributes inherited from RTLDevice
static _PROGRESS_FUNC_PTR sm_pProgressFunction = NULL
 Static function pointer used to give feedback on progress. More...
 

Constructor & Destructor Documentation

§ RTLDevice26_13xx()

RTLDevice26_13xx::RTLDevice26_13xx ( void  )

§ ~RTLDevice26_13xx()

RTLDevice26_13xx::~RTLDevice26_13xx ( void  )
virtual

Member Function Documentation

§ addDynamicOverride()

int RTLDevice26_13xx::addDynamicOverride ( const QString &  devId,
const QString &  type,
const QString &  value,
const QString &  id 
)
virtual

Add Dynamic Override.

This function can be used to add Register override elements. The default override elements are defined with the command settings and can be found under ..\config\xml\<device name>\overrides. The exact file that is used for a given setting, is specified in the setting_xxx.xml file.

Parameters
[in]devIdUSB Device ID
[in]typeType of override element. This will determine how the value will be handled.
[in]valueThe override value
[in]idAn override ID. Used to identify the override element. Using the same ID for two different elements will fail. Only the last will be remembered.
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::m_mapConDevices, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

§ connect()

int RTLDevice26_13xx::connect ( const QString  rfDevName,
const QString &  devId 
)
virtual

Connect to target device.

This function should be called to setup a connection with given target. If the target doesn't exist in the list of devices, enum in DAL must be called. If DAL object for given device already exist, it will be delete and a new object created.

Parameters
[in]rfDevNameRF Device name like "CC2650"
[in]devIdUSB Device ID. E.g.: "XDS-06EB12100472A"
Returns
int TST_OK or TST_FAILED

Reimplemented from RTLDevice.

References RTLDevice::connect().

§ removeDynamicOverride()

int RTLDevice26_13xx::removeDynamicOverride ( const QString &  devId,
const QString &  id 
)
virtual

Remove Dynamic Override.

This function is used to remove override elements that was added with addDynamicOverride()

Parameters
[in]devIdUSB Device ID
[in]idOverride ID as used in function addDynamicOverride(). Used to identify the override element.
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::m_mapConDevices, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

§ doLinkTest()

int RTLDevice26_13xx::doLinkTest ( const QString &  txId,
const QString &  rxId,
TestResult_t *  pTestResult 
)
virtual

Run link test.

Before calling this function a connection must be setup and the command settings must have been loaded for both the transmitter and the receiver. In addition packet data and number of packets must be set. See connect(), readCmdSettingsFromFile(), setPacketData() and setNbrOfPackets()

This function will set the receiver in RX mode and start sending packets from the transmitter. For each packet sent by the transmitter the receiver will do 3 attempts to check if a packet has been received. If no packet received after 3 attempts, the packet is seen as lost. If packet has been received, the packet is read from receiver and compared with the packet sent from the transmitter. The frequency offset and the RSSI value for each packet will be saved. The sequence of sending and receiving packets will be repeated for the number of packets set with the setNbrOfPackets() function.

The Packet Error Rate(PER) is calculated using the expected number of packets and the number of successfully received packets: PER = (NbrOfExpPkts - NbrOfRecPkts)/(NbrOfExpPkts * 100)

The RSSI value will be accumulated and the average value calculated at the end.

The Frequency offset value for each packet is stored in a sorted list and at the end the median value of the list will be returned.

Parameters
[in]txIdUSB Device ID of the TX device.
[in]rxIdUSB Device ID of the RX device.
[out]pTestResultPointer to structure with test results:
  • result : TEST_OK or TST_FAILED.
  • value : Packet Error Rate (PER).
  • rssi : Average RSSI value.
  • freqOff: Median Frequency offset value.
  • qsError: Error description.
Returns
int TST_OK or TST_FAILED

DEBUG

DEBUG

Implements RTLDevice.

References DUMMY_FREQUENCY_OFFSET, RTLDevice::TestResult_t::freqOff, RTLDevice::m_averageRssi, RTLDevice::m_mapConDevices, RTLDevice::m_mapFreqOffset, RTLDevice::m_nbrOfPackets, RTLDevice::m_packetData, NBR_OF_READ_ATTEMPTS, PROGRESS_START_RX, PROGRESS_START_TX, RTLDevice::TestResult_t::qsError, RTLDevice::TestResult_t::result, rssi(), RTLDevice::TestResult_t::rssi, RTLDevice::sm_pProgressFunction, RTLDevice::TST_FAILED, RTLDevice::TST_OK, and RTLDevice::TestResult_t::value.

§ startPacketTx()

int RTLDevice26_13xx::startPacketTx ( const QString &  txId)

Start a packet transmission with pre configured packets, interval and number of packets.

Parameters
[in]txIdUSB Device ID of the TX device.
Returns
int TST_OK or TST_FAILED

References RTLDevice::appendError(), RTLDevice::m_mapConDevices, RTLDevice::m_nbrOfPackets, RTLDevice::m_packetData, PROGRESS_START_TX, RTLDevice::sm_pProgressFunction, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

§ eraseFlash()

int RTLDevice26_13xx::eraseFlash ( const QString &  devName,
const QString &  devId,
EraseInfo_t *  pEraseInfo = NULL,
FPLFile *  pFile = NULL 
)
virtual

Erase Flash (FPL Feature)

This function will erase the part of flash specified in pEraseInfo.

Erase type RTLDevice::ET_ERASE_ALL_FORCED, must be followed by a device re-connect.

Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]pEraseInfoPointer to erase info. If set to NULL all main flash sectors that are not locked will be erased.
[in]pFilePointer to FPL file object. Must be given if erase type is set to RTLDevice::ET_ERASE_PAGES_IN_SOURCE.
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::appendError(), RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ executeCmd()

int RTLDevice26_13xx::executeCmd ( const QString &  devId,
quint8 *  pCmd,
const quint16 &  cmdLength,
quint32 *  pCmdResult 
)

Execute Command.

This function is an override of the exported function and support execution of commands defined by the command buffer.

Parameters
[in]devIdUSB Device ID
[in]pCmdPointer to the command buffer
[in]cmdLengthLength of the command buffer
[in]pCmdResultStatus of the command.
Returns
int TST_OK or TST_FAILED

References RTLDevice::m_mapConDevices, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

§ programFlash() [1/2]

int RTLDevice26_13xx::programFlash ( const QString &  devName,
const QString &  devId,
FPLFile *  pFplFile,
ProgramInfo_t *  pProgInfo = NULL 
)
virtual

Program Flash from file (FPL Feature)

This function will program the flash with data from the given file. The file format must be either a binary file(*.bin), an Intel hex file(*.hex), or an "elf" file (Executable and Linkable Format, *.elf).

Note
This function does not erase flash before programming. See RTLDevice26_13xx::eraseFlash().
Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]pFplFilePointer to FPL file object
[in]pProgInfoPointer to program info. If set to NULL, all pages in file will be programmed.
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::appendError(), RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ programFlash() [2/2]

int RTLDevice26_13xx::programFlash ( const QString &  devName,
const QString &  devId,
const quint32 &  address,
const quint32 &  length,
quint8 *  pBuffer 
)
virtual

Program Flash from buffer (FPL Feature)

This function will program flash with data from the given buffer. To write data to a non-flash memory, see RTLDevice26_13xx::writeMemory().

Note
This function does not erase flash before programming. See RTLDevice26_13xx::eraseFlash().
Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]addressFlash address to program
[in]lengthLength of data buffer that should be programmed
[in]pBufferBuffer with input data to be programmed
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::appendError(), RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ readCmdSettingsFromFile()

int RTLDevice26_13xx::readCmdSettingsFromFile ( const QString &  devId,
TestConfig_t &  testConfig 
)
virtual

Read command settings from file.

Called to read the command settings for CC26xx or CC13xx. The configuration data will be read from file and used to populate a data buffer on the PC side.

Parameters
[in]devIdUSB Device ID. E.g.: "XDS-06EB12100472A"
[in]testConfigStructure with configuration data.
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::appendError(), RTLDevice::clearAllErrors(), RTLDevice::m_mapConDevices, RTLDevice::TestConfig_t::qsCategory, RTLDevice::TestConfig_t::qsSetting, RTLDevice::TestConfig_t::qsTargetName, RTLDevice::TestConfig_t::testMode, RTLDevice::TM_CONT_RX, RTLDevice::TM_CONT_TX, RTLDevice::TM_PACKET_RX, RTLDevice::TM_PACKET_TX, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

§ readFrequencyOffset()

int RTLDevice26_13xx::readFrequencyOffset ( const QString &  devId,
TestResult_t *  pTestResult 
)
virtual

Read frequency offset value from given device.

The Frequency offset value is only available after receiving a packet.

Reading of frequency offset value is only supported for a given configuration of the device: CC13xx: Only supported for modulation type FSK and GFSK CC26xx: Only supported for BLE.

Parameters
[in]devIdUSB Device ID
[out]pTestResultPointer to structure with test results.
Returns
int TST_OK or TST_FAILED

Reimplemented from RTLDevice.

References FREQ_OFFSET_RESOLUTION_IEEE802_15_4, RTLDevice::TestResult_t::freqOff, RTLDevice::m_mapConDevices, RTLDevice::TestResult_t::qsError, readRfReg(), RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

§ readFrequencyOffsetCW()

int RTLDevice26_13xx::readFrequencyOffsetCW ( const QString &  devId,
TestResult_t *  pTestResult 
)
virtual

Read frequency offset value from given device when receiving CW.

This function can be used to read the frequency offset while staying in RX and receiving a Continuous Wave.

Parameters
[in]devIdUSB Device ID
[out]pTestResultPointer to structure with test results.
Returns
int TST_OK or TST_FAILED

Reimplemented from RTLDevice.

References RTLDevice::appendError(), FREQ_OFFSET_RESOLUTION_IEEE802_15_4, RTLDevice::TestResult_t::freqOff, RTLDevice::m_mapConDevices, RTLDevice::m_mapFreqOffset, MOD_TYPE_FSK, MOD_TYPE_GFSK, RTLDevice::TestResult_t::qsError, readRfReg(), RTLDevice::TestResult_t::result, RTLDevice::TST_FAILED, RTLDevice::TST_OK, and writeRfReg().

§ readMcuReg()

int RTLDevice26_13xx::readMcuReg ( const QString &  devId,
const quint32 &  address,
quint32 *  pValue 
)
virtual

Read MCU Register.

Parameters
[in]devIdUSB Device ID
[in]addressRegister address
[out]pValueRegister value
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::m_mapConDevices, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

§ readMemory()

int RTLDevice26_13xx::readMemory ( const QString &  devName,
const QString &  devId,
const quint32 &  address,
quint32 *  pLength,
quint8 *  pBuffer 
)
virtual

Read memory (FPL Feature)

Read any kind of memory that is accessible from the debug interface of the target device.

This method will use the FPL library to read the memory but it will not have any affect on the time when using any non-FPL Feature afterwards. See "Limitations" under the "Introduction" for further details.

Before reading GPRAM the user must make sure that the GPRAM is enabled. This function will return TST_OK even if the GPRAM is not enabled but the returned data will be garbage.

Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]addressMemory address to read
[in,out]pLengthMaximum length of buffer as input and actual length of data successfully read as output.
[out]pBufferBuffer to save the data
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ readRfReg()

int RTLDevice26_13xx::readRfReg ( const QString &  devId,
const quint32 &  address,
quint32 *  pValue 
)
virtual

Read RF core Register.

Parameters
[in]devIdUSB Device ID
[in]addressOffset address of HW Register bank 0x40040000
[out]pValueRegister value
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::m_mapConDevices, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

Referenced by readFrequencyOffset(), readFrequencyOffsetCW(), and writeRfReg().

§ verifyFlash()

int RTLDevice26_13xx::verifyFlash ( const QString &  devName,
const QString &  devId,
FPLFile *  pFplFile,
ProgramInfo_t *  pProgInfo = NULL 
)
virtual

Verify Flash (FPL Feature)

This function will verify the flash content by calculating the CRC checksum in flash and compare it with the CRC checksum from the file object on the host.

Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]pFplFilePointer to FPL File Object
[in]pProgInfoPointer to the program info used for programming. The verification will inherit the option set for programming. E.g. if a set of pages was excluded in programming, the same pages will be excluded in verification. If set to NULL all pages in file will be verified.
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::appendError(), RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ writeMemory()

int RTLDevice26_13xx::writeMemory ( const QString &  devName,
const QString &  devId,
const quint32 &  address,
const quint32 &  length,
quint8 *  pBuffer 
)
virtual

Write memory (FPL Feature)

This function can be used to write all non-flash memory. Before using this function the user must make sure that the requested memory range is enabled. The function will return TST_FAILED if memory not enabled. For example flash cache RAM must be configured as GPRAM before it can be written. Some memory blocks can be powered down and in that case the memory block must be powered before it can be written.

For programming flash memory, see RTLDevice26_13xx::programFlash(const QString&, const QString&, const quint32&, const quint32&, quint8*).

Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]addressMemory address to write
[in]lengthLength of buffer to be written.
[out]pBufferBuffer with data to be written.
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ writeMcuReg()

int RTLDevice26_13xx::writeMcuReg ( const QString &  devId,
const quint32 &  address,
const quint32 &  value 
)
virtual

Write MCU Register.

Parameters
[in]devIdUSB Device ID
[in]addressRegister address
[in]valueRegister value
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::m_mapConDevices, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

§ writeRfReg()

int RTLDevice26_13xx::writeRfReg ( const QString &  devId,
const quint32 &  address,
const quint32 &  value 
)
virtual

Write RF core Register.

Parameters
[in]devIdUSB Device ID
[in]addressOffset address of HW Register bank 0x40040000
[in]valueRegister value
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::m_mapConDevices, readRfReg(), RTLDevice::TST_FAILED, and RTLDevice::TST_OK.

Referenced by readFrequencyOffsetCW().

§ runCpu()

int RTLDevice26_13xx::runCpu ( const QString &  devName,
const QString &  devId,
bool  debugMode 
)
virtual

Run CPU (FPL Feature)

Start CPU (in free run [debug disabled] or in profiling mode [debug enabled])

Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]debugModeDebug mode enabled or disabled.
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ haltCpu()

int RTLDevice26_13xx::haltCpu ( const QString &  devName,
const QString &  devId 
)
virtual

Halt CPU (FPL Feature)

Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ writeCpuReg()

int RTLDevice26_13xx::writeCpuReg ( const QString &  devName,
const QString &  devId,
const CM3_CPU_REGISTERS &  regNumber,
const uint32_t &  value 
)
virtual

Write CPU register (FPL Feature)

Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]regNumberCPU Register number.
[in]valueRegister value
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ readCpuReg()

int RTLDevice26_13xx::readCpuReg ( const QString &  devName,
const QString &  devId,
const CM3_CPU_REGISTERS &  regNumber,
uint32_t *  pValue 
)
virtual

Read CPU register (FPL Feature)

Parameters
[in]devNameDevice name
[in]devIdUSB Device ID
[in]regNumberRegister number. Valid range from 0 to 20
[out]pValueRegister value
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::getFlashHandler(), and RTLDevice::TST_FAILED.

§ setCapArrayDelta()

int RTLDevice26_13xx::setCapArrayDelta ( const QString &  devId,
const qint16 &  value 
)
virtual

Set Cap Array Delta.

This function provides an easy-to-use method for modifying the load capacitor array for the HF crystal on the fly, allowing you to tune the frequency offset suitable for your HW design. Normally the default value will be set to zero. For HW designs where the HF crystal will be tuned with external capacitors the value should be set to a minimum.

For more details refer to the documentation, Technical Reference Manual or the online wiki entry

Parameters
[in]devIdUSB Device ID. E.g.: "XDS-06EB12100472A"
[in]valueThe Capacitor delta value
Returns
int TST_OK or TST_FAILED

Implements RTLDevice.

References RTLDevice::appendError(), CAP_ARRAY_AGA_MAX, CAP_ARRAY_AGA_MIN, CAP_ARRAY_CHA_MAX, CAP_ARRAY_CHA_MIN, CAP_ARRAY_CHA_WCSP_MAX, CAP_ARRAY_CHA_WCSP_MIN, RTLDevice::m_mapConDevices, RTLDevice::TST_FAILED, and RTLDevice::TST_OK.


The documentation for this class was generated from the following files:
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale