RadioTestLibrary  1.34.0
rtl_device_26_13xx.h
Go to the documentation of this file.
1 //-----------------------------------------------------------------------------
2 /*
3  * File rtl_device_26_13xx.h
4  * Revision $Revision$
5  * Description Common class for Radio Test Library of 26xx and 13xx devices in
6  * DAL
7  *
8 // ##### LICENSE HEADER #####
9  *
10  */
11  //-----------------------------------------------------------------------------
12 
13 #ifndef RTLDEVICE2613XX_H
14 #define RTLDEVICE2613XX_H
15 
16 #define DUMMY_FREQUENCY_OFFSET 999999
17 
18 #include <rtl_device.h>
19 
20 class DALRfDevice;
21 class DALRfDevice26xx;
22 
24 {
25 
26 public:
27 
28  RTLDevice26_13xx(void);
29  virtual ~RTLDevice26_13xx(void);
30 
31  int addDynamicOverride(const QString &devId, const QString &type, const QString &value, const QString &id);
32  int connect(const QString rfDevName, const QString &devId);
33  int removeDynamicOverride(const QString &devId, const QString &id);
34  int doLinkTest(const QString &txId, const QString &rxId, TestResult_t *pTestResult);
35  int startPacketTx(const QString &txId);
36 
37  int eraseFlash(const QString &devName, const QString &devId, EraseInfo_t *pEraseInfo = NULL, FPLFile *pFile = NULL);
38  int executeCmd(const QString &devId, quint8 *pCmd, const quint16 &cmdLength, quint32 *pCmdResult);
39  int programFlash(const QString &devName, const QString &devId, FPLFile *pFplFile, ProgramInfo_t *pProgInfo = NULL);
40  int programFlash(const QString &devName, const QString &devId,
41  const quint32 &address, const quint32 &length, quint8 *pBuffer);
42  int readCmdSettingsFromFile(const QString &devId, TestConfig_t &testConfig);
43  int readFrequencyOffset(const QString &devId, TestResult_t *pTestResult);
44  int readFrequencyOffsetCW(const QString &devId, TestResult_t *pTestResult);
45  int readMcuReg(const QString &devId, const quint32 &address, quint32 *pValue);
46  int readMemory(const QString &devName, const QString &devId,
47  const quint32 &address, quint32 *pLength, quint8 *pBuffer);
48  int readRfReg(const QString &devId, const quint32 &address, quint32 *pValue);
49  int verifyFlash(const QString &devName, const QString &devId, FPLFile *pFplFile, ProgramInfo_t *pProgInfo = NULL);
50  int writeMemory(const QString &devName, const QString &devId,
51  const quint32 &address, const quint32 &length, quint8 *pBuffer);
52  int writeMcuReg(const QString &devId, const quint32 &address, const quint32 &value);
53  int writeRfReg(const QString &devId, const quint32 &address, const quint32 &value);
54  int runCpu(const QString &devName, const QString &devId, bool debugMode);
55  int haltCpu(const QString &devName, const QString &devId);
56  int writeCpuReg(const QString &devName, const QString &devId,
57  const CM3_CPU_REGISTERS &regNumber, const uint32_t &value);
58  int readCpuReg(const QString &devName, const QString &devId,
59  const CM3_CPU_REGISTERS &regNumber, uint32_t *pValue);
60  int setCapArrayDelta(const QString &devId, const qint16 &value);
61 
62 private:
63  int m_accCompVal;
64  int m_nbrCompVal;
65  int getMedianFrequencyOffset(DALRfDevice *pDalRfDeviceRx, double *pFreqOffset);
66  int setCmixnValue(DALRfDevice *pDalRfDeviceRx);
67  int readFrequencyOffsetAndSaveInList(DALRfDevice *pDalRfDeviceRx);
68  int readRfReg(DALRfDevice *pDalRfDevice, const quint32 &address, quint32 *pValue);
69  int writeRfReg(DALRfDevice *pDalRfDevice, const quint32 &address, const quint32 &value);
70  int getDeviation(DALRfDevice *pDalRfDevice);
71  int getDeviationCC13xxPG1(DALRfDevice *pDalRfDevice);
72  int getDeviationCC13xxPG2(DALRfDevice *pDalRfDevice);
73  int initDALApi(const QString &devId);
74  void convertPacketDataToString(QByteArray pktRxData, QString& qsPacketData);
75  int sendPacketsTargetControlled(DALRfDevice26xx *pDalRfDevice26xx, void* pPacketSequenceConfig, QString &qsError, const bool &asynchTx = false);
76 
77  int rfcMdmRegDemmafc0;
78  int rfcMdmRegDemswqu1;
79  int rfcMdmRegDemmisc0;
80  int rfcMdmRegDemmisc3;
81  int rfcMdmRegDemmafi0;
82  int rfcMdmRegDemmafi1;
83  int rfcMdmRegDemmafi2;
84  int rfcMdmRegDemmafi3;
85  int rfcMdmRegDemfife2;
86  int rfcMdmRegRdCapt0;
87  int rfcFscaRegSynthreganadiv;
88 };
89 
90 #endif
int startPacketTx(const QString &txId)
Start a packet transmission with pre configured packets, interval and number of packets.
Definition: rtl_device_26_13xx.cpp:688
This structure is used as input to RTLDevice::programFlash() and RTLDevice::verifyFlash().
Definition: rtl_flash_handler.h:84
int eraseFlash(const QString &devName, const QString &devId, EraseInfo_t *pEraseInfo=NULL, FPLFile *pFile=NULL)
Erase Flash (FPL Feature)
Definition: rtl_device_26_13xx.cpp:1931
int writeCpuReg(const QString &devName, const QString &devId, const CM3_CPU_REGISTERS &regNumber, const uint32_t &value)
Write CPU register (FPL Feature)
Definition: rtl_device_26_13xx.cpp:2236
Definition: rtl_device.h:29
Definition: rtl_device.h:63
int verifyFlash(const QString &devName, const QString &devId, FPLFile *pFplFile, ProgramInfo_t *pProgInfo=NULL)
Verify Flash (FPL Feature)
Definition: rtl_device_26_13xx.cpp:2054
This structure is used as input to RTLDevice::eraseFlash().
Definition: rtl_flash_handler.h:58
int readCpuReg(const QString &devName, const QString &devId, const CM3_CPU_REGISTERS &regNumber, uint32_t *pValue)
Read CPU register (FPL Feature)
Definition: rtl_device_26_13xx.cpp:2268
int executeCmd(const QString &devId, quint8 *pCmd, const quint16 &cmdLength, quint32 *pCmdResult)
Execute Command.
Definition: rtl_device_26_13xx.cpp:1838
RTLDevice26_13xx(void)
Definition: rtl_device_26_13xx.cpp:71
int readCmdSettingsFromFile(const QString &devId, TestConfig_t &testConfig)
Read command settings from file.
Definition: rtl_device_26_13xx.cpp:162
CM3_CPU_REGISTERS
The XDS debug interface uses an offset of 512 to address the CPU registers.
Definition: rtl_flash_handler.h:90
int connect(const QString rfDevName, const QString &devId)
Connect to target device.
Definition: rtl_device_26_13xx.cpp:2358
int runCpu(const QString &devName, const QString &devId, bool debugMode)
Run CPU (FPL Feature)
Definition: rtl_device_26_13xx.cpp:2178
int readMcuReg(const QString &devId, const quint32 &address, quint32 *pValue)
Read MCU Register.
Definition: rtl_device_26_13xx.cpp:1648
int readFrequencyOffset(const QString &devId, TestResult_t *pTestResult)
Read frequency offset value from given device.
Definition: rtl_device_26_13xx.cpp:1001
Definition: rtl_device.h:71
virtual ~RTLDevice26_13xx(void)
Definition: rtl_device_26_13xx.cpp:81
int readFrequencyOffsetCW(const QString &devId, TestResult_t *pTestResult)
Read frequency offset value from given device when receiving CW.
Definition: rtl_device_26_13xx.cpp:1086
int programFlash(const QString &devName, const QString &devId, FPLFile *pFplFile, ProgramInfo_t *pProgInfo=NULL)
Program Flash from file (FPL Feature)
Definition: rtl_device_26_13xx.cpp:1971
int setCapArrayDelta(const QString &devId, const qint16 &value)
Set Cap Array Delta.
Definition: rtl_device_26_13xx.cpp:2429
int removeDynamicOverride(const QString &devId, const QString &id)
Remove Dynamic Override.
Definition: rtl_device_26_13xx.cpp:1785
int readMemory(const QString &devName, const QString &devId, const quint32 &address, quint32 *pLength, quint8 *pBuffer)
Read memory (FPL Feature)
Definition: rtl_device_26_13xx.cpp:2103
Definition: rtl_device_26_13xx.h:23
int writeMemory(const QString &devName, const QString &devId, const quint32 &address, const quint32 &length, quint8 *pBuffer)
Write memory (FPL Feature)
Definition: rtl_device_26_13xx.cpp:2146
int writeRfReg(const QString &devId, const quint32 &address, const quint32 &value)
Write RF core Register.
Definition: rtl_device_26_13xx.cpp:1511
int doLinkTest(const QString &txId, const QString &rxId, TestResult_t *pTestResult)
Run link test.
Definition: rtl_device_26_13xx.cpp:351
int addDynamicOverride(const QString &devId, const QString &type, const QString &value, const QString &id)
Add Dynamic Override.
Definition: rtl_device_26_13xx.cpp:1726
int writeMcuReg(const QString &devId, const quint32 &address, const quint32 &value)
Write MCU Register.
Definition: rtl_device_26_13xx.cpp:1684
int readRfReg(const QString &devId, const quint32 &address, quint32 *pValue)
Read RF core Register.
Definition: rtl_device_26_13xx.cpp:1476
int haltCpu(const QString &devName, const QString &devId)
Halt CPU (FPL Feature)
Definition: rtl_device_26_13xx.cpp:2205
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale