BLE-Stack APIs  3.00.00
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Modules | Files | Functions
GAP

This module implements the Generic Access Protocol (GAP) More...

Modules

 GAP Callbacks
 
 GAP Constants
 
 GAP Structures
 

Files

file  gap.h
 GAP layer interface.
 

Functions

bStatus_t GAP_Authenticate (gapAuthParams_t *pParams, gapPairingReq_t *pPairReq)
 Start Authentication. More...
 
bStatus_t GAP_Bond (uint16 connectionHandle, uint8 authenticated, uint8 secureConnections, smSecurityInfo_t *pParams, uint8 startEncryption)
 Set up the connection's bound paramaters. More...
 
bStatus_t GAP_ConfigDeviceAddr (uint8 addrMode, uint8 *pStaticAddr)
 Configure Device Address. More...
 
bStatus_t GAP_DeviceDiscoveryCancel (uint8 taskID)
 Cancel an existing device discovery request. More...
 
bStatus_t GAP_DeviceDiscoveryRequest (gapDevDiscReq_t *pParams)
 Start a device discovery scan. More...
 
bStatus_t GAP_DeviceInit (uint8 taskID, uint8 profileRole, uint8 maxScanResponses, uint8 *pIRK, uint8 *pSRK, uint32 *pSignCounter)
 GAP Device Initialiation. More...
 
bStatus_t GAP_EndDiscoverable (uint8 taskID)
 Stops advertising. More...
 
bStatus_t GAP_EstablishLinkReq (gapEstLinkReq_t *pParams)
 Establish a link to a slave device. More...
 
gapAdvDataToken_t * GAP_GetAdvToken (uint8 adType)
 Get Advertising Token. More...
 
uint16 GAP_GetParamValue (gapParamIDs_t paramID)
 Get a GAP Parameter value. More...
 
uint8 GAP_isPairing (void)
 Check if GAP is currently pairing. More...
 
bStatus_t GAP_MakeDiscoverable (uint8 taskID, gapAdvertisingParams_t *pParams)
 Setup or change advertising. Also starts advertising. More...
 
uint8 GAP_NumActiveConnections (void)
 Returns the number of active connections. More...
 
bStatus_t GAP_PasscodeUpdate (uint32 passcode, uint16 connectionHandle)
 Update the passkey in a numeric value (not string). More...
 
bStatus_t GAP_PasskeyUpdate (uint8 *pPasskey, uint16 connectionHandle)
 Update the passkey in string format. More...
 
void GAP_RegisterBondMgrCBs (gapBondMgrCBs_t *pCBs)
 Register bond manager call backs. More...
 
void GAP_RegisterForMsgs (uint8 taskID)
 Register for GAP Messages. More...
 
gapAdvDataToken_t * GAP_RemoveAdvToken (uint8 adType)
 Remove Advertising Token. More...
 
bStatus_t GAP_ResolvePrivateAddr (uint8 *pIRK, uint8 *pAddr)
 Resolves a private address against an IRK. More...
 
bStatus_t GAP_SendSlaveSecurityRequest (uint16 connectionHandle, uint8 authReq)
 Generate a Slave Requested Security message to the master. More...
 
bStatus_t GAP_SetAdvToken (gapAdvDataToken_t *pToken)
 Set Advertising Token. More...
 
bStatus_t GAP_SetParamValue (gapParamIDs_t paramID, uint16 paramValue)
 Set a GAP Parameter value. More...
 
bStatus_t GAP_Signable (uint16 connectionHandle, uint8 authenticated, smSigningInfo_t *pParams)
 Set up the connection to accept signed data. More...
 
bStatus_t GAP_TerminateAuth (uint16 connectionHandle, uint8 reason)
 Terminate Authnetication. More...
 
bStatus_t GAP_TerminateLinkReq (uint8 taskID, uint16 connectionHandle, uint8 reason)
 Terminate a link connection. More...
 
bStatus_t GAP_UpdateAdvertisingData (uint8 taskID, uint8 adType, uint8 dataLen, uint8 *pAdvertData)
 Setup or change advertising and scan response data. More...
 
bStatus_t GAP_UpdateAdvTokens (void)
 Update Advertising Token. More...
 
bStatus_t GAP_UpdateLinkParamReq (gapUpdateLinkParamReq_t *pParams)
 Update the link parameters to a Master or Slave device. More...
 
bStatus_t GAP_UpdateLinkParamReqReply (gapUpdateLinkParamReqReply_t *pParams)
 Reply to a Connection Parameter Update Request sent from a remote device. More...
 

Detailed Description

This module implements the Generic Access Protocol (GAP)


Function Documentation

bStatus_t GAP_Authenticate ( gapAuthParams_t *  pParams,
gapPairingReq_t *  pPairReq 
)

Start Authentication.

Start the Authentication process with the requested device. This function is used to Initiate/Allow pairing. Called by both master and slave device (Central and Peripheral).

Note
This function must only be called after the link is established.
Corresponding Events:
After pairing is completed succesfully, the calling task will receive a GAP_AUTHENTICATION_COMPLETE_EVENT of type gapAuthCompleteEvent_t
After a failed pairing, the calling task will receive a GAP_AUTHENTICATION_FAILURE_EVT
Parameters
pParams- Authentication parameters
pPairReq- Enter these parameters if the Pairing Request was already received. NULL, if waiting for Pairing Request or if initiating.
Returns
SUCCESS - authentication request sent to stack
bleIncorrectMode : Not correct profile role
INVALIDPARAMETER
bleNotConnected
bleAlreadyInRequestedMode
FAILURE - not workable
bStatus_t GAP_Bond ( uint16  connectionHandle,
uint8  authenticated,
uint8  secureConnections,
smSecurityInfo_t *  pParams,
uint8  startEncryption 
)

Set up the connection's bound paramaters.

Note
This function must only called after the link is established.
Corresponding Events:
GAP_BOND_COMPLETE_EVENT of type gapBondCompleteEvent_t
Parameters
connectionHandle- connection handle of the signing information
authenticated- TRUE if bond is authenticated.
secureConnections- TRUE if bond has Secure Connections strength.
pParams- the connected device's security parameters
startEncryption- whether or not to start encryption
Returns
SUCCESS,
bleIncorrectMode : Not correct profile role
INVALIDPARAMETER
bleNotConnected
FAILURE : not workable
bStatus_t GAP_ConfigDeviceAddr ( uint8  addrMode,
uint8 *  pStaticAddr 
)

Configure Device Address.

Setup the device's address type. If ADDRMODE_PRIVATE_RESOLVE is selected, the address will change periodically.

Note
If return value isn't SUCCESS, the address type remains the same as before this call
Corresponding Events:
If the device is correctly configured for ADDRMODE_PRIVATE_NONRESOLVE , the calling task will receive a GAP_RANDOM_ADDR_CHANGED_EVENT of type gapRandomAddrEvent_t when the random address changes
Parameters
addrMode- GAP Addressing Modes
pStaticAddr- Only used with ADDRMODE_STATIC or ADDRMODE_PRIVATE_NONRESOLVE type.
NULL to auto generate otherwise the application can specify the address value
Returns
SUCCESS : address type updated
bleNotReady : Can't be called until GAP_DeviceInit is called and the init process is completed
bleIncorrectMode : can't change with an active connection
or INVALIDPARAMETER
bStatus_t GAP_DeviceDiscoveryCancel ( uint8  taskID)

Cancel an existing device discovery request.

Corresponding Events:
When disovery is complete, the calling app will receive a GAP_DEVICE_DISCOVERY_EVENT of type gapDevDiscEvent_t
Parameters
taskID- task to receive event
Returns
SUCCESS : cancel request sent to stack
bleInvalidTaskID : Not the task that started discovery
bleIncorrectMode : not in discovery mode
bStatus_t GAP_DeviceDiscoveryRequest ( gapDevDiscReq_t *  pParams)

Start a device discovery scan.

Parameters
pParams- Device Discovery parameters
Corresponding Events:
As devices are discovered, the calling app will receive GAP_DEVICE_INFO_EVENT of type gapDeviceInfoEvent_t
When disovery is complete, the calling app will receive a GAP_DEVICE_DISCOVERY_EVENT of type gapDevDiscEvent_t
Returns
SUCCESS : scan request sent to stakc
bleIncorrectMode : invalid profile role
bleAlreadyInRequestedMode : not available
bStatus_t GAP_DeviceInit ( uint8  taskID,
uint8  profileRole,
uint8  maxScanResponses,
uint8 *  pIRK,
uint8 *  pSRK,
uint32 *  pSignCounter 
)

GAP Device Initialiation.

Setup the device. Call just once on initialization.

Corresponding Events:
GAP_DEVICE_INIT_DONE_EVENT of type gapDeviceInitDoneEvent_t
Parameters
taskID- task to receive event
profileRole- GAP Profile Roles: GAP Profile Roles
maxScanResponses- maximum number to scan responses we can receive during a device discovery.
pIRK- pointer to Identity Root Key, NULLKEY (all zeroes) if the app wants the GAP to generate the key.
pSRK- pointer to Sign Resolving Key, NULLKEY if the app wants the GAP to generate the key.
pSignCounter- 32 bit value used in the SM Signing algorithm that shall be initialized to zero and incremented with every new signing. This variable must also be maintained by the application.
Returns
SUCCESS - initialization started
INVALIDPARAMETER - for invalid profile role or role combination
bleIncorrectMode - trouble communicating with HCI
bStatus_t GAP_EndDiscoverable ( uint8  taskID)

Stops advertising.

Corresponding Events:
GAP_END_DISCOVERABLE_DONE_EVENT of type gapEndDiscoverableRspEvent_t
Parameters
taskID- task to receive event
Returns
SUCCESS : discovery cancel sent to stack
bleIncorrectMode : not in discoverable mode
bleInvalidTaskID : not correct task
bStatus_t GAP_EstablishLinkReq ( gapEstLinkReq_t *  pParams)

Establish a link to a slave device.

Corresponding Events:
GAP_LINK_ESTABLISHED_EVENT of type gapEstLinkReqEvent_t
Parameters
pParams- link establishment parameters
Returns
SUCCESS : connection request sent to stack
bleIncorrectMode : invalid profile role
bleNotReady : a scan is in progress
bleAlreadyInRequestedMode : can't process now
bleNoResources : Too many links
gapAdvDataToken_t* GAP_GetAdvToken ( uint8  adType)

Get Advertising Token.

Called to read a GAP Advertisement/Scan Response data token.

Parameters
adType- Advertisement type to get
Returns
pointer to the advertisement data token structure, NULL if not found.
uint16 GAP_GetParamValue ( gapParamIDs_t  paramID)

Get a GAP Parameter value.

Parameters
paramID- parameter ID: GAP Parameter IDs
Returns
GAP Parameter value
0xFFFF if invalid
uint8 GAP_isPairing ( void  )

Check if GAP is currently pairing.

Returns
TRUE if pairing
FALSE otherwise
bStatus_t GAP_MakeDiscoverable ( uint8  taskID,
gapAdvertisingParams_t *  pParams 
)

Setup or change advertising. Also starts advertising.

Corresponding Events:
GAP_MAKE_DISCOVERABLE_DONE_EVENT of type gapMakeDiscoverableRspEvent_t
Parameters
taskID- task to receive event
pParams- advertising parameters
Returns
SUCCESS : advertising request sent to stack
bleIncorrectMode : invalid profile role
bleAlreadyInRequestedMode : already advertising
bleNotReady : advertising data isn't set up yet
uint8 GAP_NumActiveConnections ( void  )

Returns the number of active connections.

Returns
Number of active connections.
bStatus_t GAP_PasscodeUpdate ( uint32  passcode,
uint16  connectionHandle 
)

Update the passkey in a numeric value (not string).

Note
This function is the same as GAP_PasskeyUpdate(), except that the passkey is passed in as a non-string format.
: Corresponding Events: This API should be called in response to receiving a GAP_PASSKEY_NEEDED_EVENT of type gapPasskeyNeededEvent_t
Parameters
passcode- not string - range: 0 - 999,999.
connectionHandle- connection handle.
Returns
SUCCESS : will start pairing with this entry
bleIncorrectMode : Link not found
INVALIDPARAMETER : passkey == NULL or passkey isn't formatted properly
bStatus_t GAP_PasskeyUpdate ( uint8 *  pPasskey,
uint16  connectionHandle 
)

Update the passkey in string format.

Note
This function is the same as GAP_PasscodeUpdate , except that the passkey is passed in as a string format.
: Corresponding Events: This API should be called in response to receiving a GAP_PASSKEY_NEEDED_EVENT of type gapPasskeyNeededEvent_t
Parameters
pPasskey- new passkey - pointer to numeric string (ie. "019655" ) This string's range is "000000" to "999999"
connectionHandle- connection handle.
Returns
SUCCESS : will start pairing with this entry
bleIncorrectMode : Link not found
INVALIDPARAMETER : passkey == NULL or passkey isn't formatted properly
void GAP_RegisterBondMgrCBs ( gapBondMgrCBs_t *  pCBs)

Register bond manager call backs.

Parameters
pCBs- pointer to Bond Manager Callbacks.
void GAP_RegisterForMsgs ( uint8  taskID)

Register for GAP Messages.

Register a task ID to receive extra (unprocessed) HCI status and complete, and Host events.

Parameters
taskID- Default task ID to send events.
gapAdvDataToken_t* GAP_RemoveAdvToken ( uint8  adType)

Remove Advertising Token.

Called to remove a GAP Advertisement/Scan Response data token.

Parameters
adType- Advertisement type to remove
Returns
pointer to the token structure removed from the GAP ADType list
NULL if the requested adType wasn't found.
bStatus_t GAP_ResolvePrivateAddr ( uint8 *  pIRK,
uint8 *  pAddr 
)

Resolves a private address against an IRK.

Parameters
pIRK- pointer to the IRK
pAddr- pointer to the Resolvable Private address
Returns
SUCCESS : match
FAILURE : don't match
INVALIDPARAMETER : parameters invalid
bStatus_t GAP_SendSlaveSecurityRequest ( uint16  connectionHandle,
uint8  authReq 
)

Generate a Slave Requested Security message to the master.

This API can be used to initiate security as a slave.

Parameters
connectionHandle- connection handle.
authReq- Authentication Requirements: Bit 2: MITM, Bits 0-1: bonding (0 - no bonding, 1 - bonding) Bit 3: Secure Connections
Returns
SUCCESS : will send
bleNotConnected : Link not found
bleIncorrectMode : wrong GAP role, must be a Peripheral Role
bStatus_t GAP_SetAdvToken ( gapAdvDataToken_t *  pToken)

Set Advertising Token.

Called to setup a GAP Advertisement / Scan Response data token.

Note
The data in these items are stored as low byte first (OTA format). The passed in structure "token" should be allocated by the calling app/profile and not released until after calling GAP_RemoveAdvToken
Parameters
pToken- Advertisement/Scan response token to write.
Returns
SUCCESS - advertisement token added to the GAP list
INVALIDPARAMETER - Invalid Advertisement Type or pAttrData is NULL
INVALID_MEM_SIZE - The tokens take up too much space and don't fit into Advertisement data and Scan Response Data
bleInvalidRange : token ID already exists.
bleIncorrectMode - not a peripheral device
bleMemAllocError - memory allocation failure,
bStatus_t GAP_SetParamValue ( gapParamIDs_t  paramID,
uint16  paramValue 
)

Set a GAP Parameter value.

Use this function to change the default GAP parameter values.

Parameters
paramID- parameter ID: GAP Parameter IDs
paramValue- new param value
Returns
SUCCESS
INVALIDPARAMETER
bStatus_t GAP_Signable ( uint16  connectionHandle,
uint8  authenticated,
smSigningInfo_t *  pParams 
)

Set up the connection to accept signed data.

Note
This function is called after the link is established.
Parameters
connectionHandle- connection handle of the signing information
authenticated- TRUE if the signing information is authenticated, FALSE otherwise
pParams- signing parameters
Returns
SUCCESS
bleIncorrectMode : Not correct profile role
INVALIDPARAMETER
bleNotConnected
FAILURE : not workable.
bStatus_t GAP_TerminateAuth ( uint16  connectionHandle,
uint8  reason 
)

Terminate Authnetication.

Send a Pairing Failed message and end any existing pairing.

Corresponding Events:
GAP_AUTHENTICATION_FAILURE_EVT
Parameters
connectionHandle- connection handle.
reason- Pairing Failed reason code.
Returns
SUCCESS - function was successful
bleMemAllocError - memory allocation error
INVALIDPARAMETER - one of the parameters were invalid
bleNotConnected - link not found
bleInvalidRange : one of the parameters were not within range.
bStatus_t GAP_TerminateLinkReq ( uint8  taskID,
uint16  connectionHandle,
uint8  reason 
)

Terminate a link connection.

Corresponding Events:
GAP_LINK_TERMINATED_EVENT of type gapTerminateLinkEvent_t
Parameters
taskID- requesting app's task id.
connectionHandle- connection handle of link to terminate or GAP Special Connection Handles
reason- terminate reason.
Returns
SUCCESS : termination request sent to stack
bleIncorrectMode : No Link to terminate
bleInvalidTaskID : not app that established link
bStatus_t GAP_UpdateAdvertisingData ( uint8  taskID,
uint8  adType,
uint8  dataLen,
uint8 *  pAdvertData 
)

Setup or change advertising and scan response data.

Corresponding Events:
GAP_ADV_DATA_UPDATE_DONE_EVENT of type gapAdvDataUpdateEvent_t
Parameters
taskID- task to receive event
adType- TRUE - advertisement data, FALSE - scan response data
dataLen- Octet length of advertData
pAdvertData- advertising or scan response data
Returns
SUCCESS : advertising data sent to stack
bleIncorrectMode : invalid profile role
bStatus_t GAP_UpdateAdvTokens ( void  )

Update Advertising Token.

Called to rebuild and load Advertisement and Scan Response data from existing GAP Advertisement Tokens.

Returns
SUCCESS or bleIncorrectMode
bStatus_t GAP_UpdateLinkParamReq ( gapUpdateLinkParamReq_t *  pParams)

Update the link parameters to a Master or Slave device.

Corresponding Events:
After the update procedure is complete, the calling task will recive a GAP_LINK_PARAM_UPDATE_EVENT of type gapLinkUpdateEvent_t
Parameters
pParams- link update parameters
Returns
SUCCESS : update request sent to stack
INVALIDPARAMETER : one of the parameters were invalid
bleIncorrectMode : invalid profile role
bleAlreadyInRequestedMode : already updating link parameters
bleNotConnected : not in a connection
bStatus_t GAP_UpdateLinkParamReqReply ( gapUpdateLinkParamReqReply_t *  pParams)

Reply to a Connection Parameter Update Request sent from a remote device.

Corresponding Events:
The calling task should call this API in reponse to a GAP_UPDATE_LINK_PARAM_REQ_EVENT of type gapUpdateLinkParamReqEvent_t
After the update procedure is complete, the calling task will receive a GAP_LINK_PARAM_UPDATE_EVENT of type gapLinkUpdateEvent_t
Parameters
pParams- local device's desired connection parameters.
Returns
SUCCESS : reply sent successfully
INVALIDPARAMETER : one of the parameters were invalid
bleIncorrectMode : invalid profile role
bleAlreadyInRequestedMode : already updating link parameters
bleNotConnected : not in a connection
Copyright 2016, Texas Instruments Incorporated