![]() |
![]() |
|
BLE-Stack APIs
3.00.00
|
| LE Connection Complete Event | |
| ICall_allocMsg or ICall_malloc arguments | |
| ICall_createSemaphore argument | |
| ICall_createTask argument | |
| ICall_enrollService arguments | |
| ICall_entityId2ServiceId arguments | |
| ICall_fetchServiceMsg and ICall_fetchMsg arguments | |
| ICall_freeMsg or ICall_free arguments | |
| Common service function arguments | |
| ICall_getEntityId arguments | |
| ICall_getLocalMsgEntityId arguments | |
| ICall_pwrIsStableXOSCHF arguments | |
| ICall_getTicks , ICall_getTickPeriod and ICall_getMaxMSecs arguments | |
| ICall_enableInt and ICall_disableInt arguments | |
| ICall Lite Command Status | |
| ICall_postSemaphore argument | |
| ICall_pwrConfigActivityCounterAction , ICall_pwrRequire and ICall_pwrDispense arguments | |
| ICall_pwrGetTransitionState arguments | |
| ICall_pwrGetXOSCStartupTime arguments | |
| Power state transition notify function data object type | |
| ICall_pwrRegisterNotify arguments | |
| ICall_pwrUpdActivityCounter arguments | |
| ICall_registerApp arguments | |
| ICall_registerISR_Ext arguments | |
| ICall_registerISR arguments | |
| Data type of the first argument passed to the entry point of an image which contains a remote task | |
| ICall_sendServiceMsg and ICall_send arguments | |
| ICall_setTimer arguments | |
| ICall_signal arguments | |
| ICall_signal arguments | |
| ICall_stopTimer arguments | |
| ICall_threadServes argument | |
| ICall_wait arguments | |
| ICall_waitMatch arguments | |
| ICall_waitSemaphore argument | |
| Service callbacks list item | |
| Attribute Type format (2-octet Bluetooth UUID) | |
| GATT Attribute format | |
| Attribute Type format (2 or 16 octet UUID) | |
| Error Response format | |
| Exchange MTU Request format | |
| Exchange MTU Response format | |
| Execute Write Request format | |
| Find By Type Value Request format | |
| Find By Type Value Response format | |
| Find Information Request format | |
| Find Information Response format | |
| ATT Flow Control Violated Event message format | |
| Handle and its 16-bit Bluetooth UUIDs | |
| Handles Information format | |
| Handle and its 128-bit UUID | |
| Handle Value Indication format | |
| Handle Value Notification format | |
| ATT Message format | |
| ATT MTU Updated Event message format | |
| Attribute Protocol PDU format | |
| Prepare Write Request format | |
| Prepare Write Response format | |
| Read Blob Request format | |
| Read Blob Response format | |
| Read By Group Type Request format | |
| Read By Group Type Response format | |
| Read By Type Request format | |
| Read By Type Response format | |
| Read Multiple Request format | |
| Read Multiple Response format | |
| Read Request | |
| Read Response | |
| Write Request format | |
| Encryption Params | |
| GAP Advertisement/Scan Response Data Token | |
| GAP_ADV_DATA_UPDATE_DONE_EVENT message format | |
| Advertising Parameters | |
| GAP_AUTHENTICATION_COMPLETE_EVENT message format | |
| Authentication Parameters | |
| GAP_BOND_COMPLETE_EVENT message format | |
| Public and Private ECC Keys | |
| Callback Registration Structure | |
| Secure Connections Out of Band | |
| Central GAPRole Callback Structure | |
| Central Event Structure | |
| GAP_DEVICE_DISCOVERY_EVENT message format | |
| Type of device discovery (Scan) to perform | |
| GAP_DEVICE_INFO_EVENT message format | |
| GAP_DEVICE_INIT_DONE_EVENT message format | |
| Type of device discovery (Scan) to perform | |
| GAP_END_DISCOVERABLE_DONE_EVENT message format | |
| Establish Link Request parameters | |
| GAP_LINK_ESTABLISHED_EVENT message format | |
| GAP event header format | |
| GAP_LINK_PARAM_UPDATE_EVENT message format | |
| GAP_MAKE_DISCOVERABLE_DONE_EVENT message format | |
| Multi GAPRole Event Structure | |
| Pairing Request fields - the parsed fields of the SMP Pairing Request command | |
| GAP_PAIRING_REQ_EVENT message format | |
| GAP_PASSKEY_NEEDED_EVENT message format | |
| Connection parameters for the peripheral device | |
| GAP_RANDOM_ADDR_CHANGED_EVENT message format | |
| Multi GAPRole Parameter Update Structure | |
| Peripheral GAPRole Callback structure | |
| GAP_SIGNATURE_UPDATED_EVENT message format | |
| GAP_SLAVE_REQUESTED_SECURITY_EVENT message format | |
| GAP_LINK_TERMINATED_EVENT message format | |
| Update Link Parameters Request parameters | |
| GAP_UPDATE_LINK_PARAM_REQ_EVENT message format | |
| Update Link Parameters Request Reply parameters | |
| GATT Attribute Type format | |
| Structure for Client Characteristic Configuration | |
| GATT Structure for Characteristic Presentation Format Value | |
| GATT_CLIENT_CHAR_CFG_UPDATED_EVENT message format | |
| GATT Server App event header format | |
| GATT Find By Type Value Request format | |
| GATT Message format | |
| GATT GATT_MSG_EVENT message format | |
| GATT Read By Type Request format | |
| GATT Reliable Writes Request format. Do not change the order of the members | |
| GATT Service format | |
| GATT Structure for service callback functions | |
| GATT Structure to keep CBs information for each service being registered | |
| GATT Write Long Request format. Do not change the order of the members | |
| HCI Data Packet | |
| Authenticated Payload Timeout Expired Event | |
| LE Advertising Packet Report Event | |
| LE Connection Complete Event | |
| LE Connection Update Complete Event | |
| LE Data Length Change Event | |
| LE Enhanced Connection Complete Event | |
| LE Generate DHKey Complete Event | |
| LE Long Term Key Requested Event | |
| LE Phy Update Complete Event | |
| LE Read P256 Public Key Complete Event | |
| LE Read Remote Used Features Complete Event | |
| LE Remote Connection Parameter Request Event | |
| VS LE Scan Request Report Event | |
| Data Buffer Overflow Event | |
| Command Complete Event | |
| Command Status Event | |
| LE Advertising Report Event | |
| Disconnection Complete Event | |
| LE Encryption Change Event | |
| Hardware Error Event | |
| Number of Completed Packets Event | |
| Vendor Specific Command Complete Event | |
| HCI Packet event | |
| Data structure for HCI Command Complete Event Return Parameter | |
| L2CAP_CHANNEL_ESTABLISHED_EVT message format | |
| Local channel information format | |
| L2CAP_CHANNEL_TERMINATED_EVT message format | |
| Command Reject format | |
| Connection oriented channel information format | |
| Connection Request format | |
| Connection Response format | |
| L2CAP_OUT_OF_CREDIT_EVT or L2CAP_PEER_CREDIT_THRESHOLD_EVT message format | |
| OSAL L2CAP_DATA_EVENT message format | |
| Disconnection Request format (src/dst CIDs are relative to sender of request) | |
| Disconnection Response format (src/dst CIDs are relative to sender of request) | |
| Flow Control Credit format | |
| Information Response Data field | |
| Information Request format | |
| Information Response format | |
| Invalid CID in Request format | |
| L2CAP_NUM_CTRL_DATA_PKT_EVT message format | |
| L2CAP packet structure | |
| Connection Parameter Update Request format | |
| Connection Parameter Update Response format | |
| L2CAP PSM structure. Allocated one for each registered PSM | |
| PSM information format | |
| Command Reject Reason Data format | |
| L2CAP_SEND_SDU_DONE_EVT message format | |
| Union of all L2CAP Signaling commands | |
| OSAL L2CAP_SIGNAL_EVENT message format | |
| User configurable variables format | |
| LinkDB info | |
| LinkDB item | |
| SRK and Sign Counter | |
| OSAL Event Header | |
| Structure to keep Prepare Write Requests for each Client | |
| Set of Broadcaster callbacks - must be setup by the application |