![]() |
![]() |
TI Driver for Elliptic Curve Digital Signature Algorithm.
The Elliptic Curve Digital Signature Algorithm (ECDSA) is a message authentication scheme between two parties based on operation on elliptic curves over finite fields.
Signing a message with ECDSA proves to the recipient that the sender of the message is in possession of the private key corresponding to the transmitted public key used during verification.
Before starting a ECDSA operation, the application must do the following:
To sign a message using an agreed upon hash function and elliptic curve, the application must do the following:
After receiving the message, public key, r, and s, the application should do the following to verify the signature:
The API expects elliptic curves as defined in ti/drivers/types/ECCParams.h. Several commonly used curves are provided.
Public keys and shared secrets are points on an elliptic curve. These points can be expressed in several ways. The most common one is in affine coordinates as an X,Y pair. The Y value can be omitted when using point compression and doing the calculations in the Montgomery domain with X,Z coordinates. This API currently only uses points expressed in affine coordinates. The point is stored as a concatenated array of X followed by Y.
In order to use the ECDSA APIs, the application is required to provide device-specific ECDSA configuration in the Board.c file. The ECDSA driver interface defines a configuration data structure:
The application must declare an array of ECDSA_Config elements, named ECDSA_config[]. Each element of ECDSA_config[] must be populated with pointers to a device specific ECDSA driver implementation's driver object, hardware attributes. Each element in ECDSA_config[] corresponds to an ECDSA instance, and none of the elements should have NULL pointers. There is no correlation between the index and the peripheral designation (such as ECDSA0 or ECDSA1). For example, it is possible to use ECDSA_config[0] for ECDSA1. Multiple drivers and driver instances may all access the same underlying hardware. This is transparent to the application. Mutual exclusion is performed automatically by the drivers as necessary.
Because the ECDSA configuration is highly device dependent, you will need to check the doxygen for the device specific ECDSA implementation. There you will find a description of the ECDSA hardware attributes. Please also refer to the Board.c file of any of your examples to see the ECDSA configuration.
The ECDSA_Params structure is passed to the ECDSA_open() call. If NULL is passed for the parameters, ECDSA_open() uses default parameters. An ECDSA_Params structure is initialized with default values by passing it to ECDSA_Params_init(). Some of the ECDSA parameters are described below. To see brief descriptions of all the parameters, see ECDSA_Params.
The ECDSA driver supports three return behaviors when processing data: blocking, polling, and callback. The ECDSA driver defaults to blocking mode, if the application does not set it. Once an ECDSA driver is opened, the only way to change the return behavior is to close and re-open the ECDSA instance with the new return behavior.
In blocking mode, a task's code execution is blocked until an ECDSA operation has completed. This ensures that only one ECDSA operation operates at a given time. Other tasks requesting ECDSA operations while a operation is currently taking place are also placed into a blocked state. ECDSA operations are executed in the order in which they were received. In blocking mode, you cannot perform ECDSA operations in the context of a software or hardware ISR.
In callback mode, an ECDSA operation functions asynchronously, which means that it does not block code execution. After an ECDSA operation has been completed, the ECDSA driver calls a user-provided hook function. Callback mode is supported in the task, SWI, and HWI execution context, However, if an ECDSA operation is requested while a operation is taking place, the call returns an error code.
In polling mode, an ECDSA operation behaves the almost the same way as in blocking mode. Instead of pending on a semaphore and letting other scheduled tasks run, the application task, SWI, or HWI continuously polls a flag until the operation completes. If an ECDSA operation is requested while a operation is taking place, the call returns an error code. When starting an ECDSA operation in polling mode from HWI or SWI context, the ECDSA HWI and SWI must be configured to have a higher priority to pre-empt the polling context.
#include <stdbool.h>#include <stddef.h>#include <stdint.h>#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>#include <ti/drivers/cryptoutils/ecc/ECCParams.h>Go to the source code of this file.
Data Structures | |
| struct | ECDSA_Config_ |
| ECDSA Global configuration. More... | |
| struct | ECDSA_OperationSign_ |
| Struct containing the parameters required for signing a message. More... | |
| struct | ECDSA_OperationVerify_ |
| Struct containing the parameters required for verifying a message. More... | |
| union | ECDSA_Operation_ |
| Union containing pointers to all supported operation structs. More... | |
| struct | ECDSA_Params_ |
| ECDSA Parameters. More... | |
Macros | |
| #define | ECDSA_CMD_RESERVED (32) |
| #define | ECDSA_STATUS_RESERVED (-32) |
| #define | ECDSA_STATUS_SUCCESS (0) |
| Successful status code. More... | |
| #define | ECDSA_STATUS_ERROR (-1) |
| Generic error status code. More... | |
| #define | ECDSA_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by ECDSA_control() for undefined command codes. More... | |
| #define | ECDSA_STATUS_RESOURCE_UNAVAILABLE (-3) |
| An error status code returned if the hardware or software resource is currently unavailable. More... | |
| #define | ECDSA_STATUS_RESULT_INVALID_PMSN (-4) |
| The PMSN passed into the the call is invalid. More... | |
| #define | ECDSA_STATUS_RESULT_R_LARGER_THAN_ORDER (-5) |
| The private key passed in is larger than the order of the curve. More... | |
| #define | ECDSA_STATUS_RESULT_S_LARGER_THAN_ORDER (-5) |
| The private key passed in is larger than the order of the curve. More... | |
| #define | ECDSA_STATUS_RESULT_PUBLIC_KEY_NOT_ON_CURVE (-7) |
| The public key of the other party does not lie upon the curve. More... | |
Typedefs | |
| typedef struct ECDSA_Config_ * | ECDSA_Handle |
| A handle that is returned from an ECDSA_open() call. More... | |
| typedef enum ECDSA_ReturnBehavior_ | ECDSA_ReturnBehavior |
| The way in which ECDSA function calls return after performing an encryption + authentication or decryption + verification operation. More... | |
| typedef struct ECDSA_Config_ | ECDSA_Config |
| ECDSA Global configuration. More... | |
| typedef struct ECDSA_OperationSign_ | ECDSA_OperationSign |
| Struct containing the parameters required for signing a message. More... | |
| typedef struct ECDSA_OperationVerify_ | ECDSA_OperationVerify |
| Struct containing the parameters required for verifying a message. More... | |
| typedef union ECDSA_Operation_ | ECDSA_Operation |
| Union containing pointers to all supported operation structs. More... | |
| typedef enum ECDSA_OperationType_ | ECDSA_OperationType |
| Enum for the operation types supported by the driver. More... | |
| typedef void(* | ECDSA_CallbackFxn) (ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType) |
| The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CALLBACK. More... | |
| typedef struct ECDSA_Params_ | ECDSA_Params |
| ECDSA Parameters. More... | |
Enumerations | |
| enum | ECDSA_ReturnBehavior_ { ECDSA_RETURN_BEHAVIOR_CALLBACK = 1, ECDSA_RETURN_BEHAVIOR_BLOCKING = 2, ECDSA_RETURN_BEHAVIOR_POLLING = 4 } |
| The way in which ECDSA function calls return after performing an encryption + authentication or decryption + verification operation. More... | |
| enum | ECDSA_OperationType_ { ECDSA_OPERATION_TYPE_SIGN = 1, ECDSA_OPERATION_TYPE_VERIFY = 2 } |
| Enum for the operation types supported by the driver. More... | |
Functions | |
| void | ECDSA_init (void) |
| This function initializes the ECDSA module. More... | |
| void | ECDSA_close (ECDSA_Handle handle) |
| Function to close a ECDSA peripheral specified by the ECDSA handle. More... | |
| int_fast16_t | ECDSA_control (ECDSA_Handle handle, uint32_t cmd, void *args) |
| Function performs implementation specific features on a given ECDSA_Handle. More... | |
| ECDSA_Handle | ECDSA_open (uint_least8_t index, ECDSA_Params *params) |
| This function opens a given ECDSA peripheral. More... | |
| void | ECDSA_Params_init (ECDSA_Params *params) |
| Function to initialize the ECDSA_Params struct to its defaults. More... | |
| void | ECDSA_OperationSign_init (ECDSA_OperationSign *operation) |
| Function to initialize a ECDSA_OperationSign struct to its defaults. More... | |
| void | ECDSA_OperationVerify_init (ECDSA_OperationVerify *operation) |
| Function to initialize a ECDSA_OperationSign struct to its defaults. More... | |
| int_fast16_t | ECDSA_sign (ECDSA_Handle handle, ECDSA_OperationSign *operation) |
| Signs a hashed message. More... | |
| int_fast16_t | ECDSA_verify (ECDSA_Handle handle, ECDSA_OperationVerify *operation) |
| Verifies a received signature matches a hash and public key. More... | |
| typedef struct ECDSA_Config_* ECDSA_Handle |
A handle that is returned from an ECDSA_open() call.
| typedef enum ECDSA_ReturnBehavior_ ECDSA_ReturnBehavior |
The way in which ECDSA function calls return after performing an encryption + authentication or decryption + verification operation.
Not all ECDSA operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.
ECDSA functions exhibiting the specified return behavior have restrictions on the context from which they may be called.
| Task | Hwi | Swi | |
|---|---|---|---|
| ECDSA_RETURN_BEHAVIOR_CALLBACK | X | X | X |
| ECDSA_RETURN_BEHAVIOR_BLOCKING | X | ||
| ECDSA_RETURN_BEHAVIOR_POLLING | X | X | X |
| typedef struct ECDSA_Config_ ECDSA_Config |
ECDSA Global configuration.
The ECDSA_Config structure contains a set of pointers used to characterize the ECDSA driver implementation.
This structure needs to be defined before calling ECDSA_init() and it must not be changed thereafter.
| typedef struct ECDSA_OperationSign_ ECDSA_OperationSign |
Struct containing the parameters required for signing a message.
| typedef struct ECDSA_OperationVerify_ ECDSA_OperationVerify |
Struct containing the parameters required for verifying a message.
| typedef union ECDSA_Operation_ ECDSA_Operation |
Union containing pointers to all supported operation structs.
| typedef enum ECDSA_OperationType_ ECDSA_OperationType |
Enum for the operation types supported by the driver.
| typedef void(* ECDSA_CallbackFxn) (ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType) |
The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CALLBACK.
| handle | Handle of the client that started the ECDSA operation. |
| returnStatus | The result of the ECDSA operation. May contain an error code if the result is the point at infinity for example. |
| operation | A union of pointers to operation structs. Only one type of pointer is valid per call to the callback function. Which type is currently valid is determined by /c operationType. The union allows easier access to the struct's fields without the need to typecase the result. |
| operationType | This parameter determined which operation the callback refers to and which type to access through /c operation. |
| typedef struct ECDSA_Params_ ECDSA_Params |
ECDSA Parameters.
ECDSA Parameters are used to with the ECDSA_open() call. Default values for these parameters are set using ECDSA_Params_init().
The way in which ECDSA function calls return after performing an encryption + authentication or decryption + verification operation.
Not all ECDSA operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.
ECDSA functions exhibiting the specified return behavior have restrictions on the context from which they may be called.
| Task | Hwi | Swi | |
|---|---|---|---|
| ECDSA_RETURN_BEHAVIOR_CALLBACK | X | X | X |
| ECDSA_RETURN_BEHAVIOR_BLOCKING | X | ||
| ECDSA_RETURN_BEHAVIOR_POLLING | X | X | X |
| enum ECDSA_OperationType_ |
| void ECDSA_init | ( | void | ) |
This function initializes the ECDSA module.
| void ECDSA_close | ( | ECDSA_Handle | handle | ) |
Function to close a ECDSA peripheral specified by the ECDSA handle.
| handle | A ECDSA handle returned from ECDSA_open() |
| int_fast16_t ECDSA_control | ( | ECDSA_Handle | handle, |
| uint32_t | cmd, | ||
| void * | args | ||
| ) |
Function performs implementation specific features on a given ECDSA_Handle.
Commands for ECDSA_control can originate from ECDSA.h or from implementation specific ECDSA*.h (ECDSACC26X2.h, ECDSASP432.h, etc.. ) files. While commands from ECDSA.h are API portable across driver implementations, not all implementations may support all these commands. Conversely, commands from driver implementation specific ECDSA*.h files add unique driver capabilities but are not API portable across all ECDSA driver implementations.
Commands supported by ECDSA.h follow an ECDSA_CMD_<cmd> naming convention.
Commands supported by ECDSA*.h follow an ECDSA*_CMD_<cmd> naming convention.
Each control command defines arg differently. The types of arg are documented with each command.
See ECDSA_control command codes for command codes.
See ECDSA_control return status codes for status codes.
| handle | A ECDSA handle returned from ECDSA_open() |
| cmd | ECDSA.h or ECDSA*.h commands. |
| args | An optional R/W (read/write) command argument accompanied with cmd |
| ECDSA_Handle ECDSA_open | ( | uint_least8_t | index, |
| ECDSA_Params * | params | ||
| ) |
This function opens a given ECDSA peripheral.
| index | Logical peripheral number for the ECDSA indexed into the ECDSA_config table |
| params | Pointer to an parameter block, if NULL it will use default values. |
| void ECDSA_Params_init | ( | ECDSA_Params * | params | ) |
Function to initialize the ECDSA_Params struct to its defaults.
| params | An pointer to ECDSA_Params structure for initialization |
Defaults values are: returnBehavior = ECDSA_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL
| void ECDSA_OperationSign_init | ( | ECDSA_OperationSign * | operation | ) |
Function to initialize a ECDSA_OperationSign struct to its defaults.
| operation | A pointer to ECDSA_OperationSign structure for initialization |
Defaults values are all zeros.
| void ECDSA_OperationVerify_init | ( | ECDSA_OperationVerify * | operation | ) |
Function to initialize a ECDSA_OperationSign struct to its defaults.
| operation | An pointer to ECDSA_OperationSign structure for initialization |
Defaults values are all zeros.
| int_fast16_t ECDSA_sign | ( | ECDSA_Handle | handle, |
| ECDSA_OperationSign * | operation | ||
| ) |
Signs a hashed message.
ECDSA_sign() generates a signature (r, s) of a hash of a message.
operation first. The driver must have been opened by calling ECDSA_open() first.| [in] | handle | A ECDSA handle returned from ECDSA_open() |
| [in] | operation | A struct containing the pointers to the buffers necessary to perform the operation |
| int_fast16_t ECDSA_verify | ( | ECDSA_Handle | handle, |
| ECDSA_OperationVerify * | operation | ||
| ) |
Verifies a received signature matches a hash and public key.
operation first. The driver must have been opened by calling ECDSA_open() first.| [in] | handle | A ECDSA handle returned from ECDSA_open() |
| [in] | operation | A struct containing the pointers to the buffers necessary to perform the operation |