Modules | Macros
ECDSA_control command and status codes

Modules

 Status Codes
 
 Command Codes
 

Macros

#define ECDSA_CMD_RESERVED   (32)
 
#define ECDSA_STATUS_RESERVED   (-32)
 

Detailed Description

These ECDSA macros are reservations for ECDSA.h

Macro Definition Documentation

§ ECDSA_CMD_RESERVED

#define ECDSA_CMD_RESERVED   (32)

Common ECDSA_control command code reservation offset. ECDSA driver implementations should offset command codes with ECDSA_CMD_RESERVED growing positively

Example implementation specific command codes:

#define ECDSAXYZ_CMD_COMMAND0 ECDSA_CMD_RESERVED + 0
#define ECDSAXYZ_CMD_COMMAND1 ECDSA_CMD_RESERVED + 1

§ ECDSA_STATUS_RESERVED

#define ECDSA_STATUS_RESERVED   (-32)

Common ECDSA_control status code reservation offset. ECDSA driver implementations should offset status codes with ECDSA_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define ECDSAXYZ_STATUS_ERROR0 ECDSA_STATUS_RESERVED - 0
#define ECDSAXYZ_STATUS_ERROR1 ECDSA_STATUS_RESERVED - 1
#define ECDSAXYZ_STATUS_ERROR2 ECDSA_STATUS_RESERVED - 2
Copyright 2017, Texas Instruments Incorporated