Data Fields
ECDSA_OperationSign_ Struct Reference

Struct containing the parameters required for signing a message. More...

#include <ECDSA.h>

Data Fields

const ECCParams_CurveParamscurve
 
const CryptoKeymyPrivateKey
 
const CryptoKeypmsn
 
const uint8_t * hash
 
uint8_t * r
 
uint8_t * s
 

Detailed Description

Struct containing the parameters required for signing a message.

Field Documentation

§ curve

const ECCParams_CurveParams* ECDSA_OperationSign_::curve

A pointer to the elliptic curve parameters

§ myPrivateKey

const CryptoKey* ECDSA_OperationSign_::myPrivateKey

A pointer to the private ECC key that will sign the hash of the message

§ pmsn

const CryptoKey* ECDSA_OperationSign_::pmsn

A pointer to a per message secret number (PMSN). The number must be provided by the application and be (0 < PMSN < curve order). Must be of the same length as other params of the curve used.

§ hash

const uint8_t* ECDSA_OperationSign_::hash

A pointer to the hash of the message. Must be the same length as the other curve parameters.

§ r

uint8_t* ECDSA_OperationSign_::r

A pointer to the buffer the r component of the signature will be written to. Must be of the same length as other params of the curve used.

§ s

uint8_t* ECDSA_OperationSign_::s

A pointer to the buffer the s component of the signature will be written to. Must be of the same length as other params of the curve used.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated