346 #ifndef ti_drivers_Es_ECDSA__include   347 #define ti_drivers_ECDSA__include   377 #define ECDSA_CMD_RESERVED           (32)   391 #define ECDSA_STATUS_RESERVED        (-32)   406 #define ECDSA_STATUS_SUCCESS         (0)   414 #define ECDSA_STATUS_ERROR           (-1)   423 #define ECDSA_STATUS_UNDEFINEDCMD    (-2)   433 #define ECDSA_STATUS_RESOURCE_UNAVAILABLE (-3)   442 #define ECDSA_STATUS_RESULT_INVALID_PMSN (-4)   450 #define ECDSA_STATUS_RESULT_R_LARGER_THAN_ORDER (-5)   458 #define ECDSA_STATUS_RESULT_S_LARGER_THAN_ORDER (-5)   466 #define ECDSA_STATUS_RESULT_PUBLIC_KEY_NOT_ON_CURVE (-7)   632                                    int_fast16_t returnStatus,
   713 int_fast16_t 
ECDSA_control(ECDSA_Handle handle, uint32_t cmd, 
void *args);
 void * object
Definition: ECDSA.h:541
Struct containing the parameters required for signing a message. 
Definition: ECDSA.h:550
enum ECDSA_ReturnBehavior_ ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
const uint8_t * s
Definition: ECDSA.h:591
The CryptoKey type is an opaque representation of a cryptographic key. 
Union containing pointers to all supported operation structs. 
Definition: ECDSA.h:600
struct ECDSA_OperationVerify_ ECDSA_OperationVerify
Struct containing the parameters required for verifying a message. 
void const  * hwAttrs
Definition: ECDSA.h:544
void ECDSA_OperationSign_init(ECDSA_OperationSign *operation)
Function to initialize a ECDSA_OperationSign struct to its defaults. 
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSA.h:645
void(* ECDSA_CallbackFxn)(ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)
The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CAL...
Definition: ECDSA.h:631
ECDSA_OperationVerify * verify
Definition: ECDSA.h:602
int_fast16_t ECDSA_control(ECDSA_Handle handle, uint32_t cmd, void *args)
Function performs implementation specific features on a given ECDSA_Handle. 
CryptoKey datastructure. 
Definition: CryptoKey.h:210
const uint8_t * r
Definition: ECDSA.h:587
ECDSA_Handle ECDSA_open(uint_least8_t index, ECDSA_Params *params)
This function opens a given ECDSA peripheral. 
void ECDSA_close(ECDSA_Handle handle)
Function to close a ECDSA peripheral specified by the ECDSA handle. 
A structure containing the parameters of an elliptic curve in short Weierstrass form. 
Definition: ECCParams.h:70
const ECCParams_CurveParams * curve
Definition: ECDSA.h:551
void ECDSA_init(void)
This function initializes the ECDSA module. 
ECDSA Parameters. 
Definition: ECDSA.h:644
ECDSA_CallbackFxn callbackFxn
Definition: ECDSA.h:646
ECDSA_ReturnBehavior_
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:511
const uint8_t * hash
Definition: ECDSA.h:584
struct ECDSA_Params_ ECDSA_Params
ECDSA Parameters. 
const CryptoKey * myPrivateKey
Definition: ECDSA.h:552
ECDSA Global configuration. 
Definition: ECDSA.h:539
void ECDSA_Params_init(ECDSA_Params *params)
Function to initialize the ECDSA_Params struct to its defaults. 
ECDSA_OperationType_
Enum for the operation types supported by the driver. 
Definition: ECDSA.h:608
uint8_t * s
Definition: ECDSA.h:569
struct ECDSA_OperationSign_ ECDSA_OperationSign
Struct containing the parameters required for signing a message. 
int_fast16_t ECDSA_sign(ECDSA_Handle handle, ECDSA_OperationSign *operation)
Signs a hashed message. 
int_fast16_t ECDSA_verify(ECDSA_Handle handle, ECDSA_OperationVerify *operation)
Verifies a received signature matches a hash and public key. 
uint8_t * r
Definition: ECDSA.h:564
void * custom
Definition: ECDSA.h:650
const CryptoKey * theirPublicKey
Definition: ECDSA.h:581
uint32_t timeout
Definition: ECDSA.h:647
struct ECDSA_Config_ ECDSA_Config
ECDSA Global configuration. 
union ECDSA_Operation_ ECDSA_Operation
Union containing pointers to all supported operation structs. 
struct ECDSA_Config_ * ECDSA_Handle
A handle that is returned from an ECDSA_open() call. 
Definition: ECDSA.h:488
Struct containing the parameters required for verifying a message. 
Definition: ECDSA.h:579
enum ECDSA_OperationType_ ECDSA_OperationType
Enum for the operation types supported by the driver. 
void ECDSA_OperationVerify_init(ECDSA_OperationVerify *operation)
Function to initialize a ECDSA_OperationSign struct to its defaults. 
const CryptoKey * pmsn
Definition: ECDSA.h:555
const ECCParams_CurveParams * curve
Definition: ECDSA.h:580
ECDSA_OperationSign * sign
Definition: ECDSA.h:601
const uint8_t * hash
Definition: ECDSA.h:561