Hector SLAM Application¶

SLAM (Simultaneous Localization and Mapping) is a critical technology in Robotics applications. It helps map unknown environment and localize a robot using a pre-built map. There are many open-source SLAM algorithms with camera and 2D/3D Lidar and they can run on J7 in Docker container. For example, in this demo, it is demonstrated how to build and run Hector SLAM on J7 in Docker container. 2D Lidar data, which was collected from TurtleBot3 is provided for this demo.
Figure 1 shows the output map by Hector SLAM on the 2D Lidar data from TurtleBot3. For more details on Hector SLAM, please refer to http://wiki.ros.org/hector_slam.
How to Run the Hector SLAM Application¶
Run the Hector SLAM on J7¶
Download 2D Lidar data.
root@j7-evm:~/j7ros_home$ make lidar2d_download
2D Lidar data is saved in $HOME/j7ros_home/data/lidar2d.
Clone the Hector SLAM git repository. Run the followings in $HOME/j7ros_home on the J7 host Linux:
root@j7-evm:~/j7ros_home$ export ROS_WS=$HOME/j7ros_home/ros_ws root@j7-evm:~/j7ros_home$ $ROS_WS/src/jacinto_ros_perception/ros1/slam/j7_setup_hector_slam.sh
It clones the Hector SLAM git repository and applies the patch to run it on the 2D Lidar data provided.
Launch the Docker image. For setting up the ROS1 environment on J7 host, please follow Docker Setup for ROS 1.
root@j7-evm:~/j7ros_home$ ./docker_run_ros1.sh
Compile the Hector SLAM inside the Docker container:
root@j7-evm:~/j7ros_home/ros_ws$ catkin_make --source src/jacinto_ros_perception/ros1
Run the hector SLAM
root@j7-evm:~/j7ros_home/ros_ws$ roslaunch hector_slam_launch tutorial_j7.launch
Visualize map and pose on Ubuntu PC¶
For setting up the ROS1 environment on the remote PC, please follow Docker Setup for ROS 1.
As done on the J7 host Linux, clone the Hector SLAM git repository:
user@pc:~/j7ros_home$ export ROS_WS=$HOME/j7ros_home/ros_ws user@pc:~/j7ros_home$ $ROS_WS/src/jacinto_ros_perception/ros1/slam/j7_setup_hector_slam.sh
Compile the Hector SLAM:
user@pc:~/j7ros_home$ cd ros_ws user@pc:~/j7ros_home/ros_ws$ catkin_make --source ./src/jacinto_ros_perception/ros1/slam/hector_slam
To display map and pose, run:
user@pc:~/j7ros_home/ros_ws$ roslaunch hector_slam_launch map_rviz.launch