Docker Setup for ROS 1¶
1. Set Up Docker Environment on TDA4 host¶
In ROS 1 Docker container environment, ROS Melodic and necessary libraries and tools are installed.
To generate bash scripts for building and running a Docker image for the ROS 1 Docker container:
root@j7-evm:~/j7ros_home$ make scripts ROS_VER=1
Please make sure that two bash scripts,
docker_build_ros1.shanddocker_run_ros1.sh, are generated.To build the Docker image:
root@j7-evm:~/j7ros_home$ ./docker_build_ros1.sh
This step will take several minutes, and once “docker build” is completed, you can check the resulting Docker image with
docker images.To start the Docker container:
root@j7-evm:~/j7ros_home$ ./docker_run_ros1.sh
To build the ROS applications, inside the Docker container:
root@j7-docker:~/j7ros_home/ros_ws$ catkin_make --source src/jacinto_ros_perception/ros1 root@j7-docker:~/j7ros_home/ros_ws$ source devel/setup.bash
2. Set Up Docker Environment on PC for Visualization¶
You can choose any folder, but this section assumes installation is made under ${HOME}/j7ros_home.
To generate bash scripts for building and running a Docker image for the ROS 1 Docker container:
user@pc:~/j7ros_home$ make scripts ROS_VER=1
If the Ubuntu PC uses a Nvidia GPU driver, please add one more argument
GPUS=yas follows:user@pc:~/j7ros_home$ make scripts ROS_VER=1 GPUS=y
Please make sure that two bash scripts,
docker_build_ros1.shanddocker_run_ros1.sh, are generated.To build the ROS 1 Docker image:
user@pc:~/j7ros_home$ ./docker_build_ros1.sh
It will take several minutes to build the Docker image. Once “docker run” completes, the resulting Docker image can be listed with “docker images”.
ROS network setting: We need to set up two environment variables which will be passed to the Docker container and used in configuring ROS network settings. Please update the following two lines in
setup_env_pc.sh:export J7_IP_ADDR=<J7_IP_address> export PC_IP_ADDR=<PC_IP_address>
<J7_IP_address>can be found by runningmake ip_showon a TDA4 terminal.Then, source the updated script before executing
docker_run_ros1.sh(in the next step):user@pc:~/j7ros_home$ source ./setup_env_pc.sh
Run the ROS 1 Docker container:
user@pc:~/j7ros_home$ ./docker_run_ros1.sh
Build the ROS nodes for visualization:
root@pc-docker:~/j7ros_home/ros_ws$ catkin_make root@pc-docker:~/j7ros_home/ros_ws$ source devel/setup.bash
3. Run Demo Applications¶
Table below summarizes the launch commands that you can use in the Docker container for each demo, on the TDA4/J7, and on the remote visualization PC. For more details, see the following subsections.
| Demo (Input Source) | Launch command on TDA4 | Launch command on Remote Visualization PC |
|---|---|---|
| Stereo Vision (ROSBAG) | roslaunch ti_sde bag_sde.launch | roslaunch ti_viz_nodes rviz_sde.launch |
| Stereo Vision (ZED camera) | roslaunch ti_sde zed_sde.launch | same as above |
| Stereo Vision with point-cloud (ROSBAG) | roslaunch ti_sde bag_sde_pcl.launch | roslaunch ti_viz_nodes rviz_sde_pcl.launch |
| Stereo Vision with point-cloud (ZED camera) | roslaunch ti_sde zed_sde_pcl.launch | same as above |
| Semantic Segmentation CNN (ROSBAG) | roslaunch ti_vision_cnn bag_semseg_cnn.launch | roslaunch ti_viz_nodes rviz_semseg_cnn.launch |
| Semantic Segmentation CNN (ZED camera) | roslaunch ti_vision_cnn zed_semseg_cnn.launch | same as above |
| Semantic Segmentation CNN (Mono camera) | roslaunch ti_vision_cnn mono_semseg_cnn.launch | same as above |
| Object Detection CNN (ROSBAG) | roslaunch ti_vision_cnn bag_objdet_cnn.launch | roslaunch ti_viz_nodes rviz_objdet_cnn.launch |
| Object Detection CNN (ZED camera) | roslaunch ti_vision_cnn zed_objdet_cnn.launch | same as above |
| Object Detection CNN (Mono camera) | roslaunch ti_vision_cnn mono_objdet_cnn.launch | same as above |
| 3D Obstacle Detection (ROSBAG) | roslaunch ti_estop bag_estop.launch | roslaunch ti_viz_nodes rviz_estop.launch |
| 3D Obstacle Detection (ZED camera) | roslaunch ti_estop zed_estop.launch | same as above |
| Visual Localization (ROSBAG) | roslaunch ti_vl bag_visloc.launch | roslaunch ti_viz_nodes rviz_visloc.launch |
In the following, [TDA4] and [PC] indicate where the step(s) should be launched: either on the TDA4 target, or on the PC.
3.1. Run Stereo Vision Application¶
[TDA4] To launch
ti_sdenode with playing back a ROSBAG file, run the followingroslaunchcommand inside the Docker container:root@j7-docker:~/j7ros_home/ros_ws$ roslaunch ti_sde bag_sde.launch
Alternatively, you can run the following directly on the TDA4 host Linux:
root@j7-evm:~/j7ros_home$ ./docker_run_ros1.sh roslaunch ti_sde bag_sde.launch
To process the image stream from a ZED stereo camera, replace the launch file with
zed_sde.launchin the above.[PC] For visualization, in the ROS 1 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ roslaunch ti_viz_nodes rviz_sde.launch
3.2. Run Stereo Vision Application with Point-Cloud Enabled¶
[TDA4] To launch
ti_sdenode with point-cloud enabled on a ROSBAG file, run the followingroslaunchcommand inside the Docker:root@j7-docker:~/j7ros_home/ros_ws$ roslaunch ti_sde bag_sde_pcl.launch
Alternatively, you can run the following directly on the TDA4 host Linux:
root@j7-evm:~/j7ros_home$ ./docker_run_ros1.sh roslaunch ti_sde bag_sde_pcl.launch
To process the image stream from a ZED stereo camera, replace the launch file with
zed_sde_pcl.launchin the above.[PC] For visualization, in the ROS 1 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ roslaunch ti_viz_nodes rviz_sde_pcl.launch
3.3. Run Semantic Segmentation CNN Application¶
[TDA4] To launch semantic segmentation demo with playing back a ROSBAG file, run the following
roslaunchcommand inside the Docker:root@j7-docker:~/j7ros_home/ros_ws$ roslaunch ti_vision_cnn bag_semseg_cnn.launch
Alternatively, you can run the following directly on the TDA4 host Linux:
root@j7-evm:~/j7ros_home$ ./docker_run_ros1.sh roslaunch ti_vision_cnn bag_semseg_cnn.launch
To process the image stream from a ZED stereo camera or USB mono camera, replace the launch file with
zed_semseg_cnn.launchormono_semseg_cnn.launchin the above.[PC] For visualization, in the ROS 1 container on the PC::
root@pc-docker:~/j7ros_home/ros_ws$ roslaunch ti_viz_nodes rviz_semseg_cnn.launch
3.4. Run Object Detection CNN Application¶
[TDA4] To launch object detection demo with playing back a ROSBAG file, run the following
roslaunchcommand inside the Docker:root@j7-docker:~/j7ros_home/ros_ws$ roslaunch ti_vision_cnn bag_objdet_cnn.launch
Alternatively, you can run the following directly on the TDA4 host Linux:
root@j7-evm:~/j7ros_home$ ./docker_run_ros1.sh roslaunch ti_vision_cnn bag_objdet_cnn.launch
To process the image stream from a ZED stereo camera or USB mono camera, replace the launch file with
zed_semseg_cnn.launchormono_semseg_cnn.launchin the above.[PC] For visualization, in the ROS 1 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ roslaunch ti_viz_nodes rviz_objdet_cnn.launch
3.5. Run 3D Obstacle Detection Application¶
[TDA4] To launch
ti_estopnode with playing back a ROSBAG file, run the followingroslaunchcommand inside the Docker:root@j7-docker:~/j7ros_home/ros_ws$ roslaunch ti_estop bag_estop.launch
Alternatively, you can run the following directly on the TDA4 host Linux:
root@j7-evm:~/j7ros_home$ ./docker_run_ros1.sh roslaunch ti_estop bag_estop.launch
To process the image stream from a ZED stereo camera, replace the launch file with
zed_estop.launchin the above.[PC] For visualization, in the ROS 1 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ roslaunch ti_viz_nodes rviz_estop.launch
3.6. Run Visual Localization Application¶
[J7] To launch
ti_vlnode with playing back a ROSBAG file, run the followingroslaunchcommand inside the Docker:root@j7-docker:~/j7ros_home/ros_ws$ roslaunch ti_vl bag_visloc.launch
Alternatively, you can run the following directly on the TDA4 host Linux:
root@j7-evm:~/j7ros_home$ ./docker_run_ros1.sh roslaunch ti_vl bag_visloc.launch
[PC] For visualization, in the ROS 1 container on the PC:
root@pc-docker:~/j7ros_home/ros_ws$ roslaunch ti_viz_nodes rviz_visloc.launch
3.7. Build and Run Hector SLAM Application¶
Many open source SLAM algorithms can run on TDA4. Among them, it is demonstrated how to setup and run Hector SLAM on 2D Lidar data. Please refer to Hector SLAM Application for details.