TIOVX User Guide
|
The top level TI OpenVX implementation header. More...
#include <stdarg.h>
#include <stdio.h>
#include <stdlib.h>
#include <VX/vx.h>
#include <VX/vx_khr_pipelining.h>
#include <TI/tivx.h>
#include <VX/vx_khr_safe_casts.h>
#include <TI/tivx_mem.h>
#include <TI/tivx_obj_desc.h>
#include <TI/tivx_target_kernel.h>
#include <TI/tivx_debug.h>
#include <tivx_platform.h>
#include <tivx_ipc.h>
#include <TI/tivx_mutex.h>
#include <TI/tivx_event.h>
#include <TI/tivx_task.h>
#include <TI/tivx_queue.h>
#include <TI/tivx_config.h>
#include <tivx_obj_desc_priv.h>
#include <tivx_target.h>
#include <tivx_target_kernel_priv.h>
#include <tivx_target_kernel_instance.h>
#include <tivx_obj_desc_queue.h>
#include <tivx_event_queue.h>
#include <vx_reference.h>
#include <tivx_data_ref_queue.h>
#include <vx_context.h>
#include <vx_error.h>
#include <vx_graph.h>
#include <vx_kernel.h>
#include <vx_node.h>
#include <vx_parameter.h>
#include <vx_remap.h>
#include <vx_scalar.h>
#include <vx_image.h>
#include <vx_matrix.h>
#include <vx_lut.h>
#include <vx_convolution.h>
#include <vx_distribution.h>
#include <vx_threshold.h>
#include <vx_pyramid.h>
#include <vx_objarray.h>
#include <vx_array.h>
#include <vx_user_data_object.h>
#include <tivx_raw_image.h>
#include <tivx_super_node.h>
#include <vx_tensor.h>
#include <vx_delay.h>
#include <vx_module.h>
#include <vx_meta_format.h>
#include <tivx_objects.h>
#include <tivx_log_rt_trace.h>
#include <tivx_log_resource.h>
#include <tivx_kernels_host_utils.h>
Go to the source code of this file.
Macros | |
#define | TIVX_ALIGN(value, align) ((((value)+((align)-1U))/(align))*(align)) |
Macro to align a 'value' to 'align' units. | |
#define | TIVX_FLOOR(value, align) (((value)/(align))*(align)) |
Macro to floor a 'value' to 'align' units. | |
#define | TIVX_DEFAULT_STRIDE_Y_ALIGN (16U) |
Macro to specify default alignment to use for stride in Y-direction. More... | |
#define | TIVX_TYPE_IS_SCALAR(type) (((vx_enum)VX_TYPE_INVALID < (type)) && ((type) < (vx_enum)VX_TYPE_SCALAR_MAX)) |
Used to determine if a type is a scalar. | |
#define | TIVX_TYPE_IS_STRUCT(type) (((type) >= (vx_enum)VX_TYPE_RECTANGLE) && ((type) < (vx_enum)VX_TYPE_KHRONOS_STRUCT_MAX)) |
Used to determine if a type is a struct. | |
#define | TIVX_TYPE_IS_OBJECT(type) (((type) >= (vx_enum)VX_TYPE_REFERENCE) && ((type) < (vx_enum)VX_TYPE_KHRONOS_OBJECT_END)) |
Used to determine if a type is an Khronos defined object. | |
#define | TIVX_TYPE_IS_TI_OBJECT(type) (((type) >= (vx_enum)VX_TYPE_VENDOR_OBJECT_START) && ((type) < (vx_enum)VX_TYPE_VENDOR_OBJECT_END)) |
Used to determine if a type is TI defined object. | |
#define | TIVX_MAGIC (0xFACEC0DEU) |
A magic value to look for and set in references. | |
#define | TIVX_BAD_MAGIC (42U) |
A magic value to look for and set in references. Used to indicate a free'ed reference. | |
#define | VX_CHECK_PARAM(ptr, size, type, align) ((NULL != ptr) && (size == sizeof(type)) && (((vx_size)ptr & align) == 0U)) |
A parameter checker for size and alignment. | |
Enumerations | |
enum | tivx_type_e { , TIVX_TYPE_ARRAY_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 1, TIVX_TYPE_IMAGE_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 2, TIVX_TYPE_RAW_IMAGE_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 3, TIVX_TYPE_TENSOR_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 4, TIVX_TYPE_USER_DATA_OBJECT_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 5, TIVX_TYPE_EVENT_QUEUE_ELEMENT = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 6, TIVX_TYPE_TARGET = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 7, TIVX_TYPE_TARGET_KERNEL_INSTANCE = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 8, TIVX_TYPE_TARGET_KERNEL = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 9, TIVX_TYPE_DELAY_PARAM = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 10, TIVX_TYPE_EVENT = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 11, TIVX_TYPE_UINTPTR = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 12, TIVX_TYPE_CONTEXT_USER_STRUCTS = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 13, TIVX_TYPE_GRAPH_PARAMETERS = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 14, TIVX_TYPE_DATA_REF_QUEUE_LIST = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 15, TIVX_TYPE_DELAY_DATA_REF_QUEUE_LIST = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 16 } |
TIVX defined reference types. More... | |
Functions | |
static void | tivx_uint32_to_uint64 (volatile uint64_t *val, uint32_t h, uint32_t l) |
Macro to convert 2x uint32 to uint64. | |
static void | tivx_uint64_to_uint32 (uint64_t val, volatile uint32_t *h, volatile uint32_t *l) |
Macro to convert uint64 to 2x uint32. | |
The top level TI OpenVX implementation header.
Definition in file vx_internal.h.