82 #define TIVX_MODULE_MAX_NAME (256u) 89 typedef struct _vx_module
#define TIVX_MODULE_MAX_NAME
Maximum possible name of a module in system.
vx_status(* vx_publish_kernels_f)(vx_context context)
Module object internal state.
vx_bool is_loaded
flag to indicate if module is loaded, module is counted only if it loaded
uint32_t ownGetModuleCount(void)
Returns number of registered modules.
vx_unpublish_kernels_f unpublish
callback to unpublish nodes in a module
vx_publish_kernels_f publish
callback to publish nodes in a module